Vehicle testing for the digital age

Winterthur, March 2019 - Kistler's DTI (Digital Transducer Interface) technology provides the automotive industry with a future-focused solution that takes vehicle dynamics and durability testing to a new level of efficiency. Kistler now has enhanced the capacity of the DTI data logger and added a network function for several devices. 

As the first and even today, only manufacturer on the market to do so, Kistler, the automotive industry's technology partner, enables efficient test setups with a variety of practical benefits like automatic sensor detection. For carmakers with only limited resources for the necessary testing, DTI offers an efficient option of speeding up their processes without compromising on precision, reliability and safety.

Simple installation saves time and money

Kistler provides users with an end-to-end measuring chain from sensors and the DTI logger to the user interface with KiCenter software  - to perform, for instance, the vehicle dynamics "straight-line braking" test to DIN 70028. Use of just a single cable in the complex test setup to configure the sensors, transfer and synchronize measurement data and supply the power ensures efficient, time-saving routines and lets the user focus on their measuring tasks. DTI generates added value even in smaller-scale applications and can be scaled up flexibly.

Efficient test setups also for complex measurement tasks

Comprehensive vehicle dynamics, durability and tire tests cover a host of physical variables such as acceleration, brake pressure, expansion, steering forces and torques, side-slip angle, temperature etc. Kistler has now significantly enhanced the capacity of the measurement solution in order to easily capture and analyze all these characteristics with its DTI bus system.

The new DTI logger comes with eight DTI ports with 12 channels, so that a total of 96 sensors can be connected per logger. The logger offers sampling rates of 500 to 20,000 Hz and a power supply up to 240 W. And that is far from all: as of now, you can link up three DTI loggers to a network with the new SyncSwitch - raising the connection capacity to a total of 288 sensors. All the transducers connected to the DTI network are also automatically synchronized.

Integrate any sensors into the synchronized network

Kistler's update of the DTI logger and the advanced network capability provide customers with an integrated system for efficient test setups and a variety of different sensors that are easy to integrate, configure and put into operation. The measurement technology is further optimized in close cooperation with the customer and provided as an all-in-one solution package for specific applications.

The smaller selection of DTI-enabled sensors, which frequently resulted in the use of a CAN-to-DTI converters, is now past history thanks to Kistler's updating of its entire vehicle dynamics sensor portfolio for direct DTI integration. Third-party products can also already be equipped with a DTI interface and thus included in the synchronized digital network.
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
The Kistler Group will showcase its test and analysis systems for threaded joints at the 2019 Fastener Fair in Stuttgart from 19 to 21 March.
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
Accurate and insensitive to its mounting position: the new Type 6044A M8 sensor features an anti-strain design to ensure reliable, high-quality results.
20/11/2018
Motorsport: the new 4080B/BT absolute pressure sensors from Kistler – for real-time monitoring with maximum measurement accuracy and signal quality!
16/10/2018
At Fakuma 2018, the Kistler Group is showcasing its latest monitoring and control packages for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
08/10/2018
The SMETEC Gesellschaft für Sensor-, Motor- und Energietechnik mbH recently became part of the Kistler Group.
24/09/2018
The Kistler Group is adding another variant to what is already the world's most comprehensive portfolio of wheel force measurement systems: the new RoaDyn S6GT 6-component wheel force measurement system.
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
The Kistler Group is introducing a compact mobile measurement solution for enhanced rolling stock maintenance in international railway operations in the shape of its railway brake force measuring system Type 2899A.
21/08/2018
A new Center of Competence for production control and management systems will be opened in Aachen.
31/07/2018
Competent service just a call away has always been a key aspect of Kistler's cooperation with its customers. Now, in a move to address growing demand in North Germany, the measurement technology experts are opening a new office in Wolfsburg.
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
Digitization, Internet of Things and Industry 4.0 are presenting major challenges. Discover how Kistler responds to the great challenges of our times.
09/05/2018
At Sensor + Test 2018 Kistler will be introducing a milestone in measurement technology: its new KiDAQ data acquisition system.
08/05/2018
At NPE 2018, the Kistler Group is showcasing its latest custom monitoring package for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
03/05/2018
At Automatica 2018, the Kistler Group will turn the spotlight on diverse options for using sensors and process monitoring systems to support industrial production and enhance digitalization in test and assembly technology.
24/04/2018
The Kistler Group will showcase its expanded portfolio of industrial test and inspection systems for quality assurance at the 2018 Control trade show.
12/04/2018
The global leader in dynamic measurement technology supports the passion for innovation and technology with a three-year partnership.
06/03/2018
Kistler will be showcasing at Control 2018 its portfolio of industrial testing and inspection systems with the spotlight on the very latest additions.
16/02/2018
At Intertraffic 2018 the Kistler Group is showcasing its comprehensive KiTraffic Weigh In Motion (WIM) solutions, which support road owners and authorities in road and traffic monitoring, weight enforcement and weight-based tolling.
15/02/2018
At NPE 2018 in Orlando, Florida, the Kistler Group will demonstrate a wide range of modular functionalities for ComoNeo: the process monitoring system that takes injection molding to a higher level with integrated quality monitoring geared to meet customers’ needs and requirements.
31/01/2018
The new KiSprint provides coaches and athletes with an efficient means of biomechanically optimizing sprint starts under competitive conditions. The robust and mobile solution has comprehensive software assessment options and can be individually adapted and expanded.
24/01/2018
Kistler achieved a growth rate of 18 % in 2017. Digital transformation has top priority in 2018.
23/01/2018
Surmonter les complexités du RTM - avec Kistler
12/10/2017
At the SPS IPC Drives Kistler Group will unveil the world's first digital charge amplifier Type 5974A, a milestone more in electrical automation.
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
With MARS software version 3.0, Kistler presents an extensive update of the proprietary measurement, analysis, and evaluation software for Kistler force plates.
21/10/2016
Kistler boosts the efficiency and reliability of large marine and stationary engines through monitoring and control of the combustion process
19/10/2016
Kistler is presenting the new versions of its ComoNeo and ComoDataCenter.
10/10/2016
Kistler is unveiling a new addition to its portfolio of electromechanical joining modules.
30/09/2016
The Kistler Group reported incoming orders worth CHF 233.3 million at the end of August 2016 and has therefore seen growth of 8.4 % compared to the same period in the previous year, or 5.6 % when adjusted for currency effects.
07/09/2016
At this year's K Trade Fair from 19 to 26 October in Düsseldorf, Kistler will be showcasing its latest new products and features with the focus on Industry 4.0.
24/07/2016
Kistler will be showcasing its new NCFE and NCFR joining modules, together with the latest generation of maXYmos monitoring systems on Motek 2016
12/07/2016
Kistler's Correvit® SFII sensor measures world record in 1.513 seconds
12/05/2016
Screw technology complements the range of applications.
27/04/2016
Following a long phase of planning, preparations, and conversion work, Kistler Instrumente GmbH has a new home for its German headquarters at the Böblingen/Sindelfingen airfield.
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
At Chinaplas 2015 Kistler will be presenting solutions for zero-defect production, process monitoring and data evaluation in injection molding
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
At Sensor + Test 2014 Kistler is presenting many new features from the field of measurement electronics in addition to its already proven sensor technology.
19/05/2014
Users obtain a full range of force–displacement measurement systems from one source
06/02/2014
The Kistler Group achieved sales of 285 million CHF in 2013, thus marking a slight growth in comparison with the figures for the prior year.