Universal Test Bench Interface

Winterthur, 3 September 2015 – Kistler is launching its KiBox Cockpit V2.1 – a comprehensive software update for the Kistler KiBox indication system. Kistler's KiBox delivers detailed information about the quality of combustion in each individual cylinder, with all the relevant key data for engine development available in real time. Software update V2.1 means that the system can now be used directly on engine test benches, as well for mobile applications in vehicles on the road. Additional new features also broaden the scope of use for KiBox: new calculation options, added virtual channels and valuable expert functions. Developed in close collaboration with customers, this software can now be downloaded free of charge from Kistler's website.

KiBox Cockpit V2.1 for Use on Engine Test Benches
Kistler's KiBox is now fully usable on test benches with the update to version 2.1. A universal test bench interface means that it can be integrated into commonly used automation systems such as Morphee, PUMA Open and Stars. This makes it possible not only to control the combustion analysis system but also to output measurands to the automation system, opening up a host of potential applications for users.

Extended Hardware Compatibility
KiBox Cockpit V2.1 supports accurate determination of the Top Dead Center (TDC) with the help of a capacitive TDC probe. This is an extremely useful feature, especially for high-precision test bench measurements. Another benefit of the new software: Kistler's new type 4665B piezoresistive amplifier with automatic sensor identification (PiezoSmart®) and analog sensor temperature output is now supported as well. This marks a further logical advance in the concept for shared use of Kistler's SCP (Signal Conditioning Platform) components.

Added Virtual Channels
The new software introduces virtual channels to increase the number of available channels. Multiplexed ignition or injection signals from several cylinders can now be connected to one current probe input, so ignition or injection timing calculations can be performed for all cylinders.

Calculations and Expert Functions
Several new features make the Kistler KiBox more efficient, more precise and more convenient for users: new calculation methods and calculations such as ‘indicated torque’, a general statistics package and additional expert functions for data display and analysis.

Simple Integration – Versatile Applications
The Kistler KiBox operates with the vehicle's own crank angle sensor, and it also supports simple integration into ETAS INCA®, VECTOR CANape and ATI VISION; alternatively, results can also be outputted via a CAN port or a remote API interface. What's more, standalone operating mode entirely eliminates the need for a PC when measuring (stream or CAN output).

Complete System for Cylinder Pressure Diagnostics
Kistler's KiBox is a complete system for combustion analysis. It delivers detailed information on combustion quality in each individual cylinder, and makes key data available in real time – synchronized with other measurement data and ECU control variables. The KiBox is designed for users who need information on injection valve actuation, ignition and combustion – but it can also be used as a standalone standard system for indication in vehicles or on the test bench.

You can find more details about this product here. To learn more about Kistler's solutions for on-board indication, visit: www.kistler.com/engine-mobile
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
The Kistler Group will showcase its test and analysis systems for threaded joints at the 2019 Fastener Fair in Stuttgart from 19 to 21 March.
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
Accurate and insensitive to its mounting position: the new Type 6044A M8 sensor features an anti-strain design to ensure reliable, high-quality results.
20/11/2018
Motorsport: the new 4080B/BT absolute pressure sensors from Kistler – for real-time monitoring with maximum measurement accuracy and signal quality!
16/10/2018
At Fakuma 2018, the Kistler Group is showcasing its latest monitoring and control packages for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
08/10/2018
The SMETEC Gesellschaft für Sensor-, Motor- und Energietechnik mbH recently became part of the Kistler Group.
24/09/2018
The Kistler Group is adding another variant to what is already the world's most comprehensive portfolio of wheel force measurement systems: the new RoaDyn S6GT 6-component wheel force measurement system.
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
The Kistler Group is introducing a compact mobile measurement solution for enhanced rolling stock maintenance in international railway operations in the shape of its railway brake force measuring system Type 2899A.
21/08/2018
A new Center of Competence for production control and management systems will be opened in Aachen.
31/07/2018
Competent service just a call away has always been a key aspect of Kistler's cooperation with its customers. Now, in a move to address growing demand in North Germany, the measurement technology experts are opening a new office in Wolfsburg.
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
Digitization, Internet of Things and Industry 4.0 are presenting major challenges. Discover how Kistler responds to the great challenges of our times.
09/05/2018
At Sensor + Test 2018 Kistler will be introducing a milestone in measurement technology: its new KiDAQ data acquisition system.
08/05/2018
At NPE 2018, the Kistler Group is showcasing its latest custom monitoring package for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
03/05/2018
At Automatica 2018, the Kistler Group will turn the spotlight on diverse options for using sensors and process monitoring systems to support industrial production and enhance digitalization in test and assembly technology.
24/04/2018
The Kistler Group will showcase its expanded portfolio of industrial test and inspection systems for quality assurance at the 2018 Control trade show.
12/04/2018
The global leader in dynamic measurement technology supports the passion for innovation and technology with a three-year partnership.
06/03/2018
Kistler will be showcasing at Control 2018 its portfolio of industrial testing and inspection systems with the spotlight on the very latest additions.
16/02/2018
At Intertraffic 2018 the Kistler Group is showcasing its comprehensive KiTraffic Weigh In Motion (WIM) solutions, which support road owners and authorities in road and traffic monitoring, weight enforcement and weight-based tolling.
15/02/2018
At NPE 2018 in Orlando, Florida, the Kistler Group will demonstrate a wide range of modular functionalities for ComoNeo: the process monitoring system that takes injection molding to a higher level with integrated quality monitoring geared to meet customers’ needs and requirements.
31/01/2018
The new KiSprint provides coaches and athletes with an efficient means of biomechanically optimizing sprint starts under competitive conditions. The robust and mobile solution has comprehensive software assessment options and can be individually adapted and expanded.
24/01/2018
Kistler achieved a growth rate of 18 % in 2017. Digital transformation has top priority in 2018.
23/01/2018
Surmonter les complexités du RTM - avec Kistler
12/10/2017
At the SPS IPC Drives Kistler Group will unveil the world's first digital charge amplifier Type 5974A, a milestone more in electrical automation.
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
With MARS software version 3.0, Kistler presents an extensive update of the proprietary measurement, analysis, and evaluation software for Kistler force plates.
21/10/2016
Kistler boosts the efficiency and reliability of large marine and stationary engines through monitoring and control of the combustion process
19/10/2016
Kistler is presenting the new versions of its ComoNeo and ComoDataCenter.
10/10/2016
Kistler is unveiling a new addition to its portfolio of electromechanical joining modules.
30/09/2016
The Kistler Group reported incoming orders worth CHF 233.3 million at the end of August 2016 and has therefore seen growth of 8.4 % compared to the same period in the previous year, or 5.6 % when adjusted for currency effects.
07/09/2016
At this year's K Trade Fair from 19 to 26 October in Düsseldorf, Kistler will be showcasing its latest new products and features with the focus on Industry 4.0.
24/07/2016
Kistler will be showcasing its new NCFE and NCFR joining modules, together with the latest generation of maXYmos monitoring systems on Motek 2016
12/07/2016
Kistler's Correvit® SFII sensor measures world record in 1.513 seconds
12/05/2016
Screw technology complements the range of applications.
27/04/2016
Following a long phase of planning, preparations, and conversion work, Kistler Instrumente GmbH has a new home for its German headquarters at the Böblingen/Sindelfingen airfield.
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
At Chinaplas 2015 Kistler will be presenting solutions for zero-defect production, process monitoring and data evaluation in injection molding
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
At Sensor + Test 2014 Kistler is presenting many new features from the field of measurement electronics in addition to its already proven sensor technology.
19/05/2014
Users obtain a full range of force–displacement measurement systems from one source
06/02/2014
The Kistler Group achieved sales of 285 million CHF in 2013, thus marking a slight growth in comparison with the figures for the prior year.