Smallest water-cooled miniature cylinder pressure sensor – Kistler unveils advanced version

Winterthur, January 2022 – The latest M8 miniature cylinder pressure sensor (6041C) from Kistler breaks new ground in measurement excellence. This sensor incorporates state-of-the-art PiezoStar crystals along with improvements to its design and manufacturing process, resulting in outstanding performance. This versatile, reliable cylinder pressure sensor delivers measurement results of unrivaled precision – and can be considered the solution of choice for use in thermodynamic investigations in the engine development process, where overall accuracy is of the greatest priority. 

Recent years and decades have seen continuous progress in the development of combustion engines – due to significant advances in measurement technology that play a key part in boosting performance and reducing emissions. The combustion engine is set to maintain a position in future propulsion concepts for many years to come, but new alternative fuels will challenge engine developers. Kistler's response: a portfolio of highly advanced sensors that provide maximum support for the development process.

Outstanding measurement characteristics

Kistler is known as a leader in the field of measurement technology – especially when it comes to combustion pressure measurement and analysis. The market launch of the 6041C miniature cylinder pressure sensor – the third generation of the company’s smallest water-cooled sensor (size: M8) – confirms this positioning. The 6041C combines improved thermodynamic behavior with increased stability and minimal sensor-to-sensor deviation. In terms of measurement-related attributes, the new sensor's main features are:

  • Minimal thermal sensitivity change – stable over the entire operating range
  • Very small linearity deviation – accurate measurement data at all loads
  • Low thermal shock error – assured mean effective pressure (MEP) accuracy under all conditions
  • Long-term stability – due to the optimized cooling flow around the measuring element
  • Long service life – with no loss of thermodynamic accuracy

A robust sensor for diverse applications

Compared to uncooled sensors, water-cooled sensors have the advantage that they can be flush-mounted even when subjected to high thermal loads so they can provide measurement results of maximum accuracy. This is due to the latest PiezoStar crystal technology and an advanced measuring element coupled with improvements to the production process. These advances also give the 6041C miniature cylinder pressure sensor higher natural frequency and excellent thermal stability within the application temperature range of 50±30°C, so the sensor is optimized for gas exchange analysis tasks.

The sensor can be installed in a sleeve or directly into an M8x0.75 bore, either flush-mounted or recess-mounted. Like its predecessors, the 6041C cylinder pressure sensor does not require excessive space and can be mounted in bores starting from a diameter of 12 mm. The sensor is compatible for mounting with its predecessors 6041B and 6041A, and the uncooled variants 6045A, 6045B and 6044A. The 6041C is always delivered with a mounted cable, and optionally with PiezoSmart sensor detection. 

Highest precision for engine developers

Roger Leutwyler, Product Manager for piezoelectric cylinder pressure sensors at Kistler, comments: "High sensitivity, high natural frequency, a low thermal shock error and outstanding zero-point stability: these advantages enable our new 6041C cylinder pressure sensor to deliver measurement results with the highest accuracy. As a miniature sensor with an M8 mounting thread, it is particularly suitable for compact multi-valve engines where space is limited – and obviously, its benefits also come into play whenever precision and long-term stability are critical factors." 

Dossier de press

Portrait de Kistler avec logo pour un aperçu rapide: Kistler Press Kit.zip

04/10/2022
Two new products deliver yet more improvements to cavity pressure and temperature measurements in plastics processing.
27/09/2022
The new SlimLine Sensor 9132CD is nine times more sensitive than comparable SlimLine sensors.
16/09/2022
At K 2022, Kistler will showcase its solutions for injection molding that make plastics processing more intelligent and sustainable.
06/09/2022
With ComoScout, Kistler offers a simple and cost-effective process monitoring system for injection molding processes.
31/08/2022
High-end measurement systems for rolling stock – from brake testing to traffic monitoring.
22/08/2022
Artificial intelligence in punching: AI helps manufacturers improve product quality and step up their quality assurance.
12/08/2022
New wireless dynamometer allows for highly accurate measurements of cutting forces.
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
The new joining module is highly suitable for clinching and riveting, and also for assembly processes that require force-displacement monitoring.
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
The Kistler Group will showcase its test and analysis systems for threaded joints at the 2019 Fastener Fair in Stuttgart from 19 to 21 March.
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
Accurate and insensitive to its mounting position: the new Type 6044A M8 sensor features an anti-strain design to ensure reliable, high-quality results.
20/11/2018
Motorsport: the new 4080B/BT absolute pressure sensors from Kistler – for real-time monitoring with maximum measurement accuracy and signal quality!
16/10/2018
At Fakuma 2018, the Kistler Group is showcasing its latest monitoring and control packages for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
08/10/2018
The SMETEC Gesellschaft für Sensor-, Motor- und Energietechnik mbH recently became part of the Kistler Group.
24/09/2018
The Kistler Group is adding another variant to what is already the world's most comprehensive portfolio of wheel force measurement systems: the new RoaDyn S6GT 6-component wheel force measurement system.
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
The Kistler Group is introducing a compact mobile measurement solution for enhanced rolling stock maintenance in international railway operations in the shape of its railway brake force measuring system Type 2899A.
21/08/2018
A new Center of Competence for production control and management systems will be opened in Aachen.
31/07/2018
Competent service just a call away has always been a key aspect of Kistler's cooperation with its customers. Now, in a move to address growing demand in North Germany, the measurement technology experts are opening a new office in Wolfsburg.
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
Digitization, Internet of Things and Industry 4.0 are presenting major challenges. Discover how Kistler responds to the great challenges of our times.
09/05/2018
At Sensor + Test 2018 Kistler will be introducing a milestone in measurement technology: its new KiDAQ data acquisition system.
08/05/2018
At NPE 2018, the Kistler Group is showcasing its latest custom monitoring package for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
03/05/2018
At Automatica 2018, the Kistler Group will turn the spotlight on diverse options for using sensors and process monitoring systems to support industrial production and enhance digitalization in test and assembly technology.
24/04/2018
The Kistler Group will showcase its expanded portfolio of industrial test and inspection systems for quality assurance at the 2018 Control trade show.
12/04/2018
The global leader in dynamic measurement technology supports the passion for innovation and technology with a three-year partnership.
06/03/2018
Kistler will be showcasing at Control 2018 its portfolio of industrial testing and inspection systems with the spotlight on the very latest additions.
16/02/2018
At Intertraffic 2018 the Kistler Group is showcasing its comprehensive KiTraffic Weigh In Motion (WIM) solutions, which support road owners and authorities in road and traffic monitoring, weight enforcement and weight-based tolling.
15/02/2018
At NPE 2018 in Orlando, Florida, the Kistler Group will demonstrate a wide range of modular functionalities for ComoNeo: the process monitoring system that takes injection molding to a higher level with integrated quality monitoring geared to meet customers’ needs and requirements.
31/01/2018
The new KiSprint provides coaches and athletes with an efficient means of biomechanically optimizing sprint starts under competitive conditions. The robust and mobile solution has comprehensive software assessment options and can be individually adapted and expanded.
24/01/2018
Kistler achieved a growth rate of 18 % in 2017. Digital transformation has top priority in 2018.
23/01/2018
Surmonter les complexités du RTM - avec Kistler
12/10/2017
At the SPS IPC Drives Kistler Group will unveil the world's first digital charge amplifier Type 5974A, a milestone more in electrical automation.
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
With MARS software version 3.0, Kistler presents an extensive update of the proprietary measurement, analysis, and evaluation software for Kistler force plates.
21/10/2016
Kistler boosts the efficiency and reliability of large marine and stationary engines through monitoring and control of the combustion process
19/10/2016
Kistler is presenting the new versions of its ComoNeo and ComoDataCenter.
10/10/2016
Kistler is unveiling a new addition to its portfolio of electromechanical joining modules.
30/09/2016
The Kistler Group reported incoming orders worth CHF 233.3 million at the end of August 2016 and has therefore seen growth of 8.4 % compared to the same period in the previous year, or 5.6 % when adjusted for currency effects.
07/09/2016
At this year's K Trade Fair from 19 to 26 October in Düsseldorf, Kistler will be showcasing its latest new products and features with the focus on Industry 4.0.
24/07/2016
Kistler will be showcasing its new NCFE and NCFR joining modules, together with the latest generation of maXYmos monitoring systems on Motek 2016
12/07/2016
Kistler's Correvit® SFII sensor measures world record in 1.513 seconds
12/05/2016
Screw technology complements the range of applications.
27/04/2016
Following a long phase of planning, preparations, and conversion work, Kistler Instrumente GmbH has a new home for its German headquarters at the Böblingen/Sindelfingen airfield.
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
At Chinaplas 2015 Kistler will be presenting solutions for zero-defect production, process monitoring and data evaluation in injection molding
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
At Sensor + Test 2014 Kistler is presenting many new features from the field of measurement electronics in addition to its already proven sensor technology.
19/05/2014
Users obtain a full range of force–displacement measurement systems from one source
06/02/2014
The Kistler Group achieved sales of 285 million CHF in 2013, thus marking a slight growth in comparison with the figures for the prior year.