Safe micro range machining

Winterthur, 29 May 2018 –Kistler is pleased to introduce MicroDyn, the world's smallest series-produced cutting force meter. This now provides manufacturing companies and research institutions with a solution for highly precise measurements of cutting forces in the development of micro tools.

The machining of very small workpieces puts high demands on the tools used. In order to examine cutting forces in micro machining applications for example, in watchmaking, highly compact and sensitive measuring instruments are needed. With the new MicroDyn 9109AA dynamometer, Kistler is creating new opportunities for its customers in the fields of ultra-fine machining, micro-precision machining and ultra-precision machining – especially in the development of tools for the machining of brittle-hard materials and the optimization of machining processes.

Smallest dynamometer on the market

Measuring only 30x30 mm, the MicroDyn is the smallest dynamometer in the world. Thanks to the high natural frequency of 15 kHZ in all three axes, an increase of about a factor of 2.5 compared to its predecessor, highly dynamic forces up to 500 N can be measured very accurately and the resulting torques of up to 50 Nm calculated. This makes it possible to detect forces with tool speeds of up to 120 000 RPM on individual blades of the tool. The piezoelectric measuring crystal rings ensure high sensitivity and a very low threshold. They are also installed in such a way that temperature influences are largely compensated.

Exact measurement in tool development

In particular when developing new tools, it is crucial to know how they behave. With typical ques-tions being what cutting forces occur? How does the tool behave in different situations (process stability)? How can the tool be designed so that force peaks are avoided (service life) and the ma-chining process still takes place quickly and efficiently? Only accurate measurements during the development ensure the achievement of process reliability and prevention of rejects. For example, when milling a case, a watchmaker needs to ensure that the process runs smoothly and is stable, even in constantly changing engagement conditions, and that the tool is not overstressed.

Flexible attachment and data evaluation

The new MicroDyn 9109AA is equipped with a variety of mounting options. It can be both mounted vertically and horizontally to the machine tool machine tool table and the workpiece can be clamped accordingly; this benefits measurement accuracy. For quick and error-free data recording and analysis, the combination of MicroDyn with multi-channel charge amplifiers, in particular the high-end solution 5080A; is recommended. Kistler offers corresponding complete packages including the Dynoware software for an easy and error-free configuration in which the rules for the force and torque calculation are already stored. In principle, however, the MicroDyn can also be used with other analysis systems. MicroDyn is available now.

For more information about MicroDyn Type 9109AA please click here.

Dossier de press

Portrait de Kistler avec logo pour un aperçu rapide: Kistler Press Kit.zip

12/08/2022
New wireless dynamometer allows for highly accurate measurements of cutting forces.
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
The new joining module is highly suitable for clinching and riveting, and also for assembly processes that require force-displacement monitoring.
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
The Kistler Group will showcase its test and analysis systems for threaded joints at the 2019 Fastener Fair in Stuttgart from 19 to 21 March.
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
Accurate and insensitive to its mounting position: the new Type 6044A M8 sensor features an anti-strain design to ensure reliable, high-quality results.
20/11/2018
Motorsport: the new 4080B/BT absolute pressure sensors from Kistler – for real-time monitoring with maximum measurement accuracy and signal quality!
16/10/2018
At Fakuma 2018, the Kistler Group is showcasing its latest monitoring and control packages for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
08/10/2018
The SMETEC Gesellschaft für Sensor-, Motor- und Energietechnik mbH recently became part of the Kistler Group.
24/09/2018
The Kistler Group is adding another variant to what is already the world's most comprehensive portfolio of wheel force measurement systems: the new RoaDyn S6GT 6-component wheel force measurement system.
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
The Kistler Group is introducing a compact mobile measurement solution for enhanced rolling stock maintenance in international railway operations in the shape of its railway brake force measuring system Type 2899A.
21/08/2018
A new Center of Competence for production control and management systems will be opened in Aachen.
31/07/2018
Competent service just a call away has always been a key aspect of Kistler's cooperation with its customers. Now, in a move to address growing demand in North Germany, the measurement technology experts are opening a new office in Wolfsburg.
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
Digitization, Internet of Things and Industry 4.0 are presenting major challenges. Discover how Kistler responds to the great challenges of our times.
09/05/2018
At Sensor + Test 2018 Kistler will be introducing a milestone in measurement technology: its new KiDAQ data acquisition system.
08/05/2018
At NPE 2018, the Kistler Group is showcasing its latest custom monitoring package for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
03/05/2018
At Automatica 2018, the Kistler Group will turn the spotlight on diverse options for using sensors and process monitoring systems to support industrial production and enhance digitalization in test and assembly technology.
24/04/2018
The Kistler Group will showcase its expanded portfolio of industrial test and inspection systems for quality assurance at the 2018 Control trade show.
12/04/2018
The global leader in dynamic measurement technology supports the passion for innovation and technology with a three-year partnership.
06/03/2018
Kistler will be showcasing at Control 2018 its portfolio of industrial testing and inspection systems with the spotlight on the very latest additions.
16/02/2018
At Intertraffic 2018 the Kistler Group is showcasing its comprehensive KiTraffic Weigh In Motion (WIM) solutions, which support road owners and authorities in road and traffic monitoring, weight enforcement and weight-based tolling.
15/02/2018
At NPE 2018 in Orlando, Florida, the Kistler Group will demonstrate a wide range of modular functionalities for ComoNeo: the process monitoring system that takes injection molding to a higher level with integrated quality monitoring geared to meet customers’ needs and requirements.
31/01/2018
The new KiSprint provides coaches and athletes with an efficient means of biomechanically optimizing sprint starts under competitive conditions. The robust and mobile solution has comprehensive software assessment options and can be individually adapted and expanded.
24/01/2018
Kistler achieved a growth rate of 18 % in 2017. Digital transformation has top priority in 2018.
23/01/2018
Surmonter les complexités du RTM - avec Kistler
12/10/2017
At the SPS IPC Drives Kistler Group will unveil the world's first digital charge amplifier Type 5974A, a milestone more in electrical automation.
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
With MARS software version 3.0, Kistler presents an extensive update of the proprietary measurement, analysis, and evaluation software for Kistler force plates.
21/10/2016
Kistler boosts the efficiency and reliability of large marine and stationary engines through monitoring and control of the combustion process
19/10/2016
Kistler is presenting the new versions of its ComoNeo and ComoDataCenter.
10/10/2016
Kistler is unveiling a new addition to its portfolio of electromechanical joining modules.
30/09/2016
The Kistler Group reported incoming orders worth CHF 233.3 million at the end of August 2016 and has therefore seen growth of 8.4 % compared to the same period in the previous year, or 5.6 % when adjusted for currency effects.
07/09/2016
At this year's K Trade Fair from 19 to 26 October in Düsseldorf, Kistler will be showcasing its latest new products and features with the focus on Industry 4.0.
24/07/2016
Kistler will be showcasing its new NCFE and NCFR joining modules, together with the latest generation of maXYmos monitoring systems on Motek 2016
12/07/2016
Kistler's Correvit® SFII sensor measures world record in 1.513 seconds
12/05/2016
Screw technology complements the range of applications.
27/04/2016
Following a long phase of planning, preparations, and conversion work, Kistler Instrumente GmbH has a new home for its German headquarters at the Böblingen/Sindelfingen airfield.
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
At Chinaplas 2015 Kistler will be presenting solutions for zero-defect production, process monitoring and data evaluation in injection molding
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
At Sensor + Test 2014 Kistler is presenting many new features from the field of measurement electronics in addition to its already proven sensor technology.
19/05/2014
Users obtain a full range of force–displacement measurement systems from one source
06/02/2014
The Kistler Group achieved sales of 285 million CHF in 2013, thus marking a slight growth in comparison with the figures for the prior year.