Reliable testing for threaded connections, fasteners and joints

Winterthur, February 2019 - The Kistler Group will showcase its test and analysis systems for threaded joints at the 2019 Fastener Fair in Stuttgart from 19 to 21 March. Visitors to stand 862 in hall 1 can inspect Kistler's wide-ranging portfolio of testing and quality assurance solutions for the entire value chain, from development and production through to deployment in manufacturing. This is Kistler's first appearance at the international exhibition for the fastener and fixing industry. 

Fastener assembly has to meet demanding requirements for quality and productivity – and this calls for continuous monitoring and testing of the tools and fasteners that are deployed. Kistler, a leading provider of solutions to enhance quality and boost efficiency, offers an extensive portfolio of testing and analysis systems to achieve this goal. At the Fastener Fair in Stuttgart, Kistler will showcase three solutions used for testing and inspection throughout the production chain: the Vibration Test System (a laboratory test stand), Analyse Basic (the easy-to-use inspection system) and INSPECTpro (the portable measuring instrument). Kistler's stand will also feature its flexible NCFH NC joining system. 

For laboratory applications: the Vibration Test System

Kistler's fastener test stand provides dynamic testing of the securing behavior of threaded joints, compliant with internationally defined standards. With this system, users in R&D as well as quality assurance can test out real load cases. To achieve this, test objects are inserted into special backlash-free fixtures and are then subjected to loads of up to 50 kN, transversely to the fastener axis. Stroke, test frequency and amplitude can all be adjusted while the Vibration Test System is in operation. 

All the functions of this standalone system can be monitored and controlled via the integrated testXpert software. If required, a friction coefficient test can also be integrated – a key quality assurance factor, especially in the automotive and rail sectors. Kistler's laboratory system comprises a low-maintenance mechanical assembly with drive units, together with sensors for preloading force and thread torque.

For straightforward testing: Analyse Basic with testXpert III 

Kistler's trade show stand will feature a product specifically intended for fastener manufacturers, coating providers and end users who test according to defined standard requirements: Analyse Basic, a system that makes norm-compliant testing simple – just a few clicks are all that's needed. The system allows ISO-compliant testing of bolts and nuts with torques of up to 500Nm. The integrated testXpert III software is available in multiple languages, and a new version has just been released. The restructured, intuitive user interface and the simple test rig make it easy for new users to start testing: after just one day's training, operators can use Analyse Basic for efficient, low-cost quality assurance. 

For mobile testing: INSPECTpro

A highly flexible range of applications, including quality assurance in goods receiving departments and rapid inspection of fasteners: INSPECTpro can handle them all. This portable system, powered by a rechargeable battery, is connected to Kistler sensor technology to determine the overall coefficient of friction of fasteners. Real-time wireless transmission of the measurands in graphic and numeric form takes place while the test object is actually being tightened, and the data is displayed on the screen. Then, the system automatically determines the overall coefficient of friction, which is also shown on the screen. For advanced evaluation and documentation of measurement results, data can be exported and connected to the testXpert III software. A further benefit: users can configure the system individually with the help of software modules, so they can deploy it for a vast range of other measurement tasks.

Joining instead of threaded connections: NCFH measuring system

As the global market leader in dynamic measurement technology, Kistler also offers measuring systems for other joining methods. One of the Group's electromechanical joining systems – the NCFH NC joining module – will also be on show at the Fastener Fair. This system, which comprises a hollow shaft drive, offers many outstanding benefits: compact design, excellent dynamics, two available measurement ranges, increased overload protection and a minimal spare parts inventory.
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
The Kistler Group will showcase its test and analysis systems for threaded joints at the 2019 Fastener Fair in Stuttgart from 19 to 21 March.
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
Accurate and insensitive to its mounting position: the new Type 6044A M8 sensor features an anti-strain design to ensure reliable, high-quality results.
20/11/2018
Motorsport: the new 4080B/BT absolute pressure sensors from Kistler – for real-time monitoring with maximum measurement accuracy and signal quality!
16/10/2018
At Fakuma 2018, the Kistler Group is showcasing its latest monitoring and control packages for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
08/10/2018
The SMETEC Gesellschaft für Sensor-, Motor- und Energietechnik mbH recently became part of the Kistler Group.
24/09/2018
The Kistler Group is adding another variant to what is already the world's most comprehensive portfolio of wheel force measurement systems: the new RoaDyn S6GT 6-component wheel force measurement system.
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
The Kistler Group is introducing a compact mobile measurement solution for enhanced rolling stock maintenance in international railway operations in the shape of its railway brake force measuring system Type 2899A.
21/08/2018
A new Center of Competence for production control and management systems will be opened in Aachen.
31/07/2018
Competent service just a call away has always been a key aspect of Kistler's cooperation with its customers. Now, in a move to address growing demand in North Germany, the measurement technology experts are opening a new office in Wolfsburg.
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
Digitization, Internet of Things and Industry 4.0 are presenting major challenges. Discover how Kistler responds to the great challenges of our times.
09/05/2018
At Sensor + Test 2018 Kistler will be introducing a milestone in measurement technology: its new KiDAQ data acquisition system.
08/05/2018
At NPE 2018, the Kistler Group is showcasing its latest custom monitoring package for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
03/05/2018
At Automatica 2018, the Kistler Group will turn the spotlight on diverse options for using sensors and process monitoring systems to support industrial production and enhance digitalization in test and assembly technology.
24/04/2018
The Kistler Group will showcase its expanded portfolio of industrial test and inspection systems for quality assurance at the 2018 Control trade show.
12/04/2018
The global leader in dynamic measurement technology supports the passion for innovation and technology with a three-year partnership.
06/03/2018
Kistler will be showcasing at Control 2018 its portfolio of industrial testing and inspection systems with the spotlight on the very latest additions.
16/02/2018
At Intertraffic 2018 the Kistler Group is showcasing its comprehensive KiTraffic Weigh In Motion (WIM) solutions, which support road owners and authorities in road and traffic monitoring, weight enforcement and weight-based tolling.
15/02/2018
At NPE 2018 in Orlando, Florida, the Kistler Group will demonstrate a wide range of modular functionalities for ComoNeo: the process monitoring system that takes injection molding to a higher level with integrated quality monitoring geared to meet customers’ needs and requirements.
31/01/2018
The new KiSprint provides coaches and athletes with an efficient means of biomechanically optimizing sprint starts under competitive conditions. The robust and mobile solution has comprehensive software assessment options and can be individually adapted and expanded.
24/01/2018
Kistler achieved a growth rate of 18 % in 2017. Digital transformation has top priority in 2018.
23/01/2018
Surmonter les complexités du RTM - avec Kistler
12/10/2017
At the SPS IPC Drives Kistler Group will unveil the world's first digital charge amplifier Type 5974A, a milestone more in electrical automation.
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
With MARS software version 3.0, Kistler presents an extensive update of the proprietary measurement, analysis, and evaluation software for Kistler force plates.
21/10/2016
Kistler boosts the efficiency and reliability of large marine and stationary engines through monitoring and control of the combustion process
19/10/2016
Kistler is presenting the new versions of its ComoNeo and ComoDataCenter.
10/10/2016
Kistler is unveiling a new addition to its portfolio of electromechanical joining modules.
30/09/2016
The Kistler Group reported incoming orders worth CHF 233.3 million at the end of August 2016 and has therefore seen growth of 8.4 % compared to the same period in the previous year, or 5.6 % when adjusted for currency effects.
07/09/2016
At this year's K Trade Fair from 19 to 26 October in Düsseldorf, Kistler will be showcasing its latest new products and features with the focus on Industry 4.0.
24/07/2016
Kistler will be showcasing its new NCFE and NCFR joining modules, together with the latest generation of maXYmos monitoring systems on Motek 2016
12/07/2016
Kistler's Correvit® SFII sensor measures world record in 1.513 seconds
12/05/2016
Screw technology complements the range of applications.
27/04/2016
Following a long phase of planning, preparations, and conversion work, Kistler Instrumente GmbH has a new home for its German headquarters at the Böblingen/Sindelfingen airfield.
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
At Chinaplas 2015 Kistler will be presenting solutions for zero-defect production, process monitoring and data evaluation in injection molding
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
At Sensor + Test 2014 Kistler is presenting many new features from the field of measurement electronics in addition to its already proven sensor technology.
19/05/2014
Users obtain a full range of force–displacement measurement systems from one source
06/02/2014
The Kistler Group achieved sales of 285 million CHF in 2013, thus marking a slight growth in comparison with the figures for the prior year.