Programmable sequence control for integrated quality assurance

Winterthur, September 30, 2014 – At this year's Motek from October 6-9, 2014 in Stuttgart, Kistler will be presenting the latest innovations to its maXYmos product family, which is used to visualize and evaluate production processes. The highlight at Kistler's stand is the maXYmos BL 2.2 for manual presses, visitors to the exhibition will be able to see live demonstrations. Kistler is also showing a new update to the maXYmos TL as well as its most recent addition to this product series, the maXYmos NC.

 

Quality assurance for manually operated processes

The maXYmos BL force-displacement measurement system helps manufacturers attain zero-defect production in their hand-operated press processes. Based on the course of force and displacement measurement curves, the process can be visualized and the quality of the press process evaluated. Deviations are detected immediately and faulty parts can be separated at an early stage. This enables the quality of hand-operated press processes to be reproduced – independently of the respective operating personnel. The result is 100% quality control.

Visitors to Motek are especially invited to experience the sequencer mode of the maXYmos BL. This mode enables users to define an individual sequence of steps for each press process via the intuitive user interface of the touch display. 11 digital inputs and 8 corresponding outputs can be programmed in order to query and output processrelevant statuses. Up to 128 sequence elements can be configured for each measurement program. The maXYmos BL progressively checks whether all conditions have been fulfilled. In this manner, not only the production process can be controlled and good and bad end results detected, but it can also be deducted whether the desired quality has been attained in each step of the sequence. This can subsequently be reflected graphically. Ultimately, the required quality is ensured without the need for complex external control systems (PLC). In order to update existing manual presses, the measurement system – including sequencer mode – is also available as a retrofit package.

Complete spectrum of force-displacement measurement systems from a single source

Alongside the maXYmos BL, Kistler will also be presenting new functions of its top level system in Stuttgart. The maXYmos TL 1.1.4 includes an extensible language package, which now also encompasses Japanese, Portuguese and Czech. In addition, the system offers faster back-up functionalities, for example via USB or with the related maXYmos computer software. New cable solutions have also been developed to allow the connection of torque sensors.

"With the maXYmos product family, we have set industrial standards in terms of process optimization and quality assurance," says Jens Höppner, Product Manager at Kistler. "Our customers enjoy working with these systems and do so very successfully. Thanks to the further development of the underlying technologies they now benefit even more from our expertise and do not even have to get used to a new product."

The series has been completed with the maXYmos NC, which enables control and monitoring of electro-mechanical joining systems. Now, XY sequences for joining and pressfitting processes in combination with NC joining modules can be evaluated and documented and the quality of each individual production step, component or even the entire product can be controlled. This means that optimum cycle times can be implemented with maximum repeat accuracy. In this way, unplanned downtimes are minimized and machine availability is increased, thus improving the productivity of the manufacturing process.

From October 6-9, 2014 visitors to Motek will be shown Kistler's innovative products and be advised as to how the maXYmos series can be used individually in their own companies at stand 5535 in hall 5.

 

Download Press Release (PDF/EN)

 

User contact

Jens Höppner
Product Manager
Phone: +49 7172 184 238
E-mail: jens.hoeppner@kistler.com

 

Media contact

Simone Koch
Divisional Marketing Manager IPC
Phone: +41 52 224 18 02
E-mail: simone.koch@kistler.com

 

 

Captions

Image 1: The uniform philosophy of the maXYmos product family provides user-friendly and intuitive operation. It supports simple and quick start-up of the electro-mechanical NC joining systems.

Figure 2: The Sequencer Mode in the maXYmos BL allows programming of sequence controls, which are used to control the processes. An independent sequence can be created for each measurement program.

Figure 3: Force-displacement measurement system with piezoelectric force sensor for manually operated presses.

Dossier de press

Portrait de Kistler avec logo pour un aperçu rapide: Kistler Press Kit.zip

16/10/2018
At Fakuma 2018, the Kistler Group is showcasing its latest monitoring and control packages for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
08/10/2018
The SMETEC Gesellschaft für Sensor-, Motor- und Energietechnik mbH recently became part of the Kistler Group.
24/09/2018
The Kistler Group is adding another variant to what is already the world's most comprehensive portfolio of wheel force measurement systems: the new RoaDyn S6GT 6-component wheel force measurement system.
21/09/2018
At Fakuma 2018, Vester will showcase all the benefits of automated testing
17/09/2018
Top performance, team spirit and passionate commitment are qualities shared by Tigers Tübingen and the Kistler Group.
10/09/2018
High-accuracy dynamometer combined with innovative chuck extends tool lifetime and reduces production costs
06/09/2018
Machinery manufacturer LIK joins the Kistler Group, opening up wider access to the electric vehicle market
28/08/2018
Enhanced transparency in plastics processing
21/08/2018
The Kistler Group is introducing a compact mobile measurement solution for enhanced rolling stock maintenance in international railway operations in the shape of its railway brake force measuring system Type 2899A.
21/08/2018
A new Center of Competence for production control and management systems will be opened in Aachen.
31/07/2018
Competent service just a call away has always been a key aspect of Kistler's cooperation with its customers. Now, in a move to address growing demand in North Germany, the measurement technology experts are opening a new office in Wolfsburg.
25/07/2018
On her way to Olympia 2020 she relies on Kistler Group measurement experts.
18/07/2018
Effective monitoring with strain sensors protects machines and tools
03/07/2018
The Top 100 Competition has again singled out the most innovative German small and medium-sized enterprises (SMEs) for the 10th time.
25/06/2018
Kistler is pleased to introduce MicroDyn, the world's smallest series-produced cutting force meter.
19/06/2018
Kistler introduces the world’s first high temperature accelerometer for the monitoring of gas turbines.
11/06/2018
Kistler is earmarking the highest investment budget for research and development in the company`s history.
11/05/2018
Digitization, Internet of Things and Industry 4.0 are presenting major challenges. Discover how Kistler responds to the great challenges of our times.
09/05/2018
At Sensor + Test 2018 Kistler will be introducing a milestone in measurement technology: its new KiDAQ data acquisition system.
08/05/2018
At NPE 2018, the Kistler Group is showcasing its latest custom monitoring package for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
03/05/2018
At Automatica 2018, the Kistler Group will turn the spotlight on diverse options for using sensors and process monitoring systems to support industrial production and enhance digitalization in test and assembly technology.
24/04/2018
The Kistler Group will showcase its expanded portfolio of industrial test and inspection systems for quality assurance at the 2018 Control trade show.
12/04/2018
The global leader in dynamic measurement technology supports the passion for innovation and technology with a three-year partnership.
06/03/2018
Kistler will be showcasing at Control 2018 its portfolio of industrial testing and inspection systems with the spotlight on the very latest additions.
16/02/2018
At Intertraffic 2018 the Kistler Group is showcasing its comprehensive KiTraffic Weigh In Motion (WIM) solutions, which support road owners and authorities in road and traffic monitoring, weight enforcement and weight-based tolling.
15/02/2018
At NPE 2018 in Orlando, Florida, the Kistler Group will demonstrate a wide range of modular functionalities for ComoNeo: the process monitoring system that takes injection molding to a higher level with integrated quality monitoring geared to meet customers’ needs and requirements.
31/01/2018
The new KiSprint provides coaches and athletes with an efficient means of biomechanically optimizing sprint starts under competitive conditions. The robust and mobile solution has comprehensive software assessment options and can be individually adapted and expanded.
24/01/2018
Kistler achieved a growth rate of 18 % in 2017. Digital transformation has top priority in 2018.
23/01/2018
Surmonter les complexités du RTM - avec Kistler
12/10/2017
At the SPS IPC Drives Kistler Group will unveil the world's first digital charge amplifier Type 5974A, a milestone more in electrical automation.
09/10/2017
Kistler's Type 5074A industrial charge amplifier breaks new ground in industrial charge amplifier technology
06/10/2017
Whether hybrid drives or electric vehicles: anyone who wants to make a change needs to measure and understand
27/09/2017
Our experts will present you Kistler measuring technologies for demanding space applications.
05/09/2017
At Fakuma 2017, we will demonstrate how you can benefit from new ComoNeo functionalities
31/08/2017
Kistler Group showcases the entire spectrum of its integrated quality assurance solutions
25/08/2017
Kistler Group took over near Karlsruhe-based Vester Elektronik GmbH on 25 August, a specialist in sensor technology and test automation.
11/08/2017
Jaguar Land Rover uses Kistler RoaDyn® Wheel Force Transducers for accurate tyre modelling
11/07/2017
Kistler is taking over IOS GmbH (Germany), provider of Manufacturing Execution Systems (MES).
06/07/2017
Tettnang-based firm eso GmbH was acquired by the Kistler Group on July 5.
20/06/2017
Perfect production data synchronization through direct MES system integration.
02/05/2017
Kistler presents innovative measurement equipment for demanding vehicle testing applications
25/04/2017
At Moulding Expo 2017, we will show how easy it is to install the measurement technology needed for quality assurance in injection molds.
12/04/2017
Kistler will be present at Control, the world's leading quality assurance trade fair.
12/04/2017
Advanced features for LabAmp family maximize flexibility for cutting force users.
11/04/2017
Measuring equipment for sophisticated T&M applications
01/02/2017
The Kistler Group is constantly growing and recruiting specialist staff worldwide.
17/01/2017
Olympic champion Anthony Ervin and Kistler create a Success Story together.
02/12/2016
Kistler seeks more than 40 specialists in what is likely Switzerland's largest job advertisement.
11/11/2016
With MARS software version 3.0, Kistler presents an extensive update of the proprietary measurement, analysis, and evaluation software for Kistler force plates.
21/10/2016
Kistler boosts the efficiency and reliability of large marine and stationary engines through monitoring and control of the combustion process
19/10/2016
Kistler is presenting the new versions of its ComoNeo and ComoDataCenter.
10/10/2016
Kistler is unveiling a new addition to its portfolio of electromechanical joining modules.
30/09/2016
The Kistler Group reported incoming orders worth CHF 233.3 million at the end of August 2016 and has therefore seen growth of 8.4 % compared to the same period in the previous year, or 5.6 % when adjusted for currency effects.
07/09/2016
At this year's K Trade Fair from 19 to 26 October in Düsseldorf, Kistler will be showcasing its latest new products and features with the focus on Industry 4.0.
24/07/2016
Kistler will be showcasing its new NCFE and NCFR joining modules, together with the latest generation of maXYmos monitoring systems on Motek 2016
12/07/2016
Kistler's Correvit® SFII sensor measures world record in 1.513 seconds
12/05/2016
Screw technology complements the range of applications.
27/04/2016
Following a long phase of planning, preparations, and conversion work, Kistler Instrumente GmbH has a new home for its German headquarters at the Böblingen/Sindelfingen airfield.
12/02/2016
Kistler Lorch GmbH Honored for Outstanding Qualities as Employer
02/02/2016
The Kistler Group has overcome currency-related challenges at its Swiss site to achieve continued growth.
28/01/2016
Accurate Wheel Force Measurement with Minimum Configuration Effort
26/11/2015
Increased Flexibility for High-Speed Combustion Analysis
02/11/2015
New Piezoresistive Sensor with Temperature Probe and Integrated Signal Conditioning.
27/10/2015
Kistler Provides Maximum Flexibility for Product Testing and Development
16/10/2015
Kistler's NCFR Joining Module honored in the handling and assembly category
05/10/2015
Setting the Standard for 100% Control of Linear Joining Processes with Partial Rotation
18/09/2015
Kistler Group: safeguarding the firm's competitive edge.
15/09/2015
Quick evaluation of performance and force with Kistler MARS 2.1.
03/09/2015
Major update for Kistler’s mobile engine indication system.
01/09/2015
Setting New Standards in Automated Process Monitoring for Injection Molding.
25/08/2015
Kistler Showcases Three Latest Product Innovations at Motek 2015
26/06/2015
Kistler honored with ASCO Award Gold for best corporate transformation in Switzerland.
26/06/2015
Kistler's software for force plates offers a host of new features for performance diagnostics in sports and rehabilitation.
22/04/2015
At Chinaplas 2015 Kistler will be presenting solutions for zero-defect production, process monitoring and data evaluation in injection molding
10/11/2014
New product developments for dynamic measuring technology at the Kistler booth at SPS IPC Drives 2014
14/10/2014
Wide range of options for optimizing the quality assurance through documenting and evaluating production data of CoMo Injection Systems
29/09/2014
Users obtain a full range of force–displacement measurement systems from one source
03/06/2014
Extending the maXYmos product range to control and monitor production processes and quality assurance
26/05/2014
At Sensor + Test 2014 Kistler is presenting many new features from the field of measurement electronics in addition to its already proven sensor technology.
19/05/2014
Users obtain a full range of force–displacement measurement systems from one source
06/02/2014
The Kistler Group achieved sales of 285 million CHF in 2013, thus marking a slight growth in comparison with the figures for the prior year.
11/11/2013
From flexible torque sensors to complete test stands for highly-efficient electric drives
Contact
Cara-Isabell Maercklin
Cara-Isabell Maercklin
Media Contact
Contact
(max 25 Mb)