Presenting ComoNeo at Fakuma

Winterthur, 1 September 2015 – Kistler will unveil its new ComoNeo process monitoring system at the Fakuma trade fair from 13 to 17 October 2015. The ComoNeo is the system of choice for any company that aims to optimize monitoring and analysis of the injection molding process so as to cut costs permanently.

For many years, Kistler's innovative solutions to enhance process reliability in injection molding have ensured the firm's leading position in the global market. These systems all feature mature technology with one common denominator: quality testing is integrated into the injection molding process. The benefit: faulty parts can be excluded from the production process before they cause unnecessary costs. The ComoNeo process monitoring system – to be premiered at the 2015 Fakuma – moves automated production process monitoring into a new dimension: first-time customers will find that Kistler's new system provides a simple introduction, while users with experience in this field will appreciate the technological advances that it offers.

Simple, Intuitive Operation
The ComoNeo process monitoring system breaks new ground in the development of hardware as well as integrated monitoring software. To start with, the entirely new intuitive design sets new standards. The display − equipped with optimized touch-based operation – is now more closely tailored to users' needs. Users also benefit directly from the increased number of channel inputs on the ComoNeo: twice as many cavity pressure signals can now be recorded, so molds with a large number of cavities can be connected. Likewise, the number of digital outputs is doubled, so more components can be evaluated individually. The ComoNeo software is also committed to a process-oriented operating philosophy – as is clear from the various new tools that offer active support with analyzing process fluctuations and monitoring component quality. This system is ideal for highly quality-conscious companies that aim for systematic analysis and optimization of their processes – and it is also an excellent choice for firms that focus on the transparency of their injection molding processes and comprehensive documentation of component quality.

Innovative Functions for Optimized Processes
Daniel Fick, Kistler's Product Manager in the Plastics Strategic Business Field, emphasizes the high innovative content of this newly developed product: "The launch of ComoNeo has moved auto-mated monitoring of the injection molding process into a new dimension. A host of innovative functions position ComoNeo on the market as a powerfully attractive process monitoring system." One outstanding highlight of the integrated monitoring software is the tool that generates and positions the monitoring boxes for good/bad evaluation. In the past, users had to set the monitoring boxes themselves. Now, the ComoNeo includes a systematic process (Evaluation Assistant/EO Assistant) that guides the user quickly and accurately to the rejection limits. The results from the EO Assistant therefore define the evaluation types and the relevant limits. Thanks to this approach, components can be monitored with high precision and pseudoscrap (i.e. "presumed" scrap) is reduced. Complaints from customers are also avoided because no faulty components leave the production line. Reducing pseudoscrap and eliminating rejects are two especially crucial factors in cutting production costs in the injection molding process.

The "dashboard" is a second highlight: this is an overview screen that collates all the relevant process data to give a clear picture of how the production lot is currently progressing. Thanks to the dashboard, Kistler customers can detect process fluctuations very quickly. Users can also navigate directly from the dashboard to the detailed data. Another attractive innovation: the operating controls and procedures are consistently geared to the injection molding process – for instance, cavity-specific analyses can be carried out.

Additional Tools to Improve Process Monitoring
But that's not all: ComoNeo offers even more tools – such as the newly-designed user management feature that allows every company to set up its own specific roles for various users, and automatic mold identification to prevent errors on the interface between the mold and the integrated monitoring software. Automated mold selection also reduces retooling times. In a nutshell: when the objective is to maximize production efficiency in the injection molding process, ComoNeo is the process monitoring system of choice for quality-conscious companies.

Kistler is presenting its new ComoNeo process monitoring system at Fakuma in Friedrichshafen from 13 to 17 October 2015 on stand 3104 in hall A3.

Download Press Release
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
The new joining module is highly suitable for clinching and riveting, and also for assembly processes that require force-displacement monitoring.
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
The Kistler Group will showcase its test and analysis systems for threaded joints at the 2019 Fastener Fair in Stuttgart from 19 to 21 March.
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
Accurate and insensitive to its mounting position: the new Type 6044A M8 sensor features an anti-strain design to ensure reliable, high-quality results.
20/11/2018
Motorsport: the new 4080B/BT absolute pressure sensors from Kistler – for real-time monitoring with maximum measurement accuracy and signal quality!
16/10/2018
At Fakuma 2018, the Kistler Group is showcasing its latest monitoring and control packages for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
08/10/2018
The SMETEC Gesellschaft für Sensor-, Motor- und Energietechnik mbH recently became part of the Kistler Group.
24/09/2018
The Kistler Group is adding another variant to what is already the world's most comprehensive portfolio of wheel force measurement systems: the new RoaDyn S6GT 6-component wheel force measurement system.
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
The Kistler Group is introducing a compact mobile measurement solution for enhanced rolling stock maintenance in international railway operations in the shape of its railway brake force measuring system Type 2899A.
21/08/2018
A new Center of Competence for production control and management systems will be opened in Aachen.
31/07/2018
Competent service just a call away has always been a key aspect of Kistler's cooperation with its customers. Now, in a move to address growing demand in North Germany, the measurement technology experts are opening a new office in Wolfsburg.
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
Digitization, Internet of Things and Industry 4.0 are presenting major challenges. Discover how Kistler responds to the great challenges of our times.
09/05/2018
At Sensor + Test 2018 Kistler will be introducing a milestone in measurement technology: its new KiDAQ data acquisition system.
08/05/2018
At NPE 2018, the Kistler Group is showcasing its latest custom monitoring package for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
03/05/2018
At Automatica 2018, the Kistler Group will turn the spotlight on diverse options for using sensors and process monitoring systems to support industrial production and enhance digitalization in test and assembly technology.
24/04/2018
The Kistler Group will showcase its expanded portfolio of industrial test and inspection systems for quality assurance at the 2018 Control trade show.
12/04/2018
The global leader in dynamic measurement technology supports the passion for innovation and technology with a three-year partnership.
06/03/2018
Kistler will be showcasing at Control 2018 its portfolio of industrial testing and inspection systems with the spotlight on the very latest additions.
16/02/2018
At Intertraffic 2018 the Kistler Group is showcasing its comprehensive KiTraffic Weigh In Motion (WIM) solutions, which support road owners and authorities in road and traffic monitoring, weight enforcement and weight-based tolling.
15/02/2018
At NPE 2018 in Orlando, Florida, the Kistler Group will demonstrate a wide range of modular functionalities for ComoNeo: the process monitoring system that takes injection molding to a higher level with integrated quality monitoring geared to meet customers’ needs and requirements.
31/01/2018
The new KiSprint provides coaches and athletes with an efficient means of biomechanically optimizing sprint starts under competitive conditions. The robust and mobile solution has comprehensive software assessment options and can be individually adapted and expanded.
24/01/2018
Kistler achieved a growth rate of 18 % in 2017. Digital transformation has top priority in 2018.
23/01/2018
Surmonter les complexités du RTM - avec Kistler
12/10/2017
At the SPS IPC Drives Kistler Group will unveil the world's first digital charge amplifier Type 5974A, a milestone more in electrical automation.
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
With MARS software version 3.0, Kistler presents an extensive update of the proprietary measurement, analysis, and evaluation software for Kistler force plates.
21/10/2016
Kistler boosts the efficiency and reliability of large marine and stationary engines through monitoring and control of the combustion process
19/10/2016
Kistler is presenting the new versions of its ComoNeo and ComoDataCenter.
10/10/2016
Kistler is unveiling a new addition to its portfolio of electromechanical joining modules.
30/09/2016
The Kistler Group reported incoming orders worth CHF 233.3 million at the end of August 2016 and has therefore seen growth of 8.4 % compared to the same period in the previous year, or 5.6 % when adjusted for currency effects.
07/09/2016
At this year's K Trade Fair from 19 to 26 October in Düsseldorf, Kistler will be showcasing its latest new products and features with the focus on Industry 4.0.
24/07/2016
Kistler will be showcasing its new NCFE and NCFR joining modules, together with the latest generation of maXYmos monitoring systems on Motek 2016
12/07/2016
Kistler's Correvit® SFII sensor measures world record in 1.513 seconds
12/05/2016
Screw technology complements the range of applications.
27/04/2016
Following a long phase of planning, preparations, and conversion work, Kistler Instrumente GmbH has a new home for its German headquarters at the Böblingen/Sindelfingen airfield.
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
At Chinaplas 2015 Kistler will be presenting solutions for zero-defect production, process monitoring and data evaluation in injection molding
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
At Sensor + Test 2014 Kistler is presenting many new features from the field of measurement electronics in addition to its already proven sensor technology.
19/05/2014
Users obtain a full range of force–displacement measurement systems from one source
06/02/2014
The Kistler Group achieved sales of 285 million CHF in 2013, thus marking a slight growth in comparison with the figures for the prior year.