KiXact from Kistler – the first technology to automatically calculate measurement uncertainty

Winterthur, April 2019 - As global market leader in dynamic measurement technology, the Kistler Group is proud to announce the launch of KiXact. This is the first technology that enables measurement uncertainty to be reliably and automatically calculated and interpreted intuitively by the user. Up to now, for reasons of time or cost, many measurement engineers have completely dispensed with determining measurement uncertainty. This is because the calculations are complicated and time-consuming, and the results often difficult to evaluate. With KiXact, Kistler is now offering a solution that makes it much easier for users to deal with the uncertainty of measurement.

Kistler has been supplying engineers, researchers and measurement technicians with the appropriate technology for demanding measurement tasks for decades. Based on this wealth of experience, the company has succeeded in developing a simple, precise and fast solution for calculating measurement uncertainty. As part of the KiDAQ data acquisition system, the KiXact technology automatically calculates measurement uncertainty. The results can be analyzed using the KiStudio Lab software provided. External influencing factors such as ambient temperature and humidity for the respective measurement are stored in the program and included in the KiXact calculation. Because Kistler supplies the complete measurement chain, KiXact is already optimally adjusted to the relevant setup and associated sensors.

KiXact thus offers customers from different areas an uncomplicated solution and can deliver more than just a tolerance interval. The analysis recognizes early which factors in the measurement chain are influencing the measurement, giving operators the opportunity to adjust parameters accordingly. This results in more meaningful measurements of higher quality and with less uncertainty.

Uncertainties are relevant for every measurement

An uncertainty of measurement is not an exception – every measurement result in research and industry is associated with a certain degree of inaccuracy. Even small fluctuations in the ambient temperature can lead to deviations that make the result unreliable and unusable. Whenever decisions are based on a measurement result, it is important to have an indication of the quality. Thus the knowledge of the respective measurement uncertainty is indispensable in achieving meaningful results.

The more components the measurement chain contains, the more complex the determination of uncertainty becomes, as every potential influencing factor needs to be taken into account. Up to now, it has been necessary to review the respective data sheet for each possible source of uncertainty, check individual specifications and – in addition to external influences – include them in the calculation. Both the calculation itself and the subsequent evaluation of the data require extended specialist knowledge and a great deal of experience. This procedure requires a considerable effort. To keep the measurement processes economical and manageable on the one hand, in many cases generous assumptions are made or the calculation of the uncertainty is even omitted completely. On the other hand, if an excessive allowance is made for the uncertainty, this has a negative influence on the cost-efficiency of the entire process. Where measurement uncertainty can be reliably determined, tolerance limits can be defined more narrowly and the process is more efficient as a consequence.

“Research results are only valid if they are based on precise and, above all, reliable measurement results. In this respect, KiXact can help ease the burden on the research budget”, explained Michael Lauffer, Product Manager DAQ Systems at Kistler. “In production contexts, we see the principle advantage of KiXact in optimizing processes by incorporating measurement uncertainties faster and without complicated formulas. If you have the issue of measurement uncertainty under control, you will get better results.”

The KiDAQ data acquisition system

The KiDAQ data acquisition system is modular in terms of both hardware and software. Kistler offers a wide range of measurement modules as well as various analog and digital inputs. The modules are available in three different housing variants. As a result, they offer the user maximum flexibility for every measurement task. Multiple measuring devices can be combined and are precisely time-synchronized. Furthermore the measurement platform based on cloud-technologies enables extensions for future applications, even through partner companies.
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
The new joining module is highly suitable for clinching and riveting, and also for assembly processes that require force-displacement monitoring.
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
The Kistler Group will showcase its test and analysis systems for threaded joints at the 2019 Fastener Fair in Stuttgart from 19 to 21 March.
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
Accurate and insensitive to its mounting position: the new Type 6044A M8 sensor features an anti-strain design to ensure reliable, high-quality results.
20/11/2018
Motorsport: the new 4080B/BT absolute pressure sensors from Kistler – for real-time monitoring with maximum measurement accuracy and signal quality!
16/10/2018
At Fakuma 2018, the Kistler Group is showcasing its latest monitoring and control packages for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
08/10/2018
The SMETEC Gesellschaft für Sensor-, Motor- und Energietechnik mbH recently became part of the Kistler Group.
24/09/2018
The Kistler Group is adding another variant to what is already the world's most comprehensive portfolio of wheel force measurement systems: the new RoaDyn S6GT 6-component wheel force measurement system.
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
The Kistler Group is introducing a compact mobile measurement solution for enhanced rolling stock maintenance in international railway operations in the shape of its railway brake force measuring system Type 2899A.
21/08/2018
A new Center of Competence for production control and management systems will be opened in Aachen.
31/07/2018
Competent service just a call away has always been a key aspect of Kistler's cooperation with its customers. Now, in a move to address growing demand in North Germany, the measurement technology experts are opening a new office in Wolfsburg.
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
Digitization, Internet of Things and Industry 4.0 are presenting major challenges. Discover how Kistler responds to the great challenges of our times.
09/05/2018
At Sensor + Test 2018 Kistler will be introducing a milestone in measurement technology: its new KiDAQ data acquisition system.
08/05/2018
At NPE 2018, the Kistler Group is showcasing its latest custom monitoring package for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
03/05/2018
At Automatica 2018, the Kistler Group will turn the spotlight on diverse options for using sensors and process monitoring systems to support industrial production and enhance digitalization in test and assembly technology.
24/04/2018
The Kistler Group will showcase its expanded portfolio of industrial test and inspection systems for quality assurance at the 2018 Control trade show.
12/04/2018
The global leader in dynamic measurement technology supports the passion for innovation and technology with a three-year partnership.
06/03/2018
Kistler will be showcasing at Control 2018 its portfolio of industrial testing and inspection systems with the spotlight on the very latest additions.
16/02/2018
At Intertraffic 2018 the Kistler Group is showcasing its comprehensive KiTraffic Weigh In Motion (WIM) solutions, which support road owners and authorities in road and traffic monitoring, weight enforcement and weight-based tolling.
15/02/2018
At NPE 2018 in Orlando, Florida, the Kistler Group will demonstrate a wide range of modular functionalities for ComoNeo: the process monitoring system that takes injection molding to a higher level with integrated quality monitoring geared to meet customers’ needs and requirements.
31/01/2018
The new KiSprint provides coaches and athletes with an efficient means of biomechanically optimizing sprint starts under competitive conditions. The robust and mobile solution has comprehensive software assessment options and can be individually adapted and expanded.
24/01/2018
Kistler achieved a growth rate of 18 % in 2017. Digital transformation has top priority in 2018.
23/01/2018
Surmonter les complexités du RTM - avec Kistler
12/10/2017
At the SPS IPC Drives Kistler Group will unveil the world's first digital charge amplifier Type 5974A, a milestone more in electrical automation.
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
With MARS software version 3.0, Kistler presents an extensive update of the proprietary measurement, analysis, and evaluation software for Kistler force plates.
21/10/2016
Kistler boosts the efficiency and reliability of large marine and stationary engines through monitoring and control of the combustion process
19/10/2016
Kistler is presenting the new versions of its ComoNeo and ComoDataCenter.
10/10/2016
Kistler is unveiling a new addition to its portfolio of electromechanical joining modules.
30/09/2016
The Kistler Group reported incoming orders worth CHF 233.3 million at the end of August 2016 and has therefore seen growth of 8.4 % compared to the same period in the previous year, or 5.6 % when adjusted for currency effects.
07/09/2016
At this year's K Trade Fair from 19 to 26 October in Düsseldorf, Kistler will be showcasing its latest new products and features with the focus on Industry 4.0.
24/07/2016
Kistler will be showcasing its new NCFE and NCFR joining modules, together with the latest generation of maXYmos monitoring systems on Motek 2016
12/07/2016
Kistler's Correvit® SFII sensor measures world record in 1.513 seconds
12/05/2016
Screw technology complements the range of applications.
27/04/2016
Following a long phase of planning, preparations, and conversion work, Kistler Instrumente GmbH has a new home for its German headquarters at the Böblingen/Sindelfingen airfield.
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
At Chinaplas 2015 Kistler will be presenting solutions for zero-defect production, process monitoring and data evaluation in injection molding
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
At Sensor + Test 2014 Kistler is presenting many new features from the field of measurement electronics in addition to its already proven sensor technology.
19/05/2014
Users obtain a full range of force–displacement measurement systems from one source
06/02/2014
The Kistler Group achieved sales of 285 million CHF in 2013, thus marking a slight growth in comparison with the figures for the prior year.