KiTraffic Plus from Kistler: the variable WIM ecosystem for efficient traffic monitoring

Winterthur, March 2021 – Weigh In Motion functionality tailored to each customer's specific requirements, extendable as desired by adding vehicle recognition and measurement systems: the Kistler Group's expertise in traffic data acquisition is packed into KiTraffic Plus – the new software-based modular system that helps to protect infrastructure, prevent accidents and automate traffic monitoring. 

In the 21st century, automated Weigh In Motion (WIM) systems have evolved into a technology that plays a key part in monitoring ever-increasing traffic volumes and – especially – the loads and stresses to which roads are exposed. This is because overloaded commercial vehicles contribute disproportionately to wear and tear on infrastructure, and they also heighten the risk of accidents.

Now, Kistler offers its worldwide customers the new KiTraffic Plus: a flexible modular solution that can be precisely tailored to each user's needs – for applications ranging from vehicle preselection and bridge protection to direct prosecution of violations. As well as providing a wide choice of options for WIM, KiTraffic Plus can be extended flexibly by adding functions such as vehicle identification or recording of speeds and vehicle dimensions.

Open software-based platform

The core components of KiTraffic Plus: piezoelectric Lineas quartz sensors from Kistler that capture the weight of trucks at speeds of up to 120 km/h with high accuracy. Depending on their individual requirements, customers can choose from the Lineas, Lineas Compact and Lineas Digital models. As an option, detection of tire configurations and conditions (single/double and flat tires) can also be integrated into KiTraffic Plus. 

A new feature of the KiTraffic Plus platform solution is the openness principle: alongside the advanced WIM functions, additional field devices can be integrated to ensure fully comprehensive traffic monitoring. Examples include ANPR and overview cameras, speed monitoring, dimension scanners and height detectors – the types and numbers of connected devices are fully variable according to choice. Thanks to the system's modular architecture, KiTraffic Plus can be extended at any later time, with no need for major outlay or effort. The Kistler DataMatcher software compiles all the data collected by the installed system to create a vehicle-specific dataset. This real-time process takes place in the control cabinet at the side of the road, close to the operating location. Then, the dataset is processed according to customer specifications before it is transmitted to higher-level systems via a machine interface.

The standard options for KiTraffic Plus include these modules, which can be combined as desired:

  • WIM system based on piezoelectric quartz sensors to capture axle load, overall weight and vehicle class
  • Integrated speed measurement
  • Camera with ANPR capability for vehicle photos and numberplate recognition
  • LIDAR dimension scanner to capture a vehicle's width, length and height
  • Kistler DataMatcher software to acquire and synchronize data from the field devices

As an optional addition, Kistler offers a graphic user interface for live display of preselection data during spot-check campaigns, or for post-processing of the acquired datasets in the office. To ensure maximum reliability and protection of customers' investments, Kistler offers a wide-ranging package of services for Weigh In Motion: everything is covered, from precise analysis of the physical condition of the location and road before installation, comprehensive project management and support with system integration and calibration, through to staff training and warranty extensions.
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
The Kistler Group will showcase its test and analysis systems for threaded joints at the 2019 Fastener Fair in Stuttgart from 19 to 21 March.
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
Accurate and insensitive to its mounting position: the new Type 6044A M8 sensor features an anti-strain design to ensure reliable, high-quality results.
20/11/2018
Motorsport: the new 4080B/BT absolute pressure sensors from Kistler – for real-time monitoring with maximum measurement accuracy and signal quality!
16/10/2018
At Fakuma 2018, the Kistler Group is showcasing its latest monitoring and control packages for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
08/10/2018
The SMETEC Gesellschaft für Sensor-, Motor- und Energietechnik mbH recently became part of the Kistler Group.
24/09/2018
The Kistler Group is adding another variant to what is already the world's most comprehensive portfolio of wheel force measurement systems: the new RoaDyn S6GT 6-component wheel force measurement system.
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
The Kistler Group is introducing a compact mobile measurement solution for enhanced rolling stock maintenance in international railway operations in the shape of its railway brake force measuring system Type 2899A.
21/08/2018
A new Center of Competence for production control and management systems will be opened in Aachen.
31/07/2018
Competent service just a call away has always been a key aspect of Kistler's cooperation with its customers. Now, in a move to address growing demand in North Germany, the measurement technology experts are opening a new office in Wolfsburg.
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
Digitization, Internet of Things and Industry 4.0 are presenting major challenges. Discover how Kistler responds to the great challenges of our times.
09/05/2018
At Sensor + Test 2018 Kistler will be introducing a milestone in measurement technology: its new KiDAQ data acquisition system.
08/05/2018
At NPE 2018, the Kistler Group is showcasing its latest custom monitoring package for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
03/05/2018
At Automatica 2018, the Kistler Group will turn the spotlight on diverse options for using sensors and process monitoring systems to support industrial production and enhance digitalization in test and assembly technology.
24/04/2018
The Kistler Group will showcase its expanded portfolio of industrial test and inspection systems for quality assurance at the 2018 Control trade show.
12/04/2018
The global leader in dynamic measurement technology supports the passion for innovation and technology with a three-year partnership.
06/03/2018
Kistler will be showcasing at Control 2018 its portfolio of industrial testing and inspection systems with the spotlight on the very latest additions.
16/02/2018
At Intertraffic 2018 the Kistler Group is showcasing its comprehensive KiTraffic Weigh In Motion (WIM) solutions, which support road owners and authorities in road and traffic monitoring, weight enforcement and weight-based tolling.
15/02/2018
At NPE 2018 in Orlando, Florida, the Kistler Group will demonstrate a wide range of modular functionalities for ComoNeo: the process monitoring system that takes injection molding to a higher level with integrated quality monitoring geared to meet customers’ needs and requirements.
31/01/2018
The new KiSprint provides coaches and athletes with an efficient means of biomechanically optimizing sprint starts under competitive conditions. The robust and mobile solution has comprehensive software assessment options and can be individually adapted and expanded.
24/01/2018
Kistler achieved a growth rate of 18 % in 2017. Digital transformation has top priority in 2018.
23/01/2018
Surmonter les complexités du RTM - avec Kistler
12/10/2017
At the SPS IPC Drives Kistler Group will unveil the world's first digital charge amplifier Type 5974A, a milestone more in electrical automation.
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
With MARS software version 3.0, Kistler presents an extensive update of the proprietary measurement, analysis, and evaluation software for Kistler force plates.
21/10/2016
Kistler boosts the efficiency and reliability of large marine and stationary engines through monitoring and control of the combustion process
19/10/2016
Kistler is presenting the new versions of its ComoNeo and ComoDataCenter.
10/10/2016
Kistler is unveiling a new addition to its portfolio of electromechanical joining modules.
30/09/2016
The Kistler Group reported incoming orders worth CHF 233.3 million at the end of August 2016 and has therefore seen growth of 8.4 % compared to the same period in the previous year, or 5.6 % when adjusted for currency effects.
07/09/2016
At this year's K Trade Fair from 19 to 26 October in Düsseldorf, Kistler will be showcasing its latest new products and features with the focus on Industry 4.0.
24/07/2016
Kistler will be showcasing its new NCFE and NCFR joining modules, together with the latest generation of maXYmos monitoring systems on Motek 2016
12/07/2016
Kistler's Correvit® SFII sensor measures world record in 1.513 seconds
12/05/2016
Screw technology complements the range of applications.
27/04/2016
Following a long phase of planning, preparations, and conversion work, Kistler Instrumente GmbH has a new home for its German headquarters at the Böblingen/Sindelfingen airfield.
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
At Chinaplas 2015 Kistler will be presenting solutions for zero-defect production, process monitoring and data evaluation in injection molding
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
At Sensor + Test 2014 Kistler is presenting many new features from the field of measurement electronics in addition to its already proven sensor technology.
19/05/2014
Users obtain a full range of force–displacement measurement systems from one source
06/02/2014
The Kistler Group achieved sales of 285 million CHF in 2013, thus marking a slight growth in comparison with the figures for the prior year.