Kistler unveils new electromechanical joining module

Winterthur, April 2022 – Kistler is adding a compact, weight-optimized system to its portfolio: the new NCFC electromechanical joining module. This is a highly suitable solution for clinching and riveting applications, and also for assembly and joining processes that require force-displacement monitoring. Another highlight of the new NCFC servo press: it needs very little installation space, so weight and center of gravity design are optimized – particularly for robot arm applications. 

Clinching (also known as press-joining) is an efficient and reliable joining process that is becoming increasingly attractive to industrial manufacturers because it requires no additional components such as rivets or bolts. And unlike drilling or welding, clinching does not generate any heat input. Clinching requires less energy and maintenance effort than spot welding; depending on the material and process, the strength values of clinched joints are often equal or sometimes even higher, and the processes can also be controlled with greater ease and accuracy.

Kistler presents in cooperation with BTM the first ever electromechanical joining module that is specifically optimized to meet the requirements of the clinching process. Thanks to the combination of Kistler technology with BTM's application know-how in clinch tooling and pliers, customers benefit from a servo press based on cutting-edge technology that offers high-precision, energy-efficient part joining with assured quality.

Benefits of the new NCFC joining module from Kistler at a glance:

  • Compact lightweight design – ideal for use on robots and stationary or mobile portals
  • Better dynamics than systems with comparable weight and similar dimensions
  • Optimized design to allow short distances between workstations (small center distance)
  • Easy and fast installation of servo press thanks to the new hybrid cable solution
  • Visualization, control and documentation with the proven maXYmos NC process monitoring
    system – no additional industrial PC required
  • Improved quality with lower consumption of resources and reduced CO2 emissions compared to conventional systems

The future of clinching is electromechanical

The outcome of the collaboration between clinching specialist BTM and the measurement and joining technology experts at Kistler is an exceptionally advanced solution that will benefit customers across the globe. BTM has earned worldwide renown with its flexible, customized solutions and has accumulated decades of experience with mechanical joining solutions such as clinching and self-piercing riveting. BTM's expertise played a key part in the cooperation partnership with Kistler, providing an ideal solution for customers to switch to electromechanical clinching.

An electromechanically operated clinching system offers significant energy savings as compared to pneumatic or pneumohydraulic alternatives. In this solution, the servo press is controlled by the proven maXYmos NC process monitoring system from Kistler. With continuous force-displacement monitoring by the integrated sensor, positions can be approached reliably, flexibly and at high speed; the solution also includes an additional traverse mode with safely reduced speed. The new system ensures complete control and transparency for each individual production step at all times; deflection compensation for the mounting bracket also allows very precise setting of the residual base thickness (as the quality characteristic). 

Advancing the digitalization of production processes

The new NCFC (2163A) joining module from Kistler will be offered in two versions with nominal joining forces of 55 kN and 80 kN respectively. As well as the robot arm application, the NCFC servo press can also be operated as a stationary version or as part of a complete clinching system from BTM.

Clinching delivers major benefits in line with key industrial trends: resource and energy efficiency, transparency, and automation – as well as extensive possibilities for joining components made of different materials. Given these advantages, electromechanical joining systems are set to see significant growth in sectors such as electrical engineering, white goods, refrigeration and air conditioning technology. The world's mechanical engineers and manufacturers can now use the clinch solution from BTM and Kistler to boost the economic efficiency, quality and transparency of their assembly processes – and the digitalization of clinching marks another step along the road to Industry 4.0.
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
The new joining module is highly suitable for clinching and riveting, and also for assembly processes that require force-displacement monitoring.
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
The Kistler Group will showcase its test and analysis systems for threaded joints at the 2019 Fastener Fair in Stuttgart from 19 to 21 March.
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
Accurate and insensitive to its mounting position: the new Type 6044A M8 sensor features an anti-strain design to ensure reliable, high-quality results.
20/11/2018
Motorsport: the new 4080B/BT absolute pressure sensors from Kistler – for real-time monitoring with maximum measurement accuracy and signal quality!
16/10/2018
At Fakuma 2018, the Kistler Group is showcasing its latest monitoring and control packages for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
08/10/2018
The SMETEC Gesellschaft für Sensor-, Motor- und Energietechnik mbH recently became part of the Kistler Group.
24/09/2018
The Kistler Group is adding another variant to what is already the world's most comprehensive portfolio of wheel force measurement systems: the new RoaDyn S6GT 6-component wheel force measurement system.
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
The Kistler Group is introducing a compact mobile measurement solution for enhanced rolling stock maintenance in international railway operations in the shape of its railway brake force measuring system Type 2899A.
21/08/2018
A new Center of Competence for production control and management systems will be opened in Aachen.
31/07/2018
Competent service just a call away has always been a key aspect of Kistler's cooperation with its customers. Now, in a move to address growing demand in North Germany, the measurement technology experts are opening a new office in Wolfsburg.
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
Digitization, Internet of Things and Industry 4.0 are presenting major challenges. Discover how Kistler responds to the great challenges of our times.
09/05/2018
At Sensor + Test 2018 Kistler will be introducing a milestone in measurement technology: its new KiDAQ data acquisition system.
08/05/2018
At NPE 2018, the Kistler Group is showcasing its latest custom monitoring package for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
03/05/2018
At Automatica 2018, the Kistler Group will turn the spotlight on diverse options for using sensors and process monitoring systems to support industrial production and enhance digitalization in test and assembly technology.
24/04/2018
The Kistler Group will showcase its expanded portfolio of industrial test and inspection systems for quality assurance at the 2018 Control trade show.
12/04/2018
The global leader in dynamic measurement technology supports the passion for innovation and technology with a three-year partnership.
06/03/2018
Kistler will be showcasing at Control 2018 its portfolio of industrial testing and inspection systems with the spotlight on the very latest additions.
16/02/2018
At Intertraffic 2018 the Kistler Group is showcasing its comprehensive KiTraffic Weigh In Motion (WIM) solutions, which support road owners and authorities in road and traffic monitoring, weight enforcement and weight-based tolling.
15/02/2018
At NPE 2018 in Orlando, Florida, the Kistler Group will demonstrate a wide range of modular functionalities for ComoNeo: the process monitoring system that takes injection molding to a higher level with integrated quality monitoring geared to meet customers’ needs and requirements.
31/01/2018
The new KiSprint provides coaches and athletes with an efficient means of biomechanically optimizing sprint starts under competitive conditions. The robust and mobile solution has comprehensive software assessment options and can be individually adapted and expanded.
24/01/2018
Kistler achieved a growth rate of 18 % in 2017. Digital transformation has top priority in 2018.
23/01/2018
Surmonter les complexités du RTM - avec Kistler
12/10/2017
At the SPS IPC Drives Kistler Group will unveil the world's first digital charge amplifier Type 5974A, a milestone more in electrical automation.
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
With MARS software version 3.0, Kistler presents an extensive update of the proprietary measurement, analysis, and evaluation software for Kistler force plates.
21/10/2016
Kistler boosts the efficiency and reliability of large marine and stationary engines through monitoring and control of the combustion process
19/10/2016
Kistler is presenting the new versions of its ComoNeo and ComoDataCenter.
10/10/2016
Kistler is unveiling a new addition to its portfolio of electromechanical joining modules.
30/09/2016
The Kistler Group reported incoming orders worth CHF 233.3 million at the end of August 2016 and has therefore seen growth of 8.4 % compared to the same period in the previous year, or 5.6 % when adjusted for currency effects.
07/09/2016
At this year's K Trade Fair from 19 to 26 October in Düsseldorf, Kistler will be showcasing its latest new products and features with the focus on Industry 4.0.
24/07/2016
Kistler will be showcasing its new NCFE and NCFR joining modules, together with the latest generation of maXYmos monitoring systems on Motek 2016
12/07/2016
Kistler's Correvit® SFII sensor measures world record in 1.513 seconds
12/05/2016
Screw technology complements the range of applications.
27/04/2016
Following a long phase of planning, preparations, and conversion work, Kistler Instrumente GmbH has a new home for its German headquarters at the Böblingen/Sindelfingen airfield.
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
At Chinaplas 2015 Kistler will be presenting solutions for zero-defect production, process monitoring and data evaluation in injection molding
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
At Sensor + Test 2014 Kistler is presenting many new features from the field of measurement electronics in addition to its already proven sensor technology.
19/05/2014
Users obtain a full range of force–displacement measurement systems from one source
06/02/2014
The Kistler Group achieved sales of 285 million CHF in 2013, thus marking a slight growth in comparison with the figures for the prior year.