Kistler presents innovations in process reliability through integrated quality control at SPS IPC Drives

Nuremberg, 12 November 2013 - Kistler will be presenting innovations in the fields of components, systems and complete solutions at SPS IPC Drives from 26 to 28 November 2013 in Nuremberg, focusing on increased flexibility, quality assurance and efficiency.

 

New flexibility in torque measurement

At SPS IPC Drives 2013, Kistler will be presenting the new measuring flange KiTorq System, which provides test stand operators with unrivalled flexibility in torque measurement for electric and combustion engines, gears, pumps and compressors in the fields of au-tomobile and energy engineering, aeronautical and astronautics, engineering, medicine and process engineering. The basis of this sophisticated innovation is the separation of the measurement bodies and the evaluation unit, as well as their modular combinability.

The KiTorq System consists of a measurement body, a 4551A rotor with a new flange size and a 4542A stator evaluation unit, which is expanded by the Ethercat and Ethernet/IP interface. As well as the 4551A rotor, Kistler offers the 4550A with the flange size in accordance with DIN ISO 7646. Both rotors can be combined with the same guide-less stator which is simple to install and facilitates the implementation of various testing specimens without the need of having to completely rebuild the testing facility. Users benefit from a high degree of flexibility with regard to the choice of appropriate components for the respective test stand, allowing for installation and maintenance times to be reduced. In addition, the guide-less stator design facilitates simple assembly, as the sensor does not have to be pushed through an antenna ring.

The stator receives the measurement values via a telemetric connection and processes these digitally without disruption or errors by converting the signal from digital to analogue. The sensors are parameterized by the Ethercat or Ethernet/IP eliminating the need for a second control wire. As the interface is integrated directly into the stator, no costly auxiliary equipment is needed. In addition, the stator can be combined with all rotors and can automatically identify the respective rotor type and measurement range. If the interface changes on the test stand, only the stator has to be changed, which will permit sav-ings on the cost of replacement parts.

With a fully digital transfer, the KiTorq System offers the highest dynamic and precision with an accuracy level of 0.05% and a critical frequency of up to 10 kHz. It is also possible to select a second measurement range up to a king pin inclination of 1:10.

Systems for monitoring manual and automated processes

At SPS IPC Drives 2013, Kistler will introduce the maXYmos series of XY monitors, which can be used in manual processes like hand presses and also in automated fields. The maXYmos series facilitates the visualization and evaluation of processes and thereby provides consistent, process-integrated quality assurance. Quality deviations can be identified early and faulty products can be removed from the process, thus increasing efficiency in the production process and savings on cost. As well as quality control, the XY monitors allow for increased transparency in the production process For example, wear in tools that are used can be identified early and measures to rectify can be taken immediately. This contributes to a reduction in unplanned downtimes, increases machine availability and increases total productivity of the production process. Moreover, maXYmos also allows for the traceability of process results because the monitors can document all data so that faulty parts can always be precisely identified.

Kistler offers manufacturers two different types: maXYmos BL (Basic Level) and maXYmos TL (Top Level). Both devices are user-friendly and intuitive to operate, with the maXYmos TL offering a greater variety with regards to evaluation objects, including cascadability of the XY pair of channels.

Optimizing efficiency with test stands from a single source

Furthermore, Kistler will be showcasing test stands which it has developed from a single source and with the customer in mind. The scope of application ranges from mechanical components, like drive measurement setup with torque sensors, to small test stands with torque speed measurement and manual or external control through to computer-controlled complete solutions for analyzing and documenting electrical machines.

Kistler can achieve automated test stands with up to 12 channel current/voltage measurement through an integrated power analyzer with the aim to of optimizing the efficiency of the test equipment. The field of application varies, from electric motors to vacuum and wind-screen wiper motors through to automobile generators, drill hammers, angle grinders and many more.

Kistler will be presenting innovations at SPS IPC Drives in Nuremberg, Germany from 26 to 28 November 2013 on stand 530 in hall 4A.

 

Media Release (PDF)

 

With the measurement body (rotor, above) and evaluation unit (stator, below) the measuring flange KiTorq System 4551A … by Kistler with its new flange size and digital stator provides test stand operators maximum flexibility

Dossier de press

Portrait de Kistler avec logo pour un aperçu rapide: Kistler Press Kit.zip

12/08/2022
New wireless dynamometer allows for highly accurate measurements of cutting forces.
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
The new joining module is highly suitable for clinching and riveting, and also for assembly processes that require force-displacement monitoring.
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
The Kistler Group will showcase its test and analysis systems for threaded joints at the 2019 Fastener Fair in Stuttgart from 19 to 21 March.
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
Accurate and insensitive to its mounting position: the new Type 6044A M8 sensor features an anti-strain design to ensure reliable, high-quality results.
20/11/2018
Motorsport: the new 4080B/BT absolute pressure sensors from Kistler – for real-time monitoring with maximum measurement accuracy and signal quality!
16/10/2018
At Fakuma 2018, the Kistler Group is showcasing its latest monitoring and control packages for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
08/10/2018
The SMETEC Gesellschaft für Sensor-, Motor- und Energietechnik mbH recently became part of the Kistler Group.
24/09/2018
The Kistler Group is adding another variant to what is already the world's most comprehensive portfolio of wheel force measurement systems: the new RoaDyn S6GT 6-component wheel force measurement system.
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
The Kistler Group is introducing a compact mobile measurement solution for enhanced rolling stock maintenance in international railway operations in the shape of its railway brake force measuring system Type 2899A.
21/08/2018
A new Center of Competence for production control and management systems will be opened in Aachen.
31/07/2018
Competent service just a call away has always been a key aspect of Kistler's cooperation with its customers. Now, in a move to address growing demand in North Germany, the measurement technology experts are opening a new office in Wolfsburg.
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
Digitization, Internet of Things and Industry 4.0 are presenting major challenges. Discover how Kistler responds to the great challenges of our times.
09/05/2018
At Sensor + Test 2018 Kistler will be introducing a milestone in measurement technology: its new KiDAQ data acquisition system.
08/05/2018
At NPE 2018, the Kistler Group is showcasing its latest custom monitoring package for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
03/05/2018
At Automatica 2018, the Kistler Group will turn the spotlight on diverse options for using sensors and process monitoring systems to support industrial production and enhance digitalization in test and assembly technology.
24/04/2018
The Kistler Group will showcase its expanded portfolio of industrial test and inspection systems for quality assurance at the 2018 Control trade show.
12/04/2018
The global leader in dynamic measurement technology supports the passion for innovation and technology with a three-year partnership.
06/03/2018
Kistler will be showcasing at Control 2018 its portfolio of industrial testing and inspection systems with the spotlight on the very latest additions.
16/02/2018
At Intertraffic 2018 the Kistler Group is showcasing its comprehensive KiTraffic Weigh In Motion (WIM) solutions, which support road owners and authorities in road and traffic monitoring, weight enforcement and weight-based tolling.
15/02/2018
At NPE 2018 in Orlando, Florida, the Kistler Group will demonstrate a wide range of modular functionalities for ComoNeo: the process monitoring system that takes injection molding to a higher level with integrated quality monitoring geared to meet customers’ needs and requirements.
31/01/2018
The new KiSprint provides coaches and athletes with an efficient means of biomechanically optimizing sprint starts under competitive conditions. The robust and mobile solution has comprehensive software assessment options and can be individually adapted and expanded.
24/01/2018
Kistler achieved a growth rate of 18 % in 2017. Digital transformation has top priority in 2018.
23/01/2018
Surmonter les complexités du RTM - avec Kistler
12/10/2017
At the SPS IPC Drives Kistler Group will unveil the world's first digital charge amplifier Type 5974A, a milestone more in electrical automation.
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
With MARS software version 3.0, Kistler presents an extensive update of the proprietary measurement, analysis, and evaluation software for Kistler force plates.
21/10/2016
Kistler boosts the efficiency and reliability of large marine and stationary engines through monitoring and control of the combustion process
19/10/2016
Kistler is presenting the new versions of its ComoNeo and ComoDataCenter.
10/10/2016
Kistler is unveiling a new addition to its portfolio of electromechanical joining modules.
30/09/2016
The Kistler Group reported incoming orders worth CHF 233.3 million at the end of August 2016 and has therefore seen growth of 8.4 % compared to the same period in the previous year, or 5.6 % when adjusted for currency effects.
07/09/2016
At this year's K Trade Fair from 19 to 26 October in Düsseldorf, Kistler will be showcasing its latest new products and features with the focus on Industry 4.0.
24/07/2016
Kistler will be showcasing its new NCFE and NCFR joining modules, together with the latest generation of maXYmos monitoring systems on Motek 2016
12/07/2016
Kistler's Correvit® SFII sensor measures world record in 1.513 seconds
12/05/2016
Screw technology complements the range of applications.
27/04/2016
Following a long phase of planning, preparations, and conversion work, Kistler Instrumente GmbH has a new home for its German headquarters at the Böblingen/Sindelfingen airfield.
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
At Chinaplas 2015 Kistler will be presenting solutions for zero-defect production, process monitoring and data evaluation in injection molding
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
At Sensor + Test 2014 Kistler is presenting many new features from the field of measurement electronics in addition to its already proven sensor technology.
19/05/2014
Users obtain a full range of force–displacement measurement systems from one source
06/02/2014
The Kistler Group achieved sales of 285 million CHF in 2013, thus marking a slight growth in comparison with the figures for the prior year.