Kistler Showcases Solutions for Dependable Bolted Joints

Winterthur, 27 October 2016 – At this year's SPS IPC Drives in Nuremberg from 22 to 24 November, Kistler will premiere laboratory systems to analyze bolted joints, calibration equipment and test systems for torque tools, as well as measuring systems for random sample testing. Among the products on show at the stand, the spotlight is on INSPECTpro – the new monitoring system to measure torque and rotation angle – along with cutting-edge products from Kistler's joining and torque portfolio.

In automated production, everything revolves around accurate, reliable process monitoring. Especially in the automotive industry, monitoring and control of bolted joints is hugely important for quality assurance. That's because all the influences that find their way into this process converge at the end of the process chain. Even the smallest errors in the development or assembly process can cause costs running into millions. By integrating Schatz GmbH into the Kistler Group, Kistler is deepening its application know-how in bolted joint technology – so for the first time, customers across the globe have access to bolted joint expertise from one single source.

INSPECTpro for More Transparent Testing Processes

INSPECTpro, the portable measuring device for torque and rotation angle, opens up new possibilities in terms of hardware as well as software: now, process capability checks and random sample inspections during assembly are even easier to perform. Graphic analyses of assembly processes ensure optimal quality in bolted joint assembly. Customers always need testing to be faster and more effective, so new software modules are constantly being developed to ensure easier handling for users and greater transparency in test processes. One new feature is the Tool Management license. Tools to be tested can be stored here ahead of time so they can be conveniently called up later on in Tool Testing mode. The Tolerance Classes software module handles the use of stored tolerance classes in the parameter sets for tool testing/management or bolted joint management.

NCFR – Dynamic Drive Technology and High-Precision Sensors

The latest products from Kistler's range of joining modules will also be on show at the stand: Kistler is presenting its NCFR Joining Module – as well as the classical linear joining process, this system can perform a controlled rotary movement of the ram, either sequentially or even simultaneously. Like the entire family of NC joining systems, the NCFR joining module features a variety of additional benefits: users will appreciate its enormous flexibility and excellent dynamics combined with intuitive operation – so joining processes ranging from simple to highly complex can be handled rapidly and efficiently. Thanks to the servo amplifiers used, all traverse movements that are performed can be controlled with high precision.

Torque Sensor 4503B and KiTorq 4550A: Sensor Technology for Maximum Precision

The cutting-edge sensor technology showcased by Kistler at the SPS IPC Drives in Nuremberg will convince visitors that our company also represents the state-of-the-art when it comes to the development of high-precision torque sensors. The 4503B torque sensor offers a host of extended functionalities, bringing it into line with the very latest market requirements. For instance, optical speed and angle sensing has now been replaced by magnetic technology. This gives the sensor the advantage of added resilience for reliable operation in heavily contaminated industrial environments (e.g. where oil mist is present) – thereby saving valuable time on maintenance. The torque sensor's electronics have also been optimized, and the 4503B now has a cut-off frequency of 10 kHz for highly dynamic measurements.

Another technological milestone on Kistler's stand is the KiTorq 4550A with angle sensing – to enable determination of torque, speed or rotation angle with exceptionally high resolution (up to 8192 pulses per revolution). The number of pulses can be freely adjusted to the requirements as appropriate.

The torque measuring flange system consists of a measuring element, the KiTorq rotor and a torque evaluation unit (the KiTorq stator). With a suitable selection of components for the specific test bench, this system offers excellent flexibility for manufacturers of electrical motors and combustion engines, transmissions, pumps and compressors: this is because the ringless stator makes it possible to use different measuring elements without having to rebuild the entire test setup.

maXYmos TL 1.2 and maXYmos BL 2.3: the Latest Generation of Monitoring Systems

Kistler's stand also highlights the latest generation of maXYmos monitoring systems. Their purpose: to deliver consistent, process-integrated quality assurance. The patterns of measurement curves can be used to monitor and control the quality of a single production step, a sub-assembly or an entire product. Because this control is integrated in the process, the system provides the basis for enhanced transparency in assembly and testing systems – paving the way for increased costefficiencythroughout the production facility. 

Don't miss the trade show date!

If you want to see Kistler's diverse range of solutions for interconnected quality monitoring at first hand, save the dates for the SPS IPC Drives trade show now: it runs from 22 to 24 November 2016 in Nuremberg.



Media Contact:
Simone Koch
Divisional Marketing Manager IPC
Phone: +41 52 224 18 02
Email: simone.koch@kistler.com

Dossier de press

Portrait de Kistler avec logo pour un aperçu rapide: Kistler Press Kit.zip

09/05/2018
At Sensor + Test 2018 Kistler will be introducing a milestone in measurement technology: its new KiDAQ data...
08/05/2018
At NPE 2018, the Kistler Group is showcasing its latest custom monitoring package for ComoNeo, its...
03/05/2018
At Automatica 2018, the Kistler Group will turn the spotlight on diverse options for using sensors and process...
24/04/2018
The Kistler Group will showcase its expanded portfolio of industrial test and inspection systems for quality...
12/04/2018
The global leader in dynamic measurement technology supports the passion for innovation and technology with a...
06/03/2018
Kistler will be showcasing at Control 2018 its portfolio of industrial testing and inspection systems with the...
16/02/2018
At Intertraffic 2018 the Kistler Group is showcasing its comprehensive KiTraffic Weigh In Motion (WIM)...
15/02/2018
At NPE 2018 in Orlando, Florida, the Kistler Group will demonstrate a wide range of modular functionalities...
31/01/2018
The new KiSprint provides coaches and athletes with an efficient means of biomechanically optimizing sprint...
24/01/2018
Kistler achieved a growth rate of 18 % in 2017. Digital transformation has top priority in 2018.
23/01/2018
Surmonter les complexités du RTM - avec Kistler
12/10/2017
At the SPS IPC Drives Kistler Group will unveil the world's first digital charge amplifier Type 5974A, a...
09/10/2017
Kistler's Type 5074A industrial charge amplifier breaks new ground in industrial charge amplifier technology
06/10/2017
Whether hybrid drives or electric vehicles: anyone who wants to make a change needs to measure and understand
27/09/2017
Our experts will present you Kistler measuring technologies for demanding space applications.
05/09/2017
At Fakuma 2017, we will demonstrate how you can benefit from new ComoNeo functionalities
31/08/2017
Kistler Group showcases the entire spectrum of its integrated quality assurance solutions
25/08/2017
Kistler Group took over near Karlsruhe-based Vester Elektronik GmbH on 25 August, a specialist in sensor...
11/08/2017
Jaguar Land Rover uses Kistler RoaDyn® Wheel Force Transducers for accurate tyre modelling
11/07/2017
Kistler is taking over IOS GmbH (Germany), provider of Manufacturing Execution Systems (MES).
06/07/2017
Tettnang-based firm eso GmbH was acquired by the Kistler Group on July 5.
20/06/2017
Perfect production data synchronization through direct MES system integration.
02/05/2017
Kistler presents innovative measurement equipment for demanding vehicle testing applications
25/04/2017
At Moulding Expo 2017, we will show how easy it is to install the measurement technology needed for quality...
12/04/2017
Kistler will be present at Control, the world's leading quality assurance trade fair.
12/04/2017
Advanced features for LabAmp family maximize flexibility for cutting force users.
11/04/2017
Measuring equipment for sophisticated T&M applications
01/02/2017
The Kistler Group is constantly growing and recruiting specialist staff worldwide.
17/01/2017
Olympic champion Anthony Ervin and Kistler create a Success Story together.
02/12/2016
Kistler seeks more than 40 specialists in what is likely Switzerland's largest job advertisement.
27/10/2016
At this year's SPS IPC Drives in Nuremberg Kistler will premiere laboratory systems to analyze bolted joints,...
21/10/2016
Kistler boosts the efficiency and reliability of large marine and stationary engines through monitoring and...
19/10/2016
Kistler is presenting the new versions of its ComoNeo and ComoDataCenter.
10/10/2016
Kistler is unveiling a new addition to its portfolio of electromechanical joining modules.
30/09/2016
The Kistler Group reported incoming orders worth CHF 233.3 million at the end of August 2016 and has therefore...
07/09/2016
At this year's K Trade Fair from 19 to 26 October in Düsseldorf, Kistler will be showcasing its latest new...
24/07/2016
Kistler will be showcasing its new NCFE and NCFR joining modules, together with the latest generation of...
12/07/2016
Kistler's Correvit® SFII sensor measures world record in 1.513 seconds
12/05/2016
Screw technology complements the range of applications.
27/04/2016
Following a long phase of planning, preparations, and conversion work, Kistler Instrumente GmbH has a new home...
12/02/2016
Kistler Lorch GmbH Honored for Outstanding Qualities as Employer
02/02/2016
The Kistler Group has overcome currency-related challenges at its Swiss site to achieve continued growth.
28/01/2016
Accurate Wheel Force Measurement with Minimum Configuration Effort
26/11/2015
Increased Flexibility for High-Speed Combustion Analysis
02/11/2015
New Piezoresistive Sensor with Temperature Probe and Integrated Signal Conditioning.
27/10/2015
Kistler Provides Maximum Flexibility for Product Testing and Development
16/10/2015
Kistler's NCFR Joining Module honored in the handling and assembly category
05/10/2015
Setting the Standard for 100% Control of Linear Joining Processes with Partial Rotation
18/09/2015
Kistler Group: safeguarding the firm's competitive edge.
15/09/2015
Quick evaluation of performance and force with Kistler MARS 2.1.
03/09/2015
Major update for Kistler’s mobile engine indication system.
01/09/2015
Setting New Standards in Automated Process Monitoring for Injection Molding.
25/08/2015
Kistler Showcases Three Latest Product Innovations at Motek 2015
29/06/2015
Kistler Automotive GmbH honored as one of Germany's most innovative companies
26/06/2015
Kistler honored with ASCO Award Gold for best corporate transformation in Switzerland.
26/06/2015
Kistler's software for force plates offers a host of new features for performance diagnostics in sports and...