Kistler Unveils the Latest Functionalities for Automated, Reproducible Injection Molding Processes and Their Control

Düsseldorf, 19 October 2016 – Kistler is presenting the new versions of its ComoNeo and ComoDataCenter – both with innovative options for applications in injection molding production that vastly simplify the control, reproducibility and documentation of processes in this segment of industry. First and foremost among the new features: the Restart Assistant, which allows efficient reproduction of established processes when changing machines.

With quality requirements constantly on the increase, continuous control of the entire injection molding production chain is absolutely essential. The focus here is on improving product quality and boosting cost-efficiency. Kistler has now developed the successor versions of ComoNeo and ComoDataCenter, two system components that already have excellent track records. These new versions offer the best possible basis for achieving these goals – and they are ideal for novices as well as experienced users.

Automated Process Reproduction: ComoNeo Now with Restart Assistant and OPC Interface

Kistler has now integrated a Restart Assistant into ComoNeo, making it possible for users to transfer established processes from one machine to another with no problems at all. To ensure identical quality reproduction in the new machine, this intelligent tool suggests which parameters need specific changes. For this purpose, the Assistant detects deviations in the cavity pressure and compensates for them by adapting the machine parameters. This automated analysis generates a suggestion so that users can correct the process on the basis of the cavity pressure – and no previous specialist knowledge is required.

As the era of Industry 4.0 dawns, this support places users in the best possible position to conquer the challenges posed by digital networking. For example: the system now supports the OPC-UA interface, which is on the way to becoming the standard for injection molding production. By integrating OPC-UA into ComoNeo, Kistler has now made it possible to fully implement Multiflow control (automatic hot runner balancing) as a standalone solution. In other words, users no longer need a PC for control. The benefit: significantly less effort is required for the entire setup process. Another new feature in ComoNeo: online quality forecasting is now integrated directly into the system, so the complete range of cavity pressure monitoring methods is available. The EO Assistant (for automated setting of monitoring limits), online quality forecasting and the Restart Assistant: three aids that ensure novices as well as experts will be guided to the desired results.

Control with Industry 4.0 in Mind: New Features for Real-Time Control and Hot Runner Balancing

The first version of ComoNeo already set a new standard for monitoring of injection molding production processes. This was achieved with the help of the EO Assistant: for the first time, users with no specific knowledge of cavity pressure were given a simple option for monitoring. Kistler has now developed software that goes one step further in quality optimization. The new version of ComoNeo provides feedback to the operator and the machine so that the process can be optimized even further. This advance allows perfect timing for the switchover from speed control to pressure control in response to cavity pressure. ComoNeo also offers a sampling rate that cannot be matched by any comparable system. The result: yet again, real-time control has been made vastly more responsive in every respect.

Automatic switchover control can be used in two different ways. The first option is for manual setup: control behavior is only changed after the user intervenes. The second option is called SLP (Switching Level Processor): in this case, setup is fully automated and the control behavior is optimized independently from cycle to cycle. The main advantage of the manual option is that several dependencies can be set; with SLP, the key benefit is self-optimizing calculation of the switchover point. In these ways, ComoNeo 2.0 also covers a wide range of process control applications: for molds with multiple cavities, behavior during automatic changeover has been optimized for the specific purpose of compensating for different behavior patterns during the production sequence. When conditions are set manually, additional dependencies across multiple cavities are available as control criteria. On the other hand, automated changeover is mainly used for molds with small numbers of cavities. The benefit here: ease of handling. All that is needed is to activate the process – and everything else is controlled by the internal algorithm, virtually at the touch of a button. Both switchover options actively help prevent mold damage because safety functions respond if filling differences are excessive.

Multiflow control is a method used to control hot runner balancing. Its fundamental purpose is to use appropriate temperature control of the individual hot runner nozzles to ensure that all filling curves have an identical progression, so production quality is guaranteed. In the past, conventional production methods always required a manual fill study, but Multiflow control by ComoNeo now makes it possible to fill the individual cavities automatically – with increased speed and far greater precision. This advantage can be exploited during setup and also during the actual production operation. Thanks to the readjustment option that is newly integrated in ComoNeo, process fluctuations can now be compensated during the production phase as well.

ComoDataCenter: the Vital Link for Networked Injection Molding Production

The ComoDataCenter (CDC) is also enhanced with attractive new features that make it easier to network data and improve the traceability of part quality. For instance, the CDC is now available for ComoNeo as well. Thanks to this innovation, ComoNeo and CoMo Injection are linked via a com-mon database. Another new feature: mold management is integrated into the CDC. The settings can be stored centrally, so the ComoNeo and CoMo Injection mold settings can be transferred to other plants via CDC. For existing customers, this also ensures compatibility between CoMo Injection and ComoNeo – guaranteeing that CoMo Injection users can change over gradually to ComoNeo. There is also provision for integration into higher-level systems such as SAP or other MES systems. This means that the CDC acts as the single interface between the process and higher-level MES systems. The benefit: all data can easily be networked with other systems across the company. And, last but not least, the CDC's user interface is now standardized with the tried-and-tested ComoNeo interface – entirely in keeping with the universal operating philosophy advocated by Kistler.
By enhancing ComoNeo and the ComoDataCenter with these new features, Kistler is paving the way for yet more future improvements to product quality and cost-efficiency in injection molding production.

Kistler will be showcasing the latest technologies that we have developed for quality control at K Trade Fair in Düsseldorf.

Download Press Release (PDF)

User Contact
Daniel Fick
Business Development Manager
Phone: +41 52 2241 606
Email: daniel.fick@kistler.com

Media Contact
Simone Koch
Divisional Marketing Manager IPC
Phone +41 52 2241 802
Email: simone.koch@kistler.com

Dossier de press

Portrait de Kistler avec logo pour un aperçu rapide: Kistler Press Kit.zip

31/07/2018
Competent service just a call away has always been a key aspect of Kistler's cooperation with its customers. Now, in a move to address growing demand in North Germany, the measurement technology experts are opening a new office in Wolfsburg.
25/07/2018
On her way to Olympia 2020 she relies on Kistler Group measurement experts.
18/07/2018
Effective monitoring with strain sensors protects machines and tools
03/07/2018
The Top 100 Competition has again singled out the most innovative German small and medium-sized enterprises (SMEs) for the 10th time.
25/06/2018
Kistler is pleased to introduce MicroDyn, the world's smallest series-produced cutting force meter.
19/06/2018
Kistler introduces the world’s first high temperature accelerometer for the monitoring of gas turbines.
11/06/2018
Kistler is earmarking the highest investment budget for research and development in the company`s history.
11/05/2018
Digitization, Internet of Things and Industry 4.0 are presenting major challenges. Discover how Kistler responds to the great challenges of our times.
09/05/2018
At Sensor + Test 2018 Kistler will be introducing a milestone in measurement technology: its new KiDAQ data acquisition system.
08/05/2018
At NPE 2018, the Kistler Group is showcasing its latest custom monitoring package for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
03/05/2018
At Automatica 2018, the Kistler Group will turn the spotlight on diverse options for using sensors and process monitoring systems to support industrial production and enhance digitalization in test and assembly technology.
24/04/2018
The Kistler Group will showcase its expanded portfolio of industrial test and inspection systems for quality assurance at the 2018 Control trade show.
12/04/2018
The global leader in dynamic measurement technology supports the passion for innovation and technology with a three-year partnership.
06/03/2018
Kistler will be showcasing at Control 2018 its portfolio of industrial testing and inspection systems with the spotlight on the very latest additions.
16/02/2018
At Intertraffic 2018 the Kistler Group is showcasing its comprehensive KiTraffic Weigh In Motion (WIM) solutions, which support road owners and authorities in road and traffic monitoring, weight enforcement and weight-based tolling.
15/02/2018
At NPE 2018 in Orlando, Florida, the Kistler Group will demonstrate a wide range of modular functionalities for ComoNeo: the process monitoring system that takes injection molding to a higher level with integrated quality monitoring geared to meet customers’ needs and requirements.
31/01/2018
The new KiSprint provides coaches and athletes with an efficient means of biomechanically optimizing sprint starts under competitive conditions. The robust and mobile solution has comprehensive software assessment options and can be individually adapted and expanded.
24/01/2018
Kistler achieved a growth rate of 18 % in 2017. Digital transformation has top priority in 2018.
23/01/2018
Surmonter les complexités du RTM - avec Kistler
12/10/2017
At the SPS IPC Drives Kistler Group will unveil the world's first digital charge amplifier Type 5974A, a milestone more in electrical automation.
09/10/2017
Kistler's Type 5074A industrial charge amplifier breaks new ground in industrial charge amplifier technology
06/10/2017
Whether hybrid drives or electric vehicles: anyone who wants to make a change needs to measure and understand
27/09/2017
Our experts will present you Kistler measuring technologies for demanding space applications.
05/09/2017
At Fakuma 2017, we will demonstrate how you can benefit from new ComoNeo functionalities
31/08/2017
Kistler Group showcases the entire spectrum of its integrated quality assurance solutions
25/08/2017
Kistler Group took over near Karlsruhe-based Vester Elektronik GmbH on 25 August, a specialist in sensor technology and test automation.
11/08/2017
Jaguar Land Rover uses Kistler RoaDyn® Wheel Force Transducers for accurate tyre modelling
11/07/2017
Kistler is taking over IOS GmbH (Germany), provider of Manufacturing Execution Systems (MES).
06/07/2017
Tettnang-based firm eso GmbH was acquired by the Kistler Group on July 5.
20/06/2017
Perfect production data synchronization through direct MES system integration.
02/05/2017
Kistler presents innovative measurement equipment for demanding vehicle testing applications
25/04/2017
At Moulding Expo 2017, we will show how easy it is to install the measurement technology needed for quality assurance in injection molds.
12/04/2017
Kistler will be present at Control, the world's leading quality assurance trade fair.
12/04/2017
Advanced features for LabAmp family maximize flexibility for cutting force users.
11/04/2017
Measuring equipment for sophisticated T&M applications
01/02/2017
The Kistler Group is constantly growing and recruiting specialist staff worldwide.
17/01/2017
Olympic champion Anthony Ervin and Kistler create a Success Story together.
02/12/2016
Kistler seeks more than 40 specialists in what is likely Switzerland's largest job advertisement.
27/10/2016
At this year's SPS IPC Drives in Nuremberg Kistler will premiere laboratory systems to analyze bolted joints, calibration equipment, torque tools test systems and more.
21/10/2016
Kistler boosts the efficiency and reliability of large marine and stationary engines through monitoring and control of the combustion process
19/10/2016
Kistler is presenting the new versions of its ComoNeo and ComoDataCenter.
10/10/2016
Kistler is unveiling a new addition to its portfolio of electromechanical joining modules.
30/09/2016
The Kistler Group reported incoming orders worth CHF 233.3 million at the end of August 2016 and has therefore seen growth of 8.4 % compared to the same period in the previous year, or 5.6 % when adjusted for currency effects.
07/09/2016
At this year's K Trade Fair from 19 to 26 October in Düsseldorf, Kistler will be showcasing its latest new products and features with the focus on Industry 4.0.
24/07/2016
Kistler will be showcasing its new NCFE and NCFR joining modules, together with the latest generation of maXYmos monitoring systems on Motek 2016
12/07/2016
Kistler's Correvit® SFII sensor measures world record in 1.513 seconds
12/05/2016
Screw technology complements the range of applications.
27/04/2016
Following a long phase of planning, preparations, and conversion work, Kistler Instrumente GmbH has a new home for its German headquarters at the Böblingen/Sindelfingen airfield.
12/02/2016
Kistler Lorch GmbH Honored for Outstanding Qualities as Employer
02/02/2016
The Kistler Group has overcome currency-related challenges at its Swiss site to achieve continued growth.
28/01/2016
Accurate Wheel Force Measurement with Minimum Configuration Effort
26/11/2015
Increased Flexibility for High-Speed Combustion Analysis
02/11/2015
New Piezoresistive Sensor with Temperature Probe and Integrated Signal Conditioning.
27/10/2015
Kistler Provides Maximum Flexibility for Product Testing and Development
16/10/2015
Kistler's NCFR Joining Module honored in the handling and assembly category
05/10/2015
Setting the Standard for 100% Control of Linear Joining Processes with Partial Rotation
18/09/2015
Kistler Group: safeguarding the firm's competitive edge.
15/09/2015
Quick evaluation of performance and force with Kistler MARS 2.1.
03/09/2015
Major update for Kistler’s mobile engine indication system.
01/09/2015
Setting New Standards in Automated Process Monitoring for Injection Molding.
25/08/2015
Kistler Showcases Three Latest Product Innovations at Motek 2015
29/06/2015
Kistler Automotive GmbH honored as one of Germany's most innovative companies
26/06/2015
Kistler honored with ASCO Award Gold for best corporate transformation in Switzerland.
26/06/2015
Kistler's software for force plates offers a host of new features for performance diagnostics in sports and rehabilitation.
22/04/2015
At Chinaplas 2015 Kistler will be presenting solutions for zero-defect production, process monitoring and data evaluation in injection molding
10/11/2014
New product developments for dynamic measuring technology at the Kistler booth at SPS IPC Drives 2014
14/10/2014
Wide range of options for optimizing the quality assurance through documenting and evaluating production data of CoMo Injection Systems
29/09/2014
Users obtain a full range of force–displacement measurement systems from one source
03/06/2014
Extending the maXYmos product range to control and monitor production processes and quality assurance
26/05/2014
At Sensor + Test 2014 Kistler is presenting many new features from the field of measurement electronics in addition to its already proven sensor technology.
19/05/2014
Users obtain a full range of force–displacement measurement systems from one source
06/02/2014
The Kistler Group achieved sales of 285 million CHF in 2013, thus marking a slight growth in comparison with the figures for the prior year.
11/11/2013
From flexible torque sensors to complete test stands for highly-efficient electric drives
Contact
Cara-Isabell Maercklin
Cara-Isabell Maercklin
Media Contact
Contact