Fiber-optic combustion analysis to optimize combustion engines

Winterthur, July 2020 – The Kistler Group has now added pre-chamber spark plugs to the range of applications for its fiber-optic combustion analysis. This advance gives development engineers more options to press ahead with in-depth research on engines with pre-chamber spark plugs. The objective of this development: to make engines more efficient by improving their fuel consumption and reducing CO2 emissions.

Pressure to drive the development of combustion engines ahead is growing in step with demands to cut fuel consumption and emissions. In 2021, the EU will introduce legal regulations to limit CO2 emissions from passenger cars to 95 grams of CO2 per kilometer. Any automobile manufacturers who exceed this value will be subject to heavy fines. The new limits can be met by combining an electric motor with a combustion engine, so hybrid designs are leading the way to the future. But at the same time, more efforts are needed to exploit the potential of the combustion engine. One way of achieving this is to deploy pre-chamber spark plugs to boost the efficiency of spark ignition engines. This ignition principle already has a long track record of success in large engines and motor sport – and now, it is set to make inroads into mass production.

Visualizing the effects of combustion

Fiber-optic analysis involves placing small viewing windows in the outer wall of the pre-chamber to capture a detailed record of processes in the engine so that optimization potential can be identified. The new design developed by Kistler allows analysis of more complex processes, taking account of different fuel mixes: until now, this measurement technology was only available for commonly used spark plugs.

Optical analyses provide spatial and time-based visualization of processes in the combustion chamber – such as knocking or pre-ignition – so researchers can understand them in detail. "To optimize fuel consumption and emissions in the engines of the future, we need a precise understanding of pre-chamber ignition processes. Until now, this was impossible with such a level of detail. Our sensors make the effects of combustion visible, so we can work on eliminating the disruptive factors that reduce efficiency," according to Dr. Frank Wytrykus, Kistler's expert on optical technologies. 

The challenge: dimensioning the pre-chamber

These special spark plugs ignite the fuel-air mix in a pre-chamber – hence their name. The expansion shoots the flame through small bore holes into the combustion chamber to trigger the main combustion over a large area. As the result, the main combustion is initiated at several points in the chamber: this makes it more likely that combustion will be uniform. Correct dimensioning of the pre-chamber is the challenge here: even small changes to the design have a major impact on combustion. For example, engines with a pre-chamber spark plug are more susceptible to knocking. But to optimize engine efficiency and emission levels, it is essential to prevent uncontrolled combustion processes such as knocking or pre-ignition, and to avoid any formation of soot. 

By introducing this new technology for pre-chamber spark plugs, Kistler is supporting automobile manufacturers with in-engine process optimization, and is also helping to advance research into alternative combustion processes: needs that must be met if the EU emission targets for 2021 are to be achieved.  
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
The new joining module is highly suitable for clinching and riveting, and also for assembly processes that require force-displacement monitoring.
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
The Kistler Group will showcase its test and analysis systems for threaded joints at the 2019 Fastener Fair in Stuttgart from 19 to 21 March.
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
Accurate and insensitive to its mounting position: the new Type 6044A M8 sensor features an anti-strain design to ensure reliable, high-quality results.
20/11/2018
Motorsport: the new 4080B/BT absolute pressure sensors from Kistler – for real-time monitoring with maximum measurement accuracy and signal quality!
16/10/2018
At Fakuma 2018, the Kistler Group is showcasing its latest monitoring and control packages for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
08/10/2018
The SMETEC Gesellschaft für Sensor-, Motor- und Energietechnik mbH recently became part of the Kistler Group.
24/09/2018
The Kistler Group is adding another variant to what is already the world's most comprehensive portfolio of wheel force measurement systems: the new RoaDyn S6GT 6-component wheel force measurement system.
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
The Kistler Group is introducing a compact mobile measurement solution for enhanced rolling stock maintenance in international railway operations in the shape of its railway brake force measuring system Type 2899A.
21/08/2018
A new Center of Competence for production control and management systems will be opened in Aachen.
31/07/2018
Competent service just a call away has always been a key aspect of Kistler's cooperation with its customers. Now, in a move to address growing demand in North Germany, the measurement technology experts are opening a new office in Wolfsburg.
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
Digitization, Internet of Things and Industry 4.0 are presenting major challenges. Discover how Kistler responds to the great challenges of our times.
09/05/2018
At Sensor + Test 2018 Kistler will be introducing a milestone in measurement technology: its new KiDAQ data acquisition system.
08/05/2018
At NPE 2018, the Kistler Group is showcasing its latest custom monitoring package for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
03/05/2018
At Automatica 2018, the Kistler Group will turn the spotlight on diverse options for using sensors and process monitoring systems to support industrial production and enhance digitalization in test and assembly technology.
24/04/2018
The Kistler Group will showcase its expanded portfolio of industrial test and inspection systems for quality assurance at the 2018 Control trade show.
12/04/2018
The global leader in dynamic measurement technology supports the passion for innovation and technology with a three-year partnership.
06/03/2018
Kistler will be showcasing at Control 2018 its portfolio of industrial testing and inspection systems with the spotlight on the very latest additions.
16/02/2018
At Intertraffic 2018 the Kistler Group is showcasing its comprehensive KiTraffic Weigh In Motion (WIM) solutions, which support road owners and authorities in road and traffic monitoring, weight enforcement and weight-based tolling.
15/02/2018
At NPE 2018 in Orlando, Florida, the Kistler Group will demonstrate a wide range of modular functionalities for ComoNeo: the process monitoring system that takes injection molding to a higher level with integrated quality monitoring geared to meet customers’ needs and requirements.
31/01/2018
The new KiSprint provides coaches and athletes with an efficient means of biomechanically optimizing sprint starts under competitive conditions. The robust and mobile solution has comprehensive software assessment options and can be individually adapted and expanded.
24/01/2018
Kistler achieved a growth rate of 18 % in 2017. Digital transformation has top priority in 2018.
23/01/2018
Surmonter les complexités du RTM - avec Kistler
12/10/2017
At the SPS IPC Drives Kistler Group will unveil the world's first digital charge amplifier Type 5974A, a milestone more in electrical automation.
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
With MARS software version 3.0, Kistler presents an extensive update of the proprietary measurement, analysis, and evaluation software for Kistler force plates.
21/10/2016
Kistler boosts the efficiency and reliability of large marine and stationary engines through monitoring and control of the combustion process
19/10/2016
Kistler is presenting the new versions of its ComoNeo and ComoDataCenter.
10/10/2016
Kistler is unveiling a new addition to its portfolio of electromechanical joining modules.
30/09/2016
The Kistler Group reported incoming orders worth CHF 233.3 million at the end of August 2016 and has therefore seen growth of 8.4 % compared to the same period in the previous year, or 5.6 % when adjusted for currency effects.
07/09/2016
At this year's K Trade Fair from 19 to 26 October in Düsseldorf, Kistler will be showcasing its latest new products and features with the focus on Industry 4.0.
24/07/2016
Kistler will be showcasing its new NCFE and NCFR joining modules, together with the latest generation of maXYmos monitoring systems on Motek 2016
12/07/2016
Kistler's Correvit® SFII sensor measures world record in 1.513 seconds
12/05/2016
Screw technology complements the range of applications.
27/04/2016
Following a long phase of planning, preparations, and conversion work, Kistler Instrumente GmbH has a new home for its German headquarters at the Böblingen/Sindelfingen airfield.
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
At Chinaplas 2015 Kistler will be presenting solutions for zero-defect production, process monitoring and data evaluation in injection molding
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
At Sensor + Test 2014 Kistler is presenting many new features from the field of measurement electronics in addition to its already proven sensor technology.
19/05/2014
Users obtain a full range of force–displacement measurement systems from one source
06/02/2014
The Kistler Group achieved sales of 285 million CHF in 2013, thus marking a slight growth in comparison with the figures for the prior year.