Expanded range of smart accessories give piezoelectric sensors a head start

Winterthur, May 2021 – Kistler expands its range of smart accessory equipment to ensure that piezoelectric sensors can be perfectly and securely positioned in any individual measuring system. Three-dimensional drawings and step-by step instructions make the installation process easy. Adapters, connector extenders and special reamers ensure that sensors are snugly placed into position and transmit signals perfectly. If required, they can be connected to screw-mount cable lines that offer protection even if permanently submersed in water.

In highly demanding measuring applications, the right sensor is crucial – but so is measuring periphery that meets the challenges of the respective application. Kistler offers its customers help at every step, starting with the planning documents. Testing engineers can download 3D CAD models of any sensor or adapter from the manufacturer’s webpage. This allows them to decide how best to fit the sensor and its peripheral equipment. 

The installation process can be streamlined if using a mounting adapter, available in different formats, either in metric or empirical threads. The sensor can simply be fitted into the adapter without any further work. In other circumstances, it may be necessary to flush-mount the sensor in a machine, requiring boring a hole. Special reamers help to ensure a perfect fit. When mechanical structures cannot be weakened, or if a BNC- or TNC- connection is preferred, Kistler engineers recommend connector extenders from their vast portfolio. 

Once the set-up is in place, it may be necessary to test it. There are situations when engineers cannot be sure if the pressure may exceed the sensor’s maximum load. This is where sensor dummies come in. They allow thorough testing without potential damage to expensive sensors. They will also be helpful to extend a sensor’s lifetime, for example, when cycle tests are being done without needing pressure measurements. By simply replacing the actual sensor with its dummy equivalent, the sensor can be rested and reused for additional testing cycles at a later point.

Each test-and-measurement environment is different, so there cannot be a one-size-fits-all solution. Our aim is to help customers to help themselves by providing the smart accessories and easy-to-follow instructions that they need.”

Ricardo Rodrigo, Product Manager Pressure BU Test & Measurement

 

Special conditions: waterproof equipment

Piezoelectric measurement technology requires highly insulating cables to ensure signal transmission with low loss. In some testing environments, for example in research laboratories for shipbuilding and marine, special waterproof equipment may be necessary. Kistler now offers an expanded range of waterproof sensor accessories with screw mount cable lines that meet IP protection class 68, providing protection even if permanently submersed in fresh water. This gives users additional flexibility and saves costs. If a screw mount cable is irreparably damaged, it is just the cable and not the sensor that needs to be replaced.

“We strive to make sure that our customers find a measurement solution that fits their particular circumstances,” says Ricardo Rodrigo, Product Manager Pressure BU Test & Measurement at Kistler. “Each test-and-measurement environment is different, so there cannot be a one-size-fits-all solution. Our aim is to help customers to help themselves by providing the smart accessories and easy-to-follow instructions that they need.”   

Dossier de press

Portrait de Kistler avec logo pour un aperçu rapide: Kistler Press Kit.zip

27/09/2022
The new SlimLine Sensor 9132CD is nine times more sensitive than comparable SlimLine sensors.
16/09/2022
At K 2022, Kistler will showcase its solutions for injection molding that make plastics processing more intelligent and sustainable.
06/09/2022
With ComoScout, Kistler offers a simple and cost-effective process monitoring system for injection molding processes.
31/08/2022
High-end measurement systems for rolling stock – from brake testing to traffic monitoring.
22/08/2022
Artificial intelligence in punching: AI helps manufacturers improve product quality and step up their quality assurance.
12/08/2022
New wireless dynamometer allows for highly accurate measurements of cutting forces.
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
The new joining module is highly suitable for clinching and riveting, and also for assembly processes that require force-displacement monitoring.
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
The Kistler Group will showcase its test and analysis systems for threaded joints at the 2019 Fastener Fair in Stuttgart from 19 to 21 March.
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
Accurate and insensitive to its mounting position: the new Type 6044A M8 sensor features an anti-strain design to ensure reliable, high-quality results.
20/11/2018
Motorsport: the new 4080B/BT absolute pressure sensors from Kistler – for real-time monitoring with maximum measurement accuracy and signal quality!
16/10/2018
At Fakuma 2018, the Kistler Group is showcasing its latest monitoring and control packages for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
08/10/2018
The SMETEC Gesellschaft für Sensor-, Motor- und Energietechnik mbH recently became part of the Kistler Group.
24/09/2018
The Kistler Group is adding another variant to what is already the world's most comprehensive portfolio of wheel force measurement systems: the new RoaDyn S6GT 6-component wheel force measurement system.
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
The Kistler Group is introducing a compact mobile measurement solution for enhanced rolling stock maintenance in international railway operations in the shape of its railway brake force measuring system Type 2899A.
21/08/2018
A new Center of Competence for production control and management systems will be opened in Aachen.
31/07/2018
Competent service just a call away has always been a key aspect of Kistler's cooperation with its customers. Now, in a move to address growing demand in North Germany, the measurement technology experts are opening a new office in Wolfsburg.
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
Digitization, Internet of Things and Industry 4.0 are presenting major challenges. Discover how Kistler responds to the great challenges of our times.
09/05/2018
At Sensor + Test 2018 Kistler will be introducing a milestone in measurement technology: its new KiDAQ data acquisition system.
08/05/2018
At NPE 2018, the Kistler Group is showcasing its latest custom monitoring package for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
03/05/2018
At Automatica 2018, the Kistler Group will turn the spotlight on diverse options for using sensors and process monitoring systems to support industrial production and enhance digitalization in test and assembly technology.
24/04/2018
The Kistler Group will showcase its expanded portfolio of industrial test and inspection systems for quality assurance at the 2018 Control trade show.
12/04/2018
The global leader in dynamic measurement technology supports the passion for innovation and technology with a three-year partnership.
06/03/2018
Kistler will be showcasing at Control 2018 its portfolio of industrial testing and inspection systems with the spotlight on the very latest additions.
16/02/2018
At Intertraffic 2018 the Kistler Group is showcasing its comprehensive KiTraffic Weigh In Motion (WIM) solutions, which support road owners and authorities in road and traffic monitoring, weight enforcement and weight-based tolling.
15/02/2018
At NPE 2018 in Orlando, Florida, the Kistler Group will demonstrate a wide range of modular functionalities for ComoNeo: the process monitoring system that takes injection molding to a higher level with integrated quality monitoring geared to meet customers’ needs and requirements.
31/01/2018
The new KiSprint provides coaches and athletes with an efficient means of biomechanically optimizing sprint starts under competitive conditions. The robust and mobile solution has comprehensive software assessment options and can be individually adapted and expanded.
24/01/2018
Kistler achieved a growth rate of 18 % in 2017. Digital transformation has top priority in 2018.
23/01/2018
Surmonter les complexités du RTM - avec Kistler
12/10/2017
At the SPS IPC Drives Kistler Group will unveil the world's first digital charge amplifier Type 5974A, a milestone more in electrical automation.
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
With MARS software version 3.0, Kistler presents an extensive update of the proprietary measurement, analysis, and evaluation software for Kistler force plates.
21/10/2016
Kistler boosts the efficiency and reliability of large marine and stationary engines through monitoring and control of the combustion process
19/10/2016
Kistler is presenting the new versions of its ComoNeo and ComoDataCenter.
10/10/2016
Kistler is unveiling a new addition to its portfolio of electromechanical joining modules.
30/09/2016
The Kistler Group reported incoming orders worth CHF 233.3 million at the end of August 2016 and has therefore seen growth of 8.4 % compared to the same period in the previous year, or 5.6 % when adjusted for currency effects.
07/09/2016
At this year's K Trade Fair from 19 to 26 October in Düsseldorf, Kistler will be showcasing its latest new products and features with the focus on Industry 4.0.
24/07/2016
Kistler will be showcasing its new NCFE and NCFR joining modules, together with the latest generation of maXYmos monitoring systems on Motek 2016
12/07/2016
Kistler's Correvit® SFII sensor measures world record in 1.513 seconds
12/05/2016
Screw technology complements the range of applications.
27/04/2016
Following a long phase of planning, preparations, and conversion work, Kistler Instrumente GmbH has a new home for its German headquarters at the Böblingen/Sindelfingen airfield.
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
At Chinaplas 2015 Kistler will be presenting solutions for zero-defect production, process monitoring and data evaluation in injection molding
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
At Sensor + Test 2014 Kistler is presenting many new features from the field of measurement electronics in addition to its already proven sensor technology.
19/05/2014
Users obtain a full range of force–displacement measurement systems from one source
06/02/2014
The Kistler Group achieved sales of 285 million CHF in 2013, thus marking a slight growth in comparison with the figures for the prior year.