Transparent Manufacturing Processes to Boost Cost-Effectiveness

Winterthur, 25 August 2015 – "Transparent Manufacturing Processes Mean Higher Quality and Lower Costs": this is the keynote for three new products that Kistler will unveil at this year's Motek (5 to 8 October 2015) in Stuttgart. The maXYmos TL 1.2 (equipped with sequencer mode for the first time) and the 9240A strain sensor (with a focus dimension of only 8 mm) will be flanked by the new NCFR Joining Module.


Recent years have seen the Kistler Group consolidating its global reputation as the leading provider of sensor systems by steadily expanding its product portfolio. Thanks in particular to a series of innovative developments in the maXYmos family, the consistency and continuity of these systems − as well as their simple, intuitive operation − have become familiar features of everyday industrial production. Now, at the Motek 2015, Kistler is set to unveil no less than three product innovations that will make manufacturing processes even more transparent – to increase quality and cut costs.

New Additions to the maXYmos Family
For years, the XY monitors in Kistler's maXYmos series have played a key part in consistent, pro-cess-integrated quality assurance: the patterns of measurement curves can be used to monitor and verify the quality of a single production step, a sub-assembly or an entire product. Now, maXYmos users can also measure multi-stage production processes (i.e. those with consecutive staggered steps): this has been made possible by equipping the maXYmos TL (Top-Level System) and the maXYmos BL (Basic-Level System) with a sequencer mode, in the same way as the successful maXYmos NC. Practical tests have shown the convincing results of this innovation: thanks to inte-grated sequence control, complex test processes can be mapped with no need to rely on costly external PLC programming. The programs can be set up quickly and easily with the help of the in-tuitive user interface on the touch display. Another advance: new evaluation objects (EOs) have been included in the maXYmos TL to support testing of additional applications such as switch testing. When the new cable extender is used, cables between TL / NC measuring modules and the display can be extended on one side, with data transmission via Ethernet. On the other side, up to eight measuring modules for different production processes can now be connected to one display.

In short: these new refinements to maXYmos now mean that optimal cycle times can also be achieved for multi-stage processes, with maximum repeat accuracy. Downtime is minimized and machine availability is increased – adding up to a remarkable increase in productivity for the manufacturing process.

NCFR Joining Module: Cutting Costs for the Automobile Industry and the
Automotive Supply Sector
But that's not all: Kistler will also unveil another member of the Joining Systems family at the Motek 2015. As well as the classical linear joining process, the new NCFR Joining Module can perform a rotary movement of the ram, either sequentially or even simultaneously. With its integrated hollow-shaft servo motors, the module features compact dimensions and extremely low weight. This design offers excellent dynamic characteristics, creating the basis for dramatically reduced cycle times. Integrated sensors continuously capture and evaluate force and displacement − as well as rotation angle and torque − with maximum precision, so 100% quality and control are ensured. The piezoe-lectric force sensor has two predefined measuring ranges to deliver high resolution; it also offers high overload capacity, especially in the small measuring range.

The new NCFR joining system makes mapping of complex joining processes faster and more efficient. The results: capacity utilization rates for plant are increased still further, and the commissioning and set-up phase is reduced to the minimum. And with its low energy consumption, the new NCFR Joining Module will help the automobile industry and the automotive supply sector to cut energy costs in series production.

9240A Measuring Pin: An Innovation to Meet Market Demand
To prove yet again that Kistler leads the sensor technology market, it will also unveil the 9240A measuring pin (a member of the strain sensor family) at Motek 2015. With its exceptionally narrow diameter of only 8 mm, this measuring pin is the perfect addition to Kistler's extensive range of strain sensors. In the majority of applications, these instruments are used for indirect force measurements on a component, as opposed to sensors that measure the force directly in the component. Depending on the design of the strain sensor, it can be positioned on the structure or mounted inside a structure. Measuring pins installed inside a structure need a cylindrical mounting bore. The advantage of these sensors is that the measuring element can be placed precisely at the point where the greatest strain occurs. Stefan Schäfer, Product Manager for Force and Strain Sensors at Kistler, explains how the new strain sensor was developed: "The development goal for the 9240A measuring pin was to offer the best possible solution for specific market requirements. This innovative new product succeeds in doing just that – so once again, Kistler has demonstrated its proximity to its customers all over the world."


Visitors to Motek can view Kistler's new products for themselves on stand 6311 in hall 6 from 5 to 8 October 2015. At 2 pm on 6 October 2015, there is also an entertaining op-portunity to join in a round of "blackjack" – when players will see that quality assurance by Kistler is definitely not a game of chance!

Download Press Release (PDF)

Media contact
Simone Koch
Divisional Marketing Manager IPC
Phone +41 52 2241 802
Email: simone.koch@kistler.com


User contact

Stefan Schäfer
Product Manager, Production Monitoring
Phone: +41 52 224 15 73
Email: stefan.schaefer@kistler.com

Dossier de press

Portrait de Kistler avec logo pour un aperçu rapide: Kistler Press Kit.zip

09/05/2018
At Sensor + Test 2018 Kistler will be introducing a milestone in measurement technology: its new KiDAQ data...
08/05/2018
At NPE 2018, the Kistler Group is showcasing its latest custom monitoring package for ComoNeo, its...
03/05/2018
At Automatica 2018, the Kistler Group will turn the spotlight on diverse options for using sensors and process...
24/04/2018
The Kistler Group will showcase its expanded portfolio of industrial test and inspection systems for quality...
12/04/2018
The global leader in dynamic measurement technology supports the passion for innovation and technology with a...
06/03/2018
Kistler will be showcasing at Control 2018 its portfolio of industrial testing and inspection systems with the...
16/02/2018
At Intertraffic 2018 the Kistler Group is showcasing its comprehensive KiTraffic Weigh In Motion (WIM)...
15/02/2018
At NPE 2018 in Orlando, Florida, the Kistler Group will demonstrate a wide range of modular functionalities...
31/01/2018
The new KiSprint provides coaches and athletes with an efficient means of biomechanically optimizing sprint...
24/01/2018
Kistler achieved a growth rate of 18 % in 2017. Digital transformation has top priority in 2018.
23/01/2018
Surmonter les complexités du RTM - avec Kistler
12/10/2017
At the SPS IPC Drives Kistler Group will unveil the world's first digital charge amplifier Type 5974A, a...
09/10/2017
Kistler's Type 5074A industrial charge amplifier breaks new ground in industrial charge amplifier technology
06/10/2017
Whether hybrid drives or electric vehicles: anyone who wants to make a change needs to measure and understand
27/09/2017
Our experts will present you Kistler measuring technologies for demanding space applications.
05/09/2017
At Fakuma 2017, we will demonstrate how you can benefit from new ComoNeo functionalities
31/08/2017
Kistler Group showcases the entire spectrum of its integrated quality assurance solutions
25/08/2017
Kistler Group took over near Karlsruhe-based Vester Elektronik GmbH on 25 August, a specialist in sensor...
11/08/2017
Jaguar Land Rover uses Kistler RoaDyn® Wheel Force Transducers for accurate tyre modelling
11/07/2017
Kistler is taking over IOS GmbH (Germany), provider of Manufacturing Execution Systems (MES).
06/07/2017
Tettnang-based firm eso GmbH was acquired by the Kistler Group on July 5.
20/06/2017
Perfect production data synchronization through direct MES system integration.
02/05/2017
Kistler presents innovative measurement equipment for demanding vehicle testing applications
25/04/2017
At Moulding Expo 2017, we will show how easy it is to install the measurement technology needed for quality...
12/04/2017
Kistler will be present at Control, the world's leading quality assurance trade fair.
12/04/2017
Advanced features for LabAmp family maximize flexibility for cutting force users.
11/04/2017
Measuring equipment for sophisticated T&M applications
01/02/2017
The Kistler Group is constantly growing and recruiting specialist staff worldwide.
17/01/2017
Olympic champion Anthony Ervin and Kistler create a Success Story together.
02/12/2016
Kistler seeks more than 40 specialists in what is likely Switzerland's largest job advertisement.
27/10/2016
At this year's SPS IPC Drives in Nuremberg Kistler will premiere laboratory systems to analyze bolted joints,...
21/10/2016
Kistler boosts the efficiency and reliability of large marine and stationary engines through monitoring and...
19/10/2016
Kistler is presenting the new versions of its ComoNeo and ComoDataCenter.
10/10/2016
Kistler is unveiling a new addition to its portfolio of electromechanical joining modules.
30/09/2016
The Kistler Group reported incoming orders worth CHF 233.3 million at the end of August 2016 and has therefore...
07/09/2016
At this year's K Trade Fair from 19 to 26 October in Düsseldorf, Kistler will be showcasing its latest new...
24/07/2016
Kistler will be showcasing its new NCFE and NCFR joining modules, together with the latest generation of...
12/07/2016
Kistler's Correvit® SFII sensor measures world record in 1.513 seconds
12/05/2016
Screw technology complements the range of applications.
27/04/2016
Following a long phase of planning, preparations, and conversion work, Kistler Instrumente GmbH has a new home...
12/02/2016
Kistler Lorch GmbH Honored for Outstanding Qualities as Employer
02/02/2016
The Kistler Group has overcome currency-related challenges at its Swiss site to achieve continued growth.
28/01/2016
Accurate Wheel Force Measurement with Minimum Configuration Effort
26/11/2015
Increased Flexibility for High-Speed Combustion Analysis
02/11/2015
New Piezoresistive Sensor with Temperature Probe and Integrated Signal Conditioning.
27/10/2015
Kistler Provides Maximum Flexibility for Product Testing and Development
16/10/2015
Kistler's NCFR Joining Module honored in the handling and assembly category
05/10/2015
Setting the Standard for 100% Control of Linear Joining Processes with Partial Rotation
18/09/2015
Kistler Group: safeguarding the firm's competitive edge.
15/09/2015
Quick evaluation of performance and force with Kistler MARS 2.1.
03/09/2015
Major update for Kistler’s mobile engine indication system.
01/09/2015
Setting New Standards in Automated Process Monitoring for Injection Molding.
25/08/2015
Kistler Showcases Three Latest Product Innovations at Motek 2015
29/06/2015
Kistler Automotive GmbH honored as one of Germany's most innovative companies
26/06/2015
Kistler honored with ASCO Award Gold for best corporate transformation in Switzerland.
26/06/2015
Kistler's software for force plates offers a host of new features for performance diagnostics in sports and...