Enhanced precision: Kistler showcases new torque sensors

Nuremberg, November 11, 2014 – Kistler's motto for this year's SPS IPC Drives (November 25-27) is: more accurate, more versatile and simpler. With the KiTorq 4551A and the sensor 4503B, the company showcases its latest products for measuring highly dynamic torques at test stands. Both systems deliver reliable measurement results with an accuracy of 0.05 percent. Outstanding accuracy in torque measurement With the KiTorq 4551A, Kistler presents the latest version of its proven KiTorq system, which can be used to determine torques, rotational speeds or angles with an unprecedented resolution of up to 8,192 pulses per revolution, and allows the user to adjust the pulse rate. The system offers rotational speeds or angular resolutions that can be adjusted to any requirement. The measuring flange system consists of a single measurement body, the KiTorq rotor and an evaluation unit, the KiTorq stator. As far as the selection of suitable components for each test stand is concerned, the system offers manufacturers of electric and combustion engines, drives, pumps and compactors great flexibility because the guide-less stator means that different measurement bodies can be used without having to completely rebuild the test facility.
At the same time, the newly developed speed measurement system within KiTorq 4551A is fully integrated and practically invisible. The distances between the rotational speed probe and the magnetic flywheel do not require readjustment, and its magnetic function makes the probe maintenance-free and resistant against any kind of contamination. This results in cost savings during commissioning and maintenance of the system. An additional highlight is the absolute zero value called Z-Impuls offered by the new KiTorq system, by means of which absolute angle positions can be determined. Torques can be measured across a range from 50 to 5,000 Nm in different installation sizes. Parameterization takes places by means of the complementary SensorTool software via a USB interface or directly through a PLC via the Fieldbus or Ethernet ports. Therefore, commissioning the KiTorq 4551A is easy. Proven technology The second novelty Kistler will be presenting at SPS IPC Drives is the torque sensor 4503B. The new sensor is the successor of the Type 4503A sensor with a shaft connection. The 4503B offers a number of enhanced functions and thus complies with the latest market requirements. The previous optical speed and angle measurement device was replaced with a magnetic one similar to the new KiTorq solution. This offers the advantage that the sensor is now safe and robust enough for use in contaminated industrial environments (e.g. oil mist), which saves valuable maintenance time. Furthermore, the electronics of the torque sensor have been improved. For highly dynamic measurements, the 4503B also has a cut-off frequency of 10 kHz. This can be customized by the user by means of an integrated digital low-pass filter, and the second measurement range can be flexibly scaled up to a spread of 1:10. In addition, the Type 4503B is characterized by wide measurement ranges of 0.2 to 5,000 Nm as well as combined rotational speed/angle measurement and a high speed version of up to 50,000 1/min. "Our latest torque sensors offer industrial manufacturers the greatest possible dynamics and accuracy", explains Stephan Vogel, Product Manager at Kistler. "With their fully digital transmission, the systems permit a standard accuracy of 0.05 percent as well as a cut-off frequency of up to 10 kHz. This allows our customers to benefit from sensors which enable reliable measurement results and provide a solution that is tailored to each application. Because they are compatible with previous versions, the new torque sensors can also be integrated into existing systems with minimal effort.” Kistler will be showcasing itself with innovative products and advice at SPS IPC Drives in Nuremberg, Booth 526, Hall 4A, from November 25-27, 2014. Download Press Release (PDF/EN) 

Captions Image 1: With an unprecedented resolution of up to 8 192 pulses per revolution, the KiTorq 4551A can be used to determine torques, rotational speeds or crank angles. Image 2: The 4503B offers a number of enhanced functions and thus complies with the latest market requirements.
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
The new joining module is highly suitable for clinching and riveting, and also for assembly processes that require force-displacement monitoring.
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
The Kistler Group will showcase its test and analysis systems for threaded joints at the 2019 Fastener Fair in Stuttgart from 19 to 21 March.
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
Accurate and insensitive to its mounting position: the new Type 6044A M8 sensor features an anti-strain design to ensure reliable, high-quality results.
20/11/2018
Motorsport: the new 4080B/BT absolute pressure sensors from Kistler – for real-time monitoring with maximum measurement accuracy and signal quality!
16/10/2018
At Fakuma 2018, the Kistler Group is showcasing its latest monitoring and control packages for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
08/10/2018
The SMETEC Gesellschaft für Sensor-, Motor- und Energietechnik mbH recently became part of the Kistler Group.
24/09/2018
The Kistler Group is adding another variant to what is already the world's most comprehensive portfolio of wheel force measurement systems: the new RoaDyn S6GT 6-component wheel force measurement system.
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
The Kistler Group is introducing a compact mobile measurement solution for enhanced rolling stock maintenance in international railway operations in the shape of its railway brake force measuring system Type 2899A.
21/08/2018
A new Center of Competence for production control and management systems will be opened in Aachen.
31/07/2018
Competent service just a call away has always been a key aspect of Kistler's cooperation with its customers. Now, in a move to address growing demand in North Germany, the measurement technology experts are opening a new office in Wolfsburg.
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
Digitization, Internet of Things and Industry 4.0 are presenting major challenges. Discover how Kistler responds to the great challenges of our times.
09/05/2018
At Sensor + Test 2018 Kistler will be introducing a milestone in measurement technology: its new KiDAQ data acquisition system.
08/05/2018
At NPE 2018, the Kistler Group is showcasing its latest custom monitoring package for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
03/05/2018
At Automatica 2018, the Kistler Group will turn the spotlight on diverse options for using sensors and process monitoring systems to support industrial production and enhance digitalization in test and assembly technology.
24/04/2018
The Kistler Group will showcase its expanded portfolio of industrial test and inspection systems for quality assurance at the 2018 Control trade show.
12/04/2018
The global leader in dynamic measurement technology supports the passion for innovation and technology with a three-year partnership.
06/03/2018
Kistler will be showcasing at Control 2018 its portfolio of industrial testing and inspection systems with the spotlight on the very latest additions.
16/02/2018
At Intertraffic 2018 the Kistler Group is showcasing its comprehensive KiTraffic Weigh In Motion (WIM) solutions, which support road owners and authorities in road and traffic monitoring, weight enforcement and weight-based tolling.
15/02/2018
At NPE 2018 in Orlando, Florida, the Kistler Group will demonstrate a wide range of modular functionalities for ComoNeo: the process monitoring system that takes injection molding to a higher level with integrated quality monitoring geared to meet customers’ needs and requirements.
31/01/2018
The new KiSprint provides coaches and athletes with an efficient means of biomechanically optimizing sprint starts under competitive conditions. The robust and mobile solution has comprehensive software assessment options and can be individually adapted and expanded.
24/01/2018
Kistler achieved a growth rate of 18 % in 2017. Digital transformation has top priority in 2018.
23/01/2018
Surmonter les complexités du RTM - avec Kistler
12/10/2017
At the SPS IPC Drives Kistler Group will unveil the world's first digital charge amplifier Type 5974A, a milestone more in electrical automation.
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
With MARS software version 3.0, Kistler presents an extensive update of the proprietary measurement, analysis, and evaluation software for Kistler force plates.
21/10/2016
Kistler boosts the efficiency and reliability of large marine and stationary engines through monitoring and control of the combustion process
19/10/2016
Kistler is presenting the new versions of its ComoNeo and ComoDataCenter.
10/10/2016
Kistler is unveiling a new addition to its portfolio of electromechanical joining modules.
30/09/2016
The Kistler Group reported incoming orders worth CHF 233.3 million at the end of August 2016 and has therefore seen growth of 8.4 % compared to the same period in the previous year, or 5.6 % when adjusted for currency effects.
07/09/2016
At this year's K Trade Fair from 19 to 26 October in Düsseldorf, Kistler will be showcasing its latest new products and features with the focus on Industry 4.0.
24/07/2016
Kistler will be showcasing its new NCFE and NCFR joining modules, together with the latest generation of maXYmos monitoring systems on Motek 2016
12/07/2016
Kistler's Correvit® SFII sensor measures world record in 1.513 seconds
12/05/2016
Screw technology complements the range of applications.
27/04/2016
Following a long phase of planning, preparations, and conversion work, Kistler Instrumente GmbH has a new home for its German headquarters at the Böblingen/Sindelfingen airfield.
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
At Chinaplas 2015 Kistler will be presenting solutions for zero-defect production, process monitoring and data evaluation in injection molding
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
At Sensor + Test 2014 Kistler is presenting many new features from the field of measurement electronics in addition to its already proven sensor technology.
19/05/2014
Users obtain a full range of force–displacement measurement systems from one source
06/02/2014
The Kistler Group achieved sales of 285 million CHF in 2013, thus marking a slight growth in comparison with the figures for the prior year.