The NCFR Joining Module from Kistler

Stuttgart, 5 October 2015 – At the Motek 2015, Kistler will present its new NCFR Joining Module: as well as the classical linear joining process, this system can now perform a rotary movement of the ram, either sequentially or even simultaneously. These movements are monitored and controlled by integrated sensors on the NC joining module.

Kistler's electromechanical NC joining systems are coordinated systems with integrated force sensors and high-performance force-displacement evaluation. They provide end-to-end process monitoring and documentation for all measurements and process values. The measurement range covered
is wide – from 50 N to 600 kN – and the scope for potential applications is enormous. The launch of the new NCFR Joining Module marks the completion of Kistler's family of joining modules: with this innovative new module, joining processes can now be performed in combination with rotary movements.

Dynamic Drive Technology and High-Precision Sensors
The new NCFR Joining Module reflects the state of the art in joining process technology: with its integrated hollow-shaft servo motors, the module features compact dimensions and extremely low weight. This design offers excellent dynamic characteristics, creating the basis for dramatically reduced
cycle times. Integrated sensors continuously capture and evaluate force and displacement − as well as rotation angle and torque − with maximum precision, so 100% quality and control are ensured. The piezoelectric force sensor has two predefined measuring ranges to deliver high resolution; it also offers high overload capacity, especially in the small measuring range.

The joining process is monitored by maXYmos NC: activated via fieldbus, this monitoring system evaluates and documents XY profiles for joining and press-fit processes, together with the NCFR Joining Module and the IndraDrive servo amplifier that is included in the system. The patterns of measurement curves can be used to monitor and control the quality of a single production step, a sub-assembly or an entire product. The benefits: optimal cycle times can be achieved with maximum repeat accuracy, downtime is minimized and machine availability is increased – adding up to a remarkable boost in productivity for the manufacturing process.

NC joining systems with NCFR are fully tested systems that greatly simplify installation and handling: sequence programming is child's play, with parameterization on the PC or the touch panel. Even complex joining processes are simple to display thanks to sequencer mode. Depending on
requirements, practical sequence elements (e.g. various motions) can be used for the movements. The result: both linear and rotary movements can be programmed and controlled via events – flexibly, rapidly and easily, without intermediate stops.

One Module – Multiple Benefits
Like the entire family of NC joining modules, the NCFR Joining Module delivers a host of additional benefits for its users: thanks to the servo amplifiers used in the module, for instance, all traverse movements performed in assembly and product testing can be controlled with high precision. Another example: completely different components can be manufactured on one and the same machine, because all NC joining systems allow measuring ranges to be changed over, with easy switching between measuring programs.

And there are even more advantages: the system offers substantially higher efficiency than pneumatic or hydraulic processes. The savings potential of the electrical process is up to 77 % when compared to hydraulic systems and up to 90 % when compared with pneumatic process. Maintenance outlay for these systems is low – so users can save even more on their already low production
costs. Last but not least, the consistently simple operating philosophy of the maXYmos family makes setup fast and comfortable, and adjustments after commissioning are easy to perform.

Focusing on Cost-Efficient Operation
Alexander Müller, Product Manager for NC Joining Systems at Kistler, is utterly convinced by this innovative new development: "Maximum flexibility and excellent dynamics combined with simple operation mean that complex joining processes are mapped quickly and efficiently. Capacity utilization rates for plant are increased, and the commissioning and set-up phase is reduced to the minimum. And with its low energy consumption, the new NCFR Joining Module will help the automobile industry and the automotive supply sector to cut energy costs in series production. There's enormous market demand for both factors. Together, they create the basis for sustainable optimization
of resources, paving the way for cost-efficient operation in the long term."

Download Press Release PDF

Media Contact
Simone Koch
Divisional Marketing Manager IPC
Phone +41 52 2241 802
Email: simone.koch@kistler.com

User Contact
Alexander Müller
Product Manager, NC Joining Systems
Phone +49 7172 184 176
Email: alexander.mueller@kistler.com

Dossier de press

Portrait de Kistler avec logo pour un aperçu rapide: Kistler Press Kit.zip

09/05/2018
At Sensor + Test 2018 Kistler will be introducing a milestone in measurement technology: its new KiDAQ data...
08/05/2018
At NPE 2018, the Kistler Group is showcasing its latest custom monitoring package for ComoNeo, its...
03/05/2018
At Automatica 2018, the Kistler Group will turn the spotlight on diverse options for using sensors and process...
24/04/2018
The Kistler Group will showcase its expanded portfolio of industrial test and inspection systems for quality...
12/04/2018
The global leader in dynamic measurement technology supports the passion for innovation and technology with a...
06/03/2018
Kistler will be showcasing at Control 2018 its portfolio of industrial testing and inspection systems with the...
16/02/2018
At Intertraffic 2018 the Kistler Group is showcasing its comprehensive KiTraffic Weigh In Motion (WIM)...
15/02/2018
At NPE 2018 in Orlando, Florida, the Kistler Group will demonstrate a wide range of modular functionalities...
31/01/2018
The new KiSprint provides coaches and athletes with an efficient means of biomechanically optimizing sprint...
24/01/2018
Kistler achieved a growth rate of 18 % in 2017. Digital transformation has top priority in 2018.
23/01/2018
Surmonter les complexités du RTM - avec Kistler
12/10/2017
At the SPS IPC Drives Kistler Group will unveil the world's first digital charge amplifier Type 5974A, a...
09/10/2017
Kistler's Type 5074A industrial charge amplifier breaks new ground in industrial charge amplifier technology
06/10/2017
Whether hybrid drives or electric vehicles: anyone who wants to make a change needs to measure and understand
27/09/2017
Our experts will present you Kistler measuring technologies for demanding space applications.
05/09/2017
At Fakuma 2017, we will demonstrate how you can benefit from new ComoNeo functionalities
31/08/2017
Kistler Group showcases the entire spectrum of its integrated quality assurance solutions
25/08/2017
Kistler Group took over near Karlsruhe-based Vester Elektronik GmbH on 25 August, a specialist in sensor...
11/08/2017
Jaguar Land Rover uses Kistler RoaDyn® Wheel Force Transducers for accurate tyre modelling
11/07/2017
Kistler is taking over IOS GmbH (Germany), provider of Manufacturing Execution Systems (MES).
06/07/2017
Tettnang-based firm eso GmbH was acquired by the Kistler Group on July 5.
20/06/2017
Perfect production data synchronization through direct MES system integration.
02/05/2017
Kistler presents innovative measurement equipment for demanding vehicle testing applications
25/04/2017
At Moulding Expo 2017, we will show how easy it is to install the measurement technology needed for quality...
12/04/2017
Kistler will be present at Control, the world's leading quality assurance trade fair.
12/04/2017
Advanced features for LabAmp family maximize flexibility for cutting force users.
11/04/2017
Measuring equipment for sophisticated T&M applications
01/02/2017
The Kistler Group is constantly growing and recruiting specialist staff worldwide.
17/01/2017
Olympic champion Anthony Ervin and Kistler create a Success Story together.
02/12/2016
Kistler seeks more than 40 specialists in what is likely Switzerland's largest job advertisement.
27/10/2016
At this year's SPS IPC Drives in Nuremberg Kistler will premiere laboratory systems to analyze bolted joints,...
21/10/2016
Kistler boosts the efficiency and reliability of large marine and stationary engines through monitoring and...
19/10/2016
Kistler is presenting the new versions of its ComoNeo and ComoDataCenter.
10/10/2016
Kistler is unveiling a new addition to its portfolio of electromechanical joining modules.
30/09/2016
The Kistler Group reported incoming orders worth CHF 233.3 million at the end of August 2016 and has therefore...
07/09/2016
At this year's K Trade Fair from 19 to 26 October in Düsseldorf, Kistler will be showcasing its latest new...
24/07/2016
Kistler will be showcasing its new NCFE and NCFR joining modules, together with the latest generation of...
12/07/2016
Kistler's Correvit® SFII sensor measures world record in 1.513 seconds
12/05/2016
Screw technology complements the range of applications.
27/04/2016
Following a long phase of planning, preparations, and conversion work, Kistler Instrumente GmbH has a new home...
12/02/2016
Kistler Lorch GmbH Honored for Outstanding Qualities as Employer
02/02/2016
The Kistler Group has overcome currency-related challenges at its Swiss site to achieve continued growth.
28/01/2016
Accurate Wheel Force Measurement with Minimum Configuration Effort
26/11/2015
Increased Flexibility for High-Speed Combustion Analysis
02/11/2015
New Piezoresistive Sensor with Temperature Probe and Integrated Signal Conditioning.
27/10/2015
Kistler Provides Maximum Flexibility for Product Testing and Development
16/10/2015
Kistler's NCFR Joining Module honored in the handling and assembly category
05/10/2015
Setting the Standard for 100% Control of Linear Joining Processes with Partial Rotation
18/09/2015
Kistler Group: safeguarding the firm's competitive edge.
15/09/2015
Quick evaluation of performance and force with Kistler MARS 2.1.
03/09/2015
Major update for Kistler’s mobile engine indication system.
01/09/2015
Setting New Standards in Automated Process Monitoring for Injection Molding.
25/08/2015
Kistler Showcases Three Latest Product Innovations at Motek 2015
29/06/2015
Kistler Automotive GmbH honored as one of Germany's most innovative companies
26/06/2015
Kistler honored with ASCO Award Gold for best corporate transformation in Switzerland.
26/06/2015
Kistler's software for force plates offers a host of new features for performance diagnostics in sports and...