Cylinder Pressure Measurement Cuts Fuel Consumption

Kistler boosts the efficiency and reliability of large marine and stationary engines through monitoring and control of the combustion process.

90% of all goods transported are traversing the world's oceans every day in container ships, tankers and freighters.1 Marine cargo transport offers a green alternative to road and air transportation, but even on the high seas boosting efficiency and sustainable optimization of resource usage are key concerns. The International Maritime Organization (IMO) has set a target of achieving a 10% increase in the efficiency of new ships by 2020, and CO2 emissions per tonne are to be cut by 20% across the entire industry.2 Today's shipping industry has to meet ever-greater business expectations and increasingly stricter regulatory requirements. One response to this has been more widespread use of a cutting edge engine technology that allows active control of the combustion process - closed loop combustion control (CLCC). Whenever monitoring and control of combustion in large marine and stationary engines is required, Kistler is on hand with proven, reliable solutions - customized as required for every customer, including the necessary certifications.

Cylinder pressure measurement is the crucial factor in CLCC for large engines - this provides on-line feedback information to the engine control system about the actual operating conditions in the combustion chamber. Analysis of data from CLCC systems in use today provides clear evidence on how the efficiency of 2-stroke or 4-stroke engines can be enhanced. Fuel consumption improvements, of as much as 2%, stability of emissions over long operating periods, and the ability to optimize maintenance intervals, all lead to short term operational cost savings for the engine operators. The advantages of this are even more evident when operating with mixed or variable quality fuels. The systems also provide longer term potential savings for customers; from the early warning detection of engine operating issues that could otherwise lead to very high repair costs, and from a general reduction in engine component wear that the elimination of high load combustion events made possible with CLCC can achieve.

Combustion Control in Continuous Operation with Reliable On-line Monitoring

Kistler has designed rugged piezoelectric cylinder pressure sensors to meet the special requirements of on-line combustion monitoring in marine and stationary engine installations. These long service lifetimes – installed on the cylinder head of low- and medium-speed engines – are the key to our success in this market.

Certified Industry Standard: Offline Diagnosis

Cylinder pressure also provides meaningful information about the condition of an engine when used as a regular maintenance basis – as an off-line diagnostic tool. All large engine classification companies specify regular cylinder pressure measurements as a standard – and this data provides the essential basis for maintaining good fuel consumption. Peak pressures on large engines can be recorded periodically by Kistler's diagnostic equipment, with immediate evaluation using the software supplied with the products. This rugged equipment can be installed quickly and easily on the indicator valve on the engine and delivers accurate and reliable measurement data from sensors with proven long-term stability.

Reliable Sensor and System Expertise – from One Single Source

When a customer needs to monitor and control large engines, they need look no further than Kistler: we offer cylinder pressure sensors backed by all the service and system expertise necessary – allowing us to develop cost-effective solutions tailored to the needs of each specific customer. Jürg Stadler, Head of Kistler’s Strategic Business Field Marine & Stationary, proudly explains, “Our many years of expertise in cylinder pressure measurement provide the basis for combustion control for many manufacturers of large engines, shipbuilders, shipping companies and power plant operators. One example is General Electric (GE) - this manufacturer of energy technology solutions in power generation was so enthusiastic about our professional, customer focused, service offering that the company awarded us GE's prize for innovative capacity and technology leadership in 2015.”

Kistler has over 20 years of experience in engine diagnostics, operational monitoring and engine combustion control and has cost-effective solutions that offer both long-term reliability and an early return on investment for our customers.

For more information visit Marine & Stationary.

1 International Chamber of Shipping (ICS): Shipping, World Trade and the Reduction of CO2 Emissions. United Nations Framework Convention on Climate Change (UNFCCC). 2014
2 IMO: MARPOL Annex VI, Capter 4, adopted July 2011: www.imo.org/en/OurWork/Environment/PollutionPrevention/AirPollution/Pages/Technical-and-Operational-Measures.aspx


Contact for Users
Jürg Stadler
Head of Engine Marine & Stationary
Tel.: +41 52 224 19 49
Email: jürg.stadler@kistler.com
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
The new joining module is highly suitable for clinching and riveting, and also for assembly processes that require force-displacement monitoring.
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
The Kistler Group will showcase its test and analysis systems for threaded joints at the 2019 Fastener Fair in Stuttgart from 19 to 21 March.
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
Accurate and insensitive to its mounting position: the new Type 6044A M8 sensor features an anti-strain design to ensure reliable, high-quality results.
20/11/2018
Motorsport: the new 4080B/BT absolute pressure sensors from Kistler – for real-time monitoring with maximum measurement accuracy and signal quality!
16/10/2018
At Fakuma 2018, the Kistler Group is showcasing its latest monitoring and control packages for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
08/10/2018
The SMETEC Gesellschaft für Sensor-, Motor- und Energietechnik mbH recently became part of the Kistler Group.
24/09/2018
The Kistler Group is adding another variant to what is already the world's most comprehensive portfolio of wheel force measurement systems: the new RoaDyn S6GT 6-component wheel force measurement system.
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
The Kistler Group is introducing a compact mobile measurement solution for enhanced rolling stock maintenance in international railway operations in the shape of its railway brake force measuring system Type 2899A.
21/08/2018
A new Center of Competence for production control and management systems will be opened in Aachen.
31/07/2018
Competent service just a call away has always been a key aspect of Kistler's cooperation with its customers. Now, in a move to address growing demand in North Germany, the measurement technology experts are opening a new office in Wolfsburg.
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
Digitization, Internet of Things and Industry 4.0 are presenting major challenges. Discover how Kistler responds to the great challenges of our times.
09/05/2018
At Sensor + Test 2018 Kistler will be introducing a milestone in measurement technology: its new KiDAQ data acquisition system.
08/05/2018
At NPE 2018, the Kistler Group is showcasing its latest custom monitoring package for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
03/05/2018
At Automatica 2018, the Kistler Group will turn the spotlight on diverse options for using sensors and process monitoring systems to support industrial production and enhance digitalization in test and assembly technology.
24/04/2018
The Kistler Group will showcase its expanded portfolio of industrial test and inspection systems for quality assurance at the 2018 Control trade show.
12/04/2018
The global leader in dynamic measurement technology supports the passion for innovation and technology with a three-year partnership.
06/03/2018
Kistler will be showcasing at Control 2018 its portfolio of industrial testing and inspection systems with the spotlight on the very latest additions.
16/02/2018
At Intertraffic 2018 the Kistler Group is showcasing its comprehensive KiTraffic Weigh In Motion (WIM) solutions, which support road owners and authorities in road and traffic monitoring, weight enforcement and weight-based tolling.
15/02/2018
At NPE 2018 in Orlando, Florida, the Kistler Group will demonstrate a wide range of modular functionalities for ComoNeo: the process monitoring system that takes injection molding to a higher level with integrated quality monitoring geared to meet customers’ needs and requirements.
31/01/2018
The new KiSprint provides coaches and athletes with an efficient means of biomechanically optimizing sprint starts under competitive conditions. The robust and mobile solution has comprehensive software assessment options and can be individually adapted and expanded.
24/01/2018
Kistler achieved a growth rate of 18 % in 2017. Digital transformation has top priority in 2018.
23/01/2018
Surmonter les complexités du RTM - avec Kistler
12/10/2017
At the SPS IPC Drives Kistler Group will unveil the world's first digital charge amplifier Type 5974A, a milestone more in electrical automation.
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
With MARS software version 3.0, Kistler presents an extensive update of the proprietary measurement, analysis, and evaluation software for Kistler force plates.
21/10/2016
Kistler boosts the efficiency and reliability of large marine and stationary engines through monitoring and control of the combustion process
19/10/2016
Kistler is presenting the new versions of its ComoNeo and ComoDataCenter.
10/10/2016
Kistler is unveiling a new addition to its portfolio of electromechanical joining modules.
30/09/2016
The Kistler Group reported incoming orders worth CHF 233.3 million at the end of August 2016 and has therefore seen growth of 8.4 % compared to the same period in the previous year, or 5.6 % when adjusted for currency effects.
07/09/2016
At this year's K Trade Fair from 19 to 26 October in Düsseldorf, Kistler will be showcasing its latest new products and features with the focus on Industry 4.0.
24/07/2016
Kistler will be showcasing its new NCFE and NCFR joining modules, together with the latest generation of maXYmos monitoring systems on Motek 2016
12/07/2016
Kistler's Correvit® SFII sensor measures world record in 1.513 seconds
12/05/2016
Screw technology complements the range of applications.
27/04/2016
Following a long phase of planning, preparations, and conversion work, Kistler Instrumente GmbH has a new home for its German headquarters at the Böblingen/Sindelfingen airfield.
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
At Chinaplas 2015 Kistler will be presenting solutions for zero-defect production, process monitoring and data evaluation in injection molding
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
At Sensor + Test 2014 Kistler is presenting many new features from the field of measurement electronics in addition to its already proven sensor technology.
19/05/2014
Users obtain a full range of force–displacement measurement systems from one source
06/02/2014
The Kistler Group achieved sales of 285 million CHF in 2013, thus marking a slight growth in comparison with the figures for the prior year.