Automated Tire Screening for improved road safety

Winterthur, May 2022 – Automated Tire Screening (ATS) from Kistler offers a reliable and cost-effective system for real-time screening of tire properties without disrupting traffic flow. The quartz crystal sensors deliver accurate data on missing or under-inflated tires – and thus help to prevent accidents. The technology can be integrated into existing Weigh In Motion (WIM) sites equipped with Lineas sensors from Kistler, of which many have already been installed throughout the United States.

According to the National Highway Safety Association, 738 traffic fatalities were caused by tire-related car crashes in the United States in 2017. Next to the brakes, tires are the most important safety device on a vehicle. Incorrect tire pressure poses serious risks for drivers. The severity of this issue has prompted the US government to act, providing funding and grants through several programs. 

Reliable information on tire conditions

Kistler has developed a simple solution that allows authorities to monitor the condition of tires on roads in real time: Automated Tire Screening. ATS can be added to any new or existing WIM sites that use Kistler technology. To screen for tire properties, a WIM system requires two additional Lineas quartz crystal sensors and a software update for Kistler’s Data Logger. The sensors are installed in the pavement at an angle to the standard WIM sensors. This angle enables prolonged contact with the tires which is crucial when detecting any deviation from the measurement of the standard sensors. The system uses the deviations to differentiate between single, dual, and super single tires, as well as to detect insufficiently inflated, flat, missmatched or missing tires. Tests show that ATS reliably detects underinflated tires with a tire pressure of 50 percent or less compared to normal inflation. Roadside inspectors can automatically inspect all passing vehicles with the system pointing out which tires deviate from the norm. Consequently, they need only take action when the system reports unsafe tire conditions or overloaded vehicles.

Quartz technology for better road safety

The Lineas sensors at the heart of the Weigh In Motion technology support highway operators and authorities across the globe. They are used for a range of applications, such as traffic data collection, bridge protection, weight enforcement and weight-based toll collection. Installed in saw-cut or milled slots in concrete or asphalt roads, the unique maintenance-free quartz crystal strip sensors can collect and process traffic data in real-time. With over 70,000 Lineas sensors already installed worldwide, the technology is internationally recognized as the solution of choice to protect road infrastructure, improve traffic safety, and collect toll fees. It offers a simple and effective strategy to monitor roads without disrupting traffic flow. With ATS, Kistler provides a low-cost upgrade for Weigh In Motion sites that further improves road safety.
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
The new joining module is highly suitable for clinching and riveting, and also for assembly processes that require force-displacement monitoring.
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
The Kistler Group will showcase its test and analysis systems for threaded joints at the 2019 Fastener Fair in Stuttgart from 19 to 21 March.
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
Accurate and insensitive to its mounting position: the new Type 6044A M8 sensor features an anti-strain design to ensure reliable, high-quality results.
20/11/2018
Motorsport: the new 4080B/BT absolute pressure sensors from Kistler – for real-time monitoring with maximum measurement accuracy and signal quality!
16/10/2018
At Fakuma 2018, the Kistler Group is showcasing its latest monitoring and control packages for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
08/10/2018
The SMETEC Gesellschaft für Sensor-, Motor- und Energietechnik mbH recently became part of the Kistler Group.
24/09/2018
The Kistler Group is adding another variant to what is already the world's most comprehensive portfolio of wheel force measurement systems: the new RoaDyn S6GT 6-component wheel force measurement system.
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
The Kistler Group is introducing a compact mobile measurement solution for enhanced rolling stock maintenance in international railway operations in the shape of its railway brake force measuring system Type 2899A.
21/08/2018
A new Center of Competence for production control and management systems will be opened in Aachen.
31/07/2018
Competent service just a call away has always been a key aspect of Kistler's cooperation with its customers. Now, in a move to address growing demand in North Germany, the measurement technology experts are opening a new office in Wolfsburg.
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
Digitization, Internet of Things and Industry 4.0 are presenting major challenges. Discover how Kistler responds to the great challenges of our times.
09/05/2018
At Sensor + Test 2018 Kistler will be introducing a milestone in measurement technology: its new KiDAQ data acquisition system.
08/05/2018
At NPE 2018, the Kistler Group is showcasing its latest custom monitoring package for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
03/05/2018
At Automatica 2018, the Kistler Group will turn the spotlight on diverse options for using sensors and process monitoring systems to support industrial production and enhance digitalization in test and assembly technology.
24/04/2018
The Kistler Group will showcase its expanded portfolio of industrial test and inspection systems for quality assurance at the 2018 Control trade show.
12/04/2018
The global leader in dynamic measurement technology supports the passion for innovation and technology with a three-year partnership.
06/03/2018
Kistler will be showcasing at Control 2018 its portfolio of industrial testing and inspection systems with the spotlight on the very latest additions.
16/02/2018
At Intertraffic 2018 the Kistler Group is showcasing its comprehensive KiTraffic Weigh In Motion (WIM) solutions, which support road owners and authorities in road and traffic monitoring, weight enforcement and weight-based tolling.
15/02/2018
At NPE 2018 in Orlando, Florida, the Kistler Group will demonstrate a wide range of modular functionalities for ComoNeo: the process monitoring system that takes injection molding to a higher level with integrated quality monitoring geared to meet customers’ needs and requirements.
31/01/2018
The new KiSprint provides coaches and athletes with an efficient means of biomechanically optimizing sprint starts under competitive conditions. The robust and mobile solution has comprehensive software assessment options and can be individually adapted and expanded.
24/01/2018
Kistler achieved a growth rate of 18 % in 2017. Digital transformation has top priority in 2018.
23/01/2018
Surmonter les complexités du RTM - avec Kistler
12/10/2017
At the SPS IPC Drives Kistler Group will unveil the world's first digital charge amplifier Type 5974A, a milestone more in electrical automation.
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
With MARS software version 3.0, Kistler presents an extensive update of the proprietary measurement, analysis, and evaluation software for Kistler force plates.
21/10/2016
Kistler boosts the efficiency and reliability of large marine and stationary engines through monitoring and control of the combustion process
19/10/2016
Kistler is presenting the new versions of its ComoNeo and ComoDataCenter.
10/10/2016
Kistler is unveiling a new addition to its portfolio of electromechanical joining modules.
30/09/2016
The Kistler Group reported incoming orders worth CHF 233.3 million at the end of August 2016 and has therefore seen growth of 8.4 % compared to the same period in the previous year, or 5.6 % when adjusted for currency effects.
07/09/2016
At this year's K Trade Fair from 19 to 26 October in Düsseldorf, Kistler will be showcasing its latest new products and features with the focus on Industry 4.0.
24/07/2016
Kistler will be showcasing its new NCFE and NCFR joining modules, together with the latest generation of maXYmos monitoring systems on Motek 2016
12/07/2016
Kistler's Correvit® SFII sensor measures world record in 1.513 seconds
12/05/2016
Screw technology complements the range of applications.
27/04/2016
Following a long phase of planning, preparations, and conversion work, Kistler Instrumente GmbH has a new home for its German headquarters at the Böblingen/Sindelfingen airfield.
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
At Chinaplas 2015 Kistler will be presenting solutions for zero-defect production, process monitoring and data evaluation in injection molding
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
At Sensor + Test 2014 Kistler is presenting many new features from the field of measurement electronics in addition to its already proven sensor technology.
19/05/2014
Users obtain a full range of force–displacement measurement systems from one source
06/02/2014
The Kistler Group achieved sales of 285 million CHF in 2013, thus marking a slight growth in comparison with the figures for the prior year.