ZF operates with a software-controlled fastener test bench from Kistler

In 2018, the ZF company began operating a software-controlled Kistler fastener test bench with an integrated vibration unit in its central Development Center at Friedrichshafen (Germany). The new test bench ensures reliable testing for design and development, helping ZF to achieve two objectives: capacity expansion, and the performance of complex load tests on threaded joints.

All of us are sure to encounter fasteners fairly often in our everyday lives: whether or not you're handy about the house, you're bound to have tightened a screw or bolt at some time in the past. But in industry and the transport sector, the requirements and conditions are not the same as those that apply at home. So – how complicated is the world of fasteners? Marcus Hornikel is someone who certainly knows the answer. The "Fastener King", as his colleagues fondly call him, is the Team Leader in ZF's Center of Competence for Threaded Joints at Friedrichshafen. "Whatever belongs together, must hold together" – that is Hornikel's motto, and he has been making it happen for the last 28 years.  

ZF is one of the world's largest suppliers in the vehicle technology sector. Its transmission experts operate a central Research and Development Center at the firm's headquarters near Lake Constance, flanked by local R&D units. Hornikel recalls: "I started my career at ZF in 1985. Back then, we were just beginning to acknowledge the relevance of threaded joints, so the first guidelines for friction coefficient testing were being defined. At ZF nowadays, we work to standard 5033 – a rulebook that's even more extensive than the international standard, ISO 16047." The new test bench is configured for loads of up to 1 000 Nm torque, 300 kN preloading force and 500 Nm thread torque. Hornikel continues: 

We're able to work more efficiently thanks to the Kistler test bench. But that's not all: the dynamic load test under vibration opens up entirely new possibilities for component design and engineering."

Marcus Hornikel, Team Leader in ZF’s Center of Competence for Threaded Joints

 

Load simulation on the test bench to optimize design

One of the main tasks of the six-strong ZF team is to overcome challenges in the development and design process. For example: a threaded joint on the prototype of a complex component such as a truck transmission might fail to withstand the dynamic loads, although the reason is not clear at first glance. In cases such as this, the team's expertise is needed to identify alternatives in a development process that has already reached an advanced stage. "The quality of a threaded joint depends on multiple factors. Is the component at fault – or the tool? Could there be any lubricant residues that are compromising the joint? Was the force applied to tighten the joint too high, or too low? On the fastener test bench, we simulate the different influencing parameters to discover exactly where the causes of the problem lie," Hornikel explains.

As he mainly provides services for inhouse ZF customers, Hornikel usually has to work as quickly as possible to come up with sound solutions for problematic threaded joints. The final stage in the process is often a new set of assembly instructions. Lately, however, designers are increasingly turning to Hornikel during the development process so they can collaborate to find a solution. "That's considerably more efficient, of course, because then you can influence important decisions that have to be taken in advance – about where a bolt or screw has to be positioned, for instance. There are major advantages to doing this ahead of time rather than later – which would be like closing the stable door after the horse has bolted. So that's why our approach to advice is increasingly proactive," Hornikel sums up.

As an expert on fastening technology, he also attends specialist trade fairs to learn about the cur-rent state-of-the-art and see the latest innovations and developments for himself. He first became aware of Kistler's new test system at the Motek in 2015. "In any case, we wanted to expand our capacity, so we were looking around for a new test bench. I was particularly attracted by the concept of one single device that combines three functions: fastener inspection, determination of friction coefficients, and vibration testing. As far as I'm aware, this is unique on the market," Hornikel emphasizes. He was finally won over to the Analyse system in November 2016, when he was invited by Kistler to learn about this product in greater detail; and on his way to the Kistler Center, he discovered that one of ZF's major fastener suppliers is also using a virtually identical Kistler Analyse system.

Flexible fastener, friction coefficient and vibration testing in one system

Jürgen Wahl, a sales engineer specializing in fastener technology at Kistler, provided support for this project from day one. He explains some further improvements that have been implemented in this innovative test bench: "Unlike conventional stands for the Junker test, our vibration test bench is largely controlled by software. The advantage is that it requires far less effort to set up and use. Parameters such as amplitude and frequency can even be modified while the test is running."

ZF purchased the Kistler Analyse system before the end of 2017, and it has been operating successfully ever since it was commissioned in February 2018. "This new test bench relieves pressure on the old system, which is now somewhat outmoded. And it also gives us many more options for testing threaded joints with safety elements, because it's simple to operate and very flexible thanks to software control. The integrated vibration unit is a major advantage in this regard. The result: we can offer better advice to our internal customers and give them more efficient support when they are faced with challenges," Hornikel notes. Wahl adds: "The staff at ZF already had some practical knowledge of the basic structure of the programming software used on the test bench. Of course, that makes training and practical application much easier." The key question is: what preloading force is needed? And in the future, this question can be answered faster and more reliably – especially under dynamic conditions such as those present in rail and road vehicles as well as aircraft and watercraft.

About six years ago, Hornikel set up the "Bolt Connection" working group at ZF to give participants more insights into the complexities of fastener testing. Representatives from all parts of the company attend this group to learn about the latest developments and exchange their experiences. Thanks to Kistler's cutting-edge Analyse system, Hornikel can offer a new type of service to his colleagues from local R&D departments this year, with designs for threaded joints that no other provider can currently offer in this form – so ZF's central Competence Center is fully able to handle the varied range of requirements that it must meet.

11/04/2022
On the road to success with IEPE and MEMS accelerometers for the ISTAR research aircraft – on the ground and in the air.
14/01/2022
KiTraffic Statistics delivers precise WIM data for a railway bridge in central Austria
18/11/2021
Advanced fastener testing with ANALYSE systems for reliable zink flake coatings in the automotive and wind turbine industries
12/10/2021
How Yuchai achieves more precision, transparency and resource efficiency for its production of engines conform to China VI
14/09/2021
A high precision measuring chain with dynamometer, laboratory charge amplifier and software enables objective comparison tests.
09/09/2021
SRA: Find the best spot and the ideal sensor layout for direct enforcement of overloaded vehicles.
03/09/2021
At Estudio de la Pisada in Valencia, a 3D force plate helps podiatry experts to develop treatments and orthoses for patients and athletes.
02/07/2021
Two IEPE accelerometers deliver key data for propulsion validation and optimization of flight characteristics even in the stratosphere
22/06/2021
Capturing micro-vibrations with a dynamometer leads to improved satellite technology
02/06/2021
Zero defect despite high volumes: this is the way quality assurance with Kistler test automation systems works for zinc die casting parts
26/04/2021
A digitally driven brake force measurement system makes the life of service technicians for train maintenance much easier
13/04/2021
Inside "The Atmosphere" at MARIN, 100 of our pressure sensors capture wave impacts under varying environmental conditions
22/03/2021
How MAN Energy Solutions is using sensors from Kistler to make its gas turbines fit for the future
08/02/2021
Measurement technology dedicated to the discipline and biomechanics of pole vault enables high performances
05/10/2020
How does a digital measuring chain for piezoelectric sensors work as part of a complex vehicle test stand?
18/09/2020
Convincing test results: The Ohio Department of Transportation goes on to apply Lineas from Kistler for traffic monitoring.
20/08/2020
Precision is the key to top performance: how measurement technology from Kistler supports the development team at EMUGE-FRANKEN
22/07/2020
Quality assurance solutions by Kistler like ComoNeo ensure highest accuracy at TSP Precision Tooling in Shanghai.
09/06/2020
Kistler supports Ceratizit in the development of HDT. This enables complex geometries to be produced with just one tool.
15/11/2019
Process monitoring systems and cavity pressure sensors from Kistler help to reduce the amount of scrap drastically
23/10/2019
How measurement technology from Kistler contributes toward boosting high-end powertools' quality
15/08/2019
How the ANALYSE system from Kistler is enhancing safety and transparency in the field of fastening technology
17/07/2019
Turkey opts for weight enforcement with WIM technology from Kistler
24/06/2019
For the next manned flight to the moon: safety that can be measured
20/06/2019
Segregation of good and bad parts every 1.5 seconds: process monitoring with Kistler enables high quality for over 5 million parts per year.
14/05/2019
In order to achieve excellent quality for its components and medical devices, Tessy Plastics chose sensors and solutions from Kistler.
18/04/2019
A renowned manufacturer of electrical appliances trusts testing and sorting systems by Vester to improve its quality.
02/04/2019
NFL's Jaguars boost their fitness levels with Kistler.
25/03/2019
By using process monitoring from Kistler, not only the assembly of electric fuses is validated, but even the function of the sensors itself.
18/03/2019
How to determine the fitness level of an athlete efficiently? A practical report on the Quattro Jump force plate system from Kistler.
17/12/2018
Thanks to precise Weigh in Motion technology from Kistler, Hungary's roads are sustainably protected against overloaded vehicles.
27/11/2018
Bang&Clean relies on Kistler's precise measurement of ignition processes and pressure wave propagation
10/10/2018
Sartorius applies the process monitoring system ComoNeo from Kistler and thereby increases the process quality during injection molding
08/10/2018
The Dortmund Technical University tests the new MicroDyn 9109AA cutting force dynamometer from Kistler and breaks new ground for developing its micromachining processes.
31/08/2018
The ZF company operates a software-controlled Kistler fastener test bench with an integrated vibration unit.
14/08/2018
BIG Daishowa, headquartered in Osaka, Japan, is one of the leading producers of tool holders for the machining industry. Each year the company produces over half a million collet chucks. Their products are developed using, among other resources, Kistler’s cutting force measuring device.
16/07/2018
Enhanced quality and efficiency in mobile crane manufacture – thanks to the test stand for torque tools by Kistler
11/04/2018
The world’s largest provider of rail transport technology relies on Kistler’s measurement expertise. Thanks to the only crash wall of its kind in the world, the impact forces of the trains and their components can be precisely measured and analyzed.
14/11/2017
In the development of cooling lubricants, Blaser Swisslube relies on Kistler's measurement expertise.
11/08/2017
Applus IDIADA relies on DTI in-dummy technology from Kistler for Test Device for Human Occupant Restraint (THOR).
04/01/2017
Road safety is a central topic in vehicle development. Through accurate measurements, Kistler helps increase the chance of survival in crashes.
22/12/2016
Kistler makes progress in vehicle development possible
22/12/2016
Kistler Sensor Correvit® SFII measures world record
20/12/2016
Kistler sensors deliver a maximum in data quality under any conditions.
07/11/2016
Kistler pressure sensors enabled the Rosetta space probe to fly for 6.4 billion kilometers.
05/10/2016
Since the end of 2015 FC Basel is using Kistler force plates to reduce the dropout of young talents.
17/08/2016
Kistler makes the difference in the crucial sports moments with its Performance Analysis System for Swimming.
19/02/2016
Determination of Pump Efficiency with Kistler KiTorq Measuring Flange System
04/11/2015
Piezoelectric Measurements with CompactRIO™
08/05/2015
Quality Assurance in the Automotive Industry
02/03/2015
How Brose improves the quality of its two-component production and automatically separates defective parts
02/12/2014
The Kistler Group pursues a growth policy that is both ambitious and sustainable – and strategic acquisitions are one of its core elements. ‘Strategic’ means that Kistler deliberately selects companies which can achieve more together with Kistler than they ever could by continuing alone. The takeover of Dr. Staiger Mohilo & Co. GmbH in 2006 enabled Kistler to grow jointly with the acquired company...
02/12/2014
After a ten-year voyage, the Rosetta space probe's Philae landing module finally touched down on the surface of comet ‘Chury’.
23/08/2011
HEWI and its Customers Benefit from Cavity Pressure Technology
15/02/2011
End-to-end process monitoring for critical medical moldings
07/02/2011
Cavity pressure measurement eliminates short shots at Fischer GmbH & Co KG of Sinsheim/Germany
Contact
Max 25 MB