The Technical University (TU) Dortmund tests new MicroDyn dynamometer from Kistler

The Institute of Machining Technology (ISF) at Dortmund Technical University (TU) has spent more than four decades researching and teaching in the field of machining covering all relevant machining processes and related technical subjects. A team of research associates are currently working in the Collaborative Research Center (CRC) Transregio 73. As part of sub projects B2 and B3, research is being conducted into the manufacture and modification of forming machines on which very hard tool steels (> 60 HRC) have to be machined with micro tools. Kistler provided the ISF with the new MicroDyn 9109AA cutting force dynamometer for the project. Thanks to its very high natural frequency, the world's smallest dynamometer unlocks completely new possibilities for the institute in the development of its micromachining processes – with astounding results. 

The ISF currently numbers more than 80 research associates, technical and student supporting staff, who are engaged in three research departments: machining, grinding technology and simulation and process development. The departments are equipped with modern machine tools and machining centers to achieve machining processes of the highest standard. The scientists also have access to comprehensive measurement technology and a computer infrastructure with well-developed basic equipment. Suitable premises and laboratories enable tests to be performed in the right framework conditions and the results precisely evaluated.

New manufacturing technology to master economical and ecological challenges 

As part of the Collaborative Research Center (CRC) Transregio 73, the TU Dortmund is working with the Leibnitz University Hanover and Friedrich-Alexander University Erlangen-Nürnberg. Funded by the German Research Foundation (DFG), the Collaborative Research Center was initiated to develop a new manufacturing technology called sheet-bulk metal forming (SBMF). This technology is designed to unite the advantages of sheet and bulk metal forming processes and extend possibilities with regard to component complexity. Besides the development of forming processes, the manufacture of innovative forming tools with specific characteristics represents a major step towards technology transfer into practical industrial implementation. Micromachining offers significant benefits in respect to the required form, dimensional accuracy and surface integrity, while enhancing the efficient and economical manufacture of forming tools and prolonging tool life. 

“Scientists would be fumbling in the dark if it wasn't for measurement technology” 

Eugen Krebs has been a research associate at the ISF for several years and is responsible for the sub project B2 along with Alexander Meijer in the CRC Transregio. The two colleagues' work at the institute focuses on micromachining. Their duties include process and tool development for the respective machining tasks for which they need the right measurement technology. “Micromachining demands the highest standards from measuring equipment on account of the very fine dimensions. Machining involves mechanical processes in which highly dynamic forces can occur over a very wide measurement range. Reliable measurement and analysis of these forces is crucial for our process evaluation. Without measurement technology, we scientists would be left to fumble in the dark,” explains Krebs. Along with 22 other research associates, he has been doing research in the Transregio CRC since 2010. “The Collaborative Research Center Transregio 73 plays a significant role in the necessary development of forming technology, and thus also in the mastering of current economical and ecological challenges,” adds Krebs. “This project creates the scientific fundamentals that will enable us to satisfy growing demand for customized, flexible systems of increasing functional density.” The results achieved will improve the economic and resource efficiency of forming processes. 

Daunting process requirements 

Forming tools in sheet-bulk metal forming consist of very fine, complex forming elements, which at the same time have to withstand high stresses. “We had to discount a lot of materials for the forming tools in the project because they simply didn't match up to our requirements,” continues Krebs. In the end, they opted for a powder metallurgical high speed steel with high resistance to wear and tear and dimensional stability with case hardening of up to 65 HRC. “At the beginning of the Transregio, we doubted that materials of this nature could be reliably machined at all with micro tools (less than d = 1 mm in diameter). Sub project B2 focused on tackling this challenge.”

Machining involves mechanical processes in which highly dynamic forces can occur over a very wide measurement range. Reliable measurement and analysis of these forces is crucial for our process evaluation. Without measurement technology, we scientists would be left to fumble in the dark.”

Eugen Krebs, research assistant at the ISF

 

The solution: Rugged measurement technology with high natural frequency 

Developing micromachining processes for high-strength materials with tool diameters ranging from 0.2 to 1 millimeter involved in-depth machining tests in which both suitable process parameters were to be identified and tool concepts optimized. Reliable measurement technology was required for the job, capable of both responding very sensitively and clearly while precisely mapping forces of less than 1 N to more than 200 N in a single process run. Another key criterion required by the ISF of measurement technology was high natural frequency. “If the natural frequency range of the force measurement system is less than 4,000 Hz, the force measurement platform will be excessively excited during the micromachining process, so we might end up measuring platform vibration instead of cutting force signals,” admits Krebs. Rugged qualities were also important for measurement technology to ensure that external influences like temperature or cooling lubricant did not compromise the process. And finally, repeatability and measurement accuracy were prioritized by the research team. “We frequently repeat measurements up to five to ten times. So of course it is crucial to obtain comparable, reliable results for the same tests,” concludes Krebs. 

Exploring the impossible with Kistler 

The MicroDyn 9109AA cutting force dynamometer fulfills all the above ISF requirements, and also offers many other benefits. “The TU Dortmund and the Kistler Group can look back on a long, intensive partnership. In the past, we have frequently conducted research with different Kistler dynamometers, and so far we have been very happy with them all. When we were given the opportunity to test the prototype of the new MicroDyn 9109AA dynamometer to assess our analyses of tool modifications, we jumped at the chance,” Krebs remarks.

The ISF has been using the dynamometer since February 2018. What has changed since? Krebs: “Before using the new Kistler dynamometer, our problem was that the micromachining force measurements were always compromised by the measurement instrument's natural frequencies. We no longer have to contend with this obstacle. Thanks to the high natural frequency of 15 kHz on all three axes (x, y, z), we can measure highly dynamic forces at spindle speeds of up to 160 000 rpm. This increases dynamic properties by a factor 2.5 compared to the predecessor product.” The device is also suitably dimensioned for a measurement range of up to 500 N. “We have never achieved the likes of this with our measurement technology. The MicroDyn has played an important role in extending the bounds of the possible. Now we are able to analyze processes with cutting speeds of vc > 500 m/min using small tool diameters,” remarks Krebs. “This measurement technology development provides new insights into micromachining, which used to be beyond our reach due to technological limitations.”

Although the Transregio 73 research program will finish at the end of 2020, Krebs and Meijer firmly intend to continue using the Kistler dynamometer. “We would like to explore further tool modifications and stretch the process limits of micromachining even further. So we look forward to the continued support of Kistler's measurement technology experts in the development of our processes.”

11/04/2022
On the road to success with IEPE and MEMS accelerometers for the ISTAR research aircraft – on the ground and in the air.
14/01/2022
KiTraffic Statistics delivers precise WIM data for a railway bridge in central Austria
18/11/2021
Advanced fastener testing with ANALYSE systems for reliable zink flake coatings in the automotive and wind turbine industries
12/10/2021
How Yuchai achieves more precision, transparency and resource efficiency for its production of engines conform to China VI
14/09/2021
A high precision measuring chain with dynamometer, laboratory charge amplifier and software enables objective comparison tests.
09/09/2021
SRA: Find the best spot and the ideal sensor layout for direct enforcement of overloaded vehicles.
03/09/2021
At Estudio de la Pisada in Valencia, a 3D force plate helps podiatry experts to develop treatments and orthoses for patients and athletes.
02/07/2021
Two IEPE accelerometers deliver key data for propulsion validation and optimization of flight characteristics even in the stratosphere
22/06/2021
Capturing micro-vibrations with a dynamometer leads to improved satellite technology
02/06/2021
Zero defect despite high volumes: this is the way quality assurance with Kistler test automation systems works for zinc die casting parts
26/04/2021
A digitally driven brake force measurement system makes the life of service technicians for train maintenance much easier
13/04/2021
Inside "The Atmosphere" at MARIN, 100 of our pressure sensors capture wave impacts under varying environmental conditions
22/03/2021
How MAN Energy Solutions is using sensors from Kistler to make its gas turbines fit for the future
08/02/2021
Measurement technology dedicated to the discipline and biomechanics of pole vault enables high performances
05/10/2020
How does a digital measuring chain for piezoelectric sensors work as part of a complex vehicle test stand?
18/09/2020
Convincing test results: The Ohio Department of Transportation goes on to apply Lineas from Kistler for traffic monitoring.
20/08/2020
Precision is the key to top performance: how measurement technology from Kistler supports the development team at EMUGE-FRANKEN
22/07/2020
Quality assurance solutions by Kistler like ComoNeo ensure highest accuracy at TSP Precision Tooling in Shanghai.
09/06/2020
Kistler supports Ceratizit in the development of HDT. This enables complex geometries to be produced with just one tool.
15/11/2019
Process monitoring systems and cavity pressure sensors from Kistler help to reduce the amount of scrap drastically
23/10/2019
How measurement technology from Kistler contributes toward boosting high-end powertools' quality
15/08/2019
How the ANALYSE system from Kistler is enhancing safety and transparency in the field of fastening technology
17/07/2019
Turkey opts for weight enforcement with WIM technology from Kistler
24/06/2019
For the next manned flight to the moon: safety that can be measured
20/06/2019
Segregation of good and bad parts every 1.5 seconds: process monitoring with Kistler enables high quality for over 5 million parts per year.
14/05/2019
In order to achieve excellent quality for its components and medical devices, Tessy Plastics chose sensors and solutions from Kistler.
18/04/2019
A renowned manufacturer of electrical appliances trusts testing and sorting systems by Vester to improve its quality.
02/04/2019
NFL's Jaguars boost their fitness levels with Kistler.
25/03/2019
By using process monitoring from Kistler, not only the assembly of electric fuses is validated, but even the function of the sensors itself.
18/03/2019
How to determine the fitness level of an athlete efficiently? A practical report on the Quattro Jump force plate system from Kistler.
17/12/2018
Thanks to precise Weigh in Motion technology from Kistler, Hungary's roads are sustainably protected against overloaded vehicles.
27/11/2018
Bang&Clean relies on Kistler's precise measurement of ignition processes and pressure wave propagation
10/10/2018
Sartorius applies the process monitoring system ComoNeo from Kistler and thereby increases the process quality during injection molding
08/10/2018
The Dortmund Technical University tests the new MicroDyn 9109AA cutting force dynamometer from Kistler and breaks new ground for developing its micromachining processes.
31/08/2018
The ZF company operates a software-controlled Kistler fastener test bench with an integrated vibration unit.
14/08/2018
BIG Daishowa, headquartered in Osaka, Japan, is one of the leading producers of tool holders for the machining industry. Each year the company produces over half a million collet chucks. Their products are developed using, among other resources, Kistler’s cutting force measuring device.
16/07/2018
Enhanced quality and efficiency in mobile crane manufacture – thanks to the test stand for torque tools by Kistler
11/04/2018
The world’s largest provider of rail transport technology relies on Kistler’s measurement expertise. Thanks to the only crash wall of its kind in the world, the impact forces of the trains and their components can be precisely measured and analyzed.
14/11/2017
In the development of cooling lubricants, Blaser Swisslube relies on Kistler's measurement expertise.
11/08/2017
Applus IDIADA relies on DTI in-dummy technology from Kistler for Test Device for Human Occupant Restraint (THOR).
04/01/2017
Road safety is a central topic in vehicle development. Through accurate measurements, Kistler helps increase the chance of survival in crashes.
22/12/2016
Kistler makes progress in vehicle development possible
22/12/2016
Kistler Sensor Correvit® SFII measures world record
20/12/2016
Kistler sensors deliver a maximum in data quality under any conditions.
07/11/2016
Kistler pressure sensors enabled the Rosetta space probe to fly for 6.4 billion kilometers.
05/10/2016
Since the end of 2015 FC Basel is using Kistler force plates to reduce the dropout of young talents.
17/08/2016
Kistler makes the difference in the crucial sports moments with its Performance Analysis System for Swimming.
19/02/2016
Determination of Pump Efficiency with Kistler KiTorq Measuring Flange System
04/11/2015
Piezoelectric Measurements with CompactRIO™
08/05/2015
Quality Assurance in the Automotive Industry
02/03/2015
How Brose improves the quality of its two-component production and automatically separates defective parts
02/12/2014
The Kistler Group pursues a growth policy that is both ambitious and sustainable – and strategic acquisitions are one of its core elements. ‘Strategic’ means that Kistler deliberately selects companies which can achieve more together with Kistler than they ever could by continuing alone. The takeover of Dr. Staiger Mohilo & Co. GmbH in 2006 enabled Kistler to grow jointly with the acquired company...
02/12/2014
After a ten-year voyage, the Rosetta space probe's Philae landing module finally touched down on the surface of comet ‘Chury’.
23/08/2011
HEWI and its Customers Benefit from Cavity Pressure Technology
15/02/2011
End-to-end process monitoring for critical medical moldings
07/02/2011
Cavity pressure measurement eliminates short shots at Fischer GmbH & Co KG of Sinsheim/Germany
Contact
Max 25 MB