Thanks to the system from Kistler, we can capture the movements of the body's center of gravity and also of individual parts of the body, as well as the resultant angles and the length, frequency, and speed of the run-up. What's more, the forces in all three spatial dimensions are measured – including, in particular, the force exerted by the athlete on the ground in his or her last three steps, and when the pole is planted in the box. This kind of information is not available to coaches who only observe athletes with the naked eye."