Revolutionize turning with dynamometer from Kistler

Ceratizit intends to revolutionize industrial turning technology with its High Dynamic Turning (HDT) system and FreeTurn tooling. Thanks to this innovative system, users can manufacture complex geometries with just one tool. During an extensive series of tests, measurement technology from Kistler was deployed to record the forces acting on the cutting edge. Ceratizit's engineers gained critical insights from the reliable values supplied by the dynamometer.

For over 95 years, Ceratizit has pioneered the development of sophisticated hard material solutions for cutting and wear protection. The company develops and produces highly specialized cutting tools, indexable inserts, carbide rods and wear parts. With more than 9,000 employees and 34 production facilities across the globe  - backed by a sales network of over 70 branches  - the Ceratizit Group is a global player in the carbide sector. Innovative solutions from Ceratizit are deployed in the mechanical engineering and toolmaking sectors as well as the automotive, aerospace and medical industries  - the list could go on.

New machining method revolutionizes turning

Ceratizit's experts have now developed a new machining method that is set to revolutionize turning. High Dynamic Turning (HDT) and the FreeTurn tools included in the system allow the cutting head to move freely  - so the approach angle of the cutting edge can be chosen freely at any point during the machining operation. FreeTurn tools feature a new type of indexable insert that can consist of several different cutting edges. This breakthrough allows both pull- and push-type machining of workpieces. Chip breaking can also be optimized, and the chip can be moved out of the cut zone.

HDT offers a key advantage: only one tool is needed to carry out all the familiar turning operations such as roughing, finishing, contour turning, face turning and longitudinal turning. This means that every contour of a turned part can be produced with no need to change the tool. The result: from now on, parts can be fully machined with just one single FreeTurn tool instead of the large numbers of different tools that were required in the past. Tool changes as well as empty tool runs are vastly reduced  - leading to increased productivity. And as yet another benefit, tool costs are slashed.

The values obtained with measurement technology from Kistler are plausible. Industry trusts them. And that means we can supply machine and spindle manufacturers with reliable values that they too can trust.

Dr. Uwe Schleinkofer, Head of R&D Cutting Tools

 

 

Less force is applied thanks to this innovative concept

A further advantage of HDT is the new angle of approach, which directs the cutting force vertically through the tool into the spindle. This reduces the load on the machine, making it possible to work with higher process parameters. The free choice of approach angle also extends the life expectancy of the cutting edge.

The first tests have been completed successfully, so the system is currently undergoing the release procedure for series use. For this purpose, Ceratizit's developers need detailed and reliable values for the forces that occur in the system. This data is essential to improve their understanding of the tool properties in the cutting process. Manufacturers of machines and controls as well as CAM software providers have a particular need for this information so they can drive their developments ahead towards their defined goals.

Extensive series of tests with support from Kistler

Ceratizit has already been putting its trust in solutions from Kistler for over 30 years. And in this project too, products from the Swiss measurement technology specialist have played a key part. The 9171A 4-component rotating cutting force dynamometer (RCD) was used to measure the cutting forces. This measuring instrument features a modular structure and is compatible with all commonly used machine spindles. It measures the forces acting on the cutting edge in all three axes, and can also calculate the torque on the basis of these values. Piezoelectric sensor technology gives the RCD a very high sampling rate coupled with sensitivity across an extremely wide force range. These assets guarantee that the measurement data is meaningful as well as accurate. Transmission of measured values and energy is contact-free, so wear is eliminated.

The measuring chain was completed with the 5238B signal conditioner, which is responsible for the energy supply, signal transmission and system control in the test setup at Ceratizit. Measurement range settings and adjustments to the low-pass filter are made manually on the signal conditioner or via the serial interface. System activation and data acquisition are handled via the DynoWare software from Kistler. The measurement signals are also available as analog voltage signals (±10 volts).

Cutting force measuring instrument from Kistler supplies reliable values

The tests were carried out during summer 2019 at the Innovation Center of Ceratizit Austria GmbH in Reutte (Austria). The first objective was to approach the maximum performance capability of the HDT system. Different values for the feed rate and cut depth were selected for this purpose. The steepness of the approach angle for the FreeTurn tool was then gradually increased. The dynamometer from Kistler supplied detailed and reliable values for the forces occurring during this process. This data was compared to the results for a conventional turning tool of type PCLNL 2525 M12.

Onsite support for the project was provided by Lukas Janotta, the Kistler application engineer responsible for cutting processes. He advised the Ceratizit engineers as they performed the series of tests. The DynoWare software from Kistler was used for detailed visualization, recording and analysis of the forces occurring during the tests. This made it possible to validate the results from previous simulations with real measurement values. As the end result, the customer gained in-depth insights into cutting force conditions that were previously hidden.

11/04/2022
On the road to success with IEPE and MEMS accelerometers for the ISTAR research aircraft – on the ground and in the air.
14/01/2022
KiTraffic Statistics delivers precise WIM data for a railway bridge in central Austria
18/11/2021
Advanced fastener testing with ANALYSE systems for reliable zink flake coatings in the automotive and wind turbine industries
12/10/2021
How Yuchai achieves more precision, transparency and resource efficiency for its production of engines conform to China VI
14/09/2021
A high precision measuring chain with dynamometer, laboratory charge amplifier and software enables objective comparison tests.
09/09/2021
SRA: Find the best spot and the ideal sensor layout for direct enforcement of overloaded vehicles.
03/09/2021
At Estudio de la Pisada in Valencia, a 3D force plate helps podiatry experts to develop treatments and orthoses for patients and athletes.
02/07/2021
Two IEPE accelerometers deliver key data for propulsion validation and optimization of flight characteristics even in the stratosphere
22/06/2021
Capturing micro-vibrations with a dynamometer leads to improved satellite technology
02/06/2021
Zero defect despite high volumes: this is the way quality assurance with Kistler test automation systems works for zinc die casting parts
26/04/2021
A digitally driven brake force measurement system makes the life of service technicians for train maintenance much easier
13/04/2021
Inside "The Atmosphere" at MARIN, 100 of our pressure sensors capture wave impacts under varying environmental conditions
22/03/2021
How MAN Energy Solutions is using sensors from Kistler to make its gas turbines fit for the future
08/02/2021
Measurement technology dedicated to the discipline and biomechanics of pole vault enables high performances
05/10/2020
How does a digital measuring chain for piezoelectric sensors work as part of a complex vehicle test stand?
18/09/2020
Convincing test results: The Ohio Department of Transportation goes on to apply Lineas from Kistler for traffic monitoring.
20/08/2020
Precision is the key to top performance: how measurement technology from Kistler supports the development team at EMUGE-FRANKEN
22/07/2020
Quality assurance solutions by Kistler like ComoNeo ensure highest accuracy at TSP Precision Tooling in Shanghai.
09/06/2020
Kistler supports Ceratizit in the development of HDT. This enables complex geometries to be produced with just one tool.
15/11/2019
Process monitoring systems and cavity pressure sensors from Kistler help to reduce the amount of scrap drastically
23/10/2019
How measurement technology from Kistler contributes toward boosting high-end powertools' quality
15/08/2019
How the ANALYSE system from Kistler is enhancing safety and transparency in the field of fastening technology
17/07/2019
Turkey opts for weight enforcement with WIM technology from Kistler
24/06/2019
For the next manned flight to the moon: safety that can be measured
20/06/2019
Segregation of good and bad parts every 1.5 seconds: process monitoring with Kistler enables high quality for over 5 million parts per year.
14/05/2019
In order to achieve excellent quality for its components and medical devices, Tessy Plastics chose sensors and solutions from Kistler.
18/04/2019
A renowned manufacturer of electrical appliances trusts testing and sorting systems by Vester to improve its quality.
02/04/2019
NFL's Jaguars boost their fitness levels with Kistler.
25/03/2019
By using process monitoring from Kistler, not only the assembly of electric fuses is validated, but even the function of the sensors itself.
18/03/2019
How to determine the fitness level of an athlete efficiently? A practical report on the Quattro Jump force plate system from Kistler.
17/12/2018
Thanks to precise Weigh in Motion technology from Kistler, Hungary's roads are sustainably protected against overloaded vehicles.
27/11/2018
Bang&Clean relies on Kistler's precise measurement of ignition processes and pressure wave propagation
10/10/2018
Sartorius applies the process monitoring system ComoNeo from Kistler and thereby increases the process quality during injection molding
08/10/2018
The Dortmund Technical University tests the new MicroDyn 9109AA cutting force dynamometer from Kistler and breaks new ground for developing its micromachining processes.
31/08/2018
The ZF company operates a software-controlled Kistler fastener test bench with an integrated vibration unit.
14/08/2018
BIG Daishowa, headquartered in Osaka, Japan, is one of the leading producers of tool holders for the machining industry. Each year the company produces over half a million collet chucks. Their products are developed using, among other resources, Kistler’s cutting force measuring device.
16/07/2018
Enhanced quality and efficiency in mobile crane manufacture – thanks to the test stand for torque tools by Kistler
11/04/2018
The world’s largest provider of rail transport technology relies on Kistler’s measurement expertise. Thanks to the only crash wall of its kind in the world, the impact forces of the trains and their components can be precisely measured and analyzed.
14/11/2017
In the development of cooling lubricants, Blaser Swisslube relies on Kistler's measurement expertise.
11/08/2017
Applus IDIADA relies on DTI in-dummy technology from Kistler for Test Device for Human Occupant Restraint (THOR).
04/01/2017
Road safety is a central topic in vehicle development. Through accurate measurements, Kistler helps increase the chance of survival in crashes.
22/12/2016
Kistler makes progress in vehicle development possible
22/12/2016
Kistler Sensor Correvit® SFII measures world record
20/12/2016
Kistler sensors deliver a maximum in data quality under any conditions.
07/11/2016
Kistler pressure sensors enabled the Rosetta space probe to fly for 6.4 billion kilometers.
05/10/2016
Since the end of 2015 FC Basel is using Kistler force plates to reduce the dropout of young talents.
17/08/2016
Kistler makes the difference in the crucial sports moments with its Performance Analysis System for Swimming.
19/02/2016
Determination of Pump Efficiency with Kistler KiTorq Measuring Flange System
04/11/2015
Piezoelectric Measurements with CompactRIO™
08/05/2015
Quality Assurance in the Automotive Industry
02/03/2015
How Brose improves the quality of its two-component production and automatically separates defective parts
02/12/2014
The Kistler Group pursues a growth policy that is both ambitious and sustainable – and strategic acquisitions are one of its core elements. ‘Strategic’ means that Kistler deliberately selects companies which can achieve more together with Kistler than they ever could by continuing alone. The takeover of Dr. Staiger Mohilo & Co. GmbH in 2006 enabled Kistler to grow jointly with the acquired company...
02/12/2014
After a ten-year voyage, the Rosetta space probe's Philae landing module finally touched down on the surface of comet ‘Chury’.
23/08/2011
HEWI and its Customers Benefit from Cavity Pressure Technology
15/02/2011
End-to-end process monitoring for critical medical moldings
07/02/2011
Cavity pressure measurement eliminates short shots at Fischer GmbH & Co KG of Sinsheim/Germany
Contact
Max 25 MB