Liebherr: The nuts and bolts of success

Well before you reach the factory gates, you can see them towering in the distance: the booms of the huge mobile cranes that undergo the most rigorous testing here on the test site at Ehingen, Swabia (Germany) before they are delivered to every corner of the world. These cranes are built by Liebherr, the global corporation now managed by the third generation of the same family. To meet its own high standards, Liebherr opts for the cerTest mobile test system from Kistler for all power tools in use on its production lines. With the help of this system, power tools are tested regularly to ensure that they deliver consistently high quality throughout their lifetimes – and cerTest also includes end-to-end documentation of all simulated fastening scenarios.

Starting out from its core business in the construction machines segment, Liebherr has expanded into business fields such as transportation and traffic technology, mechanical engineering and domestic appliances in recent years, and it has even opened its own hotel chain. With sales approaching EUR 10 billion and over 43 000 employees in 2017, there can be no doubt that Liebherr numbers among the global players in the sector. The entire mobile cranes business is focused here at the company's Ehingen site. All Liebherr's mobile cranes, in all their different versions, are built here: ranging from all-terrain vehicles with telescopic booms (offering both on-road and off-road capability) to crawler cranes with lattice booms. The largest crawler crane in Liebherr's range, the LR 13000, was recently deployed in Mexico for the construction of a refinery. This machine can lift weights of up to 3 000 tonnes.

Thomas Nüssle, Head of Plant Planning at the Ehingen site, outlines some of this facility's special features: "We manufacture complete vehicles here on four lines – an average of about eight vehi-cles every day, all of them built to order and just-in-time. Before delivery, they undergo extensive testing on our test sites: we have one for mobile cranes and another for crawlers." Marco Kassner, Foreman in the Operational Mechanics Department, adds: "Quality has top priority in our book. Throughout the world, Liebherr is appreciated for its outstanding products. And to make sure that this remains so, we work continuously on improving our processes in every area, including fastening technology."

Inhouse testing cuts costs and builds up know-how

Many different torque tools are used in the manufacture of mobile cranes. To ensure their machine capability, Liebherr deploys the cerTest mobile test system by Kistler. Thanks to cerTest, all the facility's power tools can be tested regularly on site; all the results are documented precisely, with torque and rotation angle control.

We currently use 128 torque wrenches from different manufacturers, and all of them have to be tested. As of 2018, we've been carrying out our own machine capability analyses based on four test points as per VDI 2645. We also carry out tests related to fastening points."

Heiko Springer, Project engineer in the Plant Planning Department at Liebherr Ehingen

 

"Springer continues with more detail: "We use nutrunners with different technologies for 'A', 'B' and 'C' joints – with electronic or hydraulic control, or with compressed air. Thanks to this new test stand from Kistler, we can successfully meet higher quality requirements. We base our work here on the strict standards specified by the automotive industry, which requires a machine capability index of Cm/Cmk > 1.6."

End-to-end documentation for all tools

The cerTest system has four simulators (two integrated and two external) to test power tools in the torque range from 250 to 6 000 Nm. This allows dynamic simulation of all joint hardnesses up to
6 000 Nm. And for tests related to fastening points, it delivers precise statements about the current performance of the tested power tools after 25 measurements. The simulator also rotates synchro-nously during the dynamic test. The advantage of this approach over the static method is that it allows simulation of "hard" joints (with a small angle of rotation) as well as "soft" ones (with a large angle of rotation). End-to-end documentation for all tools and the main joints creates an accurate picture of a machine's capability throughout its entire life expectancy.

Thanks to cerTest, Liebherr saves about EUR 30 000 on external testing costs each year – and as an added bonus, the company can build up its own valuable know-how on fastening technology here in house. As far as Springer is concerned, the benefits are obvious: "On the one hand, we save on costs – but that's by no means all: it's also easier to ensure the quality of our internal fas-tening processes. What's more, the quality is better than when tests are outsourced, because test-ing can take place under the conditions that are present right here on site (electronic control or compressed air fluctuations, for instance). Another point is that we're building up know-how on handling power tools. And last but not least, the logistics are more efficient: we eliminate the cost of sending the tools out and sorting them back in again. We gain extra time by testing right here on the spot." Because the Kistler test stand is mobile, all the power tools can be tested near the production lines. For this purpose, cerTest is equipped with a rechargeable battery that has a lifetime of up to 16 hours.

Convincing advantages: performance scope, specialization and service

One of the key points for Liebherr was that the tool testing system must cover the full bandwidth required. With a range of up to 6 000 Nm, the external dynamic simulator also gives Liebherr the capability of testing electrical power tools currently in use at Ehingen which operate at 4 000 Nm or more. "That was a decisive factor for us, of course, because no other provider was able to manufacture a dynamic simulator with a range of up to 6 000 Nm. Other advantages were Kistler's independence, its specialization in measurement technology, and its expertise in fastening technology – adding up to a complete package that we found highly convincing," Springer emphasizes. "Starting in early 2016, we began to focus more attention on the machine capability of power tools – and in any case, this aspect has become generally more important and will become even more critical in the future. So we're very well equipped to face those challenges thanks to the solution from Kistler."

Data from all the test procedures is stored and fully documented in the CEUS software that is inte-grated in cerTest. Springer comments: "There was another important point here: the data on an access point that we installed on the nutrunner test stand must be sent to a server via W-LAN. That allows everyone involved to access the test results in CEUS from their PC workstations." The Plant Planning team uses handheld scanners, making it easy to set the electrically controlled tools to a test point or a special joint at the start of the test procedure. "This prevents any operator errors that could occur with manual input of the detailed data. We benefit from accurate and reliable traceability, so we know who tested which power tool, when, and to what extent," Springer notes.

He concludes by touching on his firm's excellent working relationship with Kistler. Things were difficult at the outset, due mainly to the complexity of the subject and the sheer volume of data to be collected. But now, somewhat more than one year after the project began, he is highly satisfied with the results: "Thanks to our excellent working relationship with Kistler, we overcame all the challenges. We've now established a quality assurance process that will not only save us money in the long run, but will also offer extra security as regards product liability. And by no means least, it gives us a deeper understanding of the technology. It's highly likely that we'll be using more fastener inspection systems from Kistler in the future so that we can continue to develop our expertise. At the moment, for example, we're thinking about deploying the method known as 'joint scanning'. This involves positioning a plug-on sensor between the nutrunner and the real joint. The nutrunner test stand measures the torque and rotation angle, and stores the data for the power tool. Later on, this precise joint can be simulated dynamically for this same tool on the nutrunner test stand."

11/04/2022
On the road to success with IEPE and MEMS accelerometers for the ISTAR research aircraft – on the ground and in the air.
14/01/2022
KiTraffic Statistics delivers precise WIM data for a railway bridge in central Austria
18/11/2021
Advanced fastener testing with ANALYSE systems for reliable zink flake coatings in the automotive and wind turbine industries
12/10/2021
How Yuchai achieves more precision, transparency and resource efficiency for its production of engines conform to China VI
14/09/2021
A high precision measuring chain with dynamometer, laboratory charge amplifier and software enables objective comparison tests.
09/09/2021
SRA: Find the best spot and the ideal sensor layout for direct enforcement of overloaded vehicles.
03/09/2021
At Estudio de la Pisada in Valencia, a 3D force plate helps podiatry experts to develop treatments and orthoses for patients and athletes.
02/07/2021
Two IEPE accelerometers deliver key data for propulsion validation and optimization of flight characteristics even in the stratosphere
22/06/2021
Capturing micro-vibrations with a dynamometer leads to improved satellite technology
02/06/2021
Zero defect despite high volumes: this is the way quality assurance with Kistler test automation systems works for zinc die casting parts
26/04/2021
A digitally driven brake force measurement system makes the life of service technicians for train maintenance much easier
13/04/2021
Inside "The Atmosphere" at MARIN, 100 of our pressure sensors capture wave impacts under varying environmental conditions
22/03/2021
How MAN Energy Solutions is using sensors from Kistler to make its gas turbines fit for the future
08/02/2021
Measurement technology dedicated to the discipline and biomechanics of pole vault enables high performances
05/10/2020
How does a digital measuring chain for piezoelectric sensors work as part of a complex vehicle test stand?
18/09/2020
Convincing test results: The Ohio Department of Transportation goes on to apply Lineas from Kistler for traffic monitoring.
20/08/2020
Precision is the key to top performance: how measurement technology from Kistler supports the development team at EMUGE-FRANKEN
22/07/2020
Quality assurance solutions by Kistler like ComoNeo ensure highest accuracy at TSP Precision Tooling in Shanghai.
09/06/2020
Kistler supports Ceratizit in the development of HDT. This enables complex geometries to be produced with just one tool.
15/11/2019
Process monitoring systems and cavity pressure sensors from Kistler help to reduce the amount of scrap drastically
23/10/2019
How measurement technology from Kistler contributes toward boosting high-end powertools' quality
15/08/2019
How the ANALYSE system from Kistler is enhancing safety and transparency in the field of fastening technology
17/07/2019
Turkey opts for weight enforcement with WIM technology from Kistler
24/06/2019
For the next manned flight to the moon: safety that can be measured
20/06/2019
Segregation of good and bad parts every 1.5 seconds: process monitoring with Kistler enables high quality for over 5 million parts per year.
14/05/2019
In order to achieve excellent quality for its components and medical devices, Tessy Plastics chose sensors and solutions from Kistler.
18/04/2019
A renowned manufacturer of electrical appliances trusts testing and sorting systems by Vester to improve its quality.
02/04/2019
NFL's Jaguars boost their fitness levels with Kistler.
25/03/2019
By using process monitoring from Kistler, not only the assembly of electric fuses is validated, but even the function of the sensors itself.
18/03/2019
How to determine the fitness level of an athlete efficiently? A practical report on the Quattro Jump force plate system from Kistler.
17/12/2018
Thanks to precise Weigh in Motion technology from Kistler, Hungary's roads are sustainably protected against overloaded vehicles.
27/11/2018
Bang&Clean relies on Kistler's precise measurement of ignition processes and pressure wave propagation
10/10/2018
Sartorius applies the process monitoring system ComoNeo from Kistler and thereby increases the process quality during injection molding
08/10/2018
The Dortmund Technical University tests the new MicroDyn 9109AA cutting force dynamometer from Kistler and breaks new ground for developing its micromachining processes.
31/08/2018
The ZF company operates a software-controlled Kistler fastener test bench with an integrated vibration unit.
14/08/2018
BIG Daishowa, headquartered in Osaka, Japan, is one of the leading producers of tool holders for the machining industry. Each year the company produces over half a million collet chucks. Their products are developed using, among other resources, Kistler’s cutting force measuring device.
16/07/2018
Enhanced quality and efficiency in mobile crane manufacture – thanks to the test stand for torque tools by Kistler
11/04/2018
The world’s largest provider of rail transport technology relies on Kistler’s measurement expertise. Thanks to the only crash wall of its kind in the world, the impact forces of the trains and their components can be precisely measured and analyzed.
14/11/2017
In the development of cooling lubricants, Blaser Swisslube relies on Kistler's measurement expertise.
11/08/2017
Applus IDIADA relies on DTI in-dummy technology from Kistler for Test Device for Human Occupant Restraint (THOR).
04/01/2017
Road safety is a central topic in vehicle development. Through accurate measurements, Kistler helps increase the chance of survival in crashes.
22/12/2016
Kistler makes progress in vehicle development possible
22/12/2016
Kistler Sensor Correvit® SFII measures world record
20/12/2016
Kistler sensors deliver a maximum in data quality under any conditions.
07/11/2016
Kistler pressure sensors enabled the Rosetta space probe to fly for 6.4 billion kilometers.
05/10/2016
Since the end of 2015 FC Basel is using Kistler force plates to reduce the dropout of young talents.
17/08/2016
Kistler makes the difference in the crucial sports moments with its Performance Analysis System for Swimming.
19/02/2016
Determination of Pump Efficiency with Kistler KiTorq Measuring Flange System
04/11/2015
Piezoelectric Measurements with CompactRIO™
08/05/2015
Quality Assurance in the Automotive Industry
02/03/2015
How Brose improves the quality of its two-component production and automatically separates defective parts
02/12/2014
The Kistler Group pursues a growth policy that is both ambitious and sustainable – and strategic acquisitions are one of its core elements. ‘Strategic’ means that Kistler deliberately selects companies which can achieve more together with Kistler than they ever could by continuing alone. The takeover of Dr. Staiger Mohilo & Co. GmbH in 2006 enabled Kistler to grow jointly with the acquired company...
02/12/2014
After a ten-year voyage, the Rosetta space probe's Philae landing module finally touched down on the surface of comet ‘Chury’.
23/08/2011
HEWI and its Customers Benefit from Cavity Pressure Technology
15/02/2011
End-to-end process monitoring for critical medical moldings
07/02/2011
Cavity pressure measurement eliminates short shots at Fischer GmbH & Co KG of Sinsheim/Germany
Contact
Max 25 MB