Kistler supports development of innovative space technology test equipment at CSEM

As part of their research on magnetic bearings for satellite attitude control, two engineers at CSEM are using a dynamometer from Kistler to capture the micro-vibrations of a novel type of magnetic bearing reaction wheel. Based on precise micro-vibration measurements, they were able to characterize the effectiveness of a control algorithm that actively suppresses synchronous vibrations over the full speed range ‒ allowing higher rotational speeds thanks to reduced disturbances and power consumption. 

In 2019, the CSEM (Centre Suisse d'Electronique et de Microtechnique) headquartered in Neuchâtel celebrated 35 years of technological innovation and knowledge transfer. Headquartered in Neuchâtel, this scientific network originally had close ties with the watchmaking industry: over the years, it has evolved into a versatile and truly European research and technology hub ‒ and above all, a valuable partner for universities and industry partners in Switzerland and beyond. CSEM, a nonprofit organization, now employs more than 500 researchers and engineers who focus on a vast range of application areas: renewable energies, biomedical technology, microsystems, industrial automation, quantum and laser technologies as well as scientific instrumentation ‒ including the development of new technologies for space applications such as additive manufacturing, compliant mechanisms, and magnetically levitated actuators.

Advances in the development of innovative space technologies

In the field of space technology, CSEM has been a partner of the European Space Agency (ESA) for many years. One focus of their joint research ‒ which is also part of ESA's mid-term strategy ‒ is the elimination of vibration emissions originating from components aboard satellites. As well as limiting the precision of attitude control for satellites, these micro-vibrations lead to higher energy consumption and (in case of imaging missions) cause deterioration of image quality.

There are different ways to counter unwanted vibrations either at the source or the payload. As part of its exploration of different approaches, CSEM currently has several projects focusing on numerical models, active-passive mitigation, and algorithm-based notching. In one of these projects, CSEM and its partners are working with an innovative technology based on magnetic levitation. Leopoldo Rossini, who heads the micro-vibration facility at CSEM, reports: “With support from Kistler measurement technology, we examined a reaction wheel prototype with a magnetic bearing. This technology from Celeroton, a Swiss company, offers many advantages such as no friction, a virtually infinite lifetime, the possibility of actively suppressing unwanted vibrations by control, and the opportunity to achieve higher performance at higher speeds.”

Advanced satellite components with low vibrations

The CSEM engineers use a measuring chain from Kistler to examine the vibrations of the reaction wheel prototype. The custom dynamometer comprises four 3-component force sensors sandwich-mounted between two steel plates ‒ a design that achieves maximum mechanical stiffness (see the image). This measuring instrument is mounted on a granite block suspended over four pneumatic isolators so that environmental influences are eliminated as far as possible. Because the micro-vibrations occur in the millinewton range, a highly sensitive measuring chain with very low noise is required. As well as the reaction wheel, various actuators such as a stepper motor and a cryo-cooler can be placed on the instrumentation table to perform the desired measurements.

In the case of the magnetically levitated reaction wheel prototype, the speed range from ‒20,000 to 20,000 rpm was covered: this allowed full characterization of the effectiveness of a multiple-harmonic force rejection algorithm capable of suppressing the main vibrations generated during operation. “The lack of physical contact due to magnetic levitation opens up some very interesting opportunities,” according to Guzmán Borque Gallego, an R&D Engineer at CSEM. “It leaves us almost free to position the rotor in such a way that the vibrations are minimized ‒ for instance, by letting the rotor rotate about its main axis of inertia to suppress any vibration related to the rotor unbalance, which reduces these emissions to near zero.”

The equipment from Kistler is ideal, and it provided us with results of very high quality.

Guzmán Borque Gallego, R&D Engineer at CSEM

 

Accurate real-time measurements enable closed-loop control

Borque Gallego continues: “We're measuring rather small forces in the millinewton range ‒ but even in micronewtons, we can still see differences. This allows comfortable judgement of all the measurements, leading to high-quality data in the process.” Data acquisition is handled by a rapid prototyping system at 20 kHz and thanks to the accurate measurements, the effect of the control algorithm can be clearly identified (see the diagrams). Rossini adds: “We received positive feedback about the high quality of the measurements from partners and customers who have extensive experience with this kind of data. None of this would have been possible without support from Kistler: Application Specialist Reinhard Bosshard assisted us in many ways, for example by helping us to choose the right equipment to complete the optimal measuring chain.”

Although the researchers initially intended to use the modern LabAmp 5167A with a digital output, they finally opted for the 5080A charge amplifier from Kistler, which allows even more accurate measurements thanks to its very low-noise input stage. “We're pleased to have new Kistler technology here, because our partners at ESA and in Germany also use it for qualification purposes,” Rossini adds. “This equipment is very robust and did not break down even when stressed beyond the given constraints. Now that it has proven its abilities, we will definitely use it for future projects in the field of vibration characterization ‒ where we already operate accelerometers from Kistler.”

Best possible preparation for the long journey into space

How is the magnetic bearing reaction wheel technology developed by CSEM, Celeroton AG, and their partner in Germany likely to evolve? And will it soon be launched into space? “The advantages of magnetic bearing reaction wheels are obvious: they can generate far lower vibrations and rotate faster than conventional wheels ‒ which means improved performance as well as reduced size and weight. And thanks to the absence of friction, there is no wear and the wheel's lifetime is virtually unlimited,” Borque Gallego emphasizes. “This is a fascinating project, and we hope to move ahead to the next steps: practical use, testing, and maybe even validation together with our partners.”

11/04/2022
On the road to success with IEPE and MEMS accelerometers for the ISTAR research aircraft – on the ground and in the air.
14/01/2022
KiTraffic Statistics delivers precise WIM data for a railway bridge in central Austria
18/11/2021
Advanced fastener testing with ANALYSE systems for reliable zink flake coatings in the automotive and wind turbine industries
12/10/2021
How Yuchai achieves more precision, transparency and resource efficiency for its production of engines conform to China VI
14/09/2021
A high precision measuring chain with dynamometer, laboratory charge amplifier and software enables objective comparison tests.
09/09/2021
SRA: Find the best spot and the ideal sensor layout for direct enforcement of overloaded vehicles.
03/09/2021
At Estudio de la Pisada in Valencia, a 3D force plate helps podiatry experts to develop treatments and orthoses for patients and athletes.
02/07/2021
Two IEPE accelerometers deliver key data for propulsion validation and optimization of flight characteristics even in the stratosphere
22/06/2021
Capturing micro-vibrations with a dynamometer leads to improved satellite technology
02/06/2021
Zero defect despite high volumes: this is the way quality assurance with Kistler test automation systems works for zinc die casting parts
26/04/2021
A digitally driven brake force measurement system makes the life of service technicians for train maintenance much easier
13/04/2021
Inside "The Atmosphere" at MARIN, 100 of our pressure sensors capture wave impacts under varying environmental conditions
22/03/2021
How MAN Energy Solutions is using sensors from Kistler to make its gas turbines fit for the future
08/02/2021
Measurement technology dedicated to the discipline and biomechanics of pole vault enables high performances
05/10/2020
How does a digital measuring chain for piezoelectric sensors work as part of a complex vehicle test stand?
18/09/2020
Convincing test results: The Ohio Department of Transportation goes on to apply Lineas from Kistler for traffic monitoring.
20/08/2020
Precision is the key to top performance: how measurement technology from Kistler supports the development team at EMUGE-FRANKEN
22/07/2020
Quality assurance solutions by Kistler like ComoNeo ensure highest accuracy at TSP Precision Tooling in Shanghai.
09/06/2020
Kistler supports Ceratizit in the development of HDT. This enables complex geometries to be produced with just one tool.
15/11/2019
Process monitoring systems and cavity pressure sensors from Kistler help to reduce the amount of scrap drastically
23/10/2019
How measurement technology from Kistler contributes toward boosting high-end powertools' quality
15/08/2019
How the ANALYSE system from Kistler is enhancing safety and transparency in the field of fastening technology
17/07/2019
Turkey opts for weight enforcement with WIM technology from Kistler
24/06/2019
For the next manned flight to the moon: safety that can be measured
20/06/2019
Segregation of good and bad parts every 1.5 seconds: process monitoring with Kistler enables high quality for over 5 million parts per year.
14/05/2019
In order to achieve excellent quality for its components and medical devices, Tessy Plastics chose sensors and solutions from Kistler.
18/04/2019
A renowned manufacturer of electrical appliances trusts testing and sorting systems by Vester to improve its quality.
02/04/2019
NFL's Jaguars boost their fitness levels with Kistler.
25/03/2019
By using process monitoring from Kistler, not only the assembly of electric fuses is validated, but even the function of the sensors itself.
18/03/2019
How to determine the fitness level of an athlete efficiently? A practical report on the Quattro Jump force plate system from Kistler.
17/12/2018
Thanks to precise Weigh in Motion technology from Kistler, Hungary's roads are sustainably protected against overloaded vehicles.
27/11/2018
Bang&Clean relies on Kistler's precise measurement of ignition processes and pressure wave propagation
10/10/2018
Sartorius applies the process monitoring system ComoNeo from Kistler and thereby increases the process quality during injection molding
08/10/2018
The Dortmund Technical University tests the new MicroDyn 9109AA cutting force dynamometer from Kistler and breaks new ground for developing its micromachining processes.
31/08/2018
The ZF company operates a software-controlled Kistler fastener test bench with an integrated vibration unit.
14/08/2018
BIG Daishowa, headquartered in Osaka, Japan, is one of the leading producers of tool holders for the machining industry. Each year the company produces over half a million collet chucks. Their products are developed using, among other resources, Kistler’s cutting force measuring device.
16/07/2018
Enhanced quality and efficiency in mobile crane manufacture – thanks to the test stand for torque tools by Kistler
11/04/2018
The world’s largest provider of rail transport technology relies on Kistler’s measurement expertise. Thanks to the only crash wall of its kind in the world, the impact forces of the trains and their components can be precisely measured and analyzed.
14/11/2017
In the development of cooling lubricants, Blaser Swisslube relies on Kistler's measurement expertise.
11/08/2017
Applus IDIADA relies on DTI in-dummy technology from Kistler for Test Device for Human Occupant Restraint (THOR).
04/01/2017
Road safety is a central topic in vehicle development. Through accurate measurements, Kistler helps increase the chance of survival in crashes.
22/12/2016
Kistler makes progress in vehicle development possible
22/12/2016
Kistler Sensor Correvit® SFII measures world record
20/12/2016
Kistler sensors deliver a maximum in data quality under any conditions.
07/11/2016
Kistler pressure sensors enabled the Rosetta space probe to fly for 6.4 billion kilometers.
05/10/2016
Since the end of 2015 FC Basel is using Kistler force plates to reduce the dropout of young talents.
17/08/2016
Kistler makes the difference in the crucial sports moments with its Performance Analysis System for Swimming.
19/02/2016
Determination of Pump Efficiency with Kistler KiTorq Measuring Flange System
04/11/2015
Piezoelectric Measurements with CompactRIO™
08/05/2015
Quality Assurance in the Automotive Industry
02/03/2015
How Brose improves the quality of its two-component production and automatically separates defective parts
02/12/2014
The Kistler Group pursues a growth policy that is both ambitious and sustainable – and strategic acquisitions are one of its core elements. ‘Strategic’ means that Kistler deliberately selects companies which can achieve more together with Kistler than they ever could by continuing alone. The takeover of Dr. Staiger Mohilo & Co. GmbH in 2006 enabled Kistler to grow jointly with the acquired company...
02/12/2014
After a ten-year voyage, the Rosetta space probe's Philae landing module finally touched down on the surface of comet ‘Chury’.
23/08/2011
HEWI and its Customers Benefit from Cavity Pressure Technology
15/02/2011
End-to-end process monitoring for critical medical moldings
07/02/2011
Cavity pressure measurement eliminates short shots at Fischer GmbH & Co KG of Sinsheim/Germany
Contact
Max 25 MB