Kistler enables digital measuring chains for advanced vehicle test stands

Faced with the challenge of modernizing its kinematics and compliance test machine for automotive engineering, AB Dynamics implemented the new digital charge amplifier 5074A from Kistler. It enables a fully digital measuring chain including a set of load cells to measure tire forces and moments in real time, no matter how complex the requirements might be.

Today's cars are high-powered technology hubs, packed with mechatronic components that deliver ever-increasing levels of driver assistance; they can even perform some maneuvers autonomously. However, impressive features and functions such as these need to be supported by comprehensive testing with specialized equipment, backed by specific know-how. One leading provider of these resources is Anthony Best Dynamics Limited, a British company based in the picturesque town of Bradford on Avon in south-western England. It is a member of the international AB Dynamics Group, which offers a portfolio of solutions for measurement and analysis systems, simulation, and proving ground automation.

“We went through a period of rapid growth in recent years, so our new headquarters here in Bradford on Avon has already become too small,” says Joanna Maddams, Marketing Manager at AB Dynamics. “That's why we're currently adding another new building opposite our head office. Our worldwide headcount has increased from about 70 back in 2015 to more than 200 today. We also have a network of offices in Europe, Japan and the USA that handle the distribution of our validation and durability solutions to many automotive OEMs, suppliers and vehicle test centers across the globe.”

Seamless integration into a state-of-the-art machine design

Matthew Dustan, Product Manager for Laboratory Test Systems at AB Dynamics, singles out some current trends in automotive testing: “Progress in testing Advanced Driver Assistance Systems (ADAS) has triggered higher demand for complex track test solutions and is generating some exciting opportunities for proving ground automation. There is also a move towards simulation in vehicle development and modeling ‒ this is particularly apparent with new electric vehicle manufacturers.”

Many vehicle developers throughout the world operate one of AB Dynamics' leading solutions: the Suspension Parameter Measuring Machine (SPMM), a complex test stand that can simulate a car's behavior by applying combined roll, pitch, bounce, and yaw motions on a moving platform. Under each of the four wheel stations, a multicomponent force link set of piezoelectric load cells ensures accurate measurement of all forces and moments: the 9366CC series from Kistler is a customizable kit with four sensing elements that deliver maximum accuracy thanks to their high rigidity and natural frequency. “Load cells from Kistler have always played a key part in the success of this product, and they are highly integrated into the overall system. They deliver zero values at high resolution when the vehicle is mounted on the test stand, and they also provide very precise measurements of all the specific high-load forces applied during kinematics and compliance testing. And by no means least, they help to prevent overloading and potential damage,” Dustan explains.

Faced with the growing complexity of automotive testing, the engineers at AB Dynamics wanted to digitize the entire SPMM system to provide higher bandwidth for advanced testing requirements in the future. “Our goal was to create an updated SPMM with a fully digital measuring chain and a closed-loop force control system,” Dustan continues.

It took us about two years to complete this development project, and the digital charge amplifier from Kistler was crucial to its success.”

Matthew Dustan, Product Manager Laboratory Test Systems at AB Dynamics

 

In the new SPMM 5000e, the signals from every wheel station are digitized by two 5074A digital charge amplifiers (each with four channels); they form part of a distributed EtherCAT topology that delivers live force readings at high frequencies.

“We're currently running a 2 kHz cycle on our machine, but the Kistler amplifier is capable of doing even more ‒ the bottleneck is elsewhere,” Dustan explains. “We plan to go to 4 kHz in the near future. We've also reduced the size of the electrical cabinet by about 40 percent; the machine now requires much less cabling and wiring, and far less installation effort. It comes with advantages such as high bandwidth, low latency and resilience to drift even in humid environments ‒ to mention only a few.” AB Dynamics has already delivered its new state-of-the-art solution to several customers in Europe and Asia.

Real-time force and moment measurements: precise, robust and high-resolution

One outstanding advantage of the 5074A digital amplifier from Kistler is its switchable measuring range. This allows precise measurements covering almost five decades of amplitude, providing greater flexibility for many applications. It is also a practical instrument for optimizing the measuring chain: “The measurement range setting can be used to individually adapt the optimal load capability and resolution. Using the 16-bit signals, we can start out by estimating the load and then make adjustments based on the first measurement data,” Dustan explains. This process results in high data quality ‒ a critical factor for AB Dynamics' customers, who use the data to inform their design decisions throughout the entire vehicle development process.

Dustan sums up the collaboration between the two companies: “We couldn't have completed the new machine without the digital charge amplifier from Kistler. It allowed us to run a closed-loop force control at high frequencies and also ‒ thanks to the amplifier's form factor ‒ we were able to package the complete measuring chain locally into sections of the machine. What's more, Kistler customized the load cells to ensure smooth integration into the new setup. In short, they provided exactly what you'd expect from a market leader: innovative products and custom solutions.”

Innovative, customized solutions that push the limits of automotive testing

How will the automotive testing market evolve over the next decade? According to Matthew Dustan: “Vehicles are generally becoming more complex and computerized ‒ and for testing, that presents challenges as well as opportunities. We're seeing a strong push towards simulation and electrification to improve vehicle behavior and ADAS support. Simulation, in particular, is data-driven ‒ so good measuring equipment is more critical than ever before as a factor in generating added-value data sets. After 25 years of working with Kistler solutions, we're now developing a new type of test stand for axle suspension NVH analysis that will also include accelerometers specifically designed by Kistler to accomplish these measurement tasks.”

04/05/2022
Daimler Buses relies on MaDaM and jBEAM to further develop of its electric city buses.
11/04/2022
On the road to success with IEPE and MEMS accelerometers for the ISTAR research aircraft – on the ground and in the air.
14/01/2022
KiTraffic Statistics delivers precise WIM data for a railway bridge in central Austria
18/11/2021
Advanced fastener testing with ANALYSE systems for reliable zink flake coatings in the automotive and wind turbine industries
12/10/2021
How Yuchai achieves more precision, transparency and resource efficiency for its production of engines conform to China VI
14/09/2021
A high precision measuring chain with dynamometer, laboratory charge amplifier and software enables objective comparison tests.
09/09/2021
SRA: Find the best spot and the ideal sensor layout for direct enforcement of overloaded vehicles.
03/09/2021
At Estudio de la Pisada in Valencia, a 3D force plate helps podiatry experts to develop treatments and orthoses for patients and athletes.
02/07/2021
Two IEPE accelerometers deliver key data for propulsion validation and optimization of flight characteristics even in the stratosphere
22/06/2021
Capturing micro-vibrations with a dynamometer leads to improved satellite technology
02/06/2021
Zero defect despite high volumes: this is the way quality assurance with Kistler test automation systems works for zinc die casting parts
26/04/2021
A digitally driven brake force measurement system makes the life of service technicians for train maintenance much easier
13/04/2021
Inside "The Atmosphere" at MARIN, 100 of our pressure sensors capture wave impacts under varying environmental conditions
22/03/2021
How MAN Energy Solutions is using sensors from Kistler to make its gas turbines fit for the future
08/02/2021
Measurement technology dedicated to the discipline and biomechanics of pole vault enables high performances
05/10/2020
How does a digital measuring chain for piezoelectric sensors work as part of a complex vehicle test stand?
18/09/2020
Convincing test results: The Ohio Department of Transportation goes on to apply Lineas from Kistler for traffic monitoring.
20/08/2020
Precision is the key to top performance: how measurement technology from Kistler supports the development team at EMUGE-FRANKEN
22/07/2020
Quality assurance solutions by Kistler like ComoNeo ensure highest accuracy at TSP Precision Tooling in Shanghai.
09/06/2020
Kistler supports Ceratizit in the development of HDT. This enables complex geometries to be produced with just one tool.
15/11/2019
Process monitoring systems and cavity pressure sensors from Kistler help to reduce the amount of scrap drastically
23/10/2019
How measurement technology from Kistler contributes toward boosting high-end powertools' quality
15/08/2019
How the ANALYSE system from Kistler is enhancing safety and transparency in the field of fastening technology
17/07/2019
Turkey opts for weight enforcement with WIM technology from Kistler
24/06/2019
For the next manned flight to the moon: safety that can be measured
20/06/2019
Segregation of good and bad parts every 1.5 seconds: process monitoring with Kistler enables high quality for over 5 million parts per year.
14/05/2019
In order to achieve excellent quality for its components and medical devices, Tessy Plastics chose sensors and solutions from Kistler.
18/04/2019
A renowned manufacturer of electrical appliances trusts testing and sorting systems by Vester to improve its quality.
02/04/2019
NFL's Jaguars boost their fitness levels with Kistler.
25/03/2019
By using process monitoring from Kistler, not only the assembly of electric fuses is validated, but even the function of the sensors itself.
18/03/2019
How to determine the fitness level of an athlete efficiently? A practical report on the Quattro Jump force plate system from Kistler.
17/12/2018
Thanks to precise Weigh in Motion technology from Kistler, Hungary's roads are sustainably protected against overloaded vehicles.
27/11/2018
Bang&Clean relies on Kistler's precise measurement of ignition processes and pressure wave propagation
10/10/2018
Sartorius applies the process monitoring system ComoNeo from Kistler and thereby increases the process quality during injection molding
08/10/2018
The Dortmund Technical University tests the new MicroDyn 9109AA cutting force dynamometer from Kistler and breaks new ground for developing its micromachining processes.
31/08/2018
The ZF company operates a software-controlled Kistler fastener test bench with an integrated vibration unit.
14/08/2018
BIG Daishowa, headquartered in Osaka, Japan, is one of the leading producers of tool holders for the machining industry. Each year the company produces over half a million collet chucks. Their products are developed using, among other resources, Kistler’s cutting force measuring device.
16/07/2018
Enhanced quality and efficiency in mobile crane manufacture – thanks to the test stand for torque tools by Kistler
11/04/2018
The world’s largest provider of rail transport technology relies on Kistler’s measurement expertise. Thanks to the only crash wall of its kind in the world, the impact forces of the trains and their components can be precisely measured and analyzed.
14/11/2017
In the development of cooling lubricants, Blaser Swisslube relies on Kistler's measurement expertise.
11/08/2017
Applus IDIADA relies on DTI in-dummy technology from Kistler for Test Device for Human Occupant Restraint (THOR).
04/01/2017
Road safety is a central topic in vehicle development. Through accurate measurements, Kistler helps increase the chance of survival in crashes.
22/12/2016
Kistler makes progress in vehicle development possible
22/12/2016
Kistler Sensor Correvit® SFII measures world record
20/12/2016
Kistler sensors deliver a maximum in data quality under any conditions.
07/11/2016
Kistler pressure sensors enabled the Rosetta space probe to fly for 6.4 billion kilometers.
05/10/2016
Since the end of 2015 FC Basel is using Kistler force plates to reduce the dropout of young talents.
17/08/2016
Kistler makes the difference in the crucial sports moments with its Performance Analysis System for Swimming.
19/02/2016
Determination of Pump Efficiency with Kistler KiTorq Measuring Flange System
04/11/2015
Piezoelectric Measurements with CompactRIO™
08/05/2015
Quality Assurance in the Automotive Industry
02/03/2015
How Brose improves the quality of its two-component production and automatically separates defective parts
02/12/2014
The Kistler Group pursues a growth policy that is both ambitious and sustainable – and strategic acquisitions are one of its core elements. ‘Strategic’ means that Kistler deliberately selects companies which can achieve more together with Kistler than they ever could by continuing alone. The takeover of Dr. Staiger Mohilo & Co. GmbH in 2006 enabled Kistler to grow jointly with the acquired company...
02/12/2014
After a ten-year voyage, the Rosetta space probe's Philae landing module finally touched down on the surface of comet ‘Chury’.
23/08/2011
HEWI and its Customers Benefit from Cavity Pressure Technology
15/02/2011
End-to-end process monitoring for critical medical moldings
07/02/2011
Cavity pressure measurement eliminates short shots at Fischer GmbH & Co KG of Sinsheim/Germany
Contact
Max 25 MB