Force plates – a Spanish foot clinic puts its trust in Kistler technology

At Estudio de la Pisada in Valencia, it's all about feet: the podiatrists at this clinic analyze patients' symptoms, develop treatments and advise athletes on performance diagnostics with the help of state-of-the-art technologies – including a piezoelectric force plate from Kistler to record moments and ground reaction forces.

We're on our feet throughout our lifetimes – but we rarely pay any particular attention to them. At Estudio de la Pisada in Valencia (Spain), however, everything revolves around feet: for over 30 years, this clinic has focused intensively on podiatry and orthopedic foot care. The team is headed by two specialists: José Manuel Bru Lázaro, an expert in motion analysis and clinical biomechanics, and José Manuel Bru Juanes, a podiatrist and foot surgeon. They treat patients suffering from a wide variety of disorders such as metatarsalgia (midfoot pain), fallen arches, splayfoot and plantar fasciitis (inflammation of the sole). With the help of force plates from Kistler, the clinic also analyses pathologies that originate from parts of the body other than the feet, including Achilles tendinitis, medial tibial stress syndrome (MTSS) and other overuse reactions such as dysfunctions of the tensor fasciae latae muscle (TFL), which often occur in athletes.

The two experts make use of numerous advanced technologies as well as various diagnostic and data acquisition systems to track down the causes of these disorders and develop effective ways to treat them – mostly involving physiotherapy combined with inserts, or by performing surgery in more serious cases. Complete individual inserts and orthotic devices are also produced at Estudio de la Pisada with the help of cutting-edge laser technologies.

Accurate data acquisition makes diagnostics easier

3D force plate from Kistler has proven particularly effective for analyses of complex movement sequences – especially those that go beyond disorders of the feet as such.

We set high standards for our work, and we like to collect as much information as possible for a diagnosis. That’s why we opted for one of the systems from Kistler, which are regarded as the gold standard on the market."

José Manuel Bru Lázaro, expert in motion analysis and clinical biomechanics

 

The force plate can be used to perform numerous tests and evaluations in order to collect patients' kinetic and kinematic data. "In most cases, we use the force plate together with an optical acquisition system – and that generates some useful synergies. With this combination, for instance, we can calculate the resultant moments as well as the strength and direction of the forces that the muscle groups must apply so as to balance out certain moments," Bru Lázaro continues.

The piezoelectric technology incorporated into the force plates allows very precise acquisition of dynamic processes. In combination with high-performance visualization and data processing software, this technology also provides users with accurate knowledge of the measurands and parameters involved. Performance analysis during rehabilitation is just one example where the solution from Kistler measures moments and ground reaction forces as well as calculating overall performance. "This data is very helpful for us – we can use it to determine key parameters such as efficiency, energy recovery and energy consumption while walking or running," Bru Lázaro points out.

The results obtained from a 3D force plate are also very valuable in connection with orthotics. Usually made of silicone, orthotic inserts are used to relieve pressure, correct posture, and mobilize joints. However, podiatrists generally regard it as difficult to obtain objective scientific proof that orthoses are effective, as foot specialist and surgeon Bru Juanes explains: "It's very challenging to get reliable results about this, because no two feet are identical – and there are no identical stride patterns, either. But thanks to the system from Kistler, we can accurately measure and understand the changes that take place in each individual patient."

Relieving pain and preventing operations

This case history shows what happens in practice: a patient came to the podiatry clinic in Valencia with problems affecting both his knees. In particular, he complained of such severe medial knee pain that he had already considered surgery. The preliminary examination revealed that he had multiple imbalances and tensions in various muscle groups. In addition, the patient had a very stiff hollow foot ("pes cavus") and his forefoot was turned inward ("metatarsus adductus"); he was also suffering from stresses in his shin (tibia) and instabilities in both knees. 

"Our first goal was to locate the applied muscular forces. To do this, we used our Kistler force plate in combination with Motion Capture, as usual," Bru Juanes recalls. "Then we instrumented the patient with 22 markers to track down any kinetic and kinematic compensations." With the help of the data they obtained, the specialists at Estudio de la Pisada could prepare orthoses to reduce the adduction forces in the knee – and thus lessen the pain. Following an analysis of movement patterns, the next step was to draw up a rehabilitation plan: based on physiotherapy, this helped the patient to experience less pain and improve his quality of life without resorting to an operation.

Summing up, Bru Juanes comments: "Successes like these are only possible with the help of accurate and fit-for-purpose diagnostic instruments. The force measurement platform from Kistler proves its worth during regular use in our podiatry clinic – not only for treatments in the stricter sense, but also for analyses aimed at improving sports performance and preventing injuries. What's more, we can even use certain exercises for detailed evaluations of muscles – to determine fiber composition, elasticity and fatigue, myotatic reflex and other characteristics."

11/04/2022
On the road to success with IEPE and MEMS accelerometers for the ISTAR research aircraft – on the ground and in the air.
14/01/2022
KiTraffic Statistics delivers precise WIM data for a railway bridge in central Austria
18/11/2021
Advanced fastener testing with ANALYSE systems for reliable zink flake coatings in the automotive and wind turbine industries
12/10/2021
How Yuchai achieves more precision, transparency and resource efficiency for its production of engines conform to China VI
14/09/2021
A high precision measuring chain with dynamometer, laboratory charge amplifier and software enables objective comparison tests.
09/09/2021
SRA: Find the best spot and the ideal sensor layout for direct enforcement of overloaded vehicles.
03/09/2021
At Estudio de la Pisada in Valencia, a 3D force plate helps podiatry experts to develop treatments and orthoses for patients and athletes.
02/07/2021
Two IEPE accelerometers deliver key data for propulsion validation and optimization of flight characteristics even in the stratosphere
22/06/2021
Capturing micro-vibrations with a dynamometer leads to improved satellite technology
02/06/2021
Zero defect despite high volumes: this is the way quality assurance with Kistler test automation systems works for zinc die casting parts
26/04/2021
A digitally driven brake force measurement system makes the life of service technicians for train maintenance much easier
13/04/2021
Inside "The Atmosphere" at MARIN, 100 of our pressure sensors capture wave impacts under varying environmental conditions
22/03/2021
How MAN Energy Solutions is using sensors from Kistler to make its gas turbines fit for the future
08/02/2021
Measurement technology dedicated to the discipline and biomechanics of pole vault enables high performances
05/10/2020
How does a digital measuring chain for piezoelectric sensors work as part of a complex vehicle test stand?
18/09/2020
Convincing test results: The Ohio Department of Transportation goes on to apply Lineas from Kistler for traffic monitoring.
20/08/2020
Precision is the key to top performance: how measurement technology from Kistler supports the development team at EMUGE-FRANKEN
22/07/2020
Quality assurance solutions by Kistler like ComoNeo ensure highest accuracy at TSP Precision Tooling in Shanghai.
09/06/2020
Kistler supports Ceratizit in the development of HDT. This enables complex geometries to be produced with just one tool.
15/11/2019
Process monitoring systems and cavity pressure sensors from Kistler help to reduce the amount of scrap drastically
23/10/2019
How measurement technology from Kistler contributes toward boosting high-end powertools' quality
15/08/2019
How the ANALYSE system from Kistler is enhancing safety and transparency in the field of fastening technology
17/07/2019
Turkey opts for weight enforcement with WIM technology from Kistler
24/06/2019
For the next manned flight to the moon: safety that can be measured
20/06/2019
Segregation of good and bad parts every 1.5 seconds: process monitoring with Kistler enables high quality for over 5 million parts per year.
14/05/2019
In order to achieve excellent quality for its components and medical devices, Tessy Plastics chose sensors and solutions from Kistler.
18/04/2019
A renowned manufacturer of electrical appliances trusts testing and sorting systems by Vester to improve its quality.
02/04/2019
NFL's Jaguars boost their fitness levels with Kistler.
25/03/2019
By using process monitoring from Kistler, not only the assembly of electric fuses is validated, but even the function of the sensors itself.
18/03/2019
How to determine the fitness level of an athlete efficiently? A practical report on the Quattro Jump force plate system from Kistler.
17/12/2018
Thanks to precise Weigh in Motion technology from Kistler, Hungary's roads are sustainably protected against overloaded vehicles.
27/11/2018
Bang&Clean relies on Kistler's precise measurement of ignition processes and pressure wave propagation
10/10/2018
Sartorius applies the process monitoring system ComoNeo from Kistler and thereby increases the process quality during injection molding
08/10/2018
The Dortmund Technical University tests the new MicroDyn 9109AA cutting force dynamometer from Kistler and breaks new ground for developing its micromachining processes.
31/08/2018
The ZF company operates a software-controlled Kistler fastener test bench with an integrated vibration unit.
14/08/2018
BIG Daishowa, headquartered in Osaka, Japan, is one of the leading producers of tool holders for the machining industry. Each year the company produces over half a million collet chucks. Their products are developed using, among other resources, Kistler’s cutting force measuring device.
16/07/2018
Enhanced quality and efficiency in mobile crane manufacture – thanks to the test stand for torque tools by Kistler
11/04/2018
The world’s largest provider of rail transport technology relies on Kistler’s measurement expertise. Thanks to the only crash wall of its kind in the world, the impact forces of the trains and their components can be precisely measured and analyzed.
14/11/2017
In the development of cooling lubricants, Blaser Swisslube relies on Kistler's measurement expertise.
11/08/2017
Applus IDIADA relies on DTI in-dummy technology from Kistler for Test Device for Human Occupant Restraint (THOR).
04/01/2017
Road safety is a central topic in vehicle development. Through accurate measurements, Kistler helps increase the chance of survival in crashes.
22/12/2016
Kistler makes progress in vehicle development possible
22/12/2016
Kistler Sensor Correvit® SFII measures world record
20/12/2016
Kistler sensors deliver a maximum in data quality under any conditions.
07/11/2016
Kistler pressure sensors enabled the Rosetta space probe to fly for 6.4 billion kilometers.
05/10/2016
Since the end of 2015 FC Basel is using Kistler force plates to reduce the dropout of young talents.
17/08/2016
Kistler makes the difference in the crucial sports moments with its Performance Analysis System for Swimming.
19/02/2016
Determination of Pump Efficiency with Kistler KiTorq Measuring Flange System
04/11/2015
Piezoelectric Measurements with CompactRIO™
08/05/2015
Quality Assurance in the Automotive Industry
02/03/2015
How Brose improves the quality of its two-component production and automatically separates defective parts
02/12/2014
The Kistler Group pursues a growth policy that is both ambitious and sustainable – and strategic acquisitions are one of its core elements. ‘Strategic’ means that Kistler deliberately selects companies which can achieve more together with Kistler than they ever could by continuing alone. The takeover of Dr. Staiger Mohilo & Co. GmbH in 2006 enabled Kistler to grow jointly with the acquired company...
02/12/2014
After a ten-year voyage, the Rosetta space probe's Philae landing module finally touched down on the surface of comet ‘Chury’.
23/08/2011
HEWI and its Customers Benefit from Cavity Pressure Technology
15/02/2011
End-to-end process monitoring for critical medical moldings
07/02/2011
Cavity pressure measurement eliminates short shots at Fischer GmbH & Co KG of Sinsheim/Germany
Contact
Max 25 MB