Efficient diagnostics: accurate jump force measurements are the key

Smarter training for success with the MARS force plate system from Kistler

In today's professional sports world, the margin between winning and losing is razor-thin. Athletes need intensive, in-depth preparation so they can realize their full potential. Top performance and successful competition results depend on training programs that are monitored and individually adapted to maximize the benefit for each athlete. Keeping players at the peak of fitness is a key concern for the strength and conditioning staff at the Jacksonville Jaguars, a professional American football team in the National Football League (NFL). The Jaguars recently needed a new, solid foundation for an effective return-to-play (RTP) protocol. The solution: they added the MARS force plate system from Kistler to their training program and it quickly became a vital factor in the team's success. As well as making the playoffs for the first time in 10 years, the Jaguars also won the AFC South Championship in 2017.

The MARS force plate system from Kistler is a highly effective solution for monitoring athletes' performance and preventing injuries. To secure a winning edge over their competitors in the NFL, the Jacksonville Jaguars' strength and conditioning staff faced a difficult challenge: how to maintain a healthy roster during training camp, in-season, post bye-week, and even offseason? They realized that improved understanding of each player's unique needs is the key to keeping athletes healthy. This calls for intelligent performance analysis equipment that can map and quantify lower limb symmetry, highlighting differences between an athlete's right and left legs. Once the Jaguars had added the MARS force plate system to their strength and conditioning program, the benefits quickly became clear: now, the coaching staff can draw on reliable research and test results to adapt their training methods, boost athletic performance, prevent injuries and make better-informed return-to-play decisions. Thanks to their high precision and long-term stability, the force plates can detect even the slightest changes in an athlete's performance. Aided by this intuitive data acquisition system, the coaching staff collect accurate and reliable biometric measurement results as the basis for analyzing and evaluating each athlete's power, strength, balance, and stability.

Staying ahead of the game with strength and conditioning solutions

The Jaguars are constantly researching innovative methods of monitoring and evaluating their athletes throughout the year. Once the team's strength and conditioning staff became aware of the MARS force plate system from Kistler, they were quick to implement it in their training program. Tom Myslinski, the Jacksonville Jaguars' Strength and Conditioning Coach, explained how the system functions in a report in Men's Journal: "When each athlete jumps on the force plate, they have a movement signature; and from that jump, we can customize the athlete even further," says Myslinski. "We can see if he's more dominant anteriorly or posterially, and how he looks while jumping." The Jaguars' new training protocol gave them many advantages: the MARS force plate system by Kistler made it easy to identify and correct inconsistencies with the help of fast, precision-tailored performance analysis.

We first heard about Kistler by word of mouth; after some basic research, we found that their force plate was rated as the best on the market. The Kistler force plate is backed by 50 years of research, and it can measure in all three orthogonal directions.”

Tom Myslinski, Strength and Conditioning Coach

 

Based on his extensive experience, Strength and Conditioning Coach Tom Myslinski rates the MARS force plate system above all competitor products on the market. In his view, the MARS platform delivers rapid, targeted biometric evaluations of performance, force, balance, and stability. "We first heard about Kistler by word of mouth; after some basic research, we found that their force plate was rated as the best on the market. The force plate from Kistler is backed by 50 years of research, and it can measure in all three orthogonal directions," Myslinski says. Adaptability is another critical factor. "This is the perfect system for our needs, because we can perform both single-leg and bilateral counter-movement jumps (hopping on one leg), that provide information about jumping, power, balance and stability for each athlete," Myslinski adds.

To prepare their players for a successful season, the Jacksonville Jaguars set two key goals: more effective development of their athletes' performance, and prevention of injuries by identifying inefficiencies due to muscular imbalance and chronic pain. Data supplied by the force plate made it possible to map and quantify each athlete's strength. Myslinski explains: "During the season when we are playing each and every week, we can reassess our athletes every month and compare them to their baseline. This information allows our staff to make real-time changes when athletes return to play after an injury, and they can also detect discrepancies between the right and left legs - not only for injured athletes, but for healthy players as well." 

The initial response to testing and data analysis with the MARS force plate system was highly favorable: at last, the coaches had a clear understanding of their athletes' power and limb symmetry. "For instance, we went from measuring just unilateral jumps to countermovement jumps and then squat jumps," Myslinski points out. "We're excited to be working with Kistler as our partner," he adds. "We have an easy working relationship with them, and we're impressed by their service. Now, our team can collect data with the force plate, analyze it with the MARS software and use that information to redesign each athlete's strength program," Myslinski concludes. 

11/04/2022
On the road to success with IEPE and MEMS accelerometers for the ISTAR research aircraft – on the ground and in the air.
14/01/2022
KiTraffic Statistics delivers precise WIM data for a railway bridge in central Austria
18/11/2021
Advanced fastener testing with ANALYSE systems for reliable zink flake coatings in the automotive and wind turbine industries
12/10/2021
How Yuchai achieves more precision, transparency and resource efficiency for its production of engines conform to China VI
14/09/2021
A high precision measuring chain with dynamometer, laboratory charge amplifier and software enables objective comparison tests.
09/09/2021
SRA: Find the best spot and the ideal sensor layout for direct enforcement of overloaded vehicles.
03/09/2021
At Estudio de la Pisada in Valencia, a 3D force plate helps podiatry experts to develop treatments and orthoses for patients and athletes.
02/07/2021
Two IEPE accelerometers deliver key data for propulsion validation and optimization of flight characteristics even in the stratosphere
22/06/2021
Capturing micro-vibrations with a dynamometer leads to improved satellite technology
02/06/2021
Zero defect despite high volumes: this is the way quality assurance with Kistler test automation systems works for zinc die casting parts
26/04/2021
A digitally driven brake force measurement system makes the life of service technicians for train maintenance much easier
13/04/2021
Inside "The Atmosphere" at MARIN, 100 of our pressure sensors capture wave impacts under varying environmental conditions
22/03/2021
How MAN Energy Solutions is using sensors from Kistler to make its gas turbines fit for the future
08/02/2021
Measurement technology dedicated to the discipline and biomechanics of pole vault enables high performances
05/10/2020
How does a digital measuring chain for piezoelectric sensors work as part of a complex vehicle test stand?
18/09/2020
Convincing test results: The Ohio Department of Transportation goes on to apply Lineas from Kistler for traffic monitoring.
20/08/2020
Precision is the key to top performance: how measurement technology from Kistler supports the development team at EMUGE-FRANKEN
22/07/2020
Quality assurance solutions by Kistler like ComoNeo ensure highest accuracy at TSP Precision Tooling in Shanghai.
09/06/2020
Kistler supports Ceratizit in the development of HDT. This enables complex geometries to be produced with just one tool.
15/11/2019
Process monitoring systems and cavity pressure sensors from Kistler help to reduce the amount of scrap drastically
23/10/2019
How measurement technology from Kistler contributes toward boosting high-end powertools' quality
15/08/2019
How the ANALYSE system from Kistler is enhancing safety and transparency in the field of fastening technology
17/07/2019
Turkey opts for weight enforcement with WIM technology from Kistler
24/06/2019
For the next manned flight to the moon: safety that can be measured
20/06/2019
Segregation of good and bad parts every 1.5 seconds: process monitoring with Kistler enables high quality for over 5 million parts per year.
14/05/2019
In order to achieve excellent quality for its components and medical devices, Tessy Plastics chose sensors and solutions from Kistler.
18/04/2019
A renowned manufacturer of electrical appliances trusts testing and sorting systems by Vester to improve its quality.
02/04/2019
NFL's Jaguars boost their fitness levels with Kistler.
25/03/2019
By using process monitoring from Kistler, not only the assembly of electric fuses is validated, but even the function of the sensors itself.
18/03/2019
How to determine the fitness level of an athlete efficiently? A practical report on the Quattro Jump force plate system from Kistler.
17/12/2018
Thanks to precise Weigh in Motion technology from Kistler, Hungary's roads are sustainably protected against overloaded vehicles.
27/11/2018
Bang&Clean relies on Kistler's precise measurement of ignition processes and pressure wave propagation
10/10/2018
Sartorius applies the process monitoring system ComoNeo from Kistler and thereby increases the process quality during injection molding
08/10/2018
The Dortmund Technical University tests the new MicroDyn 9109AA cutting force dynamometer from Kistler and breaks new ground for developing its micromachining processes.
31/08/2018
The ZF company operates a software-controlled Kistler fastener test bench with an integrated vibration unit.
14/08/2018
BIG Daishowa, headquartered in Osaka, Japan, is one of the leading producers of tool holders for the machining industry. Each year the company produces over half a million collet chucks. Their products are developed using, among other resources, Kistler’s cutting force measuring device.
16/07/2018
Enhanced quality and efficiency in mobile crane manufacture – thanks to the test stand for torque tools by Kistler
11/04/2018
The world’s largest provider of rail transport technology relies on Kistler’s measurement expertise. Thanks to the only crash wall of its kind in the world, the impact forces of the trains and their components can be precisely measured and analyzed.
14/11/2017
In the development of cooling lubricants, Blaser Swisslube relies on Kistler's measurement expertise.
11/08/2017
Applus IDIADA relies on DTI in-dummy technology from Kistler for Test Device for Human Occupant Restraint (THOR).
04/01/2017
Road safety is a central topic in vehicle development. Through accurate measurements, Kistler helps increase the chance of survival in crashes.
22/12/2016
Kistler makes progress in vehicle development possible
22/12/2016
Kistler Sensor Correvit® SFII measures world record
20/12/2016
Kistler sensors deliver a maximum in data quality under any conditions.
07/11/2016
Kistler pressure sensors enabled the Rosetta space probe to fly for 6.4 billion kilometers.
05/10/2016
Since the end of 2015 FC Basel is using Kistler force plates to reduce the dropout of young talents.
17/08/2016
Kistler makes the difference in the crucial sports moments with its Performance Analysis System for Swimming.
19/02/2016
Determination of Pump Efficiency with Kistler KiTorq Measuring Flange System
04/11/2015
Piezoelectric Measurements with CompactRIO™
08/05/2015
Quality Assurance in the Automotive Industry
02/03/2015
How Brose improves the quality of its two-component production and automatically separates defective parts
02/12/2014
The Kistler Group pursues a growth policy that is both ambitious and sustainable – and strategic acquisitions are one of its core elements. ‘Strategic’ means that Kistler deliberately selects companies which can achieve more together with Kistler than they ever could by continuing alone. The takeover of Dr. Staiger Mohilo & Co. GmbH in 2006 enabled Kistler to grow jointly with the acquired company...
02/12/2014
After a ten-year voyage, the Rosetta space probe's Philae landing module finally touched down on the surface of comet ‘Chury’.
23/08/2011
HEWI and its Customers Benefit from Cavity Pressure Technology
15/02/2011
End-to-end process monitoring for critical medical moldings
07/02/2011
Cavity pressure measurement eliminates short shots at Fischer GmbH & Co KG of Sinsheim/Germany
Contact
Max 25 MB