BIG Daishowa relies on cutting force measurement from Kistler for superior tool development

BIG Daishowa, headquartered in Osaka, Japan, is one of the leading producers of tool holders for the machining industry. Each year the company produces over half a million collet chucks. Their products are developed using, among other resources, Kistler’s cutting force measuring device.

More than 500 machine tools as well as some 300 robots and automated systems — these are the figures for BIG Daishowa’s production capacity. The family-owned company was founded in 1967 and employs close to 900 employees worldwide. In Europe and North America the company is known through its subsidiary, BIG KAISER. The core competence of BIG Daishowa: high-quality tool holders for cutting with a machining run-out of max. 0.001 mm. Aside from various types of tool holders like collet chucks, hydraulic chucks, milling chucks and tapping holders, their selection encompasses angle heads, measuring devices and cutting tools.

Goal: Minimize forces on thread flanks

In order to further develop their product portfolio, BIG Daishowa is continuously developing new tool concepts in-house at the MEGA Technical Center. One of the products that emerged from these efforts is the MEGA Synchro tapping holder. It is a “compensation chuck,” which uses elastic components to compensate for the synchronization errors between tooling machines and tools. The basic challenge threads pose is to minimize the differences in length arising from the spindle speed as well as the applied feed rate in relation to thread pitch and thread depth, in order to minimize the axial forces that arise on the thread flanks. High axial forces can have a negative impact on the thread flanks and result in decreased lifetime of the tap holder: “Although modern CNC machines are equipped with synchronous spindles, minor synchronization errors still occur,” says Masayuki Doi, development manager at BIG Daishowa. Even minor deviations immediately create high axial forces on the flanks of the tap holder.

Optimized construction thanks to cutting force measuring

In order to optimize the design of the MEGA Synchro, BIG Daishowa relied on a 3-component dynamometer from Kistler. The piezoelectric cutting force measuring device measures a compact 170×140 mm and can be mounted onto the machine tool table. It is exceptionally rigid and accordingly has a high natural frequency, which allows highly precise measurement of forces per cut even at high rotation speeds. “Due to the precise measurements obtained using Kistler’s dynamometer and the conclusions drawn from those, we have been able to tailor the design to such an extent that the forces on the thread flanks have been drastically reduced,” Doi states. In concrete terms: For tapping with a collet chuck, axial forces exert up to 750 N on the tap. Whereas when it comes to MEGA Synchro this is at max. 60 N. This increases the lifetime of an M12 tap by a factor of 2.4.

Due to the precise measurements obtained using Kistler’s dynamometer and the conclusions drawn from those, we have been able to tailor the design to such an extent that the forces on the thread flanks have been drastically reduced.”

Masayuki Doi, development manager at BIG Daishowa

 

Doi is self-assured: “Without Kistler’s cutting force measuring device, we would not have been able to develop the MEGA Synchro.” BIG Daishowa has developed unique collets and nuts for their new tapping holder. In contrast to many other tooling manufacturers, BIG isn't using conventional ER collets but their proper slim collets to clamp the tap. This has a positive effect on the runout accuracy. Moreover, their slim diameter nut is avoiding interference with the work piece.

11/04/2022
On the road to success with IEPE and MEMS accelerometers for the ISTAR research aircraft – on the ground and in the air.
14/01/2022
KiTraffic Statistics delivers precise WIM data for a railway bridge in central Austria
18/11/2021
Advanced fastener testing with ANALYSE systems for reliable zink flake coatings in the automotive and wind turbine industries
12/10/2021
How Yuchai achieves more precision, transparency and resource efficiency for its production of engines conform to China VI
14/09/2021
A high precision measuring chain with dynamometer, laboratory charge amplifier and software enables objective comparison tests.
09/09/2021
SRA: Find the best spot and the ideal sensor layout for direct enforcement of overloaded vehicles.
03/09/2021
At Estudio de la Pisada in Valencia, a 3D force plate helps podiatry experts to develop treatments and orthoses for patients and athletes.
02/07/2021
Two IEPE accelerometers deliver key data for propulsion validation and optimization of flight characteristics even in the stratosphere
22/06/2021
Capturing micro-vibrations with a dynamometer leads to improved satellite technology
02/06/2021
Zero defect despite high volumes: this is the way quality assurance with Kistler test automation systems works for zinc die casting parts
26/04/2021
A digitally driven brake force measurement system makes the life of service technicians for train maintenance much easier
13/04/2021
Inside "The Atmosphere" at MARIN, 100 of our pressure sensors capture wave impacts under varying environmental conditions
22/03/2021
How MAN Energy Solutions is using sensors from Kistler to make its gas turbines fit for the future
08/02/2021
Measurement technology dedicated to the discipline and biomechanics of pole vault enables high performances
05/10/2020
How does a digital measuring chain for piezoelectric sensors work as part of a complex vehicle test stand?
18/09/2020
Convincing test results: The Ohio Department of Transportation goes on to apply Lineas from Kistler for traffic monitoring.
20/08/2020
Precision is the key to top performance: how measurement technology from Kistler supports the development team at EMUGE-FRANKEN
22/07/2020
Quality assurance solutions by Kistler like ComoNeo ensure highest accuracy at TSP Precision Tooling in Shanghai.
09/06/2020
Kistler supports Ceratizit in the development of HDT. This enables complex geometries to be produced with just one tool.
15/11/2019
Process monitoring systems and cavity pressure sensors from Kistler help to reduce the amount of scrap drastically
23/10/2019
How measurement technology from Kistler contributes toward boosting high-end powertools' quality
15/08/2019
How the ANALYSE system from Kistler is enhancing safety and transparency in the field of fastening technology
17/07/2019
Turkey opts for weight enforcement with WIM technology from Kistler
24/06/2019
For the next manned flight to the moon: safety that can be measured
20/06/2019
Segregation of good and bad parts every 1.5 seconds: process monitoring with Kistler enables high quality for over 5 million parts per year.
14/05/2019
In order to achieve excellent quality for its components and medical devices, Tessy Plastics chose sensors and solutions from Kistler.
18/04/2019
A renowned manufacturer of electrical appliances trusts testing and sorting systems by Vester to improve its quality.
02/04/2019
NFL's Jaguars boost their fitness levels with Kistler.
25/03/2019
By using process monitoring from Kistler, not only the assembly of electric fuses is validated, but even the function of the sensors itself.
18/03/2019
How to determine the fitness level of an athlete efficiently? A practical report on the Quattro Jump force plate system from Kistler.
17/12/2018
Thanks to precise Weigh in Motion technology from Kistler, Hungary's roads are sustainably protected against overloaded vehicles.
27/11/2018
Bang&Clean relies on Kistler's precise measurement of ignition processes and pressure wave propagation
10/10/2018
Sartorius applies the process monitoring system ComoNeo from Kistler and thereby increases the process quality during injection molding
08/10/2018
The Dortmund Technical University tests the new MicroDyn 9109AA cutting force dynamometer from Kistler and breaks new ground for developing its micromachining processes.
31/08/2018
The ZF company operates a software-controlled Kistler fastener test bench with an integrated vibration unit.
14/08/2018
BIG Daishowa, headquartered in Osaka, Japan, is one of the leading producers of tool holders for the machining industry. Each year the company produces over half a million collet chucks. Their products are developed using, among other resources, Kistler’s cutting force measuring device.
16/07/2018
Enhanced quality and efficiency in mobile crane manufacture – thanks to the test stand for torque tools by Kistler
11/04/2018
The world’s largest provider of rail transport technology relies on Kistler’s measurement expertise. Thanks to the only crash wall of its kind in the world, the impact forces of the trains and their components can be precisely measured and analyzed.
14/11/2017
In the development of cooling lubricants, Blaser Swisslube relies on Kistler's measurement expertise.
11/08/2017
Applus IDIADA relies on DTI in-dummy technology from Kistler for Test Device for Human Occupant Restraint (THOR).
04/01/2017
Road safety is a central topic in vehicle development. Through accurate measurements, Kistler helps increase the chance of survival in crashes.
22/12/2016
Kistler makes progress in vehicle development possible
22/12/2016
Kistler Sensor Correvit® SFII measures world record
20/12/2016
Kistler sensors deliver a maximum in data quality under any conditions.
07/11/2016
Kistler pressure sensors enabled the Rosetta space probe to fly for 6.4 billion kilometers.
05/10/2016
Since the end of 2015 FC Basel is using Kistler force plates to reduce the dropout of young talents.
17/08/2016
Kistler makes the difference in the crucial sports moments with its Performance Analysis System for Swimming.
19/02/2016
Determination of Pump Efficiency with Kistler KiTorq Measuring Flange System
04/11/2015
Piezoelectric Measurements with CompactRIO™
08/05/2015
Quality Assurance in the Automotive Industry
02/03/2015
How Brose improves the quality of its two-component production and automatically separates defective parts
02/12/2014
The Kistler Group pursues a growth policy that is both ambitious and sustainable – and strategic acquisitions are one of its core elements. ‘Strategic’ means that Kistler deliberately selects companies which can achieve more together with Kistler than they ever could by continuing alone. The takeover of Dr. Staiger Mohilo & Co. GmbH in 2006 enabled Kistler to grow jointly with the acquired company...
02/12/2014
After a ten-year voyage, the Rosetta space probe's Philae landing module finally touched down on the surface of comet ‘Chury’.
23/08/2011
HEWI and its Customers Benefit from Cavity Pressure Technology
15/02/2011
End-to-end process monitoring for critical medical moldings
07/02/2011
Cavity pressure measurement eliminates short shots at Fischer GmbH & Co KG of Sinsheim/Germany
Contact
Max 25 MB