Applus IDIADA invests in a digital future

The use of in-dummy measurement technology in vehicle crash testing has increased significantly in recent years. Leading OEMs and suppliers as well as national crash test centers in Europe rely on Kistler products and solutions for this. For instance Applus IDIADA’s passive safety department began using Kistler’s data acquisition technology for crash tests right from the conception at its site in Santa Oliva in Catalonia.

The introduction of THOR dummies means that crash test laboratories are required to process data across 120 data channels from one single dummy. Given the increasing number and complexity of the crash tests carried out today, the use of these types of dummies is almost impossible in many cases using traditional analog on-board DAS systems. The current trend, therefore, is moving towards measurement technology integrated directly into the dummies in order to exploit the available on-board systems for the vehicle sensors. This is one reason why IDIADA laboratory chose Kistler in-dummy measurement technology. The transition to DTI (Digital Transducer Interface) technology is based on confidence in a digital future with Kistler.

“Ongoing support and various on-site presentations managed to convince IDIADA of our innovative DTI technology”, says Alexander Schmitt, business driver for vehicle safety at Kistler. “Many customers follow activities in Europe with a focus on EuroNCAP (European New Car Assessment Program) laboratories with IDIADA being one of them. This is, therefore, a very important project for us.”

IDIADA has been working with Kistler for over 20 years and already uses several Kistler products from the vehicle safety area. In addition to Minidau®, it also uses the KiDAU® (Kistler Data Aquisition Unit). For the first time the plug part can be removed completely through the replaceable SD (Sensor Distribution) panel and replaced with a different attachment, meaning that no additional adapter cable is required. As well as improving the flexibility, time-saving qualities and user-friendliness of the application, this also minimizes the need for space in the vehicle.

A safe choice

The benefits of these innovations will soon become even more significant as the THOR dummy starts to replace the H3 dummy over the next few years, both in the USA and in Europe. Although the H3 dummy is still stipulated for crash tests in the regulations for crash tests, the THOR dummy will be the one in general use from 2020 in EuroNCAP testing. Many test laboratories are already using the new generation of dummies as a reference in parallel with the H3. “We also discussed the in-dummy measurement technology as a result of the THOR dummies. Our requirements for the measurement technology were clear: start/record function, 100 second recording time, double trigger and a non-volatile memory. Kistler managed to convince us with their crash recorder in particular”, says Patxi Arana, Dummy and Electronic Lab Manager – Passive Safety at IDIADA.

The newly developed compact DTI375.TH crash recorder from Kistler with integrated flash data memory can easily be inserted in the dummy and has an integrated start/record function. The recording of the data in the recorder can be initiated at the same time that all the data acquisition systems are started. The measurement data recorded is stored in a central flash memory thus having the guarantee of non-volatile storage of the crash information. “Ultimately, we no longer need to connect sensors to a data acquisition system using analogue technology. This saves us time and space. Kistler really does impress here with its high level of data quality and minimum failure rate”, says Arana.

Pioneering DTI technology

Proven DTI technology is used in the crash test dummies: this transforms the analog sensor output during the crash test into digital signals directly at the sensor and forwards it to the DTI375.TH crash recorder centrally located in the dummy. Aside from the reliability and high data quality, IDIADA benefits from increased flexibility of the measurement technology: the cabling required is reduced as just one cable is routed from the dummy and therefore greatly reduces the time required for test preparation.

Towards the next digital age as friends

“Kistler’s crash recorder impressed us in the end as an innovative and pioneering development. We have been working with Kistler since 1996, with our relationship based on friendship and close cooperation. This is why we ordered the DTI upgrade for our 2 THOR dummies following multiple tests and meetings. The new technology will make our day-to-day work a lot easier”, explains Arana. IDIADA is also currently arranging the digital sensor calibration itself in-house, with support from Kistler.

11/04/2022
On the road to success with IEPE and MEMS accelerometers for the ISTAR research aircraft – on the ground and in the air.
14/01/2022
KiTraffic Statistics delivers precise WIM data for a railway bridge in central Austria
18/11/2021
Advanced fastener testing with ANALYSE systems for reliable zink flake coatings in the automotive and wind turbine industries
12/10/2021
How Yuchai achieves more precision, transparency and resource efficiency for its production of engines conform to China VI
14/09/2021
A high precision measuring chain with dynamometer, laboratory charge amplifier and software enables objective comparison tests.
09/09/2021
SRA: Find the best spot and the ideal sensor layout for direct enforcement of overloaded vehicles.
03/09/2021
At Estudio de la Pisada in Valencia, a 3D force plate helps podiatry experts to develop treatments and orthoses for patients and athletes.
02/07/2021
Two IEPE accelerometers deliver key data for propulsion validation and optimization of flight characteristics even in the stratosphere
22/06/2021
Capturing micro-vibrations with a dynamometer leads to improved satellite technology
02/06/2021
Zero defect despite high volumes: this is the way quality assurance with Kistler test automation systems works for zinc die casting parts
26/04/2021
A digitally driven brake force measurement system makes the life of service technicians for train maintenance much easier
13/04/2021
Inside "The Atmosphere" at MARIN, 100 of our pressure sensors capture wave impacts under varying environmental conditions
22/03/2021
How MAN Energy Solutions is using sensors from Kistler to make its gas turbines fit for the future
08/02/2021
Measurement technology dedicated to the discipline and biomechanics of pole vault enables high performances
05/10/2020
How does a digital measuring chain for piezoelectric sensors work as part of a complex vehicle test stand?
18/09/2020
Convincing test results: The Ohio Department of Transportation goes on to apply Lineas from Kistler for traffic monitoring.
20/08/2020
Precision is the key to top performance: how measurement technology from Kistler supports the development team at EMUGE-FRANKEN
22/07/2020
Quality assurance solutions by Kistler like ComoNeo ensure highest accuracy at TSP Precision Tooling in Shanghai.
09/06/2020
Kistler supports Ceratizit in the development of HDT. This enables complex geometries to be produced with just one tool.
15/11/2019
Process monitoring systems and cavity pressure sensors from Kistler help to reduce the amount of scrap drastically
23/10/2019
How measurement technology from Kistler contributes toward boosting high-end powertools' quality
15/08/2019
How the ANALYSE system from Kistler is enhancing safety and transparency in the field of fastening technology
17/07/2019
Turkey opts for weight enforcement with WIM technology from Kistler
24/06/2019
For the next manned flight to the moon: safety that can be measured
20/06/2019
Segregation of good and bad parts every 1.5 seconds: process monitoring with Kistler enables high quality for over 5 million parts per year.
14/05/2019
In order to achieve excellent quality for its components and medical devices, Tessy Plastics chose sensors and solutions from Kistler.
18/04/2019
A renowned manufacturer of electrical appliances trusts testing and sorting systems by Vester to improve its quality.
02/04/2019
NFL's Jaguars boost their fitness levels with Kistler.
25/03/2019
By using process monitoring from Kistler, not only the assembly of electric fuses is validated, but even the function of the sensors itself.
18/03/2019
How to determine the fitness level of an athlete efficiently? A practical report on the Quattro Jump force plate system from Kistler.
17/12/2018
Thanks to precise Weigh in Motion technology from Kistler, Hungary's roads are sustainably protected against overloaded vehicles.
27/11/2018
Bang&Clean relies on Kistler's precise measurement of ignition processes and pressure wave propagation
10/10/2018
Sartorius applies the process monitoring system ComoNeo from Kistler and thereby increases the process quality during injection molding
08/10/2018
The Dortmund Technical University tests the new MicroDyn 9109AA cutting force dynamometer from Kistler and breaks new ground for developing its micromachining processes.
31/08/2018
The ZF company operates a software-controlled Kistler fastener test bench with an integrated vibration unit.
14/08/2018
BIG Daishowa, headquartered in Osaka, Japan, is one of the leading producers of tool holders for the machining industry. Each year the company produces over half a million collet chucks. Their products are developed using, among other resources, Kistler’s cutting force measuring device.
16/07/2018
Enhanced quality and efficiency in mobile crane manufacture – thanks to the test stand for torque tools by Kistler
11/04/2018
The world’s largest provider of rail transport technology relies on Kistler’s measurement expertise. Thanks to the only crash wall of its kind in the world, the impact forces of the trains and their components can be precisely measured and analyzed.
14/11/2017
In the development of cooling lubricants, Blaser Swisslube relies on Kistler's measurement expertise.
11/08/2017
Applus IDIADA relies on DTI in-dummy technology from Kistler for Test Device for Human Occupant Restraint (THOR).
04/01/2017
Road safety is a central topic in vehicle development. Through accurate measurements, Kistler helps increase the chance of survival in crashes.
22/12/2016
Kistler makes progress in vehicle development possible
22/12/2016
Kistler Sensor Correvit® SFII measures world record
20/12/2016
Kistler sensors deliver a maximum in data quality under any conditions.
07/11/2016
Kistler pressure sensors enabled the Rosetta space probe to fly for 6.4 billion kilometers.
05/10/2016
Since the end of 2015 FC Basel is using Kistler force plates to reduce the dropout of young talents.
17/08/2016
Kistler makes the difference in the crucial sports moments with its Performance Analysis System for Swimming.
19/02/2016
Determination of Pump Efficiency with Kistler KiTorq Measuring Flange System
04/11/2015
Piezoelectric Measurements with CompactRIO™
08/05/2015
Quality Assurance in the Automotive Industry
02/03/2015
How Brose improves the quality of its two-component production and automatically separates defective parts
02/12/2014
The Kistler Group pursues a growth policy that is both ambitious and sustainable – and strategic acquisitions are one of its core elements. ‘Strategic’ means that Kistler deliberately selects companies which can achieve more together with Kistler than they ever could by continuing alone. The takeover of Dr. Staiger Mohilo & Co. GmbH in 2006 enabled Kistler to grow jointly with the acquired company...
02/12/2014
After a ten-year voyage, the Rosetta space probe's Philae landing module finally touched down on the surface of comet ‘Chury’.
23/08/2011
HEWI and its Customers Benefit from Cavity Pressure Technology
15/02/2011
End-to-end process monitoring for critical medical moldings
07/02/2011
Cavity pressure measurement eliminates short shots at Fischer GmbH & Co KG of Sinsheim/Germany
Contact
Max 25 MB