Rockets are exposed to very high stresses, especially during launch. To prevent malfunctioning during operation, rocket components – and especially rocket engines – undergo extensive testing and inspection. For example, new or modified rocket engines require testing to ensure that no combustion instabilities will occur. When using liquid propellant, the supply mechanism needs to be characterized and optimized. Measuring the dynamic ignition pressure is essential for a safe rocket launch.
Thrust, dynamic pressure and vibration characterization
Fuel efficiency in solid propellant for solid rockets, or fuel mixture in the case of liquid rockets, is a major concern for rocket engine designers. Characterizing the thrust of the engine itself provides a clear understanding of how much thrust can be produced with a given nozzle design. This allows engineers to compute the specific impulse of the combustion material and study the different phases during the functioning of a rocket engine, such as ignition, burn-in and switch-off. Customer-specific 6-component dynamometers based on piezoelectric technology are often used for such investigations.
This approach also provides an in-depth understanding of the injection and mix of fuel components, ignition time, and combustion: essential knowledge to verify the reliable performance of a rocket engine and drive the development of propulsion technologies. Piezoelectric pressure and acceleration sensors from Kistler span the extreme range of ultra-high temperature stability and dynamics required to tackle the challenges encountered in extreme thrust chamber environments.
Important technologies for dynamic characterization