Programmable sequence control for integrated quality assurance

Winterthur, September 30, 2014 – At this year's Motek from October 6-9, 2014 in Stuttgart, Kistler will be presenting the latest innovations to its maXYmos product family, which is used to visualize and evaluate production processes. The highlight at Kistler's stand is the maXYmos BL 2.2 for manual presses, visitors to the exhibition will be able to see live demonstrations. Kistler is also showing a new update to the maXYmos TL as well as its most recent addition to this product series, the maXYmos NC.

 

Quality assurance for manually operated processes

The maXYmos BL force-displacement measurement system helps manufacturers attain zero-defect production in their hand-operated press processes. Based on the course of force and displacement measurement curves, the process can be visualized and the quality of the press process evaluated. Deviations are detected immediately and faulty parts can be separated at an early stage. This enables the quality of hand-operated press processes to be reproduced – independently of the respective operating personnel. The result is 100% quality control.

Visitors to Motek are especially invited to experience the sequencer mode of the maXYmos BL. This mode enables users to define an individual sequence of steps for each press process via the intuitive user interface of the touch display. 11 digital inputs and 8 corresponding outputs can be programmed in order to query and output processrelevant statuses. Up to 128 sequence elements can be configured for each measurement program. The maXYmos BL progressively checks whether all conditions have been fulfilled. In this manner, not only the production process can be controlled and good and bad end results detected, but it can also be deducted whether the desired quality has been attained in each step of the sequence. This can subsequently be reflected graphically. Ultimately, the required quality is ensured without the need for complex external control systems (PLC). In order to update existing manual presses, the measurement system – including sequencer mode – is also available as a retrofit package.

Complete spectrum of force-displacement measurement systems from a single source

Alongside the maXYmos BL, Kistler will also be presenting new functions of its top level system in Stuttgart. The maXYmos TL 1.1.4 includes an extensible language package, which now also encompasses Japanese, Portuguese and Czech. In addition, the system offers faster back-up functionalities, for example via USB or with the related maXYmos computer software. New cable solutions have also been developed to allow the connection of torque sensors.

"With the maXYmos product family, we have set industrial standards in terms of process optimization and quality assurance," says Jens Höppner, Product Manager at Kistler. "Our customers enjoy working with these systems and do so very successfully. Thanks to the further development of the underlying technologies they now benefit even more from our expertise and do not even have to get used to a new product."

The series has been completed with the maXYmos NC, which enables control and monitoring of electro-mechanical joining systems. Now, XY sequences for joining and pressfitting processes in combination with NC joining modules can be evaluated and documented and the quality of each individual production step, component or even the entire product can be controlled. This means that optimum cycle times can be implemented with maximum repeat accuracy. In this way, unplanned downtimes are minimized and machine availability is increased, thus improving the productivity of the manufacturing process.

From October 6-9, 2014 visitors to Motek will be shown Kistler's innovative products and be advised as to how the maXYmos series can be used individually in their own companies at stand 5535 in hall 5.

 

Download Press Release (PDF/EN)

 

User contact

Jens Höppner
Product Manager
Phone: +49 7172 184 238
E-mail: jens.hoeppner@kistler.com

 

Media contact

Simone Koch
Divisional Marketing Manager IPC
Phone: +41 52 224 18 02
E-mail: simone.koch@kistler.com

 

 

Captions

Image 1: The uniform philosophy of the maXYmos product family provides user-friendly and intuitive operation. It supports simple and quick start-up of the electro-mechanical NC joining systems.

Figure 2: The Sequencer Mode in the maXYmos BL allows programming of sequence controls, which are used to control the processes. An independent sequence can be created for each measurement program.

Figure 3: Force-displacement measurement system with piezoelectric force sensor for manually operated presses.

11/05/2018
Digitization, Internet of Things and Industry 4.0 are presenting major challenges. Discover how Kistler...
15/02/2017
Discover how Kistler contributes to face the great challenges of our times.
11/11/2016
With MARS software version 3.0, Kistler presents an extensive update of the proprietary measurement, analysis,...
14/10/2016
Reliable measurement solutions are becoming ever more important in the globally networked economy.
07/06/2016
Discover our latest Kistler News online.
03/05/2016
The latest issue of Kistler News is now online.
01/02/2016
Learn more about what motivates us and what we are striving for this year in the latest Kistler View.
04/12/2015
Kistler Japan Celebrates its 30th Anniversary and Thanks Its Loyal Customers.
22/09/2015
The latest issue of Kistler News is now online.
03/09/2015
Download KiBox Cockpit V2.1 for free and discover new features.
20/08/2015
Seminar zur Qualitätssicherung in der industriellen Fertigung – jetzt anmelden.
29/06/2015
Kistler Automotive GmbH honored as one of Germany's most innovative companies
26/06/2015
Kistler's software for force plates offers a host of new features for performance diagnostics in sports and...
12/06/2015
A fascinating TV report on the trendy sport ‘Parkour’ – with Kistler force plates playing a hidden but...
22/04/2015
At Chinaplas 2015 Kistler will be presenting solutions for zero-defect production, process monitoring and data...
23/03/2015
Kistler partners with OEMs and keeps the finger on the pulse of Industry 4.0
13/02/2015
At SIAF 2015 Kistler will be presenting advanced versions of its proven maXYmos product family
14/10/2014
Wide range of options for optimizing the quality assurance through documenting and evaluating production data...
29/09/2014
Users obtain a full range of force–displacement measurement systems from one source
24/09/2014
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
14/01/2014
Dr.-Ing. Oliver Schnerr, Head of Sales of the Industrial Process Control (IPC) division, hands over the...
11/11/2013
From flexible torque sensors to complete test stands for highly-efficient electric drives
16/09/2013
1 mm pressure sensor Type 6183C with a new design
13/08/2013
Monitoring, open- and closed-loop control of RTM and SMC processes
24/07/2013
New longitudinal measuring pin for non-contact cavity pressure measuring
06/05/2013
Kistler Goes Beyond Limits: Acceleration sensors for heavy-duty applications at the SENSOR+TEST 2013
08/04/2013
Kistler Goes Beyond Limits: High-tech sensors for heavy-duty applications at the SENSOR+TEST 2013
20/03/2013
In 2012, the Kistler Group reached a record turnover of 279 million Swiss francs with an increase in turnover...
19/03/2013
Kistler Group, a leading global provider of sensors for measuring pressure, force, torque and acceleration,...
15/11/2012
Kistler präsentiert auf der Fachmesse SPS/IPC/DRIVES in Nürnberg (24. bis 26. November 2012) am Stand 4A-451...
08/10/2012
At the Fakuma trade show in Friedrichshafen/Germany (from 16 until 20 October, 2012), Kistler will present a...
08/10/2012
At the Fakuma trade show in Friedrichshafen/Germany (from 16 until 20 October, 2012) Kistler will present its...
08/10/2012
The new firmware upgrade V2.4 for Kistler's CoMo Injection process monitoring system offers better...
10/09/2012
Kistler Group continues to expand: revenues up 20 %, strengthening of customer-specific development capacities...
10/09/2012
Kistler Gruppe weiterhin auf Expansionskurs: Umsatzsteigerung um 20 %, Stärkung der kundenspezifischen...
29/06/2012
With the acquisition of the DTI Technology ("Digital Transducer Interface") from Hentschel System GmbH,...
29/06/2012
Mit dem Erwerb der DTI-Technologie ("Digital Transducer Interface") von der Hentschel System GmbH, Hannover,...
08/05/2012
At the Automatica Trade Fair, which will take place from 22 through 24 May, 2012 in Munich/Germany, Kistler...
07/05/2012
Kistler sensors and systems deliver an impressive performance where products from other suppliers come to...
15/03/2012
CIRP focuses on cutting because this method of machining components is one of the key production processes.
17/02/2012
In-process quality assurance solutions made by Kistler Group have proven their high efficiency for...
01/02/2012
Despite difficult conditions, with sales growth over 11 % Kistler still achieved a sound result in 2011.
02/11/2011
On Stand 4A-451 in Hall 4A of the SPS/IPC/DRIVES exhibition from 22 to 24 November 2011 in Nuremberg, Kistler...
02/11/2011
By designing a measuring unit and an evaluation unit as separate assemblies, and introducing modular...
20/10/2011
This year's Fakuma sees Kistler showing a system for online prediction of the quality of injection molded...
19/10/2011
Kistler brings the quality-minded injection molder another substantial step closer to zero-defect production.
28/09/2011
As an XY monitor for process monitoring and product testing, the maXYmos BL Type 5867A… from Kistler has...
28/09/2011
Telemetric transmission of the force signal without having to rely on a cable, and suitability for use in...
28/09/2011
Kistler is expanding its selection of electromechanical NC joining modules NCFB Type 2160A… with versions...
03/02/2011
The Kistler Group based in Winterthur, Switzerland, looks back on a successful 2010 financial year with sales...
10/12/2010
Kistler, worldwide supplier of precision sensors, systems and instrumentation for the dynamic measurement of...
24/11/2010
Kistler, worldwide supplier of precision sensors, systems and instrumentation for the dynamic measurement of...
10/11/2010
Kistler's new generation of triaxial PiezoBeam® accelerometer Type 8688A(x) offers best-in-class sensitivity...
29/10/2010
Swiss company Kistler Instrumente AG of Winterthur is the leading international supplier of sensors and...
10/09/2010
The new press force sensor Type 9393A… extends the successful Press Force series of sensors to a measuring...
06/09/2010
With the new combined pressure and temperature sensor Type 6188A… Kistler establishes another milestone in the...
21/07/2010
Kistler has developed its new data acquisition (DAQ) system Type 5697A… for recording data in R&D laboratory...
09/07/2010
Kistler has commissioned an additional calibration unit for torque sensors on its Lorch production site.
08/06/2010
As a development partner of the automobile industry the Kistler Group aims to provide vehicle manufacturers...
19/04/2010
The Kistler Group has been awarded the contract for instrumentation of three crash centers for the Indian...
07/04/2010
In order to optimise processes inside an engine, it is extremely important to have a true picture of the...
13/01/2010
New Type 4520A... Basic Line provides a cost-effective torque sensor based upon strain gage technology.
10/12/2009
The well established Kistler press force sensors are based on the piezoelectric measuring principle.
18/11/2009
Successful automation of joining processes where room is at a premium and joining stations closely spaced...
23/10/2009
The Kistler Group acquired KT Automotive GmbH based in Munich, Germany, in an all-stock transaction on 22...
14/09/2009
The curve of cavity pressure during injection molding is the critical process variable for evaluating part...
01/07/2009
To allow direct incorporation of Kistler products into CAD designs, the Kistler CAD Download Service offers...
30/04/2009
The Kistler Group has acquired Corrsys-Datron Sensorsysteme GmbH based in Wetzlar, Germany, in an all-stock...
09/03/2009
The roll-out of the world's first measuring tram took place in Dresden, Germany, on 5 March with the handover...
15/01/2009
The Kistler Group took over MSC Automotive GmbH based in Schwieberdingen, Germany, in an all-stock transaction...
Contacto