Solutions from Kistler Boost Efficiency in Automated Production

Winterthur, 30 August 2016 – At this year's Motek from 10 to 13 October in Stuttgart, Kistler will be showcasing its new NCFE and NCFR joining modules, together with the latest generation of maXYmos monitoring systems. These product innovations represent outstanding examples of the trade show's theme: interconnection in automated production.

 

Especially in sectors where technology is such a strong driving force – such as the automotive industry – the vision of Industry 4.0 is becoming more relevant as time goes on, thanks to increased digitization and the growth of machine and system networking. Even so, not all market players are equally aware of the diverse possibilities for networking that are now available in automated production; nor do they fully appreciate the economic benefits that more transparent production processes can also deliver. As a leading provider of process monitoring systems, Kistler has set itself a specific goal at this year's Motek: to focus attention on this highly relevant issue by showcasing prominent examples of the technologies involved. For joining, forming and testing processes alike: Kistler offers complete systems – from the sensor to the evaluation unit – that can map processes accurately, enabling comparisons and evaluations on a standardized basis across the globe thanks to a consistent operating philosophy. 

 

Electromechanical Joining Systems: Another Addition to Kistler's Portfolio

At this year's Motek, Kistler will premiere its new NCFE (Economy) electromechanical joining module. This new product has been specifically developed for plant manufacturers and operators of conventional power packs. The functionality and design of the NCFE are deliberately geared to simple joining tasks. Plant manufacturers and operators of power packs who opt for the NCFE will benefit from a pre-tested system with integrated process control. This saves time and money on the development of users' own systems – and, because all Kistler process monitoring systems are based on a uniform operating philosophy, seamless integration into the overarching production environment is guaranteed. The NCFE is available for applications in the 10-80 kN measuring range. Kistler is also presenting its NCFR joining module – as well as the classical linear joining process, this system can perform a controlled rotary movement of the ram, either sequentially or even simultaneously.

 

Like the entire family of NC joining systems, all three new products deliver a host of benefits for their users: they offer great flexibility and excellent dynamics combined with simple operation – so simple as well as highly complex joining processes can be implemented rapidly and efficiently with one and the same product family. Thanks to the servo amplifiers used in the products, all traverse movements that are performed can be controlled with high precision. Another example: users of NCFH joining systems can switch between measuring ranges, so completely different components can be manufactured on one and the same plant. Furthermore, end-to-end standardization of the systems means that users can easily obtain spare parts – anywhere in the world. But at the end of the day, future users will probably be convinced by one argument above all others: thanks to their excellent flexibility and low energy consumption, all the joining systems can help the automobile industry and the automotive supply sector to achieve lasting reductions in their series production costs.

 

maXYmos TL 1.2 and maXYmos BL 2.3: the Latest Generation of Monitoring Systems

Yet another highlight is in store for visitors to Kistler's stand: the latest generation of maXYmos monitoring systems. Their purpose: to deliver consistent process-integrated quality assurance. The patterns of measurement curves can be used to monitor and control the quality of a single production step, a sub-assembly or an entire product. Now, maXYmos users can also measure multi-stage production processes (i.e. those with consecutive staggered steps): this has been made possible by equipping the maXYmos TL 1.2 and BL 2.3 with a sequencer mode, in the same way as the successful maXYmos NC. The benefits for users are clear to see: thanks to integrated process control, test processes can now be mapped with no need for costly external PLC programming. The programs can be set up quickly and easily with the help of the intuitive user interface on the touch display. Even for multi-stage processes, optimal cycle times can be achieved with maximum repeat accuracy. Because this control is integrated in the process, the system provides the basis for enhanced transparency in assembly and testing lines – paving the way for increased cost-efficiency throughout the production facility.

 

4503B Torque Sensor: the Rugged Sensor for Maximum Accuracy

Kistler's stand at the Motek will also present the latest state-of-the-art in high-precision torque sensor technology: the Type 4503B torque sensor, which offers a wide range of additional functions. On this new sensor, for instance, optical speed and angle sensing has now been replaced by magnetic technology. This gives the sensor added resilience for reliable operation in heavily contaminated industrial environments – thereby saving valuable time on maintenance. The torque sensor's electronics have also been optimized, and the 4503B now has a cut-off frequency of 10 kHz for highly dynamic measurements. Users can adjust this value individually with the help of an integrated digital low-pass filter, and the second measuring range is freely scalable up to a spread of 1:10. Outstanding features of the Type 4503B also include wide measuring ranges (from 0.2 to 5,000 Nm), integrated speed/angle sensing of up to 8192 pulses/revolution and a high-speed version with up to 50,000 revolutions per minute (1 min/rpm).

 

Save the Trade Show Dates!

If you want to see Kistler's diverse range of solutions for interconnected quality monitoring at first hand, save the dates for the trade show now: it runs from 10 to 13 October 2016 at Motek in Stuttgart.

11/05/2018
Digitization, Internet of Things and Industry 4.0 are presenting major challenges. Discover how Kistler...
15/02/2017
Discover how Kistler contributes to face the great challenges of our times.
11/11/2016
With MARS software version 3.0, Kistler presents an extensive update of the proprietary measurement, analysis,...
14/10/2016
Reliable measurement solutions are becoming ever more important in the globally networked economy.
07/06/2016
Discover our latest Kistler News online.
03/05/2016
The latest issue of Kistler News is now online.
01/02/2016
Learn more about what motivates us and what we are striving for this year in the latest Kistler View.
04/12/2015
Kistler Japan Celebrates its 30th Anniversary and Thanks Its Loyal Customers.
22/09/2015
The latest issue of Kistler News is now online.
03/09/2015
Download KiBox Cockpit V2.1 for free and discover new features.
20/08/2015
Seminar zur Qualitätssicherung in der industriellen Fertigung – jetzt anmelden.
29/06/2015
Kistler Automotive GmbH honored as one of Germany's most innovative companies
26/06/2015
Kistler's software for force plates offers a host of new features for performance diagnostics in sports and...
12/06/2015
A fascinating TV report on the trendy sport ‘Parkour’ – with Kistler force plates playing a hidden but...
22/04/2015
At Chinaplas 2015 Kistler will be presenting solutions for zero-defect production, process monitoring and data...
23/03/2015
Kistler partners with OEMs and keeps the finger on the pulse of Industry 4.0
13/02/2015
At SIAF 2015 Kistler will be presenting advanced versions of its proven maXYmos product family
14/10/2014
Wide range of options for optimizing the quality assurance through documenting and evaluating production data...
29/09/2014
Users obtain a full range of force–displacement measurement systems from one source
24/09/2014
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
14/01/2014
Dr.-Ing. Oliver Schnerr, Head of Sales of the Industrial Process Control (IPC) division, hands over the...
11/11/2013
From flexible torque sensors to complete test stands for highly-efficient electric drives
16/09/2013
1 mm pressure sensor Type 6183C with a new design
13/08/2013
Monitoring, open- and closed-loop control of RTM and SMC processes
24/07/2013
New longitudinal measuring pin for non-contact cavity pressure measuring
06/05/2013
Kistler Goes Beyond Limits: Acceleration sensors for heavy-duty applications at the SENSOR+TEST 2013
08/04/2013
Kistler Goes Beyond Limits: High-tech sensors for heavy-duty applications at the SENSOR+TEST 2013
20/03/2013
In 2012, the Kistler Group reached a record turnover of 279 million Swiss francs with an increase in turnover...
19/03/2013
Kistler Group, a leading global provider of sensors for measuring pressure, force, torque and acceleration,...
15/11/2012
Kistler präsentiert auf der Fachmesse SPS/IPC/DRIVES in Nürnberg (24. bis 26. November 2012) am Stand 4A-451...
08/10/2012
At the Fakuma trade show in Friedrichshafen/Germany (from 16 until 20 October, 2012), Kistler will present a...
08/10/2012
At the Fakuma trade show in Friedrichshafen/Germany (from 16 until 20 October, 2012) Kistler will present its...
08/10/2012
The new firmware upgrade V2.4 for Kistler's CoMo Injection process monitoring system offers better...
10/09/2012
Kistler Group continues to expand: revenues up 20 %, strengthening of customer-specific development capacities...
10/09/2012
Kistler Gruppe weiterhin auf Expansionskurs: Umsatzsteigerung um 20 %, Stärkung der kundenspezifischen...
29/06/2012
With the acquisition of the DTI Technology ("Digital Transducer Interface") from Hentschel System GmbH,...
29/06/2012
Mit dem Erwerb der DTI-Technologie ("Digital Transducer Interface") von der Hentschel System GmbH, Hannover,...
08/05/2012
At the Automatica Trade Fair, which will take place from 22 through 24 May, 2012 in Munich/Germany, Kistler...
07/05/2012
Kistler sensors and systems deliver an impressive performance where products from other suppliers come to...
15/03/2012
CIRP focuses on cutting because this method of machining components is one of the key production processes.
17/02/2012
In-process quality assurance solutions made by Kistler Group have proven their high efficiency for...
01/02/2012
Despite difficult conditions, with sales growth over 11 % Kistler still achieved a sound result in 2011.
02/11/2011
On Stand 4A-451 in Hall 4A of the SPS/IPC/DRIVES exhibition from 22 to 24 November 2011 in Nuremberg, Kistler...
02/11/2011
By designing a measuring unit and an evaluation unit as separate assemblies, and introducing modular...
20/10/2011
This year's Fakuma sees Kistler showing a system for online prediction of the quality of injection molded...
19/10/2011
Kistler brings the quality-minded injection molder another substantial step closer to zero-defect production.
28/09/2011
As an XY monitor for process monitoring and product testing, the maXYmos BL Type 5867A… from Kistler has...
28/09/2011
Telemetric transmission of the force signal without having to rely on a cable, and suitability for use in...
28/09/2011
Kistler is expanding its selection of electromechanical NC joining modules NCFB Type 2160A… with versions...
03/02/2011
The Kistler Group based in Winterthur, Switzerland, looks back on a successful 2010 financial year with sales...
10/12/2010
Kistler, worldwide supplier of precision sensors, systems and instrumentation for the dynamic measurement of...
24/11/2010
Kistler, worldwide supplier of precision sensors, systems and instrumentation for the dynamic measurement of...
10/11/2010
Kistler's new generation of triaxial PiezoBeam® accelerometer Type 8688A(x) offers best-in-class sensitivity...
29/10/2010
Swiss company Kistler Instrumente AG of Winterthur is the leading international supplier of sensors and...
10/09/2010
The new press force sensor Type 9393A… extends the successful Press Force series of sensors to a measuring...
06/09/2010
With the new combined pressure and temperature sensor Type 6188A… Kistler establishes another milestone in the...
21/07/2010
Kistler has developed its new data acquisition (DAQ) system Type 5697A… for recording data in R&D laboratory...
09/07/2010
Kistler has commissioned an additional calibration unit for torque sensors on its Lorch production site.
08/06/2010
As a development partner of the automobile industry the Kistler Group aims to provide vehicle manufacturers...
19/04/2010
The Kistler Group has been awarded the contract for instrumentation of three crash centers for the Indian...
07/04/2010
In order to optimise processes inside an engine, it is extremely important to have a true picture of the...
13/01/2010
New Type 4520A... Basic Line provides a cost-effective torque sensor based upon strain gage technology.
10/12/2009
The well established Kistler press force sensors are based on the piezoelectric measuring principle.
18/11/2009
Successful automation of joining processes where room is at a premium and joining stations closely spaced...
23/10/2009
The Kistler Group acquired KT Automotive GmbH based in Munich, Germany, in an all-stock transaction on 22...
14/09/2009
The curve of cavity pressure during injection molding is the critical process variable for evaluating part...
01/07/2009
To allow direct incorporation of Kistler products into CAD designs, the Kistler CAD Download Service offers...
30/04/2009
The Kistler Group has acquired Corrsys-Datron Sensorsysteme GmbH based in Wetzlar, Germany, in an all-stock...
09/03/2009
The roll-out of the world's first measuring tram took place in Dresden, Germany, on 5 March with the handover...
15/01/2009
The Kistler Group took over MSC Automotive GmbH based in Schwieberdingen, Germany, in an all-stock transaction...
Contacto