Reliable measurements for crash tests – with no interruptions

Winterthur, June 2020 - The KiDAU data acquisition system and KiBAT, the rugged special battery: a combination from Kistler that adds up to a universal system for efficient, successful measurements in crash tests – a major factor in vehicle safety.

During a crash test, several thousand sensors operate simultaneously to deliver reliable measurement data. The strong forces and accelerations that act during these tests demand measurement technology with high levels of efficiency, reliability and shock resistance. KiDAU – the new data acquisition system from the Kistler Group – is used in demanding conditions such as these. To complement the universal KiDAU technology, the rugged KiBAT battery management system is the key to guaranteed data protection.

Special battery as backup

Even the best data acquisition system is useless if measurements are interrupted during a crash test. To prevent this from happening, Kistler has developed KiBAT K3885 – an intelligent onboard battery. If the cabled power supply fails, the special battery from Kistler cuts in: it buffers all the onboard components via the CrashLink2 bus. This gives customers 400 Watts of power for a ten-minute period – so measurements can continue without interruption and the system captures reliable data. Five colored LEDs indicate status and if the energy level is low, KiBAT also emits an acoustic signal

The case for KiBAT is very robust, making it ideal for demanding crash test applications. The battery can be switched on either automatically via the CrashLink2 bus, or manually – to ensure ease of handling in different application situations. 

As an additional link in the onboard data acquisition chain, KiBAT ensures that the processes for preparing and conducting crash tests will run smoothly. Kistler draws on its extensive experience of safety system trials and tests in a wide variety of vehicles to continue improving safety for vehicles and traffic.

Efficient vehicle safety measurements – also available for the laboratory

KiDAU Stationary K3880AS combines multiple measurement technologies in one 19" rack carrier with various plug-in modules that can be used with one another. Kistler developed this universal data acquisition system for use in preparing and certifying dummies, and also for component tests. Now, thanks to this innovation, the high performance and reliability standards of mobile onboard devices are also available in a stationary application for laboratory use

The base unit includes integrated interfaces with the external crash test infrastructure. Existing onboard devices can be connected directly via four CL2 interfaces. The case for KiDAU is executed in the standard 19" design and is cooled without a fan. Modular architecture allows it to accommodate up to eight plug-in I/O modules. There is also a unit with 16 digital input channels that can save data in a cycle of 1,800 seconds with a sampling rate of 100 kHz – so recording can begin even before the test starts. And in addition, the KiDAU K3880AS features 8-channel plug-in cards for analog inputs: each one is equipped with a programmable input amplifier, bridge excitation circuit, low-pass filter and a 16-bit analog-to-digital converter. All settings can be made via software, either automatically or with commands. The extensive range of technical equipment makes this data acquisition system suitable for universal use – a straightforward, reliable solution that guarantees the availability of measurements on dummies and components.

KIT PARA MEDIOS INFORMATIVOS

Paquete multimedia con PDF, archivo Word e imágenes de alta resolución: Kistler Press Kit.zip

16/09/2022
At K 2022, Kistler will showcase its solutions for injection molding that make plastics processing more intelligent and sustainable.
06/09/2022
With ComoScout, Kistler offers a simple and cost-effective process monitoring system for injection molding processes.
31/08/2022
High-end measurement systems for rolling stock – from brake testing to traffic monitoring.
22/08/2022
Artificial intelligence in punching: AI helps manufacturers improve product quality and step up their quality assurance.
12/08/2022
New wireless dynamometer allows for highly accurate measurements of cutting forces.
28/07/2022
The most successful triaxial accelerometer 8763B measures micro-vibrations even more accurately.
31/05/2022
Kistler showcases needs-oriented solutions for the Smart Factory and presents the extensive software and service resources.
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
The new joining module is highly suitable for clinching and riveting, and also for assembly processes that require force-displacement monitoring.
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
The Kistler Group will showcase its test and analysis systems for threaded joints at the 2019 Fastener Fair in Stuttgart from 19 to 21 March.
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
Accurate and insensitive to its mounting position: the new Type 6044A M8 sensor features an anti-strain design to ensure reliable, high-quality results.
20/11/2018
Motorsport: the new 4080B/BT absolute pressure sensors from Kistler – for real-time monitoring with maximum measurement accuracy and signal quality!
16/10/2018
At Fakuma 2018, the Kistler Group is showcasing its latest monitoring and control packages for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
08/10/2018
The SMETEC Gesellschaft für Sensor-, Motor- und Energietechnik mbH recently became part of the Kistler Group.
24/09/2018
The Kistler Group is adding another variant to what is already the world's most comprehensive portfolio of wheel force measurement systems: the new RoaDyn S6GT 6-component wheel force measurement system.
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
The Kistler Group is introducing a compact mobile measurement solution for enhanced rolling stock maintenance in international railway operations in the shape of its railway brake force measuring system Type 2899A.
21/08/2018
A new Center of Competence for production control and management systems will be opened in Aachen.
31/07/2018
Competent service just a call away has always been a key aspect of Kistler's cooperation with its customers. Now, in a move to address growing demand in North Germany, the measurement technology experts are opening a new office in Wolfsburg.
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
Digitization, Internet of Things and Industry 4.0 are presenting major challenges. Discover how Kistler responds to the great challenges of our times.
09/05/2018
At Sensor + Test 2018 Kistler will be introducing a milestone in measurement technology: its new KiDAQ data acquisition system.
08/05/2018
At NPE 2018, the Kistler Group is showcasing its latest custom monitoring package for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
03/05/2018
At Automatica 2018, the Kistler Group will turn the spotlight on diverse options for using sensors and process monitoring systems to support industrial production and enhance digitalization in test and assembly technology.
24/04/2018
The Kistler Group will showcase its expanded portfolio of industrial test and inspection systems for quality assurance at the 2018 Control trade show.
12/04/2018
The global leader in dynamic measurement technology supports the passion for innovation and technology with a three-year partnership.
06/03/2018
Kistler will be showcasing at Control 2018 its portfolio of industrial testing and inspection systems with the spotlight on the very latest additions.
16/02/2018
At Intertraffic 2018 the Kistler Group is showcasing its comprehensive KiTraffic Weigh In Motion (WIM) solutions, which support road owners and authorities in road and traffic monitoring, weight enforcement and weight-based tolling.
15/02/2018
At NPE 2018 in Orlando, Florida, the Kistler Group will demonstrate a wide range of modular functionalities for ComoNeo: the process monitoring system that takes injection molding to a higher level with integrated quality monitoring geared to meet customers’ needs and requirements.
31/01/2018
The new KiSprint provides coaches and athletes with an efficient means of biomechanically optimizing sprint starts under competitive conditions. The robust and mobile solution has comprehensive software assessment options and can be individually adapted and expanded.
24/01/2018
Kistler achieved a growth rate of 18 % in 2017. Digital transformation has top priority in 2018.
23/01/2018
Overcoming the complexities of RTM – with Kistler
12/10/2017
At the SPS IPC Drives Kistler Group will unveil the world's first digital charge amplifier Type 5974A, a milestone more in electrical automation.
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
With MARS software version 3.0, Kistler presents an extensive update of the proprietary measurement, analysis, and evaluation software for Kistler force plates.
21/10/2016
Kistler boosts the efficiency and reliability of large marine and stationary engines through monitoring and control of the combustion process
19/10/2016
Kistler is presenting the new versions of its ComoNeo and ComoDataCenter.
10/10/2016
Kistler is unveiling a new addition to its portfolio of electromechanical joining modules.
30/09/2016
The Kistler Group reported incoming orders worth CHF 233.3 million at the end of August 2016 and has therefore seen growth of 8.4 % compared to the same period in the previous year, or 5.6 % when adjusted for currency effects.
07/09/2016
At this year's K Trade Fair from 19 to 26 October in Düsseldorf, Kistler will be showcasing its latest new products and features with the focus on Industry 4.0.
24/07/2016
Kistler will be showcasing its new NCFE and NCFR joining modules, together with the latest generation of maXYmos monitoring systems on Motek 2016
12/07/2016
Kistler's Correvit® SFII sensor measures world record in 1.513 seconds
12/05/2016
Screw technology complements the range of applications.
27/04/2016
Following a long phase of planning, preparations, and conversion work, Kistler Instrumente GmbH has a new home for its German headquarters at the Böblingen/Sindelfingen airfield.
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
At Chinaplas 2015 Kistler will be presenting solutions for zero-defect production, process monitoring and data evaluation in injection molding
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
At Sensor + Test 2014 Kistler is presenting many new features from the field of measurement electronics in addition to its already proven sensor technology.
19/05/2014
Users obtain a full range of force–displacement measurement systems from one source
06/02/2014
The Kistler Group achieved sales of 285 million CHF in 2013, thus marking a slight growth in comparison with the figures for the prior year.