Cylinder Pressure Measurement Cuts Fuel Consumption

Kistler boosts the efficiency and reliability of large marine and stationary engines through monitoring and control of the combustion process.

90% of all goods transported are traversing the world's oceans every day in container ships, tankers and freighters.1 Marine cargo transport offers a green alternative to road and air transportation, but even on the high seas boosting efficiency and sustainable optimization of resource usage are key concerns. The International Maritime Organization (IMO) has set a target of achieving a 10% increase in the efficiency of new ships by 2020, and CO2 emissions per tonne are to be cut by 20% across the entire industry.2 Today's shipping industry has to meet ever-greater business expectations and increasingly stricter regulatory requirements. One response to this has been more widespread use of a cutting edge engine technology that allows active control of the combustion process - closed loop combustion control (CLCC). Whenever monitoring and control of combustion in large marine and stationary engines is required, Kistler is on hand with proven, reliable solutions - customized as required for every customer, including the necessary certifications.

Cylinder pressure measurement is the crucial factor in CLCC for large engines - this provides on-line feedback information to the engine control system about the actual operating conditions in the combustion chamber. Analysis of data from CLCC systems in use today provides clear evidence on how the efficiency of 2-stroke or 4-stroke engines can be enhanced. Fuel consumption improvements, of as much as 2%, stability of emissions over long operating periods, and the ability to optimize maintenance intervals, all lead to short term operational cost savings for the engine operators. The advantages of this are even more evident when operating with mixed or variable quality fuels. The systems also provide longer term potential savings for customers; from the early warning detection of engine operating issues that could otherwise lead to very high repair costs, and from a general reduction in engine component wear that the elimination of high load combustion events made possible with CLCC can achieve.

Combustion Control in Continuous Operation with Reliable On-line Monitoring

Kistler has designed rugged piezoelectric cylinder pressure sensors to meet the special requirements of on-line combustion monitoring in marine and stationary engine installations. These long service lifetimes – installed on the cylinder head of low- and medium-speed engines – are the key to our success in this market.

Certified Industry Standard: Offline Diagnosis

Cylinder pressure also provides meaningful information about the condition of an engine when used as a regular maintenance basis – as an off-line diagnostic tool. All large engine classification companies specify regular cylinder pressure measurements as a standard – and this data provides the essential basis for maintaining good fuel consumption. Peak pressures on large engines can be recorded periodically by Kistler's diagnostic equipment, with immediate evaluation using the software supplied with the products. This rugged equipment can be installed quickly and easily on the indicator valve on the engine and delivers accurate and reliable measurement data from sensors with proven long-term stability.

Reliable Sensor and System Expertise – from One Single Source

When a customer needs to monitor and control large engines, they need look no further than Kistler: we offer cylinder pressure sensors backed by all the service and system expertise necessary – allowing us to develop cost-effective solutions tailored to the needs of each specific customer. Jürg Stadler, Head of Kistler’s Strategic Business Field Marine & Stationary, proudly explains, “Our many years of expertise in cylinder pressure measurement provide the basis for combustion control for many manufacturers of large engines, shipbuilders, shipping companies and power plant operators. One example is General Electric (GE) - this manufacturer of energy technology solutions in power generation was so enthusiastic about our professional, customer focused, service offering that the company awarded us GE's prize for innovative capacity and technology leadership in 2015.”

Kistler has over 20 years of experience in engine diagnostics, operational monitoring and engine combustion control and has cost-effective solutions that offer both long-term reliability and an early return on investment for our customers.

For more information visit Marine & Stationary.

1 International Chamber of Shipping (ICS): Shipping, World Trade and the Reduction of CO2 Emissions. United Nations Framework Convention on Climate Change (UNFCCC). 2014
2 IMO: MARPOL Annex VI, Capter 4, adopted July 2011: www.imo.org/en/OurWork/Environment/PollutionPrevention/AirPollution/Pages/Technical-and-Operational-Measures.aspx


Contact for Users
Jürg Stadler
Head of Engine Marine & Stationary
Tel.: +41 52 224 19 49
Email: jürg.stadler@kistler.com

Media Contact
Lisa Glatz
Divisional Marketing Manager ART
Tel.: +41 52 224 12 31
Email: lisa.glatz@kistler.com 

KIT PARA MEDIOS INFORMATIVOS

Kistler portrait with logo for a quick overview: Kistler Press Kit.zip

12/04/2018
The global leader in dynamic measurement technology supports the passion for innovation and technology with a...
06/03/2018
Kistler will be showcasing at Control 2018 its portfolio of industrial testing and inspection systems with the...
16/02/2018
At Intertraffic 2018 the Kistler Group is showcasing its comprehensive KiTraffic Weigh In Motion (WIM)...
15/02/2018
At NPE 2018 in Orlando, Florida, the Kistler Group will demonstrate a wide range of modular functionalities...
31/01/2018
The new KiSprint provides coaches and athletes with an efficient means of biomechanically optimizing sprint...
24/01/2018
Kistler achieved a growth rate of 18 % in 2017. Digital transformation has top priority in 2018.
23/01/2018
Overcoming the complexities of RTM – with Kistler
12/10/2017
At the SPS IPC Drives Kistler Group will unveil the world's first digital charge amplifier Type 5974A, a...
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
Kistler Group took over near Karlsruhe-based Vester Elektronik GmbH on 25 August, a specialist in sensor...
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
At Moulding Expo 2017, we will show how easy it is to install the measurement technology needed for quality...
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
27/10/2016
At this year's SPS IPC Drives in Nuremberg Kistler will premiere laboratory systems to analyze bolted joints,...
21/10/2016
Kistler boosts the efficiency and reliability of large marine and stationary engines through monitoring and...
19/10/2016
Kistler is presenting the new versions of its ComoNeo and ComoDataCenter.
10/10/2016
Kistler is unveiling a new addition to its portfolio of electromechanical joining modules.
30/09/2016
The Kistler Group reported incoming orders worth CHF 233.3 million at the end of August 2016 and has therefore...
07/09/2016
At this year's K Trade Fair from 19 to 26 October in Düsseldorf, Kistler will be showcasing its latest new...
24/07/2016
Kistler will be showcasing its new NCFE and NCFR joining modules, together with the latest generation of...
12/07/2016
Kistler's Correvit® SFII sensor measures world record in 1.513 seconds
12/05/2016
Screw technology complements the range of applications.
27/04/2016
Following a long phase of planning, preparations, and conversion work, Kistler Instrumente GmbH has a new home...