Kistler pushes the limits of sensor technology for injection molding

Winterthur, October 2022 – Thanks to a new PiezoStar crystal, the 9239B miniature longitudinal measuring pin from Kistler achieves almost five times the sensitivity of its predecessor – which already ranked as the technology leader. Also new: the 2205B thermocouple amplifier – now with multiple improvements – to integrate temperature sensors more efficiently into the measuring chain for high-grade injection molding.

Contact-free cavity pressure measurement with piezoelectric sensors is the most sophisticated of the three measurement methods used in injection molding (the other two are direct and indirect measurement). The contact-free method is mainly used where high quality and process requirements have to be met: examples include absolutely flawless products for automobile interiors, high optical quality (for items such as lenses), or situations where very compact injection molds are used.

The 9239B miniature longitudinal measuring pin from Kistler gives customers a cavity pressure sensor that takes up virtually no space when installed (diameter: 2.5 mm), and performs its task without contacting the melt. It is mounted directly behind the cavity wall in the mold structure or the embossing die, where it measures the pressure-induced compression of the mold during the injection and holding pressure phases. "Thanks to its compact dimensions for optimal installation, the 9239B gives moldmakers more freedom when positioning it in smaller molds or multi-cavity molds with more complex structures," according to Marko Marceta, Product Manager Plastics at Kistler.

Utmost accuracy – but no contact with the part

The 9239B miniature longitudinal measuring pin represents a major advance on its predecessor model: it features a PiezoStar crystal grown by Kistler itself, which increases the sensitivity many times over – to no less than 27 pC/N. The new measuring pin from Kistler is a world first that elevates contact-free cavity pressure measurement to an unprecedented level of accuracy. The mounting method eliminates the possibility of marks on the part, and the sensor is not exposed to abrasion or corrosion. Another benefit: because the measuring pin is installed in the preloaded state, it can capture both compression and tensile forces with very high accuracy.

Using temperature sensors more flexibly

Kistler has also made significant improvements to its 2205B multichannel temperature amplifier. It is used to convert signals from temperature sensors installed in the injection mold (known as thermocouples) into standardized voltage signals. These improvements have been incorporated as compared to the 2205A predecessor model:

  • Eight channels for up to eight thermocouples
  • Simultaneous connection of different types (K, J, N) is now possible
  • Type J thermocouples can also be used at 400°C
  • Uniform measurement range (0 to 400°C) reduces variants

Measuring the mold temperature opens up further scope for process monitoring and control of injection molding with thermoplastics, and for many other applications. The 2205B has a standard operating temperature range of 125°C which can be extended to 195°C with an additional housing. The temperature sensors are connected using the cut-and-grip method to avoid the need for connectors and tools.

Final words from Dr. Robert Vaculik, Head of BU Plastics at Kistler: "With these two innovations, we are offering our customers yet more opportunities to continue enhancing the quality of their products and manufacturing processes. They are ideal for Class A surfaces or in the medical sector, for instance: the key to setting new standards for industrial injection molding."

KIT PARA MEDIOS INFORMATIVOS

Paquete multimedia con PDF, archivo Word e imágenes de alta resolución: Kistler Press Kit.zip

04/10/2022
Two new products deliver yet more improvements to cavity pressure and temperature measurements in plastics processing.
27/09/2022
The new SlimLine Sensor 9132CD is nine times more sensitive than comparable SlimLine sensors.
16/09/2022
At K 2022, Kistler will showcase its solutions for injection molding that make plastics processing more intelligent and sustainable.
06/09/2022
With ComoScout, Kistler offers a simple and cost-effective process monitoring system for injection molding processes.
31/08/2022
High-end measurement systems for rolling stock – from brake testing to traffic monitoring.
22/08/2022
Artificial intelligence in punching: AI helps manufacturers improve product quality and step up their quality assurance.
12/08/2022
New wireless dynamometer allows for highly accurate measurements of cutting forces.
28/07/2022
The most successful triaxial accelerometer 8763B measures micro-vibrations even more accurately.
31/05/2022
Kistler showcases needs-oriented solutions for the Smart Factory and presents the extensive software and service resources.
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
The new joining module is highly suitable for clinching and riveting, and also for assembly processes that require force-displacement monitoring.
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
The Kistler Group will showcase its test and analysis systems for threaded joints at the 2019 Fastener Fair in Stuttgart from 19 to 21 March.
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
Accurate and insensitive to its mounting position: the new Type 6044A M8 sensor features an anti-strain design to ensure reliable, high-quality results.
20/11/2018
Motorsport: the new 4080B/BT absolute pressure sensors from Kistler – for real-time monitoring with maximum measurement accuracy and signal quality!
16/10/2018
At Fakuma 2018, the Kistler Group is showcasing its latest monitoring and control packages for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
08/10/2018
The SMETEC Gesellschaft für Sensor-, Motor- und Energietechnik mbH recently became part of the Kistler Group.
24/09/2018
The Kistler Group is adding another variant to what is already the world's most comprehensive portfolio of wheel force measurement systems: the new RoaDyn S6GT 6-component wheel force measurement system.
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
The Kistler Group is introducing a compact mobile measurement solution for enhanced rolling stock maintenance in international railway operations in the shape of its railway brake force measuring system Type 2899A.
21/08/2018
A new Center of Competence for production control and management systems will be opened in Aachen.
31/07/2018
Competent service just a call away has always been a key aspect of Kistler's cooperation with its customers. Now, in a move to address growing demand in North Germany, the measurement technology experts are opening a new office in Wolfsburg.
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
Digitization, Internet of Things and Industry 4.0 are presenting major challenges. Discover how Kistler responds to the great challenges of our times.
09/05/2018
At Sensor + Test 2018 Kistler will be introducing a milestone in measurement technology: its new KiDAQ data acquisition system.
08/05/2018
At NPE 2018, the Kistler Group is showcasing its latest custom monitoring package for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
03/05/2018
At Automatica 2018, the Kistler Group will turn the spotlight on diverse options for using sensors and process monitoring systems to support industrial production and enhance digitalization in test and assembly technology.
24/04/2018
The Kistler Group will showcase its expanded portfolio of industrial test and inspection systems for quality assurance at the 2018 Control trade show.
12/04/2018
The global leader in dynamic measurement technology supports the passion for innovation and technology with a three-year partnership.
06/03/2018
Kistler will be showcasing at Control 2018 its portfolio of industrial testing and inspection systems with the spotlight on the very latest additions.
16/02/2018
At Intertraffic 2018 the Kistler Group is showcasing its comprehensive KiTraffic Weigh In Motion (WIM) solutions, which support road owners and authorities in road and traffic monitoring, weight enforcement and weight-based tolling.
15/02/2018
At NPE 2018 in Orlando, Florida, the Kistler Group will demonstrate a wide range of modular functionalities for ComoNeo: the process monitoring system that takes injection molding to a higher level with integrated quality monitoring geared to meet customers’ needs and requirements.
31/01/2018
The new KiSprint provides coaches and athletes with an efficient means of biomechanically optimizing sprint starts under competitive conditions. The robust and mobile solution has comprehensive software assessment options and can be individually adapted and expanded.
24/01/2018
Kistler achieved a growth rate of 18 % in 2017. Digital transformation has top priority in 2018.
23/01/2018
Overcoming the complexities of RTM – with Kistler
12/10/2017
At the SPS IPC Drives Kistler Group will unveil the world's first digital charge amplifier Type 5974A, a milestone more in electrical automation.
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
With MARS software version 3.0, Kistler presents an extensive update of the proprietary measurement, analysis, and evaluation software for Kistler force plates.
21/10/2016
Kistler boosts the efficiency and reliability of large marine and stationary engines through monitoring and control of the combustion process
19/10/2016
Kistler is presenting the new versions of its ComoNeo and ComoDataCenter.
10/10/2016
Kistler is unveiling a new addition to its portfolio of electromechanical joining modules.
30/09/2016
The Kistler Group reported incoming orders worth CHF 233.3 million at the end of August 2016 and has therefore seen growth of 8.4 % compared to the same period in the previous year, or 5.6 % when adjusted for currency effects.
07/09/2016
At this year's K Trade Fair from 19 to 26 October in Düsseldorf, Kistler will be showcasing its latest new products and features with the focus on Industry 4.0.
24/07/2016
Kistler will be showcasing its new NCFE and NCFR joining modules, together with the latest generation of maXYmos monitoring systems on Motek 2016
12/07/2016
Kistler's Correvit® SFII sensor measures world record in 1.513 seconds
12/05/2016
Screw technology complements the range of applications.
27/04/2016
Following a long phase of planning, preparations, and conversion work, Kistler Instrumente GmbH has a new home for its German headquarters at the Böblingen/Sindelfingen airfield.
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
At Chinaplas 2015 Kistler will be presenting solutions for zero-defect production, process monitoring and data evaluation in injection molding
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
At Sensor + Test 2014 Kistler is presenting many new features from the field of measurement electronics in addition to its already proven sensor technology.
19/05/2014
Users obtain a full range of force–displacement measurement systems from one source
06/02/2014
The Kistler Group achieved sales of 285 million CHF in 2013, thus marking a slight growth in comparison with the figures for the prior year.