Presenting ComoNeo at Fakuma

Winterthur, 1 September 2015 – Kistler will unveil its new ComoNeo process monitoring system at the Fakuma trade fair from 13 to 17 October 2015. The ComoNeo is the system of choice for any company that aims to optimize monitoring and analysis of the injection molding process so as to cut costs permanently.

For many years, Kistler's innovative solutions to enhance process reliability in injection molding have ensured the firm's leading position in the global market. These systems all feature mature technology with one common denominator: quality testing is integrated into the injection molding process. The benefit: faulty parts can be excluded from the production process before they cause unnecessary costs. The ComoNeo process monitoring system – to be premiered at the 2015 Fakuma – moves automated production process monitoring into a new dimension: first-time customers will find that Kistler's new system provides a simple introduction, while users with experience in this field will appreciate the technological advances that it offers.

Simple, Intuitive Operation
The ComoNeo process monitoring system breaks new ground in the development of hardware as well as integrated monitoring software. To start with, the entirely new intuitive design sets new standards. The display − equipped with optimized touch-based operation – is now more closely tailored to users' needs. Users also benefit directly from the increased number of channel inputs on the ComoNeo: twice as many cavity pressure signals can now be recorded, so molds with a large number of cavities can be connected. Likewise, the number of digital outputs is doubled, so more components can be evaluated individually. The ComoNeo software is also committed to a process-oriented operating philosophy – as is clear from the various new tools that offer active support with analyzing process fluctuations and monitoring component quality. This system is ideal for highly quality-conscious companies that aim for systematic analysis and optimization of their processes – and it is also an excellent choice for firms that focus on the transparency of their injection molding processes and comprehensive documentation of component quality.

Innovative Functions for Optimized Processes
Daniel Fick, Kistler's Product Manager in the Plastics Strategic Business Field, emphasizes the high innovative content of this newly developed product: "The launch of ComoNeo has moved auto-mated monitoring of the injection molding process into a new dimension. A host of innovative functions position ComoNeo on the market as a powerfully attractive process monitoring system." One outstanding highlight of the integrated monitoring software is the tool that generates and positions the monitoring boxes for good/bad evaluation. In the past, users had to set the monitoring boxes themselves. Now, the ComoNeo includes a systematic process (Evaluation Assistant/EO Assistant) that guides the user quickly and accurately to the rejection limits. The results from the EO Assistant therefore define the evaluation types and the relevant limits. Thanks to this approach, components can be monitored with high precision and pseudoscrap (i.e. "presumed" scrap) is reduced. Complaints from customers are also avoided because no faulty components leave the production line. Reducing pseudoscrap and eliminating rejects are two especially crucial factors in cutting production costs in the injection molding process.

The "dashboard" is a second highlight: this is an overview screen that collates all the relevant process data to give a clear picture of how the production lot is currently progressing. Thanks to the dashboard, Kistler customers can detect process fluctuations very quickly. Users can also navigate directly from the dashboard to the detailed data. Another attractive innovation: the operating controls and procedures are consistently geared to the injection molding process – for instance, cavity-specific analyses can be carried out.

Additional Tools to Improve Process Monitoring
But that's not all: ComoNeo offers even more tools – such as the newly-designed user management feature that allows every company to set up its own specific roles for various users, and automatic mold identification to prevent errors on the interface between the mold and the integrated monitoring software. Automated mold selection also reduces retooling times. In a nutshell: when the objective is to maximize production efficiency in the injection molding process, ComoNeo is the process monitoring system of choice for quality-conscious companies.

Kistler is presenting its new ComoNeo process monitoring system at Fakuma in Friedrichshafen from 13 to 17 October 2015 on stand 3104 in hall A3.

Download Press Release

User Contact
Daniel Fick
Product Manager
Phone: +41 52 224 16 06
E-Mail: daniel.fick(at)kistler.com

 

Media Contact
Simone Koch
Divisional Marketing Manager IPC
Phone +41 52 2241 802
E-Mail: simone.koch(at)kistler.com

KIT PARA MEDIOS INFORMATIVOS

Kistler portrait with logo for a quick overview: Kistler Press Kit.zip

12/04/2018
The global leader in dynamic measurement technology supports the passion for innovation and technology with a...
06/03/2018
Kistler will be showcasing at Control 2018 its portfolio of industrial testing and inspection systems with the...
16/02/2018
At Intertraffic 2018 the Kistler Group is showcasing its comprehensive KiTraffic Weigh In Motion (WIM)...
15/02/2018
At NPE 2018 in Orlando, Florida, the Kistler Group will demonstrate a wide range of modular functionalities...
31/01/2018
The new KiSprint provides coaches and athletes with an efficient means of biomechanically optimizing sprint...
24/01/2018
Kistler achieved a growth rate of 18 % in 2017. Digital transformation has top priority in 2018.
23/01/2018
Overcoming the complexities of RTM – with Kistler
12/10/2017
At the SPS IPC Drives Kistler Group will unveil the world's first digital charge amplifier Type 5974A, a...
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
Kistler Group took over near Karlsruhe-based Vester Elektronik GmbH on 25 August, a specialist in sensor...
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
At Moulding Expo 2017, we will show how easy it is to install the measurement technology needed for quality...
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
27/10/2016
At this year's SPS IPC Drives in Nuremberg Kistler will premiere laboratory systems to analyze bolted joints,...
21/10/2016
Kistler boosts the efficiency and reliability of large marine and stationary engines through monitoring and...
19/10/2016
Kistler is presenting the new versions of its ComoNeo and ComoDataCenter.
10/10/2016
Kistler is unveiling a new addition to its portfolio of electromechanical joining modules.
30/09/2016
The Kistler Group reported incoming orders worth CHF 233.3 million at the end of August 2016 and has therefore...
07/09/2016
At this year's K Trade Fair from 19 to 26 October in Düsseldorf, Kistler will be showcasing its latest new...
24/07/2016
Kistler will be showcasing its new NCFE and NCFR joining modules, together with the latest generation of...
12/07/2016
Kistler's Correvit® SFII sensor measures world record in 1.513 seconds
12/05/2016
Screw technology complements the range of applications.
27/04/2016
Following a long phase of planning, preparations, and conversion work, Kistler Instrumente GmbH has a new home...