KiBox Software Update

With the new software update V2.1, Kistler’s KiBox can now be used directly on engine test benches, as well for mobile applications in vehicles on the road. Additional new features also broaden the scope of use for KiBox: new calculation options, added virtual channels and valuable expert functions. Developed in close collaboration with customers, this software can now be downloaded free of charge from Kistler's website.

KiBox Cockpit V2.1 for Use on Engine Test Benches
Kistler's KiBox is now fully usable on test benches with the update to version 2.1. A universal test bench interface means that it can be integrated into commonly used automation systems such as Morphee, PUMA Open and Stars. This makes it possible not only to control the combustion analysis system but also to output measurands to the automation system, opening up a host of potential applications for users.

Extended Hardware Compatibility
KiBox Cockpit V2.1 supports accurate determination of the Top Dead Center (TDC) with the help of a capacitive TDC probe. This is an extremely useful feature, especially for high-precision test bench measurements. Another benefit of the new software: Kistler's new Type 4665B piezoresistive amplifier with automatic sensor identification (PiezoSmart®) and analog sensor temperature output is now supported as well. This marks a further logical advance in the concept for shared use of Kistler's SCP (Signal Conditioning Platform) components.

Added Virtual Channels
The new software introduces virtual channels to increase the number of available channels. Multiplexed ignition or injection signals from several cylinders can now be connected to one current probe input, so ignition or injection timing calculations can be performed for all cylinders.

Calculations and Expert Functions
Several new features make the Kistler KiBox more efficient, more precise and more convenient for users: new calculation methods and calculations such as ‘indicated torque’, a general statistics package and additional expert functions for data display and analysis.

Key Features at a Glance:

      • Support of piezoresistive amplifier Type 4665B
      • TDC determination from capacitive probe
      • Multicylinder function (Demultiplex)
      • Extended IMEP calculation
      • CDM and Trigger
      • General statistics calculations
      • TDC determination from cylinder pressure: extended functions
      • Improved display refreshrate
      • New diagram type: X/Y
      • Improved/extended Ifile, MDF, CSV conversions

 

Click here to download our software free of charge and get to the KiBOX overview page. 

Close Collaboration with Customers
Kistler provides individual support to numerous OEMs by acting as a powerful development partner. Thanks to customized solutions and a range of services tailored to clients' requirements, Kistler meets the most diverse challenges – always on the basis of eye-to-eye relationships with customers. The new software KiBox Cockpit V2.1 was developed in close collaboration with customers.

Please click here to get an overview of Kistler's measurement solutions for engine indication.

KIT PARA MEDIOS INFORMATIVOS

Kistler portrait with logo for a quick overview: Kistler Press Kit.zip

12/04/2018
The global leader in dynamic measurement technology supports the passion for innovation and technology with a...
06/03/2018
Kistler will be showcasing at Control 2018 its portfolio of industrial testing and inspection systems with the...
16/02/2018
At Intertraffic 2018 the Kistler Group is showcasing its comprehensive KiTraffic Weigh In Motion (WIM)...
15/02/2018
At NPE 2018 in Orlando, Florida, the Kistler Group will demonstrate a wide range of modular functionalities...
31/01/2018
The new KiSprint provides coaches and athletes with an efficient means of biomechanically optimizing sprint...
24/01/2018
Kistler achieved a growth rate of 18 % in 2017. Digital transformation has top priority in 2018.
23/01/2018
Overcoming the complexities of RTM – with Kistler
12/10/2017
At the SPS IPC Drives Kistler Group will unveil the world's first digital charge amplifier Type 5974A, a...
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
Kistler Group took over near Karlsruhe-based Vester Elektronik GmbH on 25 August, a specialist in sensor...
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
At Moulding Expo 2017, we will show how easy it is to install the measurement technology needed for quality...
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
27/10/2016
At this year's SPS IPC Drives in Nuremberg Kistler will premiere laboratory systems to analyze bolted joints,...
21/10/2016
Kistler boosts the efficiency and reliability of large marine and stationary engines through monitoring and...
19/10/2016
Kistler is presenting the new versions of its ComoNeo and ComoDataCenter.
10/10/2016
Kistler is unveiling a new addition to its portfolio of electromechanical joining modules.
30/09/2016
The Kistler Group reported incoming orders worth CHF 233.3 million at the end of August 2016 and has therefore...
07/09/2016
At this year's K Trade Fair from 19 to 26 October in Düsseldorf, Kistler will be showcasing its latest new...
24/07/2016
Kistler will be showcasing its new NCFE and NCFR joining modules, together with the latest generation of...
12/07/2016
Kistler's Correvit® SFII sensor measures world record in 1.513 seconds
12/05/2016
Screw technology complements the range of applications.
27/04/2016
Following a long phase of planning, preparations, and conversion work, Kistler Instrumente GmbH has a new home...