Torque Sensors and maXYmos

Winterthur, October 27, 2015 – At this year's SPS IPC Drives (November 24-26,2015), Kistler will be presenting its latest torque sensor portfolio in combination with the extended maXYmos family, as well as the latest applications in the field of product testing and development.

In the industrial production sector, more and more manufacturers rely on Kistler sensor technology to monitor each stage of the assembly process when manufacturing safety-related components. As a leader in the field of measuring and system technology with a wide range of torque sensors, Kistler provides the ideal solution for every application – whether in testing couplings, testing torque to determine screw quality, or testing the push-and-turn caps on nasal sprays. In addition, Kistler's high-precision torque sensors are also used in the field of development; for example, to determine the efficiency of electric motors or friction coefficients at test benches.

Product Testing with maXYmos TL: Higher Quality and Lower Costs
By gradually expanding its product portfolio, Kistler has secured its reputation worldwide as a leading supplier of sensor systems. Thanks to the innovative development of the maXYmos family in particular, the uniformity of the systems and their simple, intuitive handling are now part of day-today industrial manufacturing operations. When testing products, users can access a simple system that enables them to perform various tests quickly and accurately – not only by force-displacement monitoring, but now also by monitoring the torque over time or angle of rotation.

With its wide range of interfaces, the system provides an ideal platform for recording a large number of measurands and their evaluation. Thanks to the user-friendly ‘Sequencer Mode’, test sequences can be programmed in the device and analyzed online in real-time. These sequences can easily be parameterized on the device and perform simple control tasks.

The maXYmos TL detects defective parts or deviations early in the production process and displays them transparently. This leads to minimized downtimes, optimized test sequences, and improved plant availability. Thus, the integrated process control enables higher quality and lower costs in assembly and testing.

Torque Sensors: Central Role in Product Development
Kistler’s sensor technology is not only used in direct product testing in the production process, but also in the test bench field for quality monitoring. The accuracy and flexibility requirements for test systems, i.e. evaluating the efficiency of power train components, continue to grow. Robust, highly accurate torque sensors are particularly in demand for determining friction coefficients and performance factors.

Latest Torque Portfolio for Maximum Accuracy
Visitors to this year's SPS IPC Drives can be convinced that Kistler is leading in the development of high-precision torque sensors. Kistler will be presenting the KiTorq Type 4550A with angle measurement for the first time. Compared to the KiTorq Type 4551A, this newly developed sensor now enables the measurement of torque, speed, and rotation of angle with an unprecedented resolutionof up to 8 192 pulses per revolution. The number of pulses can be freely adjusted to meet the user’s requirements. The torque measuring flange system consists of a measurement body, the KiTorq rotor, and an evaluation unit (the KiTorq stator). For manufacturers of electric and combustion engines, drives, pumps and compactors, the system provides wide flexibility thanks to the guideless stator in that measurement bodies can be used without having to completely rebuild the test facility.

Type 4503B, also being presented at this year’s SPS IPC Drives, offers a number of enhanced functions to satisfy current industry standards. For example, optical speed and angle measurement have been replaced by a magnetic one. This means the sensor is now safe and robust enough for use in contaminated industrial environments (e.g., oil mist), which saves valuable maintenance time. Furthermore, the electronics of the torque sensor have been improved. For highly dynamic measurements, Type 4503B also has a cut-off frequency of 10 kHz. Users can customize it individually via an integrated digital low-pass filter, while the second measuring range can be flexibly scaled up to a spread of 1:10. In addition, the Type 4503B is characterized by large measuring ranges of 0.2 … 5 000 Nm, as well as an integrated rotational speed/angle measurement up to 8 192 pulses/revolution and a high-speed version with up to 50 000 rpm.

Innovative Products for a Dynamic Market
With the KiTorq Type 4551A and 4503B torque sensors, as well as the new KiTorq Type 4550A with angle measurement, Kistler's torque sensor portfolio fulfills all market requirements as these sensors offer maximum dynamics and accuracy for industrial manufacturers. Compatible with previous
versions, the new torque sensors can also be integrated in existing systems with minimal effort. The key benefits of the maXYmos monitoring system also apply to the torque sensors presented at the SPS IPC Drives: They improve transparency in the testing process, and therefore boost quality and reduce production costs.

Kistler is presenting its newest sensors and systems at SPS IPC Drives in Nuremberg from 24 to 26 November 2015, booth 526 in hall 4A.


Download Press Release (PDF)

User Contact
Stephan Vogel
Business Development Manager
Phone: +49 7172 184 187
Email: stephan.vogel@kistler.com

 

Media Contact
Simone Koch
Divisional Marketing Manager IPC
Phone +41 52 2241 802
Email: simone.koch@kistler.com

KIT PARA MEDIOS INFORMATIVOS

Kistler portrait with logo for a quick overview: Kistler Press Kit.zip

18/07/2018
Effective monitoring with strain sensors protects machines and tools
03/07/2018
The Top 100 Competition has again singled out the most innovative German small and medium-sized enterprises...
25/06/2018
Kistler is pleased to introduce MicroDyn, the world's smallest series-produced cutting force meter.
19/06/2018
Kistler introduces the world’s first high temperature accelerometer for the monitoring of gas turbines.
11/06/2018
Kistler is earmarking the highest investment budget for research and development in the company`s history.
09/05/2018
At Sensor + Test 2018 Kistler will be introducing a milestone in measurement technology: its new KiDAQ data...
08/05/2018
At NPE 2018, the Kistler Group is showcasing its latest custom monitoring package for ComoNeo, its...
03/05/2018
At Automatica 2018, the Kistler Group will turn the spotlight on diverse options for using sensors and process...
24/04/2018
The Kistler Group will showcase its expanded portfolio of industrial test and inspection systems for quality...
12/04/2018
The global leader in dynamic measurement technology supports the passion for innovation and technology with a...
06/03/2018
Kistler will be showcasing at Control 2018 its portfolio of industrial testing and inspection systems with the...
16/02/2018
At Intertraffic 2018 the Kistler Group is showcasing its comprehensive KiTraffic Weigh In Motion (WIM)...
15/02/2018
At NPE 2018 in Orlando, Florida, the Kistler Group will demonstrate a wide range of modular functionalities...
31/01/2018
The new KiSprint provides coaches and athletes with an efficient means of biomechanically optimizing sprint...
24/01/2018
Kistler achieved a growth rate of 18 % in 2017. Digital transformation has top priority in 2018.
23/01/2018
Overcoming the complexities of RTM – with Kistler
12/10/2017
At the SPS IPC Drives Kistler Group will unveil the world's first digital charge amplifier Type 5974A, a...
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
Kistler Group took over near Karlsruhe-based Vester Elektronik GmbH on 25 August, a specialist in sensor...
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
At Moulding Expo 2017, we will show how easy it is to install the measurement technology needed for quality...
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
27/10/2016
At this year's SPS IPC Drives in Nuremberg Kistler will premiere laboratory systems to analyze bolted joints,...
21/10/2016
Kistler boosts the efficiency and reliability of large marine and stationary engines through monitoring and...
19/10/2016
Kistler is presenting the new versions of its ComoNeo and ComoDataCenter.
10/10/2016
Kistler is unveiling a new addition to its portfolio of electromechanical joining modules.
30/09/2016
The Kistler Group reported incoming orders worth CHF 233.3 million at the end of August 2016 and has therefore...
07/09/2016
At this year's K Trade Fair from 19 to 26 October in Düsseldorf, Kistler will be showcasing its latest new...
24/07/2016
Kistler will be showcasing its new NCFE and NCFR joining modules, together with the latest generation of...
12/07/2016
Kistler's Correvit® SFII sensor measures world record in 1.513 seconds
12/05/2016
Screw technology complements the range of applications.
27/04/2016
Following a long phase of planning, preparations, and conversion work, Kistler Instrumente GmbH has a new home...