Accurate measurement under extreme conditions

Winterthur, July 2020 – The Kistler Group has launched a new cylinder pressure sensor for the continuous monitoring of large marine and stationary engines. Used in four-stroke gas, dual-fuel and diesel engines in shipping as well as power stations, closed loop combustion control can achieve fuel savings of up to two percent annually. The new sensor 6635A1 from Kistler stands out for its high measuring accuracy under extreme conditions in the combustion chamber.

Dual-fuel engines can be operated with natural gas or renewable fuels in addition to conventional liquid fuels, thus helping reduce fuel oil consumption and CO2 emissions. For dual-fuel engines to perform optimally, their combustion processes must be continuously monitored and controlled. This is the main application of the new 6635A1 cylinder pressure sensor. The sensors are used to monitor all cylinders simultaneously and provide accurate data. Knocking in the combustion chamber is determined just as precisely as the prevailing indicated mean effective pressure. The continuous monitoring of cylinder pressure enables closed loop combustion control, which results in increased engine performance as well as fuel savings. With the help of closed loop combustion control, fuel consumption can be reduced by approximately two percent per engine per year, amounting to an average reduction of 200 tons of hazardous CO2.

Continuous monitoring in the combustion chamber

In the combustion chamber, harsh conditions such as extreme mechanical shocks and vibrations, high temperatures and high pressures are at play. This requires particularly resilient sensors. To ensure reliable signal transmission, the 6635A1 cylinder pressure sensor utilizes welded connections instead of traditional plug connectors. Thus, mechanical shocks of up to 2000 g are no problem. The optimized diaphragm design minimizes the thermal shock error while enabling reliable peak pressure measurement up to 350 bar. PiezoStar crystals, which are grown specially by Kistler, are another new feature. They offer exceptional measurement stability and minimal temperature dependence in demanding environments. The sensors function reliably at temperatures of up to 350°C. 

"Thanks to many years of experience in cylinder pressure measurement, Kistler guarantees reliable measurement data that can be used to detect problems early on and enable optimum control of the combustion process. Based on this measurement data, maintenance intervals can be optimized and downtimes can be planned," Miika Jussila, head of marine & stationary engines at Kistler, explains. 

Operators of large marine and stationary engines thus benefit from high-quality measurement data, which can be used to optimize the combustion process. As a result, tons of fuel and CO2 emissions can be saved.

KIT PARA MEDIOS INFORMATIVOS

Paquete multimedia con PDF, archivo Word e imágenes de alta resolución: Kistler Press Kit.zip

31/05/2022
Kistler showcases needs-oriented solutions for the Smart Factory and presents the extensive software and service resources.
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
The new joining module is highly suitable for clinching and riveting, and also for assembly processes that require force-displacement monitoring.
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
The Kistler Group will showcase its test and analysis systems for threaded joints at the 2019 Fastener Fair in Stuttgart from 19 to 21 March.
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
Accurate and insensitive to its mounting position: the new Type 6044A M8 sensor features an anti-strain design to ensure reliable, high-quality results.
20/11/2018
Motorsport: the new 4080B/BT absolute pressure sensors from Kistler – for real-time monitoring with maximum measurement accuracy and signal quality!
16/10/2018
At Fakuma 2018, the Kistler Group is showcasing its latest monitoring and control packages for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
08/10/2018
The SMETEC Gesellschaft für Sensor-, Motor- und Energietechnik mbH recently became part of the Kistler Group.
24/09/2018
The Kistler Group is adding another variant to what is already the world's most comprehensive portfolio of wheel force measurement systems: the new RoaDyn S6GT 6-component wheel force measurement system.
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
The Kistler Group is introducing a compact mobile measurement solution for enhanced rolling stock maintenance in international railway operations in the shape of its railway brake force measuring system Type 2899A.
21/08/2018
A new Center of Competence for production control and management systems will be opened in Aachen.
31/07/2018
Competent service just a call away has always been a key aspect of Kistler's cooperation with its customers. Now, in a move to address growing demand in North Germany, the measurement technology experts are opening a new office in Wolfsburg.
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
Digitization, Internet of Things and Industry 4.0 are presenting major challenges. Discover how Kistler responds to the great challenges of our times.
09/05/2018
At Sensor + Test 2018 Kistler will be introducing a milestone in measurement technology: its new KiDAQ data acquisition system.
08/05/2018
At NPE 2018, the Kistler Group is showcasing its latest custom monitoring package for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
03/05/2018
At Automatica 2018, the Kistler Group will turn the spotlight on diverse options for using sensors and process monitoring systems to support industrial production and enhance digitalization in test and assembly technology.
24/04/2018
The Kistler Group will showcase its expanded portfolio of industrial test and inspection systems for quality assurance at the 2018 Control trade show.
12/04/2018
The global leader in dynamic measurement technology supports the passion for innovation and technology with a three-year partnership.
06/03/2018
Kistler will be showcasing at Control 2018 its portfolio of industrial testing and inspection systems with the spotlight on the very latest additions.
16/02/2018
At Intertraffic 2018 the Kistler Group is showcasing its comprehensive KiTraffic Weigh In Motion (WIM) solutions, which support road owners and authorities in road and traffic monitoring, weight enforcement and weight-based tolling.
15/02/2018
At NPE 2018 in Orlando, Florida, the Kistler Group will demonstrate a wide range of modular functionalities for ComoNeo: the process monitoring system that takes injection molding to a higher level with integrated quality monitoring geared to meet customers’ needs and requirements.
31/01/2018
The new KiSprint provides coaches and athletes with an efficient means of biomechanically optimizing sprint starts under competitive conditions. The robust and mobile solution has comprehensive software assessment options and can be individually adapted and expanded.
24/01/2018
Kistler achieved a growth rate of 18 % in 2017. Digital transformation has top priority in 2018.
23/01/2018
Overcoming the complexities of RTM – with Kistler
12/10/2017
At the SPS IPC Drives Kistler Group will unveil the world's first digital charge amplifier Type 5974A, a milestone more in electrical automation.
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
With MARS software version 3.0, Kistler presents an extensive update of the proprietary measurement, analysis, and evaluation software for Kistler force plates.
21/10/2016
Kistler boosts the efficiency and reliability of large marine and stationary engines through monitoring and control of the combustion process
19/10/2016
Kistler is presenting the new versions of its ComoNeo and ComoDataCenter.
10/10/2016
Kistler is unveiling a new addition to its portfolio of electromechanical joining modules.
30/09/2016
The Kistler Group reported incoming orders worth CHF 233.3 million at the end of August 2016 and has therefore seen growth of 8.4 % compared to the same period in the previous year, or 5.6 % when adjusted for currency effects.
07/09/2016
At this year's K Trade Fair from 19 to 26 October in Düsseldorf, Kistler will be showcasing its latest new products and features with the focus on Industry 4.0.
24/07/2016
Kistler will be showcasing its new NCFE and NCFR joining modules, together with the latest generation of maXYmos monitoring systems on Motek 2016
12/07/2016
Kistler's Correvit® SFII sensor measures world record in 1.513 seconds
12/05/2016
Screw technology complements the range of applications.
27/04/2016
Following a long phase of planning, preparations, and conversion work, Kistler Instrumente GmbH has a new home for its German headquarters at the Böblingen/Sindelfingen airfield.
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
At Chinaplas 2015 Kistler will be presenting solutions for zero-defect production, process monitoring and data evaluation in injection molding
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
At Sensor + Test 2014 Kistler is presenting many new features from the field of measurement electronics in addition to its already proven sensor technology.
19/05/2014
Users obtain a full range of force–displacement measurement systems from one source
06/02/2014
The Kistler Group achieved sales of 285 million CHF in 2013, thus marking a slight growth in comparison with the figures for the prior year.