Kistler unveils new products at Space Tech Expo Europe

Winterthur, 27 September 2017 – Space Tech Expo Europe, the main meeting-place for representatives of the European space industry, will open its doors from 24 to 26 October in Bremen, Germany. This international exposition is also a fixed event on Kistler's trade fair program: our experts will be on hand at stand A51 in hall 5 to show visitors measurement technology capabilities and solutions for challenging space applications.

Sensors play a key role in Space Payload, Propulsion and subsystem testing and provide valuable measurements to support quality, safety and reliability of space systems and subsystems. In this sector, products have to meet very demanding requirements due to extreme conditions that include wide temperature ranges, pressure fluctuations, high shock and vibration levels. At the same time, the measurement equipment often has to be lightweight as well as rugged and durable. Kistler offers the right force, vibration and pressure sensors for virtually every application.

As the highlight of our presence at Space Tech Expo Europe, we shall be presenting product solutions for selected space applications to the show visitors. At our fair stand, attendees can see exhibits such as a rocket engine test bench with built-in pressure, force and acceleration sensors, as well as the new piezoelectric 6-component force/torque link, Type 9306A.”

Manuel Blattner, Head of Kistler's Strategic Business Field Test & Measurement

 

Direct, accurate measurements – in every direction

Entire satellites and their subsystems could sustain severe damage due to overloads during vibration tests. Force Limited Vibration Testing is used to prevent this from happening. This testing uses 3-component force sensors at the shaker to payload interface to monitor the introduced forces. Kistler will exhibit the ideal solution for this application at the Space Tech Expo: preloaded 3-component piezoelectric force sensors connected to cutting edge signal conditioning and data acquisition systems. Installed between two mounting flanges, these preloaded sensors can measure compression and tensile forces in every direction. Accurate results are insured thanks to very high rigidity allowing for a high natural frequency as well as a very low crosstalk.

Signals are measured and conditioned with the LabAmp 5167A, Kistler's first multi-channel quasistatic and dynamic charge amplifier with analog output and integrated data acquisition. The benefit: a scalable and configurable high performance signal conditioner and data acquisition system offering channel synchronizations, signal filtering, virtual channels and convenient evaluation of individual force signals. Integrated data acquisition simplifies the measuring chain and provides added flexibility.

Optimal results – even under extreme stress

Rockets are exposed to very high stresses, especially during launch. To prevent malfunctions during operation, rocket components – and especially rocket engines – undergo extensive testing and inspection during the testing phase. Kistler is also showcasing the Type 6021A high-temperature pressure sensor at the Space Tech Expo Europe. This uncooled pressure sensor is suitable for application temperatures of up to 700°C and provides is high resolution pressure measurements to understand the combustion processes and related instabilities. For this purpose, the pressure sensor is ground-isolated and is connected to a differential charge amplifier providing low noise and EMI immunity to support accurate measurements.

Tradeshow visitors will also have the chance to appreciate the benefits of Kistler's Type 5181A differential charge amplifier for high temperature test requirements.

Reliable measurements of small torques and forces

Yet another highlight to be unveiled by Kistler at the Space Tech Expo Europe is the first piezoelectric 6-component force/torque link, Type 9306A. This sensor can deliver precise and direct measurements of three forces and three torques without calculation: an excellent choice for measurements in wind tunnels. Kistler charge amplifiers provide users with the ability of adjusting the torque and force measuring ranges independently for each axis. Thanks to the piezoelectric measurement principle and 9306A performance very small torques and forces can be easily measured with high resolution.

More information about Kistler's exhibit at the Space Tech Expo Europe

Media contact
Manuel Blattner
Head of Strategic Business Field
Test & Measurement
Tel.: +41 52 2241 273
Email: manuel.blattner@kistler.com

KIT PARA MEDIOS INFORMATIVOS

Kistler portrait with logo for a quick overview: Kistler Press Kit.zip

03/07/2018
The Top 100 Competition has again singled out the most innovative German small and medium-sized enterprises...
25/06/2018
Kistler is pleased to introduce MicroDyn, the world's smallest series-produced cutting force meter.
19/06/2018
Kistler introduces the world’s first high temperature accelerometer for the monitoring of gas turbines.
11/06/2018
Kistler is earmarking the highest investment budget for research and development in the company`s history.
09/05/2018
At Sensor + Test 2018 Kistler will be introducing a milestone in measurement technology: its new KiDAQ data...
08/05/2018
At NPE 2018, the Kistler Group is showcasing its latest custom monitoring package for ComoNeo, its...
03/05/2018
At Automatica 2018, the Kistler Group will turn the spotlight on diverse options for using sensors and process...
24/04/2018
The Kistler Group will showcase its expanded portfolio of industrial test and inspection systems for quality...
12/04/2018
The global leader in dynamic measurement technology supports the passion for innovation and technology with a...
06/03/2018
Kistler will be showcasing at Control 2018 its portfolio of industrial testing and inspection systems with the...
16/02/2018
At Intertraffic 2018 the Kistler Group is showcasing its comprehensive KiTraffic Weigh In Motion (WIM)...
15/02/2018
At NPE 2018 in Orlando, Florida, the Kistler Group will demonstrate a wide range of modular functionalities...
31/01/2018
The new KiSprint provides coaches and athletes with an efficient means of biomechanically optimizing sprint...
24/01/2018
Kistler achieved a growth rate of 18 % in 2017. Digital transformation has top priority in 2018.
23/01/2018
Overcoming the complexities of RTM – with Kistler
12/10/2017
At the SPS IPC Drives Kistler Group will unveil the world's first digital charge amplifier Type 5974A, a...
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
Kistler Group took over near Karlsruhe-based Vester Elektronik GmbH on 25 August, a specialist in sensor...
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
At Moulding Expo 2017, we will show how easy it is to install the measurement technology needed for quality...
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
27/10/2016
At this year's SPS IPC Drives in Nuremberg Kistler will premiere laboratory systems to analyze bolted joints,...
21/10/2016
Kistler boosts the efficiency and reliability of large marine and stationary engines through monitoring and...
19/10/2016
Kistler is presenting the new versions of its ComoNeo and ComoDataCenter.
10/10/2016
Kistler is unveiling a new addition to its portfolio of electromechanical joining modules.
30/09/2016
The Kistler Group reported incoming orders worth CHF 233.3 million at the end of August 2016 and has therefore...
07/09/2016
At this year's K Trade Fair from 19 to 26 October in Düsseldorf, Kistler will be showcasing its latest new...
24/07/2016
Kistler will be showcasing its new NCFE and NCFR joining modules, together with the latest generation of...
12/07/2016
Kistler's Correvit® SFII sensor measures world record in 1.513 seconds
12/05/2016
Screw technology complements the range of applications.
27/04/2016
Following a long phase of planning, preparations, and conversion work, Kistler Instrumente GmbH has a new home...