Fines for overloaded trucks – soon possible with automatic cameras?

Due to the current decline in traffic, wheel ruts, potholes and other types of road damage are becoming more visible. They cost the taxpayer billions every year and they are also frequent causes of disruptions and hazards in road traffic. Responsibility for the condition of our highways lies mainly with overloaded trucks that inflict stress on roads and vulnerable infrastructures such as bridges. To reduce wear and tear in the long term, overloaded vehicles must be detected and the culprits must be held to account.

Consumer spending is on the increase all over the world, and online trade is setting new records. In Germany alone, three million registered trucks are on the roads to transport all the goods involved and ensure that consumers receive their supplies every day. Vast numbers of goods shipments are also driven into the country from abroad. The weight of every overloaded vehicle places a load on traffic infrastructures: the impact on the road's life expectancy is related to the vehicle's weight by a power of four. To take an actual example: a truck weighing a total of 30 tonnes causes the same wear and tear on the road as 7,500 passenger cars. The results? Lasting damage, construction sites and soaring maintenance costs. In many places, trucks are randomly diverted from traffic to a weigh station where violations of the maximum authorized mass (MAM) can be individually identified and penalized. In some cases, Weigh In Motion (WIM) is deployed to preselect vehicles before they are diverted. For this purpose, Weigh In Motion systems use sensors recessed into the asphalt to measure the weight of passing vehicles. However, the accuracy of these systems does not yet meet the legal requirements, so police must individually check vehicles that trigger the system's alarm. A static platform scale then confirms the result from the WIM sensors. This procedure inevitably takes up a lot of police time.

Automatic notification of charges for overloaded vehicles

Now, a technological innovation from the Kistler Group promises to remedy this situation: a new Weigh In Motion system with significantly improved measurement accuracy can use camera technology to detect overloaded vehicles automatically – just like a speed check. The notification of charges is then sent by post. This requires appropriate legislation, which has already been introduced in several European countries. Why is this system more reliable? Because it is based on a new type of sensor that measures the vehicle's exact weight – irrespective of road quality, speed or the angle at which the vehicle passes the sensors. Data is transmitted digitally to ensure added protection against signal interference. Another advantage: the WIM system no longer disrupts the traffic flow. Drivers only realize that their truck was just weighed because of the flash from the camera. In the future, it will also be possible to use WIM systems to detect inadequate tire pressure. As well as reducing tire lifetimes, insufficient pressure makes the braking distance longer. It also entails the risk of overheating, which can cause parts of tires to become detached.

The new system has already been tested on some Swiss roads and at the Kefikon experimental center and will undergo further testing on Switzerland's motorways. Deployment of this technology on main arterial routes could very quickly boost traffic safety – and it could also have a deterrent effect on trucking companies that overload their vehicles in an attempt to save money at the taxpayer's expense.

You might be interested also in:

Solutions from Kistler:
Singling out potentially overloaded vehicles is now a thing of the past. Today, these traffic offenders can be identified using automatic cameras.
“Everyone makes mistakes” – except in the field of medical technology. In the worst-case scenario, defects in the production of insulin pens could put patients’ safety at risk.
Stunned pigs, self-experimentation with showers of glass splinters – these were just some of the ways that vehicles were crash-tested in the first half of the 20th century. Today, crash testing involves high-tech crash dummies.
Preventing ligament tears with advanced technology: tailoring training and physiotherapy precisely to the athlete or patient using highly sophisticated measurement technology is becoming increasingly popular.
Turn, press or tilt: control elements such as hand brakes are put to the test before being installed in vehicles.
If the fasteners that secure the swiveling arm of a crane were to fail, people could be injured – or even lose their lives. Our inspection systems make sure that this could never happen.
Space is the environment that presents the most challenging possible conditions for technical equipment. In order for spacecraft to withstand these extremes and safely transport their crews, our sensors guarantee reliability before the launch.
While container ships, tankers and freighters are essential for the international transport of goods, they are also responsible for around 3 percent of global CO2 emissions. However, our sensors can significantly reduce this.
Contacto
Max 25 MB