World’s first crash wall for high-speed trains

A distance of 1,318 kilometers separates the megacities of Beijing and Shanghai. Since June 2011 passengers have been able to travel between these Chinese cities several times a day, with a journey time of less than five hours, and at speeds of up to 380 kilometers per hour. The third longest high-speed line in the world is one of the most used in the country, with approximately 100 million passengers per annum. To ensure that Chinese rail transport can continue to handle such large passenger numbers and cycle times in the future, the high-speed trains must fulfill strict safety requirements. To that end, the world’s largest provider of rail transport technology relies on Kistler’s measurement expertise. Thanks to the only crash wall of its kind in the world, the impact forces of the trains and their components can be precisely measured and analyzed.

High-speed trains are a key to the development of the Chinese economy. They are safe, fast and comfortable. It is not without reason that China currently possesses one of the largest highspeed networks in the world, with approximately 20,000 kilometers of track. Since the Chinese railway authority records a year-on-year increase in passengers of almost one third, the rail
network for fast trains will be extended 50 per cent by 2020.

However, wherever high speeds are involved there is also an increased safety risk. Therefore, allied to the extension of the high-speed rail network, passenger safety is also a key issue in China, particularly in the wake of the rail accident in Shuangyu (province of Zhejiang) in 2011, which resulted in the deaths of 40 people. Following this incident the speed of travel for the super express trains was initially limited to around 300 kilometers per hour. However since September 2017 the speed limit has been increased and is now 350 kilometers per hour.

Crash tests with high measuring ranges

The world’s largest provider of rail transport technology has worked for years on optimizing its railway vehicles. In its own technology and product development center the Chinese corporation regularly carries out extensive crash and component tests on its high-speed trains. The declared objective of this extensive test program is to minimize personal injury and material damage in the event of a crash, and to sustainably develop rail transport. In tests to determine what impact forces operate on the trains and their components, the company relies on measurement technology provided by Kistler. Since the end of 2017 a ground-breaking Kistler application has been in use in the crash hall: the world’s first ever crash wall for high-speed trains.

Christof Sonderegger, the Product Manager for Test & Measurement at Kistler, is responsible for this major project. “This is the first time in the entire history of our company that we have had the opportunity to handle an application like this. With the crash wall for high-speed trains we enter a measurement range that is up to twenty times higher than in the typical crash tests performed in the automotive industry. Cars are driven into the wall with up to 64 kilometers per hour, while our Chinese client’s trains crash into the walls with up to 72 kilometers, generating a force equivalent to a mass of 10,000 tons.“ 

Modular concept with freely combinable sensors

The challenge for Kistler was to develop a custom-built crash wall, which could not only handle the high impact forces of the high-speed trains, but was also modular and extendable. On top of that Kistler had to adhere to a very tight delivery schedule and was required to provide a full turnkey solution. “We were only able to handle such a demanding task thanks to outstanding internal cooperation,” explains Sonderegger.

After an intensive engineering phase lasting several weeks, the measurement technology experts were able to develop a crash wall with a total of six segment plates, each of which allowed for 36 sensors to be installed on them. A key advantage is that the sensors can be flexibly combined with each other and cover all load requirements. If required, the crash wall can be extended by a further three segment plates, again, each with additional sensors. In the Chinese client’s crash wall the Kistler engineers installed 1-component force sensors with measuring ranges of 700 kN, 2.5 MN, 5 MN and 10 MN. The sensors come ready calibrated and guarantee constant measuring precision over a broad force range.

Ground-breaking DTI technology

The digital electronics, the so-called DTI (Digital Transducer Interface) technology, is integrated into Kistler’s force sensors.

The DTI technology has already been successfully used for several years in vehicle safety, driving dynamics and operational stability. Our engineers were also able to integrate this unique technology for our client in China.

Christof Sonderegger, Product Manager for Test & Measurement at Kistler

 

In sensors with DTI technology, the signal is digitalized in the sensor and relayed with a bus. The sensor data flows interference-free into the central Kistler DTI logger and is transferred into the computer and recorded via Ethernet.

Excellent on-site service

The sensors, electronics and testing equipment were produced in Winterthur (Switzerland), where Kistler is based, and the measurement technology experts had the segment plates manufactured by a local supplier. The Kistler Tech Center in Shanghai was responsible for the segment plates system test and installation at the client’s facility. Finally, the custom-built crash wall was installed in the Chinese corporation’s technology and product development center. Kistler’s crash wall has been in operation since the end of 2017. “Our client is very satisfied with the modular concept with freely combinable sensors and the robust interface. For future tests the company plans to order further sensors and segment plates from us,” says Sonderegger.

26/06/2022
Heavy-duty application on the test track: S6XT delivers high-precision load measurements in Japan
04/05/2022
Daimler Buses relies on MaDaM and jBEAM to further develop of its electric city buses.
11/04/2022
On the road to success with IEPE and MEMS accelerometers for the ISTAR research aircraft – on the ground and in the air.
14/01/2022
KiTraffic Statistics delivers precise WIM data for a railway bridge in central Austria
18/11/2021
Advanced fastener testing with ANALYSE systems for reliable zink flake coatings in the automotive and wind turbine industries
12/10/2021
How Yuchai achieves more precision, transparency and resource efficiency for its production of engines conform to China VI
14/09/2021
A high precision measuring chain with dynamometer, laboratory charge amplifier and software enables objective comparison tests.
09/09/2021
SRA: Find the best spot and the ideal sensor layout for direct enforcement of overloaded vehicles.
03/09/2021
At Estudio de la Pisada in Valencia, a 3D force plate helps podiatry experts to develop treatments and orthoses for patients and athletes.
02/07/2021
Two IEPE accelerometers deliver key data for propulsion validation and optimization of flight characteristics even in the stratosphere
22/06/2021
Capturing micro-vibrations with a dynamometer leads to improved satellite technology
02/06/2021
Zero defect despite high volumes: this is the way quality assurance with Kistler test automation systems works for zinc die casting parts
26/04/2021
A digitally driven brake force measurement system makes the life of service technicians for train maintenance much easier
13/04/2021
Inside "The Atmosphere" at MARIN, 100 of our pressure sensors capture wave impacts under varying environmental conditions
22/03/2021
How MAN Energy Solutions is using sensors from Kistler to make its gas turbines fit for the future
08/02/2021
Measurement technology dedicated to the discipline and biomechanics of pole vault enables high performances
05/10/2020
How does a digital measuring chain for piezoelectric sensors work as part of a complex vehicle test stand?
18/09/2020
Convincing test results: The Ohio Department of Transportation goes on to apply Lineas from Kistler for traffic monitoring.
20/08/2020
Precision is the key to top performance: how measurement technology from Kistler supports the development team at EMUGE-FRANKEN
22/07/2020
Quality assurance solutions by Kistler like ComoNeo ensure highest accuracy at TSP Precision Tooling in Shanghai.
09/06/2020
Kistler supports Ceratizit in the development of HDT. This enables complex geometries to be produced with just one tool.
15/11/2019
Process monitoring systems and cavity pressure sensors from Kistler help to reduce the amount of scrap drastically
23/10/2019
How measurement technology from Kistler contributes toward boosting high-end powertools' quality
15/08/2019
How the ANALYSE system from Kistler is enhancing safety and transparency in the field of fastening technology
17/07/2019
Turkey opts for weight enforcement with WIM technology from Kistler
24/06/2019
For the next manned flight to the moon: safety that can be measured
20/06/2019
Segregation of good and bad parts every 1.5 seconds: process monitoring with Kistler enables high quality for over 5 million parts per year.
14/05/2019
In order to achieve excellent quality for its components and medical devices, Tessy Plastics chose sensors and solutions from Kistler.
18/04/2019
A renowned manufacturer of electrical appliances trusts testing and sorting systems by Vester to improve its quality.
02/04/2019
NFL's Jaguars boost their fitness levels with Kistler.
25/03/2019
By using process monitoring from Kistler, not only the assembly of electric fuses is validated, but even the function of the sensors itself.
18/03/2019
How to determine the fitness level of an athlete efficiently? A practical report on the Quattro Jump force plate system from Kistler.
17/12/2018
Thanks to precise Weigh in Motion technology from Kistler, Hungary's roads are sustainably protected against overloaded vehicles.
27/11/2018
Bang&Clean relies on Kistler's precise measurement of ignition processes and pressure wave propagation
10/10/2018
Sartorius applies the process monitoring system ComoNeo from Kistler and thereby increases the process quality during injection molding
08/10/2018
The Dortmund Technical University tests the new MicroDyn 9109AA cutting force dynamometer from Kistler and breaks new ground for developing its micromachining processes.
31/08/2018
The ZF company operates a software-controlled Kistler fastener test bench with an integrated vibration unit.
14/08/2018
BIG Daishowa, headquartered in Osaka, Japan, is one of the leading producers of tool holders for the machining industry. Each year the company produces over half a million collet chucks. Their products are developed using, among other resources, Kistler’s cutting force measuring device.
16/07/2018
Enhanced quality and efficiency in mobile crane manufacture – thanks to the test stand for torque tools by Kistler
11/04/2018
The world’s largest provider of rail transport technology relies on Kistler’s measurement expertise. Thanks to the only crash wall of its kind in the world, the impact forces of the trains and their components can be precisely measured and analyzed.
14/11/2017
In the development of cooling lubricants, Blaser Swisslube relies on Kistler's measurement expertise.
11/08/2017
Applus IDIADA relies on DTI in-dummy technology from Kistler for Test Device for Human Occupant Restraint (THOR).
04/01/2017
Road safety is a central topic in vehicle development. Through accurate measurements, Kistler helps increase the chance of survival in crashes.
22/12/2016
Kistler makes progress in vehicle development possible
22/12/2016
Kistler Sensor Correvit® SFII measures world record
20/12/2016
Kistler sensors deliver a maximum in data quality under any conditions.
07/11/2016
Kistler pressure sensors enabled the Rosetta space probe to fly for 6.4 billion kilometers.
05/10/2016
Since the end of 2015 FC Basel is using Kistler force plates to reduce the dropout of young talents.
17/08/2016
Kistler makes the difference in the crucial sports moments with its Performance Analysis System for Swimming.
19/02/2016
Determination of Pump Efficiency with Kistler KiTorq Measuring Flange System
04/11/2015
Piezoelectric Measurements with CompactRIO™
15/06/2015
Measurement Solutions for Automotive Test Systems
08/05/2015
Quality Assurance in the Automotive Industry
02/03/2015
How Brose improves the quality of its two-component production and automatically separates defective parts
02/12/2014
The Kistler Group pursues a growth policy that is both ambitious and sustainable – and strategic acquisitions are one of its core elements. ‘Strategic’ means that Kistler deliberately selects companies which can achieve more together with Kistler than they ever could by continuing alone. The takeover of Dr. Staiger Mohilo & Co. GmbH in 2006 enabled Kistler to grow jointly with the acquired company...
02/12/2014
After a ten-year voyage, the Rosetta space probe's Philae landing module finally touched down on the surface of comet ‘Chury’.
23/08/2011
HEWI and its Customers Benefit from Cavity Pressure Technology
15/02/2011
End-to-end process monitoring for critical medical moldings
07/02/2011
Cavity pressure measurement eliminates short shots at Fischer GmbH & Co KG of Sinsheim/Germany
Contacto
Max 25 MB