Ohio authorities rely on Weigh In Motion technology from Kistler

The US state of Ohio is stepping up its efforts to collect traffic data so that it can claim important Federal budget funding to conserve infrastructure. Kistler Lineas sensors achieved exceptionally convincing results in the state's tests on Weigh In Motion systems.

Although Ohio is one of the smaller US states in terms of area, it is a key center of industry and business. From Cleveland on the shore of Lake Erie in the north to Columbus and Cincinnati in the southwest, Ohio has the seventh largest gross domestic product (GDP) of all US states, and is second only to neighboring Michigan in automobile production. Ohio is known as the Buckeye State, after the native tree similar to a horse chestnut that has a characteristic tan-colored eye in the middle of its seed. In US Presidential elections, Ohio is traditionally regarded as a swing state and a bellwether that usually votes with the winning party.

In some ways, Ohio resembles the German Federal State of Baden-Württemberg: the two territories have similar populations (about 11 million), their GDPs are comparable (about EUR 500,000 million), and the enterprise structure of both Ohio and Baden-Württemberg is defined by the automotive industry and its supply sector. However, Ohio has three times the area of Baden-Württemberg: it is located centrally in the United States, within one day's drive for 60% of the North American population. Responsibility for developing and conserving the highway infrastructure is assigned to the Ohio Department of Transportation (ODOT): with a workforce of over 4,500, this state agency controls all aspects of construction, planning, traffic monitoring and transportation safety.

For installation, operation and durability – quality is the focus

Dave Gardner, Manager of ODOT's Traffic Monitoring Section, shares responsibility for traffic oversight throughout the state of Ohio with his colleague Sandie Mapel, Field Manager. “Acquiring precise traffic data is very important for us because allocation of Federal budget funds depends on those statistics,” Gardner explains. “Axle loads and overall truck weights are recorded and submitted for the Federal Data Plan.”

ODOT currently operates 22 Weigh In Motion (WIM) stations to monitor stress on Ohio's roads caused by trucks and heavy commercial vehicles. “We'll gradually be adding more installations in the coming years,” Mapel adds. “We believe it's very important to deploy the correct systems in terms of installation, operation and data quality.”

A practical, high-performance system: Kistler Lineas scores convincingly in field tests

To investigate its options, ODOT installed a WIM test section on US Route 23, which links the country's far north to Florida and crosses Ohio from north to south. The traffic monitoring experts at ODOT were impressed by the performance of quartz-based Lineas sensors from Kistler. “Their compact design makes them easy to install, especially in existing roads. The Lineas sensors combine long service lifetimes with data quality that leaves nothing to be desired,” Mapel comments. “For all these reasons, we'll be deploying more Kistler sensor technology to acquire traffic data in the future. We're also examining how much use we could make of the complete KiTraffic Statistics system,” she concludes. Another test section to assess this option is due to be set up in Ohio before long.

Progressive expansion with technology from Kistler on board

ODOT’s first Kistler Lineas sensor installation was back in 2007, and the agency has been increasing its use of Lineas sensors since 2016. The oldest Kistler installation still operating in the state today dates from 2011. 

When asked if more WIM applications could be implemented with Kistler – such as direct camera-based collection of fees for overloaded vehicles (“direct enforcement”) or protection of bridges against overloaded trucks – Gardner slows the pace: “We aren't there yet! Law enforcement carry out random checks on trucks, and we also send them traffic monitoring data for analysis purposes. But the data isn't forwarded to Law Enforcement in real time.”

On the other hand, the situation for bridges could be different. Ohio has the second largest number of bridges of all 50 US states and many of them were built after the second world war, so they require appropriate monitoring, protection and maintenance. Technology from Kistler can help prevent damage inflicted on bridges by overloaded vehicles. Such vehicles can be prevented from driving onto a bridge with the help of accurate WIM data that is available in real time – so bridge lifetimes become substantially longer. “However, a different department at ODOT is responsible for that,” Gardner notes. Including Ohio, 48 out of the 50 US states are now operating WIM technology from Kistler. With over 50,000 Lineas sensors already installed in more than 50 countries, WIM by Kistler is internationally recognized as the solution of choice to protect road infrastructure, improve traffic safety, and collect weight-based toll fees.

Lineas quartz sensors for Weigh In Motion (WIM)

Lineas quartz sensors (9195G) are used to measure wheel and axle loads, and they can also determine gross vehicle weights with no disruption to traffic flow. Installed in the road pavement, these sensors deliver highly accurate measurement signals.

Key product features and user benefits at a glance:

  • Quartz technology for high-precision measurements and long-term stability
  • Compliant with OIML R134 (accuracy class 2)
  • Long life expectancy thanks to rugged sensor design
  • Wide measuring range
  • Nonstop weighing at low to high speeds
  • Insensitive to temperature fluctuations
  • Installation in the road pavement is fast and easy
11/04/2022
On the road to success with IEPE and MEMS accelerometers for the ISTAR research aircraft – on the ground and in the air.
14/01/2022
KiTraffic Statistics delivers precise WIM data for a railway bridge in central Austria
18/11/2021
Advanced fastener testing with ANALYSE systems for reliable zink flake coatings in the automotive and wind turbine industries
12/10/2021
How Yuchai achieves more precision, transparency and resource efficiency for its production of engines conform to China VI
14/09/2021
A high precision measuring chain with dynamometer, laboratory charge amplifier and software enables objective comparison tests.
09/09/2021
SRA: Find the best spot and the ideal sensor layout for direct enforcement of overloaded vehicles.
03/09/2021
At Estudio de la Pisada in Valencia, a 3D force plate helps podiatry experts to develop treatments and orthoses for patients and athletes.
02/07/2021
Two IEPE accelerometers deliver key data for propulsion validation and optimization of flight characteristics even in the stratosphere
22/06/2021
Capturing micro-vibrations with a dynamometer leads to improved satellite technology
02/06/2021
Zero defect despite high volumes: this is the way quality assurance with Kistler test automation systems works for zinc die casting parts
26/04/2021
A digitally driven brake force measurement system makes the life of service technicians for train maintenance much easier
13/04/2021
Inside "The Atmosphere" at MARIN, 100 of our pressure sensors capture wave impacts under varying environmental conditions
22/03/2021
How MAN Energy Solutions is using sensors from Kistler to make its gas turbines fit for the future
08/02/2021
Measurement technology dedicated to the discipline and biomechanics of pole vault enables high performances
05/10/2020
How does a digital measuring chain for piezoelectric sensors work as part of a complex vehicle test stand?
18/09/2020
Convincing test results: The Ohio Department of Transportation goes on to apply Lineas from Kistler for traffic monitoring.
20/08/2020
Precision is the key to top performance: how measurement technology from Kistler supports the development team at EMUGE-FRANKEN
22/07/2020
Quality assurance solutions by Kistler like ComoNeo ensure highest accuracy at TSP Precision Tooling in Shanghai.
09/06/2020
Kistler supports Ceratizit in the development of HDT. This enables complex geometries to be produced with just one tool.
15/11/2019
Process monitoring systems and cavity pressure sensors from Kistler help to reduce the amount of scrap drastically
23/10/2019
How measurement technology from Kistler contributes toward boosting high-end powertools' quality
15/08/2019
How the ANALYSE system from Kistler is enhancing safety and transparency in the field of fastening technology
17/07/2019
Turkey opts for weight enforcement with WIM technology from Kistler
24/06/2019
For the next manned flight to the moon: safety that can be measured
20/06/2019
Segregation of good and bad parts every 1.5 seconds: process monitoring with Kistler enables high quality for over 5 million parts per year.
14/05/2019
In order to achieve excellent quality for its components and medical devices, Tessy Plastics chose sensors and solutions from Kistler.
18/04/2019
A renowned manufacturer of electrical appliances trusts testing and sorting systems by Vester to improve its quality.
02/04/2019
NFL's Jaguars boost their fitness levels with Kistler.
25/03/2019
By using process monitoring from Kistler, not only the assembly of electric fuses is validated, but even the function of the sensors itself.
18/03/2019
How to determine the fitness level of an athlete efficiently? A practical report on the Quattro Jump force plate system from Kistler.
17/12/2018
Thanks to precise Weigh in Motion technology from Kistler, Hungary's roads are sustainably protected against overloaded vehicles.
27/11/2018
Bang&Clean relies on Kistler's precise measurement of ignition processes and pressure wave propagation
10/10/2018
Sartorius applies the process monitoring system ComoNeo from Kistler and thereby increases the process quality during injection molding
08/10/2018
The Dortmund Technical University tests the new MicroDyn 9109AA cutting force dynamometer from Kistler and breaks new ground for developing its micromachining processes.
31/08/2018
The ZF company operates a software-controlled Kistler fastener test bench with an integrated vibration unit.
14/08/2018
BIG Daishowa, headquartered in Osaka, Japan, is one of the leading producers of tool holders for the machining industry. Each year the company produces over half a million collet chucks. Their products are developed using, among other resources, Kistler’s cutting force measuring device.
16/07/2018
Enhanced quality and efficiency in mobile crane manufacture – thanks to the test stand for torque tools by Kistler
11/04/2018
The world’s largest provider of rail transport technology relies on Kistler’s measurement expertise. Thanks to the only crash wall of its kind in the world, the impact forces of the trains and their components can be precisely measured and analyzed.
14/11/2017
In the development of cooling lubricants, Blaser Swisslube relies on Kistler's measurement expertise.
11/08/2017
Applus IDIADA relies on DTI in-dummy technology from Kistler for Test Device for Human Occupant Restraint (THOR).
04/01/2017
Road safety is a central topic in vehicle development. Through accurate measurements, Kistler helps increase the chance of survival in crashes.
22/12/2016
Kistler makes progress in vehicle development possible
22/12/2016
Kistler Sensor Correvit® SFII measures world record
20/12/2016
Kistler sensors deliver a maximum in data quality under any conditions.
07/11/2016
Kistler pressure sensors enabled the Rosetta space probe to fly for 6.4 billion kilometers.
05/10/2016
Since the end of 2015 FC Basel is using Kistler force plates to reduce the dropout of young talents.
17/08/2016
Kistler makes the difference in the crucial sports moments with its Performance Analysis System for Swimming.
19/02/2016
Determination of Pump Efficiency with Kistler KiTorq Measuring Flange System
04/11/2015
Piezoelectric Measurements with CompactRIO™
15/06/2015
Measurement Solutions for Automotive Test Systems
08/05/2015
Quality Assurance in the Automotive Industry
02/03/2015
How Brose improves the quality of its two-component production and automatically separates defective parts
02/12/2014
The Kistler Group pursues a growth policy that is both ambitious and sustainable – and strategic acquisitions are one of its core elements. ‘Strategic’ means that Kistler deliberately selects companies which can achieve more together with Kistler than they ever could by continuing alone. The takeover of Dr. Staiger Mohilo & Co. GmbH in 2006 enabled Kistler to grow jointly with the acquired company...
02/12/2014
After a ten-year voyage, the Rosetta space probe's Philae landing module finally touched down on the surface of comet ‘Chury’.
23/08/2011
HEWI and its Customers Benefit from Cavity Pressure Technology
15/02/2011
End-to-end process monitoring for critical medical moldings
07/02/2011
Cavity pressure measurement eliminates short shots at Fischer GmbH & Co KG of Sinsheim/Germany
Contacto
Max 25 MB