How Polyfab trims its injection molding production to the highest quality

Polyfab uses process monitoring systems from Kistler based on cavity pressure measurement to sustainably optimize the high-volume production of plastic parts for various industries. Thanks to them, it was possible to reduce the number of faulty parts in injection molding to a record-breaking 1 PPM (parts per million).

Since 1971, Polyfab Corp. has been a custom thermoplastic injection molder. The American company supports the plastics molding industry needs of four major markets: medical, packaging, industrial, and commercial. In order to remain competitive in the ever-changing plastic molding industry, they must continuously adapt their monitoring processes with the ultimate goal of producing zero-defect quality assured parts.

Brian Burhop is a Project Engineer with over 16 years of experience at Polyfab Corp. located in Sheboygan, Wisconsin. He takes the quality of their molded parts seriously. Monitoring the molding process for suspect parts prior to packaging or assembly easily with guaranteed results is key. For nine years now, cavity pressure technology with sensors and systems of Kistler have provided a highly effective, reliable basis for automated inspection.

Integrated quality assurance increases customer satisfaction

Burhop says, “Our partnership with Kistler came about because Polyfab Corp. is very much a molder based on scientific principles which we employ to establish and monitor our molding processes. Process monitoring and containment is very important for our high-volume jobs. Our decision was based on very important factors, such as how user-friendly the monitoring equipment is, how easy it is to acquire and interpret the data, how easily configurable it is with our machinery, and how easy it is to incorporate Kistler's sensors into the mold itself. Kistler's products were really hands down the best choice for us in all those categories. Approximately 66% of Polyfab Corp. machinery is now equipped with Kistler monitoring and sensor technology.”

The first challenge Burhop and his team faced was to greatly improve the accuracy of short-shot monitoring for a dispenser lid with a living hinge. To reduce non-fills during the injection molding process, the pressure at end of fill was monitored with a flush mounted sensor directly in the cavity. This allows for more accurate setting of the required minimum pressure which is affected by process variables including injection speed, and melt temperature.

The installation of Kistler’s monitoring systems with our molding machines couldn’t be any easier. We can pick up just one signal and that’s really all we need because it is so streamlined, and we are able to start collecting data quickly."

Brian Burhop, Project Engineer at Polyfab Corp. in Sheboygan, Wisconsin

 

Burhop states, “Polyfab's customer return score prior to implementing Kistler in 2009 was above 10,000 PPM (parts per million). In 2017, we molded approximately 200 million parts and our rate for customer returns was 98 PPM, which is `world class' performance. Our 2018 year-to-date PPM customer return rate is now `1 PPM'. This represents a drastic improvement after implementing Kistler's process monitoring systems (ComoNeo/ CoMo Injection), as well as Kistler's direct and indirect cavity pressure sensors into our machinery.”

Automated assembly thanks to cavity pressure sensors

Polyfab Corp. has also integrated Kistler's sensors into their automated assembly process, producing very positive results. Burhop explains, “For automated assembly in terms of parts which have a lot of value added as they step through the assembly process, Kistler's sensors ensure that we are not assembling parts with suspect (defective) plastic components. For example, we have a commercial inkjet cartridge that we have completely automated the assembly.

The cell incorporates two molding machines, six robots, and two 4-cavity molds. We have placed a Kistler sensor in each one of those cavities so if there is a suspect or questionable shot, it segregates it so that those parts don't enter the assembly process. This has proven very beneficial and valuable to our automated assembly application needs.”

Process monitoring systems of Kistler save valuable time, reduce costs, and increase ROI

Kistler's process monitoring systems have been saving time, reducing costs, and increasing the Return on Investment (ROI). Burhop says, “From my perspective: reducing re-validations was key. For instance, if we need to validate a tool in another press, either for capacity reasons or for risk mitigation for a customer, Kistler's technology has made the process of duplicating a process much more straightforward and scientific in terms of the acquisition of data and the actual pressure curve data from the cavity.”

Bob Hendricks, Product Sales Manager with Kistler, who worked closely with Burhop, further explains this time-saving benefit of incorporating Kistler's process monitoring systems and sensors: “When you have a reference curve that represents the part quality, and you need to move it from one machine to another, the benefit is you no longer have to revalidate the whole process every time because that reference curve remains valid on any machine.”

Shorter set-up times ensure optimized production

According to Burhop, the set-up was quick and easy to learn and use. Kistler's contact elements for injection molds have also proven to be highly beneficial. Burhop says, “The use of Kistler's contact elements have greatly simplified our mold disassembly and maintenance process. At Polyfab Corp., we focus on lean production, set-up reduction and quick-change. By utilizing Kistler's multi-channel connectors, it's just one quick connection.” This allows Burhop and his team to save a lot of time and reduce costs by greatly decreasing the molding defect rate.

“Kistler's piezoelectric sensor technology, in my opinion, is much more straightforward and easier to use than a lot of the other sensors currently on the market. The installation of Kistler's monitoring systems with our molding machines couldn't be any easier. We can pick up just one signal and that's really all we need because it is so streamlined, and we are able to start collecting data quickly,” Burhop adds.

Customer satisfaction is key at Kistler

Hendricks is also enthusiastic about the long, successful cooperation and emphasizes: “At Kistler, we are focused on fulfilling our customer's needs with the goal of ensuring that they are completely satisfied. Our aim is to help our customers achieve zero-defect in series production, offering specialized, expert advice and onsite technical support including calibration services no matter where you are in the world.”

“We are very satisfied with Kistler's services and support,” Burhop elates. “If an issue does arise, which is not often, Kistler's support team responds very quickly and their services are fantastic. With regard to the implementation and installation of Kistler's piezoelectric sensors, our tool shops have had no issues installing the sensors in the molds. The implementation is very streamlined and almost transparent.”

14/01/2022
KiTraffic Statistics delivers precise WIM data for a railway bridge in central Austria
18/11/2021
Advanced fastener testing with ANALYSE systems for reliable zink flake coatings in the automotive and wind turbine industries
12/10/2021
How Yuchai achieves more precision, transparency and resource efficiency for its production of engines conform to China VI
14/09/2021
A high precision measuring chain with dynamometer, laboratory charge amplifier and software enables objective comparison tests.
09/09/2021
SRA: Find the best spot and the ideal sensor layout for direct enforcement of overloaded vehicles.
03/09/2021
At Estudio de la Pisada in Valencia, a 3D force plate helps podiatry experts to develop treatments and orthoses for patients and athletes.
02/07/2021
Two IEPE accelerometers deliver key data for propulsion validation and optimization of flight characteristics even in the stratosphere
22/06/2021
Capturing micro-vibrations with a dynamometer leads to improved satellite technology
02/06/2021
Zero defect despite high volumes: this is the way quality assurance with Kistler test automation systems works for zinc die casting parts
26/04/2021
A digitally driven brake force measurement system makes the life of service technicians for train maintenance much easier
13/04/2021
Inside "The Atmosphere" at MARIN, 100 of our pressure sensors capture wave impacts under varying environmental conditions
22/03/2021
How MAN Energy Solutions is using sensors from Kistler to make its gas turbines fit for the future
08/02/2021
Measurement technology dedicated to the discipline and biomechanics of pole vault enables high performances
05/10/2020
How does a digital measuring chain for piezoelectric sensors work as part of a complex vehicle test stand?
18/09/2020
Convincing test results: The Ohio Department of Transportation goes on to apply Lineas from Kistler for traffic monitoring.
20/08/2020
Precision is the key to top performance: how measurement technology from Kistler supports the development team at EMUGE-FRANKEN
22/07/2020
Quality assurance solutions by Kistler like ComoNeo ensure highest accuracy at TSP Precision Tooling in Shanghai.
09/06/2020
Kistler supports Ceratizit in the development of HDT. This enables complex geometries to be produced with just one tool.
15/11/2019
Process monitoring systems and cavity pressure sensors from Kistler help to reduce the amount of scrap drastically
23/10/2019
How measurement technology from Kistler contributes toward boosting high-end powertools' quality
15/08/2019
How the ANALYSE system from Kistler is enhancing safety and transparency in the field of fastening technology
17/07/2019
Turkey opts for weight enforcement with WIM technology from Kistler
24/06/2019
For the next manned flight to the moon: safety that can be measured
20/06/2019
Segregation of good and bad parts every 1.5 seconds: process monitoring with Kistler enables high quality for over 5 million parts per year.
14/05/2019
In order to achieve excellent quality for its components and medical devices, Tessy Plastics chose sensors and solutions from Kistler.
18/04/2019
A renowned manufacturer of electrical appliances trusts testing and sorting systems by Vester to improve its quality.
02/04/2019
NFL's Jaguars boost their fitness levels with Kistler.
25/03/2019
By using process monitoring from Kistler, not only the assembly of electric fuses is validated, but even the function of the sensors itself.
18/03/2019
How to determine the fitness level of an athlete efficiently? A practical report on the Quattro Jump force plate system from Kistler.
17/12/2018
Thanks to precise Weigh in Motion technology from Kistler, Hungary's roads are sustainably protected against overloaded vehicles.
27/11/2018
Bang&Clean relies on Kistler's precise measurement of ignition processes and pressure wave propagation
10/10/2018
Sartorius applies the process monitoring system ComoNeo from Kistler and thereby increases the process quality during injection molding
08/10/2018
The Dortmund Technical University tests the new MicroDyn 9109AA cutting force dynamometer from Kistler and breaks new ground for developing its micromachining processes.
31/08/2018
The ZF company operates a software-controlled Kistler fastener test bench with an integrated vibration unit.
14/08/2018
BIG Daishowa, headquartered in Osaka, Japan, is one of the leading producers of tool holders for the machining industry. Each year the company produces over half a million collet chucks. Their products are developed using, among other resources, Kistler’s cutting force measuring device.
16/07/2018
Enhanced quality and efficiency in mobile crane manufacture – thanks to the test stand for torque tools by Kistler
11/04/2018
The world’s largest provider of rail transport technology relies on Kistler’s measurement expertise. Thanks to the only crash wall of its kind in the world, the impact forces of the trains and their components can be precisely measured and analyzed.
14/11/2017
In the development of cooling lubricants, Blaser Swisslube relies on Kistler's measurement expertise.
11/08/2017
Applus IDIADA relies on DTI in-dummy technology from Kistler for Test Device for Human Occupant Restraint (THOR).
04/01/2017
Road safety is a central topic in vehicle development. Through accurate measurements, Kistler helps increase the chance of survival in crashes.
22/12/2016
Kistler makes progress in vehicle development possible
22/12/2016
Kistler Sensor Correvit® SFII measures world record
20/12/2016
Kistler sensors deliver a maximum in data quality under any conditions.
07/11/2016
Kistler pressure sensors enabled the Rosetta space probe to fly for 6.4 billion kilometers.
05/10/2016
Since the end of 2015 FC Basel is using Kistler force plates to reduce the dropout of young talents.
17/08/2016
Kistler makes the difference in the crucial sports moments with its Performance Analysis System for Swimming.
19/02/2016
Determination of Pump Efficiency with Kistler KiTorq Measuring Flange System
04/11/2015
Piezoelectric Measurements with CompactRIO™
15/06/2015
Measurement Solutions for Automotive Test Systems
08/05/2015
Quality Assurance in the Automotive Industry
02/03/2015
How Brose improves the quality of its two-component production and automatically separates defective parts
02/12/2014
The Kistler Group pursues a growth policy that is both ambitious and sustainable – and strategic acquisitions are one of its core elements. ‘Strategic’ means that Kistler deliberately selects companies which can achieve more together with Kistler than they ever could by continuing alone. The takeover of Dr. Staiger Mohilo & Co. GmbH in 2006 enabled Kistler to grow jointly with the acquired company...
02/12/2014
After a ten-year voyage, the Rosetta space probe's Philae landing module finally touched down on the surface of comet ‘Chury’.
23/08/2011
HEWI and its Customers Benefit from Cavity Pressure Technology
15/02/2011
End-to-end process monitoring for critical medical moldings
07/02/2011
Cavity pressure measurement eliminates short shots at Fischer GmbH & Co KG of Sinsheim/Germany
Contacto
Max 25 MB