Bang&Clean puts its trust in Kistler's blast measurement expertise

Bang&Clean Technologies AG: the name says it all. This Swiss company uses controlled gas explosions to clean industrial plants in a variety of sectors. What makes Bang&Clean so special? Cleaning is carried out while the plant is actually running, in compliance with the strictest safety regulations. Bang&Clean puts its trust in Kistler's pressure measurement technology know-how for blast testing  - not only to optimize the safety and efficiency of this patented process, but also for the development of new products. Kistler's sensors supply valuable insights into ignition processes and pressure wave propagation.

Markus Bürgin is the founder and Managing Director of Bang&Clean Technologies AG. Back in 2000, he developed and patented the Bang&Clean system for cleaning with controlled and dosed explosions. Since 2001, this process has been used in virtually every sector of industry where fuel-fired energy and power generation plants are in operation. Typical examples include waste-fed heating plants, biomass power stations and hazardous waste incineration plants, as well as chemical and pharmaceutical facilities. Ash and slag deposits must be removed regularly from plant components such as boilers, catalytic converters and reactors  - otherwise, performance will be reduced, faults will occur and operators will be faced with high outage costs. "With our services and products, we aim to increase the availability, efficiency and performance of industrial plants and components. Our customers benefit from longer service lifetimes for their plant components, and they avoid downtime," Bürgin explains.

Another advantage: plant components continue to operate during the cleaning process. As Bürgin points out: "Shutting the plants down for every cleaning operation would saddle our customers with enormous costs." 

Maximum safety for people and plant 

How does Bang&Clean's patented explosive cleaning system work? The company's experts introduce a water-cooled lance (pre-fitted with a special bag) through the boiler's doors or portholes, near the heating surface to be cleaned. The bag is inflated with a combustible gas mixture which is then ignited to cause an explosion. This generates a highly dynamic pressure wave and causes vibrations in the pipes and walls that dislodge deposits of ash and slag. Throughout the process, Bang&Clean accords top priority to safety for people and machines. "Our cleaning equipment is CE-compliant, and it is inspected by the German Federal Institute for Materials Research and Testing (BAM). Our certified experts only prepare the explosive gas mixture a few moments before the detonation in the boiler. This guarantees maximum safety for people as well as plant," Bürgin emphasizes. 

Special assignment near a nuclear power plant

Cleaning systems by Bang&Clean are in operation every day, throughout the world. "Most of our deployments are planned well in advance. But customers occasionally call on us to deal with emergencies or carry out special assignments with only a few days' or hours' notice," Bürgin notes. This is exactly what happened last fall, when an American plant operator contacted Bürgin with a request to clean its components. "That really was a very special case, because our customer's facility was in the immediate vicinity of a nuclear power plant," he recalls. "To obtain approval for cleaning the plants, our customer had to submit advance proof that the cleaning method was safe."

Thanks to Kistler's measurement results, we proved that our explosive cleaning system poses no danger either to people or the environment. So we were able to carry out the cleaning operations at our customer's plant safely and promptly."

Markus Bürgin, Founder and Managing Director of Bang&Clean Technologies AG

 

Special assignment near a nuclear power plant

Cleaning systems by Bang&Clean are in operation every day, throughout the world. "Most of our deployments are planned well in advance. But customers occasionally call on us to deal with emergencies or carry out special assignments with only a few days' or hours' notice," Bürgin notes. This is exactly what happened last fall, when an American plant operator contacted Bürgin with a request to clean its components. "That really was a very special case, because our customer's facility was in the immediate vicinity of a nuclear power plant," he recalls. "To obtain approval for cleaning the plants, our customer had to submit advance proof that the cleaning method was safe." 

Vast application expertise in blast pressure measurements

Bang&Clean did not have the measurement expertise required to provide the necessary proof, so Bürgin decided to call in a cooperation partner  - and he chose Kistler: "We've known Kistler for quite a few years already, and we're well aware of their vast application expertise in blast pressure measurements. When we received this inquiry from the US at such short notice, we immediately realized that we couldn't handle this project unless we called in the measurement technology specialists from Winterthur." 

Simple test setup in a test gallery

Given the time pressure, Bang&Clean and Kistler had to prepare a measurement campaign within the shortest possible time. Philipp Schenkel and David Weber, Kistler's development engineers, provided support and advice for the team headed by Bürgin throughout the project. To ensure correct measurement of the pressure values required, they opted for a relatively simple test setup in an experimental gallery at Lungern. Weber describes the procedure: "For the test setup, we attached a bag to a lance, filled the bag with a gas mixture and then detonated it." The parameters under examination included different distances, the gas volume and the bag material. About 30 test cycles were needed to arrive at a full understanding of the ignition processes and the propagation of the pressure waves. 

Measuring precise pressure signals in extremely harsh environments

To measure the pressure values, Weber and Schenkel chose Kistler's Type 6233A pencil probes. These piezoelectric sensors are ideal for measuring highly dynamic pressures in blast tests. "In our tests, we aligned the pencil probes radially in relation to the detonation source. That allowed us to measure the pressure of the propagating blast wave directly and precisely," Schenkel explains. As their name suggests, these sensors have a characteristic pencil shape: this feature minimizes the influence of the sensor geometry on the propagation of the blast wave and the measured signal. Rugged structural design and minimal bending sensitivity make these sensors ideal for measuring high-precision pressure signals in very harsh environments. An integrated amplifier circuit (IEPE) converts the charge signal into a voltage  - another advantage for applications with severe vibrations.

Successful proof of safety 

Bürgin and his team are more than satisfied with the measurement results. "Thanks to Kistler's measurement results, we proved that our explosive cleaning system poses no danger either to people or the environment. So we were able to carry out the cleaning operations at our customer's plant safely and promptly," Bürgin comments. And there was another benefit: the measurement results helped Bürgin and his team to achieve a better understanding of the product and its effectiveness. "In the future, we shall make use of the know-how we've acquired to optimize our products and continue developing them." For this purpose, Bürgin is planning additional measurement campaigns in the coming months. "We'll be taking advantage of Kistler's expertise for those measurements too  - but hopefully this project will be more straightforward than the last one," says Bürgin with a knowing wink. 

14/01/2022
KiTraffic Statistics delivers precise WIM data for a railway bridge in central Austria
18/11/2021
Advanced fastener testing with ANALYSE systems for reliable zink flake coatings in the automotive and wind turbine industries
12/10/2021
How Yuchai achieves more precision, transparency and resource efficiency for its production of engines conform to China VI
14/09/2021
A high precision measuring chain with dynamometer, laboratory charge amplifier and software enables objective comparison tests.
09/09/2021
SRA: Find the best spot and the ideal sensor layout for direct enforcement of overloaded vehicles.
03/09/2021
At Estudio de la Pisada in Valencia, a 3D force plate helps podiatry experts to develop treatments and orthoses for patients and athletes.
02/07/2021
Two IEPE accelerometers deliver key data for propulsion validation and optimization of flight characteristics even in the stratosphere
22/06/2021
Capturing micro-vibrations with a dynamometer leads to improved satellite technology
02/06/2021
Zero defect despite high volumes: this is the way quality assurance with Kistler test automation systems works for zinc die casting parts
26/04/2021
A digitally driven brake force measurement system makes the life of service technicians for train maintenance much easier
13/04/2021
Inside "The Atmosphere" at MARIN, 100 of our pressure sensors capture wave impacts under varying environmental conditions
22/03/2021
How MAN Energy Solutions is using sensors from Kistler to make its gas turbines fit for the future
08/02/2021
Measurement technology dedicated to the discipline and biomechanics of pole vault enables high performances
05/10/2020
How does a digital measuring chain for piezoelectric sensors work as part of a complex vehicle test stand?
18/09/2020
Convincing test results: The Ohio Department of Transportation goes on to apply Lineas from Kistler for traffic monitoring.
20/08/2020
Precision is the key to top performance: how measurement technology from Kistler supports the development team at EMUGE-FRANKEN
22/07/2020
Quality assurance solutions by Kistler like ComoNeo ensure highest accuracy at TSP Precision Tooling in Shanghai.
09/06/2020
Kistler supports Ceratizit in the development of HDT. This enables complex geometries to be produced with just one tool.
15/11/2019
Process monitoring systems and cavity pressure sensors from Kistler help to reduce the amount of scrap drastically
23/10/2019
How measurement technology from Kistler contributes toward boosting high-end powertools' quality
15/08/2019
How the ANALYSE system from Kistler is enhancing safety and transparency in the field of fastening technology
17/07/2019
Turkey opts for weight enforcement with WIM technology from Kistler
24/06/2019
For the next manned flight to the moon: safety that can be measured
20/06/2019
Segregation of good and bad parts every 1.5 seconds: process monitoring with Kistler enables high quality for over 5 million parts per year.
14/05/2019
In order to achieve excellent quality for its components and medical devices, Tessy Plastics chose sensors and solutions from Kistler.
18/04/2019
A renowned manufacturer of electrical appliances trusts testing and sorting systems by Vester to improve its quality.
02/04/2019
NFL's Jaguars boost their fitness levels with Kistler.
25/03/2019
By using process monitoring from Kistler, not only the assembly of electric fuses is validated, but even the function of the sensors itself.
18/03/2019
How to determine the fitness level of an athlete efficiently? A practical report on the Quattro Jump force plate system from Kistler.
17/12/2018
Thanks to precise Weigh in Motion technology from Kistler, Hungary's roads are sustainably protected against overloaded vehicles.
27/11/2018
Bang&Clean relies on Kistler's precise measurement of ignition processes and pressure wave propagation
10/10/2018
Sartorius applies the process monitoring system ComoNeo from Kistler and thereby increases the process quality during injection molding
08/10/2018
The Dortmund Technical University tests the new MicroDyn 9109AA cutting force dynamometer from Kistler and breaks new ground for developing its micromachining processes.
31/08/2018
The ZF company operates a software-controlled Kistler fastener test bench with an integrated vibration unit.
14/08/2018
BIG Daishowa, headquartered in Osaka, Japan, is one of the leading producers of tool holders for the machining industry. Each year the company produces over half a million collet chucks. Their products are developed using, among other resources, Kistler’s cutting force measuring device.
16/07/2018
Enhanced quality and efficiency in mobile crane manufacture – thanks to the test stand for torque tools by Kistler
11/04/2018
The world’s largest provider of rail transport technology relies on Kistler’s measurement expertise. Thanks to the only crash wall of its kind in the world, the impact forces of the trains and their components can be precisely measured and analyzed.
14/11/2017
In the development of cooling lubricants, Blaser Swisslube relies on Kistler's measurement expertise.
11/08/2017
Applus IDIADA relies on DTI in-dummy technology from Kistler for Test Device for Human Occupant Restraint (THOR).
04/01/2017
Road safety is a central topic in vehicle development. Through accurate measurements, Kistler helps increase the chance of survival in crashes.
22/12/2016
Kistler makes progress in vehicle development possible
22/12/2016
Kistler Sensor Correvit® SFII measures world record
20/12/2016
Kistler sensors deliver a maximum in data quality under any conditions.
07/11/2016
Kistler pressure sensors enabled the Rosetta space probe to fly for 6.4 billion kilometers.
05/10/2016
Since the end of 2015 FC Basel is using Kistler force plates to reduce the dropout of young talents.
17/08/2016
Kistler makes the difference in the crucial sports moments with its Performance Analysis System for Swimming.
19/02/2016
Determination of Pump Efficiency with Kistler KiTorq Measuring Flange System
04/11/2015
Piezoelectric Measurements with CompactRIO™
15/06/2015
Measurement Solutions for Automotive Test Systems
08/05/2015
Quality Assurance in the Automotive Industry
02/03/2015
How Brose improves the quality of its two-component production and automatically separates defective parts
02/12/2014
The Kistler Group pursues a growth policy that is both ambitious and sustainable – and strategic acquisitions are one of its core elements. ‘Strategic’ means that Kistler deliberately selects companies which can achieve more together with Kistler than they ever could by continuing alone. The takeover of Dr. Staiger Mohilo & Co. GmbH in 2006 enabled Kistler to grow jointly with the acquired company...
02/12/2014
After a ten-year voyage, the Rosetta space probe's Philae landing module finally touched down on the surface of comet ‘Chury’.
23/08/2011
HEWI and its Customers Benefit from Cavity Pressure Technology
15/02/2011
End-to-end process monitoring for critical medical moldings
07/02/2011
Cavity pressure measurement eliminates short shots at Fischer GmbH & Co KG of Sinsheim/Germany
Contacto
Max 25 MB