XY Monitor maXYmos BL now with Enhanced Functions and PC Software for Analyzing and Documenting Process Data

As an XY monitor for process monitoring and product testing, the maXYmos BL Type 5867A… from Kistler has extremely quickly established a wide base of actual and potential customers in industrial joining and assembly, and in product testing. From the time (10 to 13 October 2011) of the MOTEK International Trade Fair for Handling, Assembly and Automation Technology being held in Stuttgart, even the standard version of the very versatile and compact monitor, which already offers unbeatable value for money, will be enhanced with additional practical features.

 

Automatic Trend Tracking for the ENVELOPE CURVE Evaluation Object

The maXYmos BL records the interrelation of all of the measurands that can be measured with piezoelectric or strain gage sensors on the Y-channel, and with potentiometric sensors on the X-channel. It can monitor and evaluate the quality of a product or production step on the basis of the curve and different evaluation objects.

The update will make the ENVELOPE CURVE available as an evaluation object. During setup the band of this curve automatically wraps around the outside contour of a previously measured bundle of curves evaluated as GOOD. Automatic trend tracking, which can be activated for the band of the envelope curve, tracks the setpoint limits, for example with progressive tool wear, and adjusts the evaluation function to suit the actual process situation. One or two separate envelope curves in addition to the other evaluation objects UNI-BOX, LINE or NO-PASS are available for each measurement curve.

Comprehensive Analyses with PC Software maXYmos PC

The program maXYmos PC for the PC allows direct transfer of the test record from the maXYmos BL to the PC, saving as a CSV file and visualization of measurement curves and process values. Searching and filtering can be performed in the saved test records under date, station, part number, evaluation result and other criteria. Measurement curve analysis allows measurement of specific significant points on the curve using the cursor. Analysis of saved bundles of curves allows subjective evaluation of process capability. Thus a sharply contoured bundle indicates a stable process, whereas a scattered bundle is a sign of instabilities.

Process values are available in the Excel format (XLS) for trend analyses This enables process values from saved record files to be automatically filtered out, written into the Excel file column by column, displayed graphically or subjected to specific analysis. The function for setting up the maXYmos BL online or offline is displayed in Windows-compatible masks. This also allows backup files to be opened, interpreted, edited, printed or exported as PDF file.

A backup restore function supports saving and restoring of complete equipment setups. The integral updater keeps the firmware up to date. Updates can be performed at any time using the Kistler server.

Background: maXYmos BL

The XY monitor maXYmos BL records the interrelation of all of the measurands that can be measured with, for example, force or torque sensors on the Y-channel, and potentiometric displacement or rotation angle sensors on the X-channel. It can monitor and evaluate the quality of a product or production step on the basis of the curve and different evaluation objects.

The maXYmos BL features practical functions, a sophisticated menu concept, a bright 3,5" color touch screen display and numerous interfaces, yet offers particularly good value for money. The main areas of application are monitoring joining and assembly operations, and testing products and materials. In press-fit processes, for example, it monitors force against displacement or time, in screwing processes torque against rotation angle or time.

With the aid of evaluation objects it analyzes quality-relevant sections of the measurement curves recorded by means of measurement functions Y=f(X), Y=f(t), Y=f(X,t) or X=f(t). This involves the maXYmos BL checking whether the curves consisting of a maximum of 8 000 pairs of X/Y values pass through the evaluation objects as predefined. If they do, it generates an OK, otherwise a "not OK" (NOK) result. Up to four UNI-BOX, ENVELOPE CURVE or LINE type evaluation objects can be allocated for each measuring program or measurement curve.

The basic version of the maXYmos BL is optimized for mounting in a front panel. An optional additional case allows mounting on a vertical panel of a machine or on a desktop, and continuous adjustment of the angle of view.

For the maXYmos BL Kistler offers a wide selection of force, torque, displacement and angle sensors, which are accordingly based on the piezoelectric, strain gage or potentiometric measuring principle (see left column).

2/15/2017
Discover how Kistler contributes to face the great challenges of our times.
11/11/2016
With MARS software version 3.0, Kistler presents an extensive update of the proprietary measurement, analysis,...
10/14/2016
Reliable measurement solutions are becoming ever more important in the globally networked economy.
6/7/2016
Discover our latest Kistler News online.
5/3/2016
The latest issue of Kistler News is now online.
2/1/2016
Learn more about what motivates us and what we are striving for this year in the latest Kistler View.
12/4/2015
Kistler Japan Celebrates its 30th Anniversary and Thanks Its Loyal Customers.
10/15/2015
NCFR Joining Module Honored at Motek for Best Handling and Assembly
9/22/2015
The latest issue of Kistler News is now online.
9/3/2015
Download KiBox Cockpit V2.1 for free and discover new features.
8/20/2015
Seminar zur Qualitätssicherung in der industriellen Fertigung – jetzt anmelden.
6/29/2015
Kistler Automotive GmbH honored as one of Germany's most innovative companies
6/26/2015
Kistler's software for force plates offers a host of new features for performance diagnostics in sports and...
6/12/2015
A fascinating TV report on the trendy sport ‘Parkour’ – with Kistler force plates playing a hidden but...
4/22/2015
At Chinaplas 2015 Kistler will be presenting solutions for zero-defect production, process monitoring and data...
3/23/2015
Kistler partners with OEMs and keeps the finger on the pulse of Industry 4.0
2/13/2015
At SIAF 2015 Kistler will be presenting advanced versions of its proven maXYmos product family
10/14/2014
Wide range of options for optimizing the quality assurance through documenting and evaluating production data...
9/29/2014
Users obtain a full range of force–displacement measurement systems from one source
9/24/2014
At Motek 2014 Kistler will be presenting advanced versions of its proven maXYmos product family
6/3/2014
Extending the maXYmos product range to control and monitor production processes and quality assurance
5/26/2014
At Sensor + Test 2014 Kistler is presenting many new features from the field of measurement electronics in...
5/19/2014
Users obtain a full range of force–displacement measurement systems from one source
2/6/2014
The Kistler Group achieved sales of 285 million CHF in 2013, thus marking a slight growth in comparison with...
1/14/2014
Dr.-Ing. Oliver Schnerr, Head of Sales of the Industrial Process Control (IPC) division, hands over the...
11/11/2013
From flexible torque sensors to complete test stands for highly-efficient electric drives
9/16/2013
1 mm pressure sensor Type 6183C with a new design
8/13/2013
Monitoring, open- and closed-loop control of RTM and SMC processes
7/24/2013
New longitudinal measuring pin for non-contact cavity pressure measuring
5/6/2013
Kistler Goes Beyond Limits: Acceleration sensors for heavy-duty applications at the SENSOR+TEST 2013
4/8/2013
Kistler Goes Beyond Limits: High-tech sensors for heavy-duty applications at the SENSOR+TEST 2013
3/20/2013
In 2012, the Kistler Group reached a record turnover of 279 million Swiss francs with an increase in turnover...
3/19/2013
Kistler Group, a leading global provider of sensors for measuring pressure, force, torque and acceleration,...
11/15/2012
Kistler präsentiert auf der Fachmesse SPS/IPC/DRIVES in Nürnberg (24. bis 26. November 2012) am Stand 4A-451...
10/8/2012
At the Fakuma trade show in Friedrichshafen/Germany (from 16 until 20 October, 2012), Kistler will present a...
10/8/2012
At the Fakuma trade show in Friedrichshafen/Germany (from 16 until 20 October, 2012) Kistler will present its...
10/8/2012
The new firmware upgrade V2.4 for Kistler's CoMo Injection process monitoring system offers better...
9/10/2012
Kistler Group continues to expand: revenues up 20 %, strengthening of customer-specific development capacities...
9/10/2012
Kistler Gruppe weiterhin auf Expansionskurs: Umsatzsteigerung um 20 %, Stärkung der kundenspezifischen...
6/29/2012
With the acquisition of the DTI Technology ("Digital Transducer Interface") from Hentschel System GmbH,...
6/29/2012
Mit dem Erwerb der DTI-Technologie ("Digital Transducer Interface") von der Hentschel System GmbH, Hannover,...
5/8/2012
At the Automatica Trade Fair, which will take place from 22 through 24 May, 2012 in Munich/Germany, Kistler...
5/7/2012
Kistler sensors and systems deliver an impressive performance where products from other suppliers come to...
3/15/2012
CIRP focuses on cutting because this method of machining components is one of the key production processes.
2/17/2012
In-process quality assurance solutions made by Kistler Group have proven their high efficiency for...
2/1/2012
Despite difficult conditions, with sales growth over 11 % Kistler still achieved a sound result in 2011.
11/2/2011
On Stand 4A-451 in Hall 4A of the SPS/IPC/DRIVES exhibition from 22 to 24 November 2011 in Nuremberg, Kistler...
11/2/2011
By designing a measuring unit and an evaluation unit as separate assemblies, and introducing modular...
10/20/2011
This year's Fakuma sees Kistler showing a system for online prediction of the quality of injection molded...
10/19/2011
Kistler brings the quality-minded injection molder another substantial step closer to zero-defect production.
9/28/2011
As an XY monitor for process monitoring and product testing, the maXYmos BL Type 5867A… from Kistler has...
9/28/2011
Telemetric transmission of the force signal without having to rely on a cable, and suitability for use in...
9/28/2011
Kistler is expanding its selection of electromechanical NC joining modules NCFB Type 2160A… with versions...
2/3/2011
The Kistler Group based in Winterthur, Switzerland, looks back on a successful 2010 financial year with sales...
12/10/2010
Kistler, worldwide supplier of precision sensors, systems and instrumentation for the dynamic measurement of...
11/24/2010
Kistler, worldwide supplier of precision sensors, systems and instrumentation for the dynamic measurement of...
11/10/2010
Kistler's new generation of triaxial PiezoBeam® accelerometer Type 8688A(x) offers best-in-class sensitivity...
10/29/2010
Swiss company Kistler Instrumente AG of Winterthur is the leading international supplier of sensors and...
9/10/2010
The new press force sensor Type 9393A… extends the successful Press Force series of sensors to a measuring...
9/6/2010
With the new combined pressure and temperature sensor Type 6188A… Kistler establishes another milestone in the...
7/21/2010
Kistler has developed its new data acquisition (DAQ) system Type 5697A… for recording data in R&D laboratory...
7/9/2010
Kistler has commissioned an additional calibration unit for torque sensors on its Lorch production site.
6/8/2010
As a development partner of the automobile industry the Kistler Group aims to provide vehicle manufacturers...
4/19/2010
The Kistler Group has been awarded the contract for instrumentation of three crash centers for the Indian...
4/7/2010
In order to optimise processes inside an engine, it is extremely important to have a true picture of the...
1/13/2010
New Type 4520A... Basic Line provides a cost-effective torque sensor based upon strain gage technology.
12/10/2009
The well established Kistler press force sensors are based on the piezoelectric measuring principle.
11/18/2009
Successful automation of joining processes where room is at a premium and joining stations closely spaced...
10/23/2009
The Kistler Group acquired KT Automotive GmbH based in Munich, Germany, in an all-stock transaction on 22...
9/14/2009
The curve of cavity pressure during injection molding is the critical process variable for evaluating part...
7/1/2009
To allow direct incorporation of Kistler products into CAD designs, the Kistler CAD Download Service offers...
4/30/2009
The Kistler Group has acquired Corrsys-Datron Sensorsysteme GmbH based in Wetzlar, Germany, in an all-stock...
3/9/2009
The roll-out of the world's first measuring tram took place in Dresden, Germany, on 5 March with the handover...
1/15/2009
The Kistler Group took over MSC Automotive GmbH based in Schwieberdingen, Germany, in an all-stock transaction...