The NCFE Joining Module from Kistler

Winterthur, 10 October 2016 – Kistler is unveiling a new addition to its portfolio of electromechanical joining modules. The NCFE joining module is specifically designed for simple joining processes – so plant manufacturers and power pack operators now have a cost-effective alternative to conventional pneumatic or hydraulic systems.

Kistler is launching its new NCFE joining module, developed especially for plant manufacturers who nowadays build their own joining units and also for operators of conventional power packs. This innovation unlocks entirely new possibilities for all those customers who previously found it unprofitable to use Kistler's electromechanical joining systems. The new joining module is specifi-cally intended for simple joining processes that feature low requirements as regards cycle times, design and measuring ranges. As compared to hydraulic or pneumatic units, the NCFE module (the 'E' stands for Economy) offers convincing advantages such as low energy consumption, simple handling and fast commissioning. The new NCFE joining module is designed for applications in the 10 – 80 kN measuring range.

A New Era Dawns for Plant Manufacturers and Power Pack Operators

Every day, customers all over the world benefit from Kistler's enormous stock of know-how in the field of electromechanical joining systems. Kistler set out to identify additional markets where its flexible, energy-saving joining units could be used. The Swiss sensor manufacturer singled out two particularly important target groups: operators of conventional pneumatically driven power packs, and plant manufacturers.

Alexander Müller, Product Manager for NC Joining Systems, explains that Kistler's existing portfolio of joining systems does not fully cover the highly specific requirements of these users. This prompted Kistler's product management team to develop a new joining module for this target group.

Alexander Müller adds that the new module opens up entirely new prospects for all plant manufac-turers who previously developed their own joining systems. The NCFE module offers them a cost-effective alternative to developing their own systems. All the systems are pre-tested, so fast com-missioning is guaranteed. Thanks to the advantage of integrated sensor technology, this module provides plant manufacturers and power pack operators with complete, end-to-end monitoring and control of the entire joining process. Installation as well as handling are made far simpler, so plant manufacturers can present convincing arguments to their customers on points such as energy savings, short delivery times and flexibility.

Comprehensive Control Thanks to the maXYmos NC Monitoring System

The joining process is monitored by the maXYmos NC monitoring system, which evaluates and documents XY curves for joining and press-fit processes in conjunction with the NC joining mod-ules and the IndraDrive servo amplifier that is included in the system. The patterns of measure-ment curves can be used to monitor the quality of a single production step, a sub-assembly or an entire product, with control in real time via SERCOS III. The benefits: optimal cycle times can be achieved with maximum repeat accuracy, downtime is minimized and machine availability is in-creased – adding up to a boost in productivity for the entire manufacturing process.

Thanks to integrated sequence control (sequencer mode), processes can be mapped with no need to rely on costly external PLC programming. The programs can be set up quickly and easily with the help of the intuitive user interface on the touch display. A total of up to 128 programs can be saved and for each program, an independent sequence with as many as 255 objects can be defined. Processes are evaluated with the help of profiles for two interrelated measurands that are assessed as good (OK) or bad (NOK). Ten Evaluation Objects (EOs) are available for each program, so process deviations can be detected and complex process sequences can be regulated and controlled.

The Right Joining System for Every Application

Alexander Müller sums up the benefits for new users in a nutshell:

"As compared to pneumatic or hydraulic processes, the NCFE module offers substantially higher efficiency – like all Kistler's joining systems. Savings potential with the electrical process is up to 77% as compared to the hydraulic process, and about 90% in relation to the pneumatic process. Maintenance outlay for these systems is minimal – so users can save even more on their already low production costs. What's more, scrap is reduced because 100% quality control is achieved with this module."

As the product manager responsible for joining systems, Müller is especially proud that Kistler can now offer its highly advanced NC joining technology to a broader market thanks to this cost-effective new development:

"With this new bandwidth of products – from compact high-end joining modules (NCFH) through to simple joining units (NCFE) – Kistler now offers the right system to meet every requirement. Another plus: seamless integration into an overarching production envi-ronment is possible thanks to the flexible interfaces that are included in maXYmos NC as standard. This means that we have passed another milestone in our success story as a global provider of joining systems: with the NCFE module, we can now offer our customers even more specific support as they endeavor to cut costs, save time and strengthen their competitive edge on the market!"

Download Press Release (PDF)

Media Contact
Simone Koch
Divisional Marketing Manager IPC
Phone +41 52 2241 802
Email: simone.koch@kistler.com

User Contact
Alexander Müller
Product Manager, NC Joining Systems
Phone +49 7172 184 176
Email: alexander.mueller@kistler.com

Press kit

Kistler portrait with logo for a quick overview: Kistler Press Kit.zip

4/12/2018
The global leader in dynamic measurement technology supports the passion for innovation and technology with a...
3/6/2018
Kistler will be showcasing at Control 2018 its portfolio of industrial testing and inspection systems with the...
2/16/2018
At Intertraffic 2018 the Kistler Group is showcasing its comprehensive KiTraffic Weigh In Motion (WIM)...
2/15/2018
At NPE 2018 in Orlando, Florida, the Kistler Group will demonstrate a wide range of modular functionalities...
1/31/2018
The new KiSprint provides coaches and athletes with an efficient means of biomechanically optimizing sprint...
1/24/2018
Kistler achieved a growth rate of 18 % in 2017. Digital transformation has top priority in 2018.
1/23/2018
Overcoming the complexities of RTM – with Kistler
10/12/2017
At the SPS IPC Drives Kistler Group will unveil the world's first digital charge amplifier Type 5974A, a...
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
Kistler Group took over near Karlsruhe-based Vester Elektronik GmbH on 25 August, a specialist in sensor...
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
At Moulding Expo 2017, we will show how easy it is to install the measurement technology needed for quality...
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
10/27/2016
At this year's SPS IPC Drives in Nuremberg Kistler will premiere laboratory systems to analyze bolted joints,...
10/21/2016
Kistler boosts the efficiency and reliability of large marine and stationary engines through monitoring and...
10/19/2016
Kistler is presenting the new versions of its ComoNeo and ComoDataCenter.
10/10/2016
Kistler is unveiling a new addition to its portfolio of electromechanical joining modules.
9/30/2016
The Kistler Group reported incoming orders worth CHF 233.3 million at the end of August 2016 and has therefore...
9/7/2016
At this year's K Trade Fair from 19 to 26 October in Düsseldorf, Kistler will be showcasing its latest new...
7/24/2016
Kistler will be showcasing its new NCFE and NCFR joining modules, together with the latest generation of...
7/12/2016
Kistler's Correvit® SFII sensor measures world record in 1.513 seconds
5/12/2016
Screw technology complements the range of applications.
4/27/2016
Following a long phase of planning, preparations, and conversion work, Kistler Instrumente GmbH has a new home...