Kistler unveils new products at Space Tech Expo Europe

Winterthur, 27 September 2017 – Space Tech Expo Europe, the main meeting-place for representatives of the European space industry, will open its doors from 24 to 26 October in Bremen, Germany. This international exposition is also a fixed event on Kistler's trade fair program: our experts will be on hand at stand A51 in hall 5 to show visitors measurement technology capabilities and solutions for challenging space applications.

Sensors play a key role in Space Payload, Propulsion and subsystem testing and provide valuable measurements to support quality, safety and reliability of space systems and subsystems. In this sector, products have to meet very demanding requirements due to extreme conditions that include wide temperature ranges, pressure fluctuations, high shock and vibration levels. At the same time, the measurement equipment often has to be lightweight as well as rugged and durable. Kistler offers the right force, vibration and pressure sensors for virtually every application.

As the highlight of our presence at Space Tech Expo Europe, we shall be presenting product solutions for selected space applications to the show visitors. At our fair stand, attendees can see exhibits such as a rocket engine test bench with built-in pressure, force and acceleration sensors, as well as the new piezoelectric 6-component force/torque link, Type 9306A.”

Manuel Blattner, Head of Kistler's Strategic Business Field Test & Measurement

 

Direct, accurate measurements – in every direction

Entire satellites and their subsystems could sustain severe damage due to overloads during vibration tests. Force Limited Vibration Testing is used to prevent this from happening. This testing uses 3-component force sensors at the shaker to payload interface to monitor the introduced forces. Kistler will exhibit the ideal solution for this application at the Space Tech Expo: preloaded 3-component piezoelectric force sensors connected to cutting edge signal conditioning and data acquisition systems. Installed between two mounting flanges, these preloaded sensors can measure compression and tensile forces in every direction. Accurate results are insured thanks to very high rigidity allowing for a high natural frequency as well as a very low crosstalk.

Signals are measured and conditioned with the LabAmp 5167A, Kistler's first multi-channel quasistatic and dynamic charge amplifier with analog output and integrated data acquisition. The benefit: a scalable and configurable high performance signal conditioner and data acquisition system offering channel synchronizations, signal filtering, virtual channels and convenient evaluation of individual force signals. Integrated data acquisition simplifies the measuring chain and provides added flexibility.

Optimal results – even under extreme stress

Rockets are exposed to very high stresses, especially during launch. To prevent malfunctions during operation, rocket components – and especially rocket engines – undergo extensive testing and inspection during the testing phase. Kistler is also showcasing the Type 6021A high-temperature pressure sensor at the Space Tech Expo Europe. This uncooled pressure sensor is suitable for application temperatures of up to 700°C and provides is high resolution pressure measurements to understand the combustion processes and related instabilities. For this purpose, the pressure sensor is ground-isolated and is connected to a differential charge amplifier providing low noise and EMI immunity to support accurate measurements.

Tradeshow visitors will also have the chance to appreciate the benefits of Kistler's Type 5181A differential charge amplifier for high temperature test requirements.

Reliable measurements of small torques and forces

Yet another highlight to be unveiled by Kistler at the Space Tech Expo Europe is the first piezoelectric 6-component force/torque link, Type 9306A. This sensor can deliver precise and direct measurements of three forces and three torques without calculation: an excellent choice for measurements in wind tunnels. Kistler charge amplifiers provide users with the ability of adjusting the torque and force measuring ranges independently for each axis. Thanks to the piezoelectric measurement principle and 9306A performance very small torques and forces can be easily measured with high resolution.

More information about Kistler's exhibit at the Space Tech Expo Europe

Media contact
Manuel Blattner
Head of Strategic Business Field
Test & Measurement
Tel.: +41 52 2241 273
Email: manuel.blattner@kistler.com

Press kit

Kistler portrait with logo for a quick overview: Kistler Press Kit.zip

7/31/2018
Competent service just a call away has always been a key aspect of Kistler's cooperation with its customers. Now, in a move to address growing demand in North Germany, the measurement technology experts are opening a new office in Wolfsburg.
7/25/2018
On her way to Olympia 2020 she relies on Kistler Group measurement experts.
7/18/2018
Effective monitoring with strain sensors protects machines and tools
7/3/2018
The Top 100 Competition has again singled out the most innovative German small and medium-sized enterprises (SMEs) for the 10th time.
6/25/2018
Kistler is pleased to introduce MicroDyn, the world's smallest series-produced cutting force meter.
6/19/2018
Kistler introduces the world’s first high temperature accelerometer for the monitoring of gas turbines.
6/11/2018
Kistler is earmarking the highest investment budget for research and development in the company`s history.
5/11/2018
Digitization, Internet of Things and Industry 4.0 are presenting major challenges. Discover how Kistler responds to the great challenges of our times.
5/9/2018
At Sensor + Test 2018 Kistler will be introducing a milestone in measurement technology: its new KiDAQ data acquisition system.
5/8/2018
At NPE 2018, the Kistler Group is showcasing its latest custom monitoring package for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
5/3/2018
At Automatica 2018, the Kistler Group will turn the spotlight on diverse options for using sensors and process monitoring systems to support industrial production and enhance digitalization in test and assembly technology.
4/24/2018
The Kistler Group will showcase its expanded portfolio of industrial test and inspection systems for quality assurance at the 2018 Control trade show.
4/12/2018
The global leader in dynamic measurement technology supports the passion for innovation and technology with a three-year partnership.
3/6/2018
Kistler will be showcasing at Control 2018 its portfolio of industrial testing and inspection systems with the spotlight on the very latest additions.
2/16/2018
At Intertraffic 2018 the Kistler Group is showcasing its comprehensive KiTraffic Weigh In Motion (WIM) solutions, which support road owners and authorities in road and traffic monitoring, weight enforcement and weight-based tolling.
2/15/2018
At NPE 2018 in Orlando, Florida, the Kistler Group will demonstrate a wide range of modular functionalities for ComoNeo: the process monitoring system that takes injection molding to a higher level with integrated quality monitoring geared to meet customers’ needs and requirements.
1/31/2018
The new KiSprint provides coaches and athletes with an efficient means of biomechanically optimizing sprint starts under competitive conditions. The robust and mobile solution has comprehensive software assessment options and can be individually adapted and expanded.
1/24/2018
Kistler achieved a growth rate of 18 % in 2017. Digital transformation has top priority in 2018.
1/23/2018
Overcoming the complexities of RTM – with Kistler
10/12/2017
At the SPS IPC Drives Kistler Group will unveil the world's first digital charge amplifier Type 5974A, a milestone more in electrical automation.
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
Kistler Group took over near Karlsruhe-based Vester Elektronik GmbH on 25 August, a specialist in sensor technology and test automation.
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
At Moulding Expo 2017, we will show how easy it is to install the measurement technology needed for quality assurance in injection molds.
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
10/27/2016
At this year's SPS IPC Drives in Nuremberg Kistler will premiere laboratory systems to analyze bolted joints, calibration equipment, torque tools test systems and more.
10/21/2016
Kistler boosts the efficiency and reliability of large marine and stationary engines through monitoring and control of the combustion process
10/19/2016
Kistler is presenting the new versions of its ComoNeo and ComoDataCenter.
10/10/2016
Kistler is unveiling a new addition to its portfolio of electromechanical joining modules.
9/30/2016
The Kistler Group reported incoming orders worth CHF 233.3 million at the end of August 2016 and has therefore seen growth of 8.4 % compared to the same period in the previous year, or 5.6 % when adjusted for currency effects.
9/7/2016
At this year's K Trade Fair from 19 to 26 October in Düsseldorf, Kistler will be showcasing its latest new products and features with the focus on Industry 4.0.
7/24/2016
Kistler will be showcasing its new NCFE and NCFR joining modules, together with the latest generation of maXYmos monitoring systems on Motek 2016
7/12/2016
Kistler's Correvit® SFII sensor measures world record in 1.513 seconds
5/12/2016
Screw technology complements the range of applications.
4/27/2016
Following a long phase of planning, preparations, and conversion work, Kistler Instrumente GmbH has a new home for its German headquarters at the Böblingen/Sindelfingen airfield.
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
Kistler's software for force plates offers a host of new features for performance diagnostics in sports and rehabilitation.
4/22/2015
At Chinaplas 2015 Kistler will be presenting solutions for zero-defect production, process monitoring and data evaluation in injection molding
11/10/2014
New product developments for dynamic measuring technology at the Kistler booth at SPS IPC Drives 2014
10/14/2014
Wide range of options for optimizing the quality assurance through documenting and evaluating production data of CoMo Injection Systems
9/29/2014
Users obtain a full range of force–displacement measurement systems from one source
6/3/2014
Extending the maXYmos product range to control and monitor production processes and quality assurance
5/26/2014
At Sensor + Test 2014 Kistler is presenting many new features from the field of measurement electronics in addition to its already proven sensor technology.
5/19/2014
Users obtain a full range of force–displacement measurement systems from one source
2/6/2014
The Kistler Group achieved sales of 285 million CHF in 2013, thus marking a slight growth in comparison with the figures for the prior year.